summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (from parent 1: dfa141b)
raw | patch | inline | side by side (from parent 1: dfa141b)
author | Jouni Malinen <j@w1.fi> | |
Tue, 6 Jan 2009 18:11:15 +0000 (20:11 +0200) | ||
committer | Jouni Malinen <j@w1.fi> | |
Tue, 6 Jan 2009 18:11:15 +0000 (20:11 +0200) |
14 files changed:
diff --git a/hostapd/ChangeLog b/hostapd/ChangeLog
index 09b34cd9bf50260da1e447e79d51779cfe510c67..f85a4fb1187429b7900abae7062e9a32f9662d9f 100644 (file)
--- a/hostapd/ChangeLog
+++ b/hostapd/ChangeLog
ChangeLog for hostapd
-????-??-?? - v0.6.7
+2009-01-06 - v0.6.7
* added support for Wi-Fi Protected Setup (WPS)
(hostapd can now be configured to act as an integrated WPS Registrar
and provision credentials for WPS Enrollees using PIN and PBC
- methods; external WPS Registrars are not supported); WPS support can
+ methods; external wireless Registrar can configure the AP, but
+ external WLAN Manager Registrars are not supported); WPS support can
be enabled by adding CONFIG_WPS=y into .config and setting the
runtime configuration variables in hostapd.conf (see WPS section in
the example configuration file); new hostapd_cli commands wps_pin and
diff --git a/hostapd/README b/hostapd/README
index 674377470ccf9df4485397429bf69ce214707af0..eb9aa4815b4f5ad1fa0f5b1fa5b1772204cb8147 100644 (file)
--- a/hostapd/README
+++ b/hostapd/README
Authenticator and RADIUS authentication server
================================================================
-Copyright (c) 2002-2008, Jouni Malinen <j@w1.fi> and contributors
+Copyright (c) 2002-2009, Jouni Malinen <j@w1.fi> and contributors
All Rights Reserved.
This program is dual-licensed under both the GPL version 2 and BSD
diff --git a/hostapd/hostapd.c b/hostapd/hostapd.c
index 1da0bf52acfdd3afe042aa0b800f07833a8a79a5..8f2ec4cb64f2fa6e76df533d697866bed472b6f1 100644 (file)
--- a/hostapd/hostapd.c
+++ b/hostapd/hostapd.c
/*
* hostapd / Initialization and configuration
- * Copyright (c) 2002-2008, Jouni Malinen <j@w1.fi>
+ * Copyright (c) 2002-2009, Jouni Malinen <j@w1.fi>
*
* This program is free software; you can redistribute it and/or modify
* it under the terms of the GNU General Public License version 2 as
"hostapd v" VERSION_STR "\n"
"User space daemon for IEEE 802.11 AP management,\n"
"IEEE 802.1X/WPA/WPA2/EAP/RADIUS Authenticator\n"
- "Copyright (c) 2002-2008, Jouni Malinen <j@w1.fi> "
+ "Copyright (c) 2002-2009, Jouni Malinen <j@w1.fi> "
"and contributors\n");
}
diff --git a/hostapd/hostapd_cli.c b/hostapd/hostapd_cli.c
index 68ff091cf50927973a8e7215cd84abb4e1e3d7cf..9c3e65b2a690848fd54148c70608bcde4a8717d0 100644 (file)
--- a/hostapd/hostapd_cli.c
+++ b/hostapd/hostapd_cli.c
/*
* hostapd - command line interface for hostapd daemon
- * Copyright (c) 2004-2008, Jouni Malinen <j@w1.fi>
+ * Copyright (c) 2004-2009, Jouni Malinen <j@w1.fi>
*
* This program is free software; you can redistribute it and/or modify
* it under the terms of the GNU General Public License version 2 as
static const char *hostapd_cli_version =
"hostapd_cli v" VERSION_STR "\n"
-"Copyright (c) 2004-2008, Jouni Malinen <j@w1.fi> and contributors";
+"Copyright (c) 2004-2009, Jouni Malinen <j@w1.fi> and contributors";
static const char *hostapd_cli_license =
diff --git a/src/common/version.h b/src/common/version.h
index cf137f9f42e497ed2eabaf3fc30009cd2cae9e18..7651b48a1e300ab9738562d45fc1ef78caacdcfa 100644 (file)
--- a/src/common/version.h
+++ b/src/common/version.h
#ifndef VERSION_H
#define VERSION_H
-#define VERSION_STR "0.6.6"
+#define VERSION_STR "0.6.7"
#endif /* VERSION_H */
index 361c17126e37a770bfb224b95339d9b4fff88bde..37ab7224b20d2b374d4b83f6cea84429d9afdc78 100644 (file)
--- a/wpa_supplicant/ChangeLog
+++ b/wpa_supplicant/ChangeLog
ChangeLog for wpa_supplicant
-????-??-?? - v0.6.7
+2009-01-06 - v0.6.7
* added support for Wi-Fi Protected Setup (WPS)
(wpa_supplicant can now be configured to act as a WPS Enrollee to
enroll credentials for a network using PIN and PBC methods; in
diff --git a/wpa_supplicant/README b/wpa_supplicant/README
index 643a727a8bc08d16e7ce92281f84b70673faca0f..778b0ba7270e224105426e6e9aa534a25e63d3c4 100644 (file)
--- a/wpa_supplicant/README
+++ b/wpa_supplicant/README
WPA Supplicant
==============
-Copyright (c) 2003-2008, Jouni Malinen <j@w1.fi> and contributors
+Copyright (c) 2003-2009, Jouni Malinen <j@w1.fi> and contributors
All Rights Reserved.
This program is dual-licensed under both the GPL version 2 and BSD
index e2b75bdde0bfacd28ae2230eb64bdbb3caa1642d..292223d2d5fea0ab5746da1bd41825c37b3b4626 100644 (file)
wpa_supplicant for Windows
==========================
-Copyright (c) 2003-2008, Jouni Malinen <j@w1.fi> and
-contributors
+Copyright (c) 2003-2009, Jouni Malinen <j@w1.fi> and contributors
All Rights Reserved.
This program is dual-licensed under both the GPL version 2 and BSD
index c36277a0e2407bb33f1e032d6a3d7fde8318c107..c49b674011ac633e4663e67d22eee20940bc0502 100644 (file)
--- a/wpa_supplicant/wpa_cli.c
+++ b/wpa_supplicant/wpa_cli.c
/*
* WPA Supplicant - command line interface for wpa_supplicant daemon
- * Copyright (c) 2004-2008, Jouni Malinen <j@w1.fi>
+ * Copyright (c) 2004-2009, Jouni Malinen <j@w1.fi>
*
* This program is free software; you can redistribute it and/or modify
* it under the terms of the GNU General Public License version 2 as
static const char *wpa_cli_version =
"wpa_cli v" VERSION_STR "\n"
-"Copyright (c) 2004-2008, Jouni Malinen <j@w1.fi> and contributors";
+"Copyright (c) 2004-2009, Jouni Malinen <j@w1.fi> and contributors";
static const char *wpa_cli_license =
index d23220d3a79979d9bcb9a0e0b087e6f2c0470e77..d2c45525e30643237c29bf336689c5d0ec42bf32 100644 (file)
/*
* WPA Supplicant
- * Copyright (c) 2003-2008, Jouni Malinen <j@w1.fi>
+ * Copyright (c) 2003-2009, Jouni Malinen <j@w1.fi>
*
* This program is free software; you can redistribute it and/or modify
* it under the terms of the GNU General Public License version 2 as
const char *wpa_supplicant_version =
"wpa_supplicant v" VERSION_STR "\n"
-"Copyright (c) 2003-2008, Jouni Malinen <j@w1.fi> and contributors";
+"Copyright (c) 2003-2009, Jouni Malinen <j@w1.fi> and contributors";
const char *wpa_supplicant_license =
"This program is free software. You can distribute it and/or modify it\n"
diff --git a/www/hostapd/index.html b/www/hostapd/index.html
index 0b89eb3afa2a886570a9bd146f1f0aead580dcaf..551d31b0e44d909971e5da9ed822f93206b432b3 100644 (file)
--- a/www/hostapd/index.html
+++ b/www/hostapd/index.html
<head>
<title>hostapd: IEEE 802.11 AP, IEEE 802.1X/WPA/WPA2/EAP/RADIUS Authenticator</title>
<meta name="description" content="hostapd (IEEE 802.1X, WPA, WPA2, RSN, IEEE 802.11i Authenticator and RADIUS authentication server)">
- <meta name="keywords" content="WPA, WPA2, IEEE 802.11i, IEEE 802.1X, WPA Authenticator, hostapd, TKIP, CCMP, EAP-PEAP, EAP-TLS, EAP-TTLS, EAP-SIM, EAP-AKA, EAP-GTC, EAP-MSCHAPv2, EAP-MD5, EAP-PAX, EAP-PSK, EAP-FAST, IEEE 802.1X Supplicant, IEEE 802.1aa, EAPOL, RSN, pre-authentication, PMKSA caching, BSD WPA Authenticator, FreeBSD WPA Authenticator, RADIUS authentication server, EAP authenticator, EAP server, EAP-TNC, TNCS, IF-IMV, IF-TNCCS">
+ <meta name="keywords" content="WPA, WPA2, IEEE 802.11i, IEEE 802.1X, WPA Authenticator, hostapd, TKIP, CCMP, EAP-PEAP, EAP-TLS, EAP-TTLS, EAP-SIM, EAP-AKA, EAP-GTC, EAP-MSCHAPv2, EAP-MD5, EAP-PAX, EAP-PSK, EAP-FAST, IEEE 802.1X Supplicant, IEEE 802.1aa, EAPOL, RSN, pre-authentication, PMKSA caching, BSD WPA Authenticator, FreeBSD WPA Authenticator, RADIUS authentication server, EAP authenticator, EAP server, EAP-TNC, TNCS, IF-IMV, IF-TNCCS, WPS">
<meta http-equiv="Content-Type" content="text/html; charset=iso-8859-1">
</head>
<li>RSN: PMKSA caching, pre-authentication</li>
<li>RADIUS accounting</li>
<li>RADIUS authentication server with EAP</li>
+<li>Wi-Fi Protected Setup (WPS)</li>
</ul>
<h4>Supported EAP methods (integrated EAP server and RADIUS authentication server)</h4>
<li>EAP-SAKE</li>
<li>EAP-FAST</li>
<li>EAP-IKEv2</li>
-<li>EAP-GPSK (experimental)</li>
+<li>EAP-GPSK</li>
</ul>
<p>Following methods are also supported, but since they do not generate keying
<p>
<b>hostapd</b><br>
-Copyright (c) 2002-2008, Jouni Malinen <j@w1.fi>
+Copyright (c) 2002-2009, Jouni Malinen <j@w1.fi>
and contributors.
</p>
</ul>
<li>Latest development release:
<ul>
-<li><a href="../releases/hostapd-0.6.6.tar.gz">hostapd-0.6.6.tar.gz</a></li>
+<li><a href="../releases/hostapd-0.6.7.tar.gz">hostapd-0.6.7.tar.gz</a></li>
</ul>
<li>ChangeLog:
<ul>
<address><a href="mailto:j@w1.fi">Jouni Malinen</a></address>
<!-- Created: Sun Jan 2 17:20:17 PST 2005 -->
<!-- hhmts start -->
-Last modified: Fri Dec 26 15:37:54 EET 2008
+Last modified: Tue Jan 6 20:05:09 EET 2009
<!-- hhmts end -->
</div>
</body>
diff --git a/www/index.html b/www/index.html
index 2f67c734c9014fdcdda60c68d8ea848d8e5ed181..0f0a4a976ae8c1af8ace94641b2b9f508ded5e9b 100644 (file)
--- a/www/index.html
+++ b/www/index.html
<p>
<b>hostapd</b><br>
-Copyright (c) 2002-2008, Jouni Malinen <j@w1.fi>
+Copyright (c) 2002-2009, Jouni Malinen <j@w1.fi>
and contributors.
</p>
<p>
<b>wpa_supplicant</b><br>
-Copyright (c) 2003-2008, Jouni Malinen <j@w1.fi>
+Copyright (c) 2003-2009, Jouni Malinen <j@w1.fi>
and contributors.
</p>
</ul>
<li>Latest development release:
<ul>
-<li><a href="releases/hostapd-0.6.6.tar.gz">hostapd-0.6.6.tar.gz</a>
-<li><a href="releases/wpa_supplicant-0.6.6.tar.gz">wpa_supplicant-0.6.6.tar.gz</a> (source code for all versions)</li>
-<li><a href="releases/wpa_supplicant-windows-bin-0.6.6.zip">wpa_supplicant-windows-bin-0.6.6.zip</a> (binaries for Windows)</li>
+<li><a href="releases/hostapd-0.6.7.tar.gz">hostapd-0.6.7.tar.gz</a>
+<li><a href="releases/wpa_supplicant-0.6.7.tar.gz">wpa_supplicant-0.6.7.tar.gz</a> (source code for all versions)</li>
+<li><a href="releases/wpa_supplicant-0.6.7.exe">wpa_supplicant-0.6.7.exe</a> (binary installer for Windows)</li>
+<li><a href="releases/wpa_supplicant-windows-bin-0.6.7.zip">wpa_supplicant-windows-bin-0.6.7.zip</a> (binaries for Windows)</li>
<li><a href="wpa_supplicant/qt4/wpa_gui-qt433-windows-dll.zip">wpa_gui-qt433-windows-dll.zip</a> (Qt4 libraries from wpa_gui/Windows)</li>
</ul>
<li>ChangeLog:
<address><a href="mailto:j@w1.fi">Jouni Malinen</a></address>
<!-- Created: Mon May 27 20:08:41 EEST 2002 -->
<!-- hhmts start -->
-Last modified: Fri Dec 26 15:37:35 EET 2008
+Last modified: Tue Jan 6 20:03:17 EET 2009
<!-- hhmts end -->
</div>
</body>
diff --git a/www/versions.dot b/www/versions.dot
index d24abe95e03bb7b15b1060a6704eb3498c853e53..4a0a5a89c2d641cde7b3c2c21bb40baeb353350d 100644 (file)
--- a/www/versions.dot
+++ b/www/versions.dot
v064 [label="0.6.4 hw\n2008-08-10"]
v065 [label="0.6.5 hw\n2008-11-01"]
v066 [label="0.6.6 hw\n2008-11-23"]
+ v067 [label="0.6.7 hw\n2009-01-06"]
# stable releases
v024 -> v030 -> v031 -> v032 -> v033 -> v034 -> v035 -> v036 -> v037
v037 -> v040 -> v041 -> v042 -> v043 -> v044 -> v045 -> v046 -> v047
v047 -> v050 -> v051 -> v052 -> v053 -> v054 -> v055 -> v056 -> v057
- v057 -> v060 -> v061 -> v062 -> v063 -> v064 -> v065 -> v066
+ v057 -> v060 -> v061 -> v062 -> v063 -> v064 -> v065 -> v066 -> v067
{rank=same; v001 v024}
{rank=same; v030 v037}
index cfb128a3faecba122c7a669f8cb3428d54507a47..05042a0cbd7f34dcf7b965f1d39ce93a3d626edb 100644 (file)
<head>
<title>Linux WPA Supplicant (IEEE 802.1X, WPA, WPA2, RSN, IEEE 802.11i)</title>
<meta name="description" content="WPA Supplicant for Linux, BSD, and Windows (IEEE 802.1X, WPA, WPA2, RSN, IEEE 802.11i)">
- <meta name="keywords" content="WPA, WPA2, IEEE 802.11i, IEEE 802.1X, WPA Supplicant, wpa_supplicant, TKIP, CCMP, EAP-PEAP, EAP-TLS, EAP-TTLS, EAP-SIM, EAP-AKA, EAP-PSK, EAP-GTC, EAP-MSCHAPv2, EAP-MD5, EAP-FAST, EAP-PAX, EAP-IKEv2IEEE 802.1X Supplicant, IEEE 802.1aa, EAPOL, RSN, pre-authentication, PMKSA caching, BSD WPA Supplicant, FreeBSD WPA Supplicant, wireless, WinXP WPA Supplicant, EAP-TNC, TNCC, IF-IMC, IF-TNCCS">
+ <meta name="keywords" content="WPA, WPA2, IEEE 802.11i, IEEE 802.1X, WPA Supplicant, wpa_supplicant, TKIP, CCMP, EAP-PEAP, EAP-TLS, EAP-TTLS, EAP-SIM, EAP-AKA, EAP-PSK, EAP-GTC, EAP-MSCHAPv2, EAP-MD5, EAP-FAST, EAP-PAX, EAP-IKEv2IEEE 802.1X Supplicant, IEEE 802.1aa, EAPOL, RSN, pre-authentication, PMKSA caching, BSD WPA Supplicant, FreeBSD WPA Supplicant, wireless, WinXP WPA Supplicant, EAP-TNC, TNCC, IF-IMC, IF-TNCCS, WPS">
<meta http-equiv="Content-Type" content="text/html; charset=iso-8859-1">
</head>
<li>key management for CCMP, TKIP, WEP104, WEP40</li>
<li>WPA and full IEEE 802.11i/RSN/WPA2</li>
<li>RSN: PMKSA caching, pre-authentication</li>
+<li>Wi-Fi Protected Setup (WPS)</li>
</ul>
<h4>Supported EAP methods (IEEE 802.1X Supplicant)</h4>
<li>EAP-PAX</li>
<li>EAP-SAKE</li>
<li>EAP-IKEv2</li>
-<li>EAP-GPSK (experimental)</li>
+<li>EAP-GPSK</li>
<li>LEAP (note: requires special support from the driver)</li>
</ul>
<p>
<b>wpa_supplicant</b><br>
-Copyright (c) 2003-2008, Jouni Malinen <j@w1.fi>
+Copyright (c) 2003-2009, Jouni Malinen <j@w1.fi>
and contributors.
</p>
</ul>
<li>Latest development release:
<ul>
-<li><a href="../releases/wpa_supplicant-0.6.6.tar.gz">wpa_supplicant-0.6.6.tar.gz</a> (source code for all versions)</li>
-<li><a href="../releases/wpa_supplicant-windows-bin-0.6.6.zip">wpa_supplicant-windows-bin-0.6.6.zip</a> (binaries for Windows)</li>
+<li><a href="../releases/wpa_supplicant-0.6.7.tar.gz">wpa_supplicant-0.6.7.tar.gz</a> (source code for all versions)</li>
+<li><a href="../releases/wpa_supplicant-0.6.7.exe">wpa_supplicant-0.6.7.exe</a> (binary installer for Windows)</li>
+<li><a href="../releases/wpa_supplicant-windows-bin-0.6.7.zip">wpa_supplicant-windows-bin-0.6.7.zip</a> (binaries for Windows)</li>
<li><a href="qt4/wpa_gui-qt433-windows-dll.zip">wpa_gui-qt433-windows-dll.zip</a> (Qt4 libraries from wpa_gui/Windows)</li>
</ul>
<li>ChangeLog:
<address><a href="mailto:j@w1.fi">Jouni Malinen</a></address>
<!-- Created: Sat May 22 21:41:58 PDT 2004 -->
<!-- hhmts start -->
-Last modified: Fri Dec 26 15:37:46 EET 2008
+Last modified: Tue Jan 6 20:06:04 EET 2009
<!-- hhmts end -->
</div>
</body>