summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 48f8e03)
raw | patch | inline | side by side (parent: 48f8e03)
author | Jouni Malinen <jouni@qca.qualcomm.com> | |
Fri, 21 Oct 2011 16:09:25 +0000 (19:09 +0300) | ||
committer | Jouni Malinen <j@w1.fi> | |
Fri, 21 Oct 2011 16:09:25 +0000 (19:09 +0300) |
src/drivers/driver_wext.c | patch | blob | history |
index 27171d69e9d0cadc3d8c8eb8f7028bdadc050e4d..6f58175f20674ed404934d704034a31e3acd1bfc 100644 (file)
}
if (iwr.u.mode == IW_MODE_INFRA) {
+ /* Clear the BSSID selection */
+ if (wpa_driver_wext_set_bssid(drv, null_bssid) < 0) {
+ wpa_printf(MSG_DEBUG, "WEXT: Failed to clear BSSID "
+ "selection on disconnect");
+ }
+
if (drv->cfg80211) {
/*
* cfg80211 supports SIOCSIWMLME commands, so there is
* no need for the random SSID hack, but clear the
- * BSSID and SSID.
+ * SSID.
*/
- if (wpa_driver_wext_set_bssid(drv, null_bssid) < 0 ||
- wpa_driver_wext_set_ssid(drv, (u8 *) "", 0) < 0) {
+ if (wpa_driver_wext_set_ssid(drv, (u8 *) "", 0) < 0) {
wpa_printf(MSG_DEBUG, "WEXT: Failed to clear "
- "to disconnect");
+ "SSID on disconnect");
}
return;
}
+
/*
- * Clear the BSSID selection and set a random SSID to make sure
- * the driver will not be trying to associate with something
- * even if it does not understand SIOCSIWMLME commands (or
- * tries to associate automatically after deauth/disassoc).
+ * Set a random SSID to make sure the driver will not be trying
+ * to associate with something even if it does not understand
+ * SIOCSIWMLME commands (or tries to associate automatically
+ * after deauth/disassoc).
*/
for (i = 0; i < 32; i++)
ssid[i] = rand() & 0xFF;
- if (wpa_driver_wext_set_bssid(drv, null_bssid) < 0 ||
- wpa_driver_wext_set_ssid(drv, ssid, 32) < 0) {
+ if (wpa_driver_wext_set_ssid(drv, ssid, 32) < 0) {
wpa_printf(MSG_DEBUG, "WEXT: Failed to set bogus "
- "BSSID/SSID to disconnect");
+ "SSID to disconnect");
}
}
}