]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - build-utilities/hostap.git/history - hostapd/Makefile
Fix crash when a local deauth occurs (squash)
[build-utilities/hostap.git] / hostapd / Makefile
2012-02-26 Jay KatabathuniInterworking: Add GAS server support for AP mode
2011-11-27 Jouni MalinenTLS: Add build configuration for TLS v1.2 support
2011-11-27 Jouni MalinenAdd implementation of TLS v1.2 PRF (P_SHA256)
2011-11-27 Jouni Malinenhostapd: Define CONFIG_SHA256 for SHA256 builds
2011-11-13 Jouni MalinenMove wpa_scan_results_free() into shared C file
2011-10-17 Jouni MalinenStart deprecating various AP mode driver_ops
2011-10-17 Mahesh PalivelaMove SA Query mechanism into a file that can be shared...
2011-10-16 Jouni MalinenIEEE 802.11u: Add configuration and advertisement for...
2011-10-15 Mukesh AgrawalFix object file list for hlr_auc_gw
2011-09-25 Jouni MalinenRemove EAP-TTLSv1 and TLS/IA
2011-09-25 Jouni MalinenTLS: Add support for TLS v1.1 (RFC 4346) with internal TLS
2011-07-19 VladimirFix hostapd_cli linking without CONFIG_WPA_TRACE=y
2011-07-16 Jouni Malinenhostapd_cli: Start using src/utils/edit*.c
2011-03-17 Jouni MalinenMake the link process quieter unless V=1 is specified
2011-02-06 Ben Greearhostapd: Allow logging to file
2011-01-30 Mike Crowehostapd: Ensure that the destination directory exists
2011-01-30 Mike CroweUse DESTDIR when installing hostapd to support cross...
2010-11-23 Jouni MalinenMaintain internal entropy pool for augmenting random...
2010-11-23 Jouni MalinenFix hlr_auc_gw build with CONFIG_WPA_TRACE=y
2010-10-08 Jouni MalinenP2P: Extend P2P manager functionality to work with...
2010-09-22 Jouni MalinenWPS: Make testing operations configurable at runtime
2010-09-15 Dan HarkinsEAP-pwd: Add support for EAP-pwd server and peer functi...
2010-09-09 Jouni MalinenWPS: Fix CONFIG_WPS_STRICT build option
2010-09-09 Jouni MalinenWPS 2.0: Make WSC 2.0 support to be build option (CONFI...
2010-09-09 Jouni MalinenWPS 2.0: Validate WPS attributes in management frames...
2010-09-05 Jouni MalinenFix hostapd build with CONFIG_IEEE80211N but without...
2010-04-17 Jouni MalinenWPS: Include CONFIG_EAP automatically if WPS is enabled
2010-04-17 Masashi HonmaSupport for Solaris default shell restriction
2010-04-06 Michael Bueschhostapd: Use cp -f in make install
2010-02-19 Jouni MalinenRename EAP server source files to avoid duplicate names
2010-01-16 Jouni MalinenFix linking of nt_password_hash
2010-01-03 Jouni MalinenRemove src/drivers/scan_helpers.c
2009-12-25 Jouni MalinenRename some src/ap files to avoid duplicate file names
2009-12-25 Jouni MalinenMove rest of the generic AP mode functionality into...
2009-12-25 Jouni MalinenMove WPA authenticator glue code into a separate file
2009-12-25 Jouni MalinenMove authentication server setup into separate file
2009-12-25 Jouni MalinenMove iapp.c into src/ap
2009-12-25 Jouni MalinenMove ctrl_iface_ap.c into src/ap
2009-12-24 Jouni MalinenMove wps_hostapd.c into src/ap
2009-12-24 Jouni MalinenMove generic AP functionality implementation into src/ap
2009-12-24 Jouni MalinenMove hostapd configuration parser into separate file
2009-12-24 Jouni Malinenhostapd: Use separate driver operations abstraction
2009-12-20 Jouni MalinenAdd option libbfd support for tracing code
2009-12-19 Jouni MalinenAdd memory allocation analyzer to verify OS wrapper use
2009-12-19 Jouni MalinenAdd backtrace support for debugging
2009-12-12 Jouni MalinenWPS: Handle Selected Registrar as a union of info from...
2009-12-11 Jouni MalinenFix dh_groups.o build for some configurations
2009-12-06 Jouni MalinenMove IEEE 802.11n HT management code into a separate...
2009-12-06 Jouni MalinenMove hlr_auc_gw into hostapd directory
2009-12-06 Jouni MalinenRemove unneeded CONFIG_INTERNAL_X509 and NEED_SHA256...
2009-12-06 Jouni MalinenSplit crypto_internal.c into parts to clean up build
2009-12-06 Jouni MalinenMove EAP method registration away from src/eap_{peer...
2009-12-05 Jouni MalinenRemove Milenage test from hostapd/Makefile
2009-12-05 Jouni MalinenMove milenage.[ch] into src/crypto
2009-11-29 Jouni MalinenRemove src/crypto from default include path
2009-11-29 Jouni MalinenMake HOSTAPD_DUMP_STATE configurable with CONFIG_NO_DUM...
2009-11-29 Jouni MalinenMove EAPOL authenticator state machine into src/eapol_auth
2009-11-29 Jouni MalinenRemove src/common from default header file path
2009-11-28 Jouni MalinenRemove old wpa_supplicant/hostapd doxygen files
2009-11-24 Jouni MalinenFix internal crypto build with some configurations
2009-11-10 Jouni MalinenFix hlr_auc_gw build (wpabuf.o is needed now for tls_op...
2009-11-08 Jouni MalinenWPS: Add HTTP server module
2009-11-08 Jouni MalinenWPS: Move generic UPnP XML helper functionality into...
2009-11-08 Jouni MalinenWPS: Add HTTP client module to clean up code
2009-10-17 Jouni MalinenMove PKCS# {1,5,8} functionality into separate files
2009-10-13 Masashi HonmaFix IEEE 802.11r/w compilation error
2009-10-12 Jouni MalinenInclude aes_unwrap in build when needed (FT and EAP...
2009-10-11 Jouni MalinenReplace CONFIG_NO_AES_EXTRAS with auto-detection during...
2009-10-11 Jouni MalinenClean up crypto makefile segments
2009-10-11 Jouni MalinenMove TLS_FUNCS and NEED_CRYPTO segment next to each...
2009-10-11 Jouni MalinenFurther crypto makefile unification
2009-10-11 Jouni MalinenFix crypto config for minimal builds
2009-10-11 Jouni MalinenCleaned up and unified some of the crypto Makefile...
2009-10-11 Jouni MalinenAllow the internal DH implementation to be overridden
2009-10-11 Jouni MalinenInclude only the used DH groups in the build
2009-09-08 Jouni MalinenMove STA list ctrl_iface handlers to a separate file
2009-08-16 Jouni MalinenUse OpenSSL for RC4 instead of internal implementation
2009-08-16 Jouni MalinenMove RC4 into crypto.h as a replaceable crypto function
2009-08-16 Jouni MalinenFix OpenSSL build (internal SHA256 not used anymore)
2009-08-16 Bjarke Istrup PedersenUse LDFLAGS in all linker commands
2009-08-14 Jouni MalinenForce rebuilding of src/drivers between hostapd and...
2009-08-14 Johannes BergReplace NEED_MLME with NEED_AP_MLME
2009-08-14 Johannes BergCreate a common drivers makefile snippet
2009-08-13 Jouni MalinenFix hlr_auc_gw build after crypto build cleanup
2009-08-13 Johannes BergCrypto build cleanup: remove CONFIG_NO_AES_*
2009-08-13 Johannes BergCrypto build cleanup: remove CONFIG_NO_AES_ENCRYPT
2009-08-13 Johannes BergCrypto build cleanup: remove CONFIG_NO_AES_DECRYPT
2009-08-11 Johannes BergCrypto build cleanup: remove CONFIG_NO_PBKDF2
2009-08-11 Johannes BergCrypto build cleanup: remove CONFIG_NO_TLS_PRF
2009-08-11 Johannes BergCrypto build cleanup: remove CONFIG_NO_T_PRF
2009-08-11 Johannes BergCrypto build cleanup: remove NEED_FIPS186_2_PRF
2009-07-28 Johannes BergCrypto build cleanup: remove INTERNAL_MD5
2009-07-28 Johannes BergCrypto build cleanup: remove INTERNAL_MD4
2009-07-28 Johannes BergCrypto build cleanup: remove INTERNAL_SHA256
2009-07-28 Johannes BergCrypto build cleanup: remove INTERNAL_AES
2009-07-28 Johannes BergCrypto build cleanup: remove INTERNAL_DES
2009-07-28 Johannes BergCrypto build cleanup: remove INTERNAL_SHA1
2009-07-28 Johannes Bergmake the build process quieter to see warnings
2009-05-29 Jouni Malinenhostapd: EAP-AKA' needs SHA256
2009-05-26 Jouni Malinenhostapd: Fix internal crypto build without TLS
next