]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - build-utilities/hostap.git/history - wpa_supplicant/sme.c
Fix crash when a local deauth occurs (squash)
[build-utilities/hostap.git] / wpa_supplicant / sme.c
2012-03-15 Eyal ShapiraRoam back to the origin AP when assoc/auth times out
2012-03-15 Eliad Pellerinitiate roaming on beacon_loss
2012-02-11 Jouni MalinenRemove the GPL notification from files contributed...
2012-01-29 Ben GreearSupport HT capability overrides
2012-01-29 Eyal ShapiraSME: Fix processing of Authentication timeout and failure
2011-12-04 Jouni MalinenSME: Fix processing of Authentication timeout
2011-12-04 Jouni MalinenSME: Fix processing of Authentication request failure
2011-11-24 Jouni MalinenUse wpa_key_mgmt_*() helpers
2011-11-18 Jouni MalinenMark local functions static
2011-11-13 Jouni MalinenRemove unnecessary include file inclusion
2011-10-29 Jouni MalinenAdd no_cck parameter for send_action() driver_ops
2011-10-22 Jouni MalinenRemove user space client MLME
2011-10-16 Jouni MalinenAdd Extended Capability element to AssocReq for Interwo...
2011-10-15 Luciano CoelhoUse sched_scan in driver init
2011-09-02 Jouni Malinennl80211: Fix WPA_VERSIONS attribute for Connect command
2011-07-17 Jouni MalinenP2P: Set p2p auth/assoc parameter based on connection...
2011-07-17 Eliad Pellernl80211: Change vif type to P2P_CLI upon P2P authentication
2011-02-24 Ben GreearSME: Add timers for authentication and asscoiation
2011-02-10 Ben GreearUse wpa_msg() instead of wpa_printf()
2010-12-29 Johannes BergP2P: Add option for offloading off-channel TX to the...
2010-12-19 Jouni MalinenUse SA Query procedure to recovery from AP/STA state...
2010-12-13 Jouni Malinennl80211: Set cipher suites when using user space SME
2010-11-26 Jouni MalinenSME: Optimize recovery from assocication command failures
2010-11-26 Jouni MalinenExtend load balancing optimization in BSS blacklisting
2010-11-25 Jouni MalinenSME: Optimize recovery from common load balancing mecha...
2010-11-25 Jouni MalinenSME: Fix re-try after auth/assoc timeout/failure
2010-09-09 Jouni MalinenP2P: Add mechanism for configuring UAPSD parameters...
2010-09-09 Jouni MalinenP2P: Include P2P IE in (Re)AssocReq to infra AP if...
2010-09-09 Jouni MalinenP2P: Add P2P IE into (Re)Association Request frames
2010-09-09 Jouni MalinenP2P: Let the driver wrapper know if association is...
2010-08-18 Samuel Ortizsme: Check for prev_bssid from sme_event_disassoc
2010-08-17 Samuel Ortizsme: Try all authentication algorithms when the first...
2010-07-18 Jouni MalinenSME: Retry scan after authentication failure
2010-04-11 Jouni MalinenSME: Handle association without own extra IEs
2010-04-10 Jouni MalinenSME: Do not try to use FT over-the-air if PTK is not...
2010-04-10 Jouni MalinenFT: Clean up wpa_sm_set_ft_params() by using common...
2010-04-09 Jouni MalinenFT: Set FT Capability and Policy properly in MDIE durin...
2010-04-09 Jouni MalinenFT: Copy FT Capability and Policy to MDIE from target AP
2010-04-07 Jouni MalinenFix SME to update WPA/RSN IE for rsn_supp module based...
2010-03-13 Jouni MalinenFT: Process reassoc resp FT IEs when using wpa_supplica...
2010-03-13 Jouni MalinenFT: Request reassociation after successful FT Action...
2010-01-25 Jouni MalinenSME: Request a new scan if SME association command...
2010-01-10 Jouni MalinenRemove unnecessary bss != NULL checks from sme_authenti...
2010-01-03 Jouni MalinenStandardize on a single definition of auth_alg bitfield...
2010-01-03 Jouni MalinenShare the same enum for MFP configuration
2010-01-03 Jouni MalinenMove wpa_supplicant specific scan code away from src...
2010-01-03 Jouni MalinenFix CONFIG_AP=y build after driver API changes
2010-01-02 Jouni MalinenMaintain a pointer to the current BSS table entry
2010-01-02 Jouni MalinenUse BSS table entry instead of raw scan result for...
2009-12-02 Jouni MalinenSME: Deauthenticate to clear state after disassociation...
2009-11-29 Jouni MalinenRemove src/rsn_supp from default header path
2009-11-29 Jouni MalinenRemove src/common from default header file path
2009-11-17 Jouni Malinennl80211/SME: Use reassociation when roaming within...
2009-10-31 Jouni MalinenSME: Improve processing of association rejection
2009-09-13 Jouni MalinenAdd wpa_supplicant notification calls
2009-04-23 Jouni MalinenAdd handling of SME auth/assoc timeout events
2009-04-04 Jouni Malinennl80211: Fix static WEP key configuration when using SME
2009-04-01 Jouni MalinenSME: Add processing for rejected associations
2009-03-26 Jouni MalinenAdd preliminary hostapd data structure initialization...
2009-03-20 Jouni MalinenAdd SME support (separate authentication and association)