]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - build-utilities/hostap.git/history - wpa_supplicant/wpa_supplicant.c
Select the BSD license terms as the only license alternative
[build-utilities/hostap.git] / wpa_supplicant / wpa_supplicant.c
2012-02-11 Jouni MalinenSelect the BSD license terms as the only license altern...
2012-02-04 Dan WilliamsTry fallback drivers if global init for preferred drive...
2012-02-04 Jouni MalinenUse PMKSA cache entries with only a single network...
2012-02-04 Jouni MalinenDelay scan request on select_network if disconnecting
2012-01-29 Ben GreearSupport HT capability overrides
2012-01-29 Jouni MalinenRemove duplicated TERMINATING event
2012-01-29 Dmitry ShmidtMove ctrl_iface deinit into the end of interface deinit
2012-01-29 Dmitry ShmidtDeinit driver before notifying interface has been removed
2012-01-29 Dmitry ShmidtLet wpa_supplicant_deinit_iface() know that process...
2012-01-29 Eyal ShapiraInterleave wildcard and specific SSID scans when max_ss...
2012-01-28 Nicolas CavallariSupport fixing the BSSID in IBSS mode
2012-01-01 Jouni MalinenUpdate copyright notices to include year 2012
2011-12-31 Jouni MalinenRemove possible authentication timeout on connection...
2011-12-10 Arik NemtsovMaintain internal copy of Probe Response offload capabi...
2011-12-03 Jouni MalinenUpdate internal MAC address on EVENT_INTERFACE_ENABLED...
2011-12-03 Johan HedlundUpdate RSN supplicant MAC address on driver reinitializ...
2011-11-24 Jouni MalinenUse wpa_key_mgmt_*() helpers
2011-11-03 Jouni Malinenndis: Work around lack of C99 designated initializers...
2011-10-30 Jouni MalinenFix TKIP countermeasures stopping in deinit paths
2011-10-23 Arik NemtsovTDLS: Get TDLS related capabilities from driver
2011-10-23 Christian Lamparterwpa_supplicant: Unify hardware feature data
2011-10-23 Jouni MalinenPostpone global_init() call until first driver instance...
2011-10-22 Jouni MalinenRemove user space client MLME
2011-10-21 Dmitry ShmidtPrevent ap_scan change during association
2011-10-16 Jouni MalinenAdd Extended Capability element to AssocReq for Interwo...
2011-10-15 Luciano CoelhoAdd delayed scheduled scan request
2011-10-15 Luciano CoelhoAdd filter support to scheduled scans
2011-10-15 Luciano CoelhoUse sched_scan in driver init
2011-10-15 Luciano CoelhoAdd scheduled scan driver operations
2011-10-02 Jithu JanceDo not re-associate on SELECT_NETWORK to current network
2011-09-30 Zhi ChenAllow wildcard SSID to be used with WPA-PSK if bssid...
2011-09-29 Jouni MalinenGAS: Use off-channel operations for requests
2011-09-29 Jouni MalinenGAS: Add a generic GAS query module
2011-09-26 Jouni MalinenDo not enable bgscan when driver takes care of BSS...
2011-09-26 Jouni MalinenSupport driver-based BSS selection in ap_scan=1 mode
2011-09-08 Edward LuMake sure wpa_proto gets cleared for WPS and non-WPA...
2011-09-07 Jouni MalinenFlush PMKSA cache entries and invalidate EAP state...
2011-09-02 Jouni Malinennl80211: Fix WPA_VERSIONS attribute for Connect command
2011-07-17 Jouni MalinenP2P: Set p2p auth/assoc parameter based on connection...
2011-07-16 Jouni MalinenDeauthenticate on reconfiguration
2011-06-21 Jouni MalinenP2P: Start GO without extra scan step
2011-05-31 Jouni Malinenrandom: Add support for maintaining internal entropy...
2011-04-15 Jouni MalinenUpdate driver country info on 'SET country <value>'
2011-04-14 Jouni MalinenTDLS: Verify that scan results for BSS are available...
2011-04-11 Dmitry ShmidtMake scan interval configurable
2011-03-31 Paul Stewartdbus: Add "excessive" to debug_strings
2011-03-23 Jouni MalinenRSN IBSS: Restart IBSS state machines for each new...
2011-03-22 Jouni Malinenrandom: Read /dev/random in the background with eloop...
2011-03-20 Sam Lefflerwpa_supplicant: Parameterize BSS table expiration age...
2011-03-20 Paul Stewartwpa_supplicant: Start bgscan on COMPLETED, not ASSOCIATED
2011-03-15 Paul StewartAdd DBus state change notification for AuthMode property
2011-03-15 Paul Stewartwpa_supplicant: Add wpa_supplicant_get_eap_mode method
2011-03-06 Jouni MalinenTDLS: Do not allow setup to be started if AP prohibits...
2011-03-06 Ganesh PrasadhTDLS: Add initial support for TDLS (IEEE Std 802.11z...
2011-02-27 Jouni MalinenUpdate copyright notices to include the new year
2011-02-24 Ben GreearWait 1 second before (re)scanning on authentication...
2011-02-24 Ben GreearSME: Add timers for authentication and asscoiation
2011-02-10 Jouni MalinenFix CONFIG_NO_STDOUT_DEBUG=y build
2011-02-10 Ben GreearUse wpa_msg() instead of wpa_printf()
2011-02-06 Ben GreearAdd interface name to wpa_msg() output
2011-01-09 Jouni MalinenUse set_key addr to distinguish default and multicast...
2011-01-09 Jouni MalinenUse more consistent set_key seq value when nothing...
2010-12-19 Jouni MalinenFix CONFIG_SME build without CONFIG_IEEE80211W
2010-12-19 Jouni MalinenUse SA Query procedure to recovery from AP/STA state...
2010-11-26 Ben GreearAdd interface name to some debug prints
2010-11-26 Jouni MalinenAllow driver wrappers to indicate whether result codes...
2010-11-26 Jouni MalinenExtend load balancing optimization in BSS blacklisting
2010-11-25 Jouni MalinenSME: Optimize recovery from common load balancing mecha...
2010-11-09 Samuel Ortizwpa_supplicant: Test all compiled drivers before failing
2010-11-09 Felix Fietkauwpa_supplicant: Fix port state management without IEEE8...
2010-10-27 Jouni MalinenFix memory leak in P2P build without MLME
2010-10-22 Jouni MalinenShow wpa_supplicant version number in the debug log
2010-09-09 Jouni MalinenP2P: Allow driver wrapper to indicate how many stations...
2010-09-09 Jouni MalinenP2P: Add mechanism for configuring UAPSD parameters...
2010-09-09 Jouni MalinenP2P: Add support for cross connection
2010-09-09 Jouni MalinenP2P: Include P2P IE in (Re)AssocReq to infra AP if...
2010-09-09 Jouni MalinenTrigger scan on reload-config only if there are enabled...
2010-09-09 Jouni MalinenP2P: Add P2P IE into (Re)Association Request frames
2010-09-09 Jouni MalinenP2P: Let the driver wrapper know if association is...
2010-09-09 Jouni MalinenP2P: Add initial version of P2P Module
2010-09-09 Jouni MalinenP2P: Do not register l2_packet on dedicated P2P device...
2010-09-09 Jouni MalinenP2P: Use config block with disabled==2 to store persist...
2010-09-09 Jouni MalinenP2P: Add dynamic network config block parameters for P2P
2010-09-09 Jouni MalinenAllow ctrl_iface SET command to change global config...
2010-09-04 Jouni MalinenNDIS: Fix association for WPS provisioning with protect...
2010-08-26 Jouni MalinenShare common code in wpa_supplicant_{disassociate,deaut...
2010-08-26 Jouni MalinenCancel authentication timeout on local deauth/disassoc...
2010-05-23 Jouni MalinenAdd Linux rfkill support
2010-05-02 Kel ModdermanFix enabling of networks while another network is being...
2010-04-16 Jouni MalinenDo not trigger initial scan if there are no enabled...
2010-04-11 Jouni MalinenAdd more wpa_supplicant AP mode parameters for the...
2010-04-11 Jouni MalinenAllow driver wrappers to indicate maximum remain-on...
2010-04-11 Jouni MalinenOptimize post-WPS scan based on channel used during...
2010-04-10 Jouni MalinenFT: Clean up wpa_sm_set_ft_params() by using common...
2010-04-09 Jouni MalinenFT: Copy FT Capability and Policy to MDIE from target AP
2010-03-29 Jouni MalinenMFP: Add MFPR flag into station RSN IE if 802.11w is...
2010-01-16 Jouni MalinenPreparations for v0.7.1 release hostap_0_7_1
2010-01-04 Marcel Holtmanndbus: Replace StateChanged with PropertiesChanged signal
2010-01-03 Jouni MalinenStandardize on a single definition of auth_alg bitfield...
2010-01-03 Jouni MalinenShare the same enum for MFP configuration
next