]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - build-utilities/hostap.git/history - wpa_supplicant/wps_supplicant.c
Fix crash when a local deauth occurs (squash)
[build-utilities/hostap.git] / wpa_supplicant / wps_supplicant.c
2012-03-15 Eyal ShapiraP2P: Ignore PBC overlap in P2P provisioning
2012-02-12 Jouni MalinenWPS: Fix regression in post-WPS scan optimization
2012-02-11 Jouni MalinenRemove the GPL notification from files contributed...
2012-01-30 Jouni MalinenWPS: Disable AP PIN after 10 consecutive failures
2011-12-31 Jouni MalinenWPS: Use single channel scan if AP channel already...
2011-12-11 Jouni MalinenDisassociate when starting WPS search
2011-11-28 Jouni MalinenUse normal scan before sched_scan if that can speed...
2011-10-23 Christian Lamparterwpa_supplicant: Unify hardware feature data
2011-10-22 Andrii BordunovWPS: Use ifdef blocks consistently for CONFIG_WPS_REG_D...
2011-09-01 Bharat ChakravartyWPS: Set Probe Request config methods based on configur...
2011-08-31 Bharat ChakravartyWPS: Set RF bands based on driver capabilities
2011-07-15 Jouni MalinenWPS: Check malloc success on workaround path
2011-06-27 Jouni MalinenClear WPA and EAPOL state machine config pointer on...
2011-06-25 Jayant SaneP2P: Add WpsFailed signal in P2P D-Bus
2011-06-23 Jayant SaneP2P: Update D-Bus network object semantics during group...
2011-03-17 Johannes BergWPS: Store (secondary) device type as binary
2011-03-17 Jouni MalinenWPS: Fix copying of UUID from the first interface
2011-03-17 Jean-Michel BachotWPS: Add secondary device types into Probe Request...
2011-03-10 Jouni MalinenWPS: Copy UUID from the first interface
2011-02-22 Jouni MalinenP2P: Notify WPS-M2D event on parent interface and handl...
2011-02-21 Ben GreearWPS ER: Stop eloop only on the last terminate_cb
2011-02-02 Johannes BergDBus: Publish provisioned keys in network properties
2011-01-13 Chao-Wen YangWPS: Indicate WPS-FAIL event on EAPOL timeout-based...
2011-01-13 Chao-Wen YangWPS: Add mechanism for indicating non-standard WPS...
2011-01-05 Jouni MalinenWPS: Make WPS-AP-AVAILABLE* events a bit more consistent
2010-12-30 Jouni MalinenWPS: Add option to disable open networks by default
2010-11-17 Jouni MalinenWPS: Add wps_ap_pin ctrl_iface command for wpa_supplica...
2010-10-25 Jouni MalinenWPS ER: Show SetSelectedRegistrar events as ctrl_iface...
2010-10-20 Jouni MalinenWPS ER: Add wps_er_set_config to use local configuration
2010-10-16 Jouni MalinenWPS: Add virtual flags in Config Methods for WPS 2...
2010-10-14 Jouni MalinenP2P: Send WPS-FAIL event to parent interface, too
2010-10-14 Jouni MalinenWPS: Add Config Error into WPS-FAIL events
2010-10-06 Jouni MalinenFix build with CONFIG_WPS_OOB
2010-09-20 Jouni MalinenWPS: Add more verbose debug info on PBC session overlap...
2010-09-20 Jouni MalinenWPS: Add BSSID to strict validation error messages
2010-09-10 Ardong ChenWPS: Allow pending WPS operation to be cancelled
2010-09-10 Ardong ChenWPS: Fix timeout event to be sent over ctrl_interface
2010-09-09 Jouni MalinenFix build without CONFIG_P2P=y
2010-09-09 Jouni MalinenP2P: Use SSID from GO Negotiation to limit WPS provisio...
2010-09-09 Jouni MalinenTrigger WPS configuration update on string changes
2010-09-09 Jouni MalinenWPS: Fix configuration strings on config reload
2010-09-09 Jouni MalinenP2P: Set Device Password ID in WPS M1/M2 per new rules
2010-09-09 Jouni MalinenP2P: Add initial version of P2P Module
2010-09-09 Jouni MalinenP2P: Do not save temporary networks
2010-09-09 Jouni MalinenP2P: Do not filter BSSes based on SSID during P2P Provi...
2010-09-09 Jouni MalinenP2P: Let WPS code know if it is used in a P2P group
2010-09-09 Jouni MalinenAllow ctrl_iface SET command to change global config...
2010-09-09 Jouni MalinenWPS: Make fragment size configurable for EAP-WSC peer
2010-09-09 Jouni MalinenWPS 2.0: Make sure PHY/VIRT flag gets set for PBC
2010-09-09 Jouni MalinenWPS 2.0: Validate WPS attributes in management frames...
2010-09-09 Jouni MalinenWPS 2.0: Add support for AuthorizedMACs attribute
2010-07-18 Jouni MalinenWPS: Do not allow Label and Display config methods...
2010-06-11 Jouni MalinenWPS: Use different scan result sorting rules when doing...
2010-05-27 Jouni MalinenWPS ER: Add command for configuring an AP
2010-05-27 Jouni MalinenWPS ER: Add ctrl_iface event for learned AP settings
2010-05-27 Jouni MalinenWPS ER: Allow AP filtering based on IP address
2010-04-11 Jouni MalinenOptimize post-WPS scan based on channel used during...
2010-01-03 Jouni MalinenMove wpa_supplicant specific scan code away from src...
2010-01-02 Jouni MalinenUse BSS table entry instead of raw scan result for...
2010-01-02 Jouni MalinenWPS: Use BSS table instead of raw scan results
2009-12-28 Jouni MalinenWPS: Clear SSID selection if more than one BSSID match...
2009-12-27 Jouni MalinenUse wpa_msg_ctrl() for WPS AP available events
2009-12-21 Jouni MalinenWPS: Make Config Methods configurable for wpa_supplicant
2009-12-19 Jouni MalinenWPS ER: Delay wpa_supplicant termination to allow unsub...
2009-12-12 Jouni MalinenWPS: Add display and keypad config methods for WPS ER
2009-11-29 Jouni MalinenRemove src/crypto from default include path
2009-11-29 Jouni MalinenRemove src/rsn_supp from default header path
2009-11-29 Jouni MalinenRemove src/common from default header file path
2009-11-26 Jouni MalinenWPS: Update couple of missed Primary Device Type uses
2009-11-26 Jouni MalinenWPS: Clean up Primary Device Type handling
2009-11-21 Jouni MalinenWPS ER: Add more AP information into the ctrl_interface...
2009-11-20 Jouni MalinenWPS ER: Refresh ER data on WPS_ER_START when already...
2009-11-15 Jouni MalinenWPS ER: Deinit ER before WPS registrar/context
2009-11-15 Jouni MalinenWPS ER: Add command for fetching current AP settings
2009-11-15 Jouni MalinenWPS ER: Add preliminary PBC support
2009-11-15 Jouni MalinenWPS ER: Add ctrl_iface notifications for AP/Enrollee...
2009-11-13 Jouni MalinenWPS ER: Add PIN configuration and SetSelectedRegistrar...
2009-11-10 Jouni MalinenWPS: Fix WPS build with ER support disabled
2009-11-07 Jouni MalinenWPS: Add initial part of External Registrar functionality
2009-11-01 Oleg KravtsovWPS: Add PBC overlap and timeout events from WPS module
2009-10-11 Jouni MalinenAllow the internal DH implementation to be overridden
2009-09-13 Jouni MalinenAdd wpa_supplicant notification calls
2009-09-11 Jouni MalinenAdd parsed information from WPS IE(s) into scan results
2009-09-06 Jouni MalinenWPS: Add support for AP reconfiguration with wps_reg
2009-08-15 Jouni MalinenWPS: Workaround mixed-mode WPA+WPA2 auth type in creden...
2009-03-30 Jouni MalinenWPS: Fix local configuration update after AP configuration
2009-03-26 Jouni MalinenAdd preliminary hostapd data structure initialization...
2009-03-06 Masashi HonmaWPS: Add support for NFC out-of-band mechanism
2009-03-05 Jouni MalinenWPS: Add a workaround for TKIP/CCMP mixed mode credentials
2009-02-26 Jouni MalinenWPS UFD: Build OOB functionality only if UFD is enabled
2009-02-26 Jouni MalinenWPS UFD: Use pre-configured DH keys only with OOB
2009-02-26 Jouni MalinenWPS UFD: Remove oob_dev pointer from wps_context
2009-02-26 Masashi HonmaWPS: Add UFD support (USBA out-of-band mechanism)
2009-02-18 Andriy TkachukWPS: Fix WEP key index to use 1..4 instead of 0..3
2009-02-17 Andriy TkachukWPS: support WEP keys in hex characters format in recei...
2009-01-23 Jouni MalinenWPS: Lock AP Setup on multiple AP PIN validation failures
2009-01-23 Jouni MalinenAllow WPS APs for PIN enrollment even without Selected...
2009-01-18 Jouni MalinenWPS: Add configurable option for processing credentials...
2009-01-17 Jouni MalinenWPS: Provide the unparsed Credential attribute to cred_cb()
2009-01-17 Jouni MalinenWPS: Ignore credentials for unsupported authentication...
next