Fix crash when a local deauth occurs (squash)
[build-utilities/hostap.git] / wpa_supplicant /
2012-03-15 Eyal ShapiraFix crash when a local deauth occurs (squash) p2p-upstream-android
2012-03-15 Eyal ShapiraP2P: Ignore PBC overlap in P2P provisioning
2012-03-15 Eyal ShapiraIncrease the scan_interval to 15 secs
2012-03-15 Eyal ShapiraInitiate a periodic normal scan in addition to sched...
2012-03-15 Eliad Pellerincrease the eapol pending timer to 500ms
2012-03-15 Eliad PellerP2P: notify about disconnection only when needed
2012-03-15 Eliad PellerExecute p2p_find instead of p2p_listen
2012-03-15 Eyal ShapiraAdd CONFIG_ROAMING to wpa_s Makefile
2012-03-15 Eyal ShapiraPrevent roaming to a different ESS while connected
2012-03-15 Eliad PellerP2P: Add p2p_cli deinit op
2012-03-15 Eyal ShapiraIgnore a deauth from a different BSS than the current one
2012-03-15 Eyal ShapiraRoam back to the origin AP when assoc/auth times out
2012-03-15 Eyal Shapirabgscan_learn: implement notify_beacon_loss hook
2012-03-15 Eyal Shapirabgscan_learn: Scan all channels in certain scenarios
2012-03-15 Eliad Pellerinitiate roaming on beacon_loss
2012-03-15 Eliad PellerAdd blacklist expiration
2012-03-15 Eyal ShapiraFix initial interval of bgscan_learn
2012-03-15 Eyal ShapiraAdd API and CLI command to control sched scan intervals
2012-03-15 Luciano Coelhoconfig: enable NL80211
2012-03-15 Eyal Shapirawpa_s: add API to disable or enable roaming
2012-03-15 Ido Reiswpa_supplicant: update config file to support bgscan
2012-03-15 Eyal Shapirawpa_s: Disable bgscan and roaming when driver support...
2012-03-15 Eyal Shapirasched scan: add support for short and long intervals
2012-03-15 Eyal Shapirasched scan: Add config parameters for short and long...
2012-03-15 Eyal Shapirasched scan: read driver support for sched scan intervals
2012-03-13 Eliad PellerAP: use uapsd if go_apsd was set
2012-03-13 Eliad PellerP2P: use GO channel for Operating Channel IE
2012-03-13 Eyal Shapirasched scan: Continue to scan even if previous scan...
2012-03-13 Eyal Shapirasched scan: Avoid changing state to SCANNING
2012-03-13 Eyal Shapirasched scan: Logic changes
2012-03-13 Eyal Shapirasched scan: Avoid scan if no enabled networks
2012-03-13 Eyal Shapirasched scan: Continue to scan even if previous scan...
2012-03-13 Eyal Shapirasched scan: Update scan according to changes in network...
2012-03-13 Eyal Shapirasched scan: Turn passive scan into active
2012-03-13 Eyal Shapirasched scan: Fallback to normal scan during WPS
2012-03-13 Yotam Rubinwpa_supplicant: change config - enable ROAMING, 11n...
2012-03-09 Jouni MalinenAndroid: Implement SETBAND for scan requests
2012-03-05 Jouni MalinenAndroid: Do not use separate private lib
2012-03-05 Dmitry ShmidtSet buffer length the same as in wpa_supplicant_ctrl_if...
2012-03-05 Dmitry ShmidtFix reporting hidden APs during scan
2012-03-05 Dmitry ShmidtAdd P2P support for BRCM CFG80211 driver (P2P invite...
2012-03-05 Dmitry ShmidtAndroid: Define ANDROID_BRCM_P2P_PATCH for Broadcom...
2012-03-05 Dmitry ShmidtAdd WPA_UNICODE_SSID support
2012-03-05 Jouni MalinenAndroid: Convert driver_cmd BGSCAN-START/STOP to proper...
2012-03-05 Dmitry ShmidtAdd extended 'driver' command
2012-03-05 Dmitry ShmidtSet ap_scan to default in case of disassociation
2012-03-05 Dmitry ShmidtFix scan notification in case of canceling scan
2012-03-05 Dmitry ShmidtAndroid: Add src directory symlinks
2012-03-05 Todd Previtedbus: Make P2P group properties accessible individually
2012-03-05 Eliad PellerBSS: Fix use-after-realloc
2012-03-05 Grzegorz BajorskiP2P: Filter input parameters in p2p_serv_disc_external
2012-03-05 Jouni MalinenFilter station mode EAPOL RX on bridge interface based...
2012-03-04 Jouni MalinenFix memory leak on parsing multiple network block eap...
2012-03-04 Jouni MalinenInterworking: Use EAP-AKA if USIM is used
2012-03-04 Jouni MalinenInterworking: Support real SIM/USIM card for network...
2012-03-04 Jouni MalinenInterworking: Make plmn_id_match() for generic
2012-03-04 Jouni MalinenInterworking: Fix credential block example
2012-03-03 Jouni MalinenInterworking: Update configuration file documentation...
2012-03-03 Jouni MalinenInterworking: Add support for certificate credentials...
2012-03-01 Jouni MalinenP2P: Fix provisioning info clearing after successful...
2012-03-01 Jouni MalinenFix processing of channel list update events
2012-03-01 Jouni MalinenFix CTRL-EVENT-DISCONNECTED event for locally generated...
2012-02-29 Jouni MalinenP2P: Fix p2p_cancel to return success if GO Negotiation...
2012-02-28 Jouni MalinenP2P: Use scan optimization for post-provisioning connection
2012-02-28 Jouni MalinenP2P: Optimize provisioning step scan for join-a-group...
2012-02-28 Jouni MalinenP2P: Use specific SSID in scan for provisioning step
2012-02-27 Jouni MalinenP2P: Advertise immediate availability of WPS credential
2012-02-27 Vivek NatarajanAdd support for hidden SSID in wpa_supplicant AP mode
2012-02-27 Jouni MalinenFix CONFIG_AP + CONFIG_INTERWORKING build
2012-02-26 Jouni MalinenAllow PC/SC reader to be selected and initialized at...
2012-02-25 Dmitry ShmidtAndroid: Build wpa_supplicant.conf from a template
2012-02-25 Dmitry ShmidtAndroid: Add PLATFORM_VERSION to VERSION_STR_POSTFIX...
2012-02-25 Dmitry ShmidtAndroid: Add build configuration files
2012-02-25 Dmitry ShmidtAdd CONFIG_NO_ROAMING option
2012-02-25 Jithu JanceAdd wpa_supplicant AP mode STA deauthenticate/disassoci...
2012-02-25 Reinette Chatredbus: return NULL data for peer IEs
2012-02-25 Reinette Chatredbus: revert changes to some peer properties
2012-02-25 Jayant Sanedbus: utility to create dbus message from wpabuf array
2012-02-19 Jouni MalinenP2P: Add more debug on group idle timeout
2012-02-19 Jouni MalinenP2P: Fix group idle timer cancellation on group removal
2012-02-19 Jouni MalinenClean up array insertion to skip unnecessary memmove
2012-02-19 Jouni MalinenFix memory leak on set_cred error path
2012-02-19 Jouni MalinenFix memory leak on error path in bssid_filter setting
2012-02-19 Jouni MalinenInterworking: Fix SIM/USIM NAI construction
2012-02-18 Jouni MalinenUse WPA_INTERFACE_DISABLED with interface removed events
2012-02-17 Jouni MalinenP2P: Allow channels to be removed from P2P use
2012-02-17 Jouni MalinenP2P: Do not include P2P IE in association request to...
2012-02-16 Jouni MalinenInterworking: Allow network block -based connection...
2012-02-16 Jouni MalinenInterworking: Add verbose error message on cred block...
2012-02-16 Jouni MalinenInterworking: Add support for credential priorities
2012-02-16 Jouni MalinenInterworking: Add ctrl_iface commands for managing...
2012-02-16 Jouni MalinenInterworking: Write cred blocks into configuration...
2012-02-16 Jouni MalinenInterworking: Add support for multiple credentials
2012-02-16 Jouni MalinenInterworking: Use 3gppnetwork.org for matching home...
2012-02-16 Jouni MalinenInterworking: Use anonymous NAI in EAP-TTLS Phase 1
2012-02-16 Jouni MalinenInterworking: Add support for home vs. visited SP deter...
2012-02-16 Jouni MalinenInterworking: Do not disable other network profiles
2012-02-16 Jouni MalinenAdd BSSID filter for testing purposes
2012-02-16 Jouni MalinenAllow legacy PS param to be set with SET in addition...
2012-02-16 Jouni MalinenAllow U-APSD parameters to be configured with SET command
next