1 /*
3 BLIS
4 An object-based framework for developing high-performance BLAS-like
5 libraries.
7 Copyright (C) 2014, The University of Texas at Austin
9 Redistribution and use in source and binary forms, with or without
10 modification, are permitted provided that the following conditions are
11 met:
12 - Redistributions of source code must retain the above copyright
13 notice, this list of conditions and the following disclaimer.
14 - Redistributions in binary form must reproduce the above copyright
15 notice, this list of conditions and the following disclaimer in the
16 documentation and/or other materials provided with the distribution.
17 - Neither the name of The University of Texas at Austin nor the names
18 of its contributors may be used to endorse or promote products
19 derived from this software without specific prior written permission.
21 THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
22 "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
23 LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
24 A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
25 HOLDER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
26 SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
27 LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
28 DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
29 THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
30 (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
31 OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
33 */
35 #include "blis.h"
37 #define FUNCPTR_T unpackv_fp
39 typedef void (*FUNCPTR_T)( obj_t* p,
40 obj_t* a,
41 unpackv_t* cntl );
43 static FUNCPTR_T vars[1][3] =
44 {
45 // unblocked optimized unblocked blocked
46 { bli_unpackv_unb_var1, NULL, NULL }
47 };
49 void bli_unpackv_int( obj_t* p,
50 obj_t* a,
51 unpackv_t* cntl )
52 {
53 // The unpackv operation consists of an optional casting post-process.
54 // (This post-process is analogous to the cast pre-process in packv.)
55 // Here are the following possible ways unpackv can execute:
56 // 1. unpack and cast: Unpack to a temporary vector c and then cast
57 // c to a.
58 // 2. unpack only: Unpack directly to vector a since typecasting is
59 // not needed.
60 // 3. cast only: Not yet supported / not used.
61 // 4. no-op: The control tree directs us to skip the unpack operation
62 // entirely. No action is taken.
64 obj_t c;
66 varnum_t n;
67 impl_t i;
68 FUNCPTR_T f;
70 // Check parameters.
71 if ( bli_error_checking_is_enabled() )
72 bli_unpackv_check( p, a, cntl );
74 // Sanity check; A should never have a zero dimension. If we must support
75 // it, then we should fold it into the next alias-and-early-exit block.
76 if ( bli_obj_has_zero_dim( *a ) ) bli_abort();
78 // First check if we are to skip this operation because the control tree
79 // is NULL, and if so, simply return.
80 if ( cntl_is_noop( cntl ) )
81 {
82 return;
83 }
85 // If p was aliased to a during the pack stage (because it was already
86 // in an acceptable packed/contiguous format), then no unpack is actually
87 // necessary, so we return.
88 if ( bli_obj_is_alias_of( *p, *a ) )
89 {
90 return;
91 }
93 // Now, if we are not skipping the unpack operation, then the only
94 // question left is whether we are to typecast vector a after unpacking.
95 if ( bli_obj_datatype( *p ) != bli_obj_datatype( *a ) )
96 bli_abort();
97 /*
98 if ( bli_obj_datatype( *p ) != bli_obj_datatype( *a ) )
99 {
100 // Initialize an object c for the intermediate typecast vector.
101 bli_unpackv_init_cast( p,
102 a,
103 &c );
104 }
105 else
106 */
107 {
108 // If no cast is needed, then aliasing object c to the original
109 // vector serves as a minor optimization. This causes the unpackv
110 // implementation to unpack directly into vector a.
111 bli_obj_alias_to( *a, c );
112 }
114 // Now we are ready to proceed with the unpacking.
116 // Extract the variant number and implementation type.
117 n = cntl_var_num( cntl );
118 i = cntl_impl_type( cntl );
120 // Index into the variant array to extract the correct function pointer.
121 f = vars[n][i];
123 // Invoke the variant.
124 f( p,
125 &c,
126 cntl );
128 // Now, if necessary, we cast the contents of c to vector a. If casting
129 // was not necessary, then we are done because the call to the unpackv
130 // implementation would have unpacked directly to vector a.
131 /*
132 if ( bli_obj_datatype( *p ) != bli_obj_datatype( *a ) )
133 {
134 // Copy/typecast vector c to vector a.
135 // NOTE: Here, we use copynzv instead of copym because, in the cases
136 // where we are unpacking/typecasting a real vector c to a complex
137 // vector a, we want to touch only the real components of a, rather
138 // than also set the imaginary components to zero. This comes about
139 // because of the fact that, if we are unpacking real-to-complex,
140 // then it is because all of the computation occurred in the real
141 // domain, and so we would want to leave whatever imaginary values
142 // there are in vector a untouched. Notice that for unpackings that
143 // entail complex-to-complex data movements, the copynzv operation
144 // behaves exactly as copym, so no use cases are lost (at least none
145 // that I can think of).
146 bli_copynzv( &c,
147 a );
149 // NOTE: The above code/comment is outdated. What should happen is
150 // as follows:
151 // - If dt(a) is complex and dt(p) is real, then create an alias of
152 // a and then tweak it so that it looks like a real domain object.
153 // This will involve:
154 // - projecting the datatype to real domain
155 // - scaling both the row and column strides by 2
156 // ALL OF THIS should be done in the front-end, NOT here, as
157 // unpackv() won't even be needed in that case.
158 }
159 */
160 }
162 /*
163 void bli_unpackv_init_cast( obj_t* p,
164 obj_t* a,
165 obj_t* c )
166 {
167 // The idea here is that we want to create an object c that is identical
168 // to object a, except that:
169 // (1) the storage datatype of c is equal to the target datatype of a,
170 // with the element size of c adjusted accordingly,
171 // (2) object c is marked as being stored in a standard, contiguous
172 // format (ie: a column vector),
173 // (3) the view offset of c is reset to (0,0), and
174 // (4) object c's main buffer is set to a new memory region acquired
175 // from the memory manager, or extracted from p if a mem entry is
176 // already available. (After acquring a mem entry from the memory
177 // manager, it is cached within p for quick access later on.)
179 num_t dt_targ_a = bli_obj_target_datatype( *a );
180 dim_t dim_a = bli_obj_vector_dim( *a );
181 siz_t elem_size_c = bli_datatype_size( dt_targ_a );
183 // We begin by copying the basic fields of a.
184 bli_obj_alias_to( *a, *c );
186 // Update datatype and element size fields.
187 bli_obj_set_datatype( dt_targ_a, *c );
188 bli_obj_set_elem_size( elem_size_c, *c );
190 // Update the strides and dimensions. We set the increments to reflect a
191 // column-stored vector. Note that the column stride is set to dim(a),
192 // though it should never be used because there is no second column to
193 // index into (and therefore it also does not need to be aligned).
194 bli_obj_set_dims( dim_a, 1, *c );
195 bli_obj_set_incs( 1, dim_a, *c );
197 // Reset the view offsets to (0,0).
198 bli_obj_set_offs( 0, 0, *c );
200 // Check the mem_t entry of p associated with the cast buffer. If it is
201 // NULL, then acquire memory sufficient to hold the object data and cache
202 // it to p. (Otherwise, if it is non-NULL, then memory has already been
203 // acquired from the memory manager and cached.) We then set the main
204 // buffer of c to the cached address of the cast memory.
205 bli_obj_set_buffer_with_cached_cast_mem( *p, *c );
206 }
207 */