1 # Doxyfile 1.7.6.1
3 # This file describes the settings to be used by the documentation system
4 # doxygen (www.doxygen.org) for a project.
5 #
6 # All text after a hash (#) is considered a comment and will be ignored.
7 # The format is:
8 # TAG = value [value, ...]
9 # For lists items can also be appended using:
10 # TAG += value [value, ...]
11 # Values that contain spaces should be placed between quotes (" ").
13 #---------------------------------------------------------------------------
14 # Project related configuration options
15 #---------------------------------------------------------------------------
17 # This tag specifies the encoding used for all characters in the config file
18 # that follow. The default is UTF-8 which is also the encoding used for all
19 # text before the first occurrence of this tag. Doxygen uses libiconv (or the
20 # iconv built into libc) for the transcoding. See
21 # http://www.gnu.org/software/libiconv for the list of possible encodings.
23 DOXYFILE_ENCODING = UTF-8
25 # The PROJECT_NAME tag is a single word (or sequence of words) that should
26 # identify the project. Note that if you do not use Doxywizard you need
27 # to put quotes around the project name if it contains spaces.
29 PROJECT_NAME = "LINALG "
31 # The PROJECT_NUMBER tag can be used to enter a project or revision number.
32 # This could be handy for archiving the generated documentation or
33 # if some version control system is used.
35 PROJECT_NUMBER =
37 # Using the PROJECT_BRIEF tag one can provide an optional one line description
38 # for a project that appears at the top of each page and should give viewer
39 # a quick idea about the purpose of the project. Keep the description short.
41 PROJECT_BRIEF = "Linear Algebra Library"
43 # With the PROJECT_LOGO tag one can specify an logo or icon that is
44 # included in the documentation. The maximum height of the logo should not
45 # exceed 55 pixels and the maximum width should not exceed 200 pixels.
46 # Doxygen will copy the logo to the output directory.
48 PROJECT_LOGO =
50 # The OUTPUT_DIRECTORY tag is used to specify the (relative or absolute)
51 # base path where the generated documentation will be put.
52 # If a relative path is entered, it will be relative to the location
53 # where doxygen was started. If left blank the current directory will be used.
55 OUTPUT_DIRECTORY = ./docs/doxygen
57 # If the CREATE_SUBDIRS tag is set to YES, then doxygen will create
58 # 4096 sub-directories (in 2 levels) under the output directory of each output
59 # format and will distribute the generated files over these directories.
60 # Enabling this option can be useful when feeding doxygen a huge amount of
61 # source files, where putting all generated files in the same directory would
62 # otherwise cause performance problems for the file system.
64 CREATE_SUBDIRS = YES
66 # The OUTPUT_LANGUAGE tag is used to specify the language in which all
67 # documentation generated by doxygen is written. Doxygen will use this
68 # information to generate all constant output in the proper language.
69 # The default language is English, other supported languages are:
70 # Afrikaans, Arabic, Brazilian, Catalan, Chinese, Chinese-Traditional,
71 # Croatian, Czech, Danish, Dutch, Esperanto, Farsi, Finnish, French, German,
72 # Greek, Hungarian, Italian, Japanese, Japanese-en (Japanese with English
73 # messages), Korean, Korean-en, Lithuanian, Norwegian, Macedonian, Persian,
74 # Polish, Portuguese, Romanian, Russian, Serbian, Serbian-Cyrillic, Slovak,
75 # Slovene, Spanish, Swedish, Ukrainian, and Vietnamese.
77 OUTPUT_LANGUAGE = English
79 # If the BRIEF_MEMBER_DESC tag is set to YES (the default) Doxygen will
80 # include brief member descriptions after the members that are listed in
81 # the file and class documentation (similar to JavaDoc).
82 # Set to NO to disable this.
84 BRIEF_MEMBER_DESC = YES
86 # If the REPEAT_BRIEF tag is set to YES (the default) Doxygen will prepend
87 # the brief description of a member or function before the detailed description.
88 # Note: if both HIDE_UNDOC_MEMBERS and BRIEF_MEMBER_DESC are set to NO, the
89 # brief descriptions will be completely suppressed.
91 REPEAT_BRIEF = YES
93 # This tag implements a quasi-intelligent brief description abbreviator
94 # that is used to form the text in various listings. Each string
95 # in this list, if found as the leading text of the brief description, will be
96 # stripped from the text and the result after processing the whole list, is
97 # used as the annotated text. Otherwise, the brief description is used as-is.
98 # If left blank, the following values are used ("$name" is automatically
99 # replaced with the name of the entity): "The $name class" "The $name widget"
100 # "The $name file" "is" "provides" "specifies" "contains"
101 # "represents" "a" "an" "the"
103 ABBREVIATE_BRIEF =
105 # If the ALWAYS_DETAILED_SEC and REPEAT_BRIEF tags are both set to YES then
106 # Doxygen will generate a detailed section even if there is only a brief
107 # description.
109 ALWAYS_DETAILED_SEC = NO
111 # If the INLINE_INHERITED_MEMB tag is set to YES, doxygen will show all
112 # inherited members of a class in the documentation of that class as if those
113 # members were ordinary class members. Constructors, destructors and assignment
114 # operators of the base classes will not be shown.
116 INLINE_INHERITED_MEMB = NO
118 # If the FULL_PATH_NAMES tag is set to YES then Doxygen will prepend the full
119 # path before files name in the file list and in the header files. If set
120 # to NO the shortest path that makes the file name unique will be used.
122 FULL_PATH_NAMES = YES
124 # If the FULL_PATH_NAMES tag is set to YES then the STRIP_FROM_PATH tag
125 # can be used to strip a user-defined part of the path. Stripping is
126 # only done if one of the specified strings matches the left-hand part of
127 # the path. The tag can be used to show relative paths in the file list.
128 # If left blank the directory from which doxygen is run is used as the
129 # path to strip.
131 STRIP_FROM_PATH =
133 # The STRIP_FROM_INC_PATH tag can be used to strip a user-defined part of
134 # the path mentioned in the documentation of a class, which tells
135 # the reader which header file to include in order to use a class.
136 # If left blank only the name of the header file containing the class
137 # definition is used. Otherwise one should specify the include paths that
138 # are normally passed to the compiler using the -I flag.
140 STRIP_FROM_INC_PATH =
142 # If the SHORT_NAMES tag is set to YES, doxygen will generate much shorter
143 # (but less readable) file names. This can be useful if your file system
144 # doesn't support long names like on DOS, Mac, or CD-ROM.
146 SHORT_NAMES = NO
148 # If the JAVADOC_AUTOBRIEF tag is set to YES then Doxygen
149 # will interpret the first line (until the first dot) of a JavaDoc-style
150 # comment as the brief description. If set to NO, the JavaDoc
151 # comments will behave just like regular Qt-style comments
152 # (thus requiring an explicit @brief command for a brief description.)
154 JAVADOC_AUTOBRIEF = NO
156 # If the QT_AUTOBRIEF tag is set to YES then Doxygen will
157 # interpret the first line (until the first dot) of a Qt-style
158 # comment as the brief description. If set to NO, the comments
159 # will behave just like regular Qt-style comments (thus requiring
160 # an explicit \brief command for a brief description.)
162 QT_AUTOBRIEF = NO
164 # The MULTILINE_CPP_IS_BRIEF tag can be set to YES to make Doxygen
165 # treat a multi-line C++ special comment block (i.e. a block of //! or ///
166 # comments) as a brief description. This used to be the default behaviour.
167 # The new default is to treat a multi-line C++ comment block as a detailed
168 # description. Set this tag to YES if you prefer the old behaviour instead.
170 MULTILINE_CPP_IS_BRIEF = NO
172 # If the INHERIT_DOCS tag is set to YES (the default) then an undocumented
173 # member inherits the documentation from any documented member that it
174 # re-implements.
176 INHERIT_DOCS = YES
178 # If the SEPARATE_MEMBER_PAGES tag is set to YES, then doxygen will produce
179 # a new page for each member. If set to NO, the documentation of a member will
180 # be part of the file/class/namespace that contains it.
182 SEPARATE_MEMBER_PAGES = NO
184 # The TAB_SIZE tag can be used to set the number of spaces in a tab.
185 # Doxygen uses this value to replace tabs by spaces in code fragments.
187 TAB_SIZE = 8
189 # This tag can be used to specify a number of aliases that acts
190 # as commands in the documentation. An alias has the form "name=value".
191 # For example adding "sideeffect=\par Side Effects:\n" will allow you to
192 # put the command \sideeffect (or @sideeffect) in the documentation, which
193 # will result in a user-defined paragraph with heading "Side Effects:".
194 # You can put \n's in the value part of an alias to insert newlines.
196 ALIASES =
198 # This tag can be used to specify a number of word-keyword mappings (TCL only).
199 # A mapping has the form "name=value". For example adding
200 # "class=itcl::class" will allow you to use the command class in the
201 # itcl::class meaning.
203 TCL_SUBST =
205 # Set the OPTIMIZE_OUTPUT_FOR_C tag to YES if your project consists of C
206 # sources only. Doxygen will then generate output that is more tailored for C.
207 # For instance, some of the names that are used will be different. The list
208 # of all members will be omitted, etc.
210 OPTIMIZE_OUTPUT_FOR_C = YES
212 # Set the OPTIMIZE_OUTPUT_JAVA tag to YES if your project consists of Java
213 # sources only. Doxygen will then generate output that is more tailored for
214 # Java. For instance, namespaces will be presented as packages, qualified
215 # scopes will look different, etc.
217 OPTIMIZE_OUTPUT_JAVA = NO
219 # Set the OPTIMIZE_FOR_FORTRAN tag to YES if your project consists of Fortran
220 # sources only. Doxygen will then generate output that is more tailored for
221 # Fortran.
223 OPTIMIZE_FOR_FORTRAN = NO
225 # Set the OPTIMIZE_OUTPUT_VHDL tag to YES if your project consists of VHDL
226 # sources. Doxygen will then generate output that is tailored for
227 # VHDL.
229 OPTIMIZE_OUTPUT_VHDL = NO
231 # Doxygen selects the parser to use depending on the extension of the files it
232 # parses. With this tag you can assign which parser to use for a given extension.
233 # Doxygen has a built-in mapping, but you can override or extend it using this
234 # tag. The format is ext=language, where ext is a file extension, and language
235 # is one of the parsers supported by doxygen: IDL, Java, Javascript, CSharp, C,
236 # C++, D, PHP, Objective-C, Python, Fortran, VHDL, C, C++. For instance to make
237 # doxygen treat .inc files as Fortran files (default is PHP), and .f files as C
238 # (default is Fortran), use: inc=Fortran f=C. Note that for custom extensions
239 # you also need to set FILE_PATTERNS otherwise the files are not read by doxygen.
241 EXTENSION_MAPPING =
243 # If you use STL classes (i.e. std::string, std::vector, etc.) but do not want
244 # to include (a tag file for) the STL sources as input, then you should
245 # set this tag to YES in order to let doxygen match functions declarations and
246 # definitions whose arguments contain STL classes (e.g. func(std::string); v.s.
247 # func(std::string) {}). This also makes the inheritance and collaboration
248 # diagrams that involve STL classes more complete and accurate.
250 BUILTIN_STL_SUPPORT = NO
252 # If you use Microsoft's C++/CLI language, you should set this option to YES to
253 # enable parsing support.
255 CPP_CLI_SUPPORT = NO
257 # Set the SIP_SUPPORT tag to YES if your project consists of sip sources only.
258 # Doxygen will parse them like normal C++ but will assume all classes use public
259 # instead of private inheritance when no explicit protection keyword is present.
261 SIP_SUPPORT = NO
263 # For Microsoft's IDL there are propget and propput attributes to indicate getter
264 # and setter methods for a property. Setting this option to YES (the default)
265 # will make doxygen replace the get and set methods by a property in the
266 # documentation. This will only work if the methods are indeed getting or
267 # setting a simple type. If this is not the case, or you want to show the
268 # methods anyway, you should set this option to NO.
270 IDL_PROPERTY_SUPPORT = YES
272 # If member grouping is used in the documentation and the DISTRIBUTE_GROUP_DOC
273 # tag is set to YES, then doxygen will reuse the documentation of the first
274 # member in the group (if any) for the other members of the group. By default
275 # all members of a group must be documented explicitly.
277 DISTRIBUTE_GROUP_DOC = NO
279 # Set the SUBGROUPING tag to YES (the default) to allow class member groups of
280 # the same type (for instance a group of public functions) to be put as a
281 # subgroup of that type (e.g. under the Public Functions section). Set it to
282 # NO to prevent subgrouping. Alternatively, this can be done per class using
283 # the \nosubgrouping command.
285 SUBGROUPING = YES
287 # When the INLINE_GROUPED_CLASSES tag is set to YES, classes, structs and
288 # unions are shown inside the group in which they are included (e.g. using
289 # @ingroup) instead of on a separate page (for HTML and Man pages) or
290 # section (for LaTeX and RTF).
292 INLINE_GROUPED_CLASSES = NO
294 # When the INLINE_SIMPLE_STRUCTS tag is set to YES, structs, classes, and
295 # unions with only public data fields will be shown inline in the documentation
296 # of the scope in which they are defined (i.e. file, namespace, or group
297 # documentation), provided this scope is documented. If set to NO (the default),
298 # structs, classes, and unions are shown on a separate page (for HTML and Man
299 # pages) or section (for LaTeX and RTF).
301 INLINE_SIMPLE_STRUCTS = NO
303 # When TYPEDEF_HIDES_STRUCT is enabled, a typedef of a struct, union, or enum
304 # is documented as struct, union, or enum with the name of the typedef. So
305 # typedef struct TypeS {} TypeT, will appear in the documentation as a struct
306 # with name TypeT. When disabled the typedef will appear as a member of a file,
307 # namespace, or class. And the struct will be named TypeS. This can typically
308 # be useful for C code in case the coding convention dictates that all compound
309 # types are typedef'ed and only the typedef is referenced, never the tag name.
311 TYPEDEF_HIDES_STRUCT = NO
313 # The SYMBOL_CACHE_SIZE determines the size of the internal cache use to
314 # determine which symbols to keep in memory and which to flush to disk.
315 # When the cache is full, less often used symbols will be written to disk.
316 # For small to medium size projects (<1000 input files) the default value is
317 # probably good enough. For larger projects a too small cache size can cause
318 # doxygen to be busy swapping symbols to and from disk most of the time
319 # causing a significant performance penalty.
320 # If the system has enough physical memory increasing the cache will improve the
321 # performance by keeping more symbols in memory. Note that the value works on
322 # a logarithmic scale so increasing the size by one will roughly double the
323 # memory usage. The cache size is given by this formula:
324 # 2^(16+SYMBOL_CACHE_SIZE). The valid range is 0..9, the default is 0,
325 # corresponding to a cache size of 2^16 = 65536 symbols.
327 SYMBOL_CACHE_SIZE = 0
329 # Similar to the SYMBOL_CACHE_SIZE the size of the symbol lookup cache can be
330 # set using LOOKUP_CACHE_SIZE. This cache is used to resolve symbols given
331 # their name and scope. Since this can be an expensive process and often the
332 # same symbol appear multiple times in the code, doxygen keeps a cache of
333 # pre-resolved symbols. If the cache is too small doxygen will become slower.
334 # If the cache is too large, memory is wasted. The cache size is given by this
335 # formula: 2^(16+LOOKUP_CACHE_SIZE). The valid range is 0..9, the default is 0,
336 # corresponding to a cache size of 2^16 = 65536 symbols.
338 LOOKUP_CACHE_SIZE = 0
340 #---------------------------------------------------------------------------
341 # Build related configuration options
342 #---------------------------------------------------------------------------
344 # If the EXTRACT_ALL tag is set to YES doxygen will assume all entities in
345 # documentation are documented, even if no documentation was available.
346 # Private class members and static file members will be hidden unless
347 # the EXTRACT_PRIVATE and EXTRACT_STATIC tags are set to YES
349 EXTRACT_ALL = YES
351 # If the EXTRACT_PRIVATE tag is set to YES all private members of a class
352 # will be included in the documentation.
354 EXTRACT_PRIVATE = NO
356 # If the EXTRACT_STATIC tag is set to YES all static members of a file
357 # will be included in the documentation.
359 EXTRACT_STATIC = YES
361 # If the EXTRACT_LOCAL_CLASSES tag is set to YES classes (and structs)
362 # defined locally in source files will be included in the documentation.
363 # If set to NO only classes defined in header files are included.
365 EXTRACT_LOCAL_CLASSES = YES
367 # This flag is only useful for Objective-C code. When set to YES local
368 # methods, which are defined in the implementation section but not in
369 # the interface are included in the documentation.
370 # If set to NO (the default) only methods in the interface are included.
372 EXTRACT_LOCAL_METHODS = NO
374 # If this flag is set to YES, the members of anonymous namespaces will be
375 # extracted and appear in the documentation as a namespace called
376 # 'anonymous_namespace{file}', where file will be replaced with the base
377 # name of the file that contains the anonymous namespace. By default
378 # anonymous namespaces are hidden.
380 EXTRACT_ANON_NSPACES = NO
382 # If the HIDE_UNDOC_MEMBERS tag is set to YES, Doxygen will hide all
383 # undocumented members of documented classes, files or namespaces.
384 # If set to NO (the default) these members will be included in the
385 # various overviews, but no documentation section is generated.
386 # This option has no effect if EXTRACT_ALL is enabled.
388 HIDE_UNDOC_MEMBERS = NO
390 # If the HIDE_UNDOC_CLASSES tag is set to YES, Doxygen will hide all
391 # undocumented classes that are normally visible in the class hierarchy.
392 # If set to NO (the default) these classes will be included in the various
393 # overviews. This option has no effect if EXTRACT_ALL is enabled.
395 HIDE_UNDOC_CLASSES = NO
397 # If the HIDE_FRIEND_COMPOUNDS tag is set to YES, Doxygen will hide all
398 # friend (class|struct|union) declarations.
399 # If set to NO (the default) these declarations will be included in the
400 # documentation.
402 HIDE_FRIEND_COMPOUNDS = NO
404 # If the HIDE_IN_BODY_DOCS tag is set to YES, Doxygen will hide any
405 # documentation blocks found inside the body of a function.
406 # If set to NO (the default) these blocks will be appended to the
407 # function's detailed documentation block.
409 HIDE_IN_BODY_DOCS = NO
411 # The INTERNAL_DOCS tag determines if documentation
412 # that is typed after a \internal command is included. If the tag is set
413 # to NO (the default) then the documentation will be excluded.
414 # Set it to YES to include the internal documentation.
416 INTERNAL_DOCS = NO
418 # If the CASE_SENSE_NAMES tag is set to NO then Doxygen will only generate
419 # file names in lower-case letters. If set to YES upper-case letters are also
420 # allowed. This is useful if you have classes or files whose names only differ
421 # in case and if your file system supports case sensitive file names. Windows
422 # and Mac users are advised to set this option to NO.
424 CASE_SENSE_NAMES = YES
426 # If the HIDE_SCOPE_NAMES tag is set to NO (the default) then Doxygen
427 # will show members with their full class and namespace scopes in the
428 # documentation. If set to YES the scope will be hidden.
430 HIDE_SCOPE_NAMES = NO
432 # If the SHOW_INCLUDE_FILES tag is set to YES (the default) then Doxygen
433 # will put a list of the files that are included by a file in the documentation
434 # of that file.
436 SHOW_INCLUDE_FILES = YES
438 # If the FORCE_LOCAL_INCLUDES tag is set to YES then Doxygen
439 # will list include files with double quotes in the documentation
440 # rather than with sharp brackets.
442 FORCE_LOCAL_INCLUDES = NO
444 # If the INLINE_INFO tag is set to YES (the default) then a tag [inline]
445 # is inserted in the documentation for inline members.
447 INLINE_INFO = YES
449 # If the SORT_MEMBER_DOCS tag is set to YES (the default) then doxygen
450 # will sort the (detailed) documentation of file and class members
451 # alphabetically by member name. If set to NO the members will appear in
452 # declaration order.
454 SORT_MEMBER_DOCS = YES
456 # If the SORT_BRIEF_DOCS tag is set to YES then doxygen will sort the
457 # brief documentation of file, namespace and class members alphabetically
458 # by member name. If set to NO (the default) the members will appear in
459 # declaration order.
461 SORT_BRIEF_DOCS = NO
463 # If the SORT_MEMBERS_CTORS_1ST tag is set to YES then doxygen
464 # will sort the (brief and detailed) documentation of class members so that
465 # constructors and destructors are listed first. If set to NO (the default)
466 # the constructors will appear in the respective orders defined by
467 # SORT_MEMBER_DOCS and SORT_BRIEF_DOCS.
468 # This tag will be ignored for brief docs if SORT_BRIEF_DOCS is set to NO
469 # and ignored for detailed docs if SORT_MEMBER_DOCS is set to NO.
471 SORT_MEMBERS_CTORS_1ST = NO
473 # If the SORT_GROUP_NAMES tag is set to YES then doxygen will sort the
474 # hierarchy of group names into alphabetical order. If set to NO (the default)
475 # the group names will appear in their defined order.
477 SORT_GROUP_NAMES = NO
479 # If the SORT_BY_SCOPE_NAME tag is set to YES, the class list will be
480 # sorted by fully-qualified names, including namespaces. If set to
481 # NO (the default), the class list will be sorted only by class name,
482 # not including the namespace part.
483 # Note: This option is not very useful if HIDE_SCOPE_NAMES is set to YES.
484 # Note: This option applies only to the class list, not to the
485 # alphabetical list.
487 SORT_BY_SCOPE_NAME = NO
489 # If the STRICT_PROTO_MATCHING option is enabled and doxygen fails to
490 # do proper type resolution of all parameters of a function it will reject a
491 # match between the prototype and the implementation of a member function even
492 # if there is only one candidate or it is obvious which candidate to choose
493 # by doing a simple string match. By disabling STRICT_PROTO_MATCHING doxygen
494 # will still accept a match between prototype and implementation in such cases.
496 STRICT_PROTO_MATCHING = NO
498 # The GENERATE_TODOLIST tag can be used to enable (YES) or
499 # disable (NO) the todo list. This list is created by putting \todo
500 # commands in the documentation.
502 GENERATE_TODOLIST = YES
504 # The GENERATE_TESTLIST tag can be used to enable (YES) or
505 # disable (NO) the test list. This list is created by putting \test
506 # commands in the documentation.
508 GENERATE_TESTLIST = YES
510 # The GENERATE_BUGLIST tag can be used to enable (YES) or
511 # disable (NO) the bug list. This list is created by putting \bug
512 # commands in the documentation.
514 GENERATE_BUGLIST = YES
516 # The GENERATE_DEPRECATEDLIST tag can be used to enable (YES) or
517 # disable (NO) the deprecated list. This list is created by putting
518 # \deprecated commands in the documentation.
520 GENERATE_DEPRECATEDLIST= YES
522 # The ENABLED_SECTIONS tag can be used to enable conditional
523 # documentation sections, marked by \if sectionname ... \endif.
525 ENABLED_SECTIONS =
527 # The MAX_INITIALIZER_LINES tag determines the maximum number of lines
528 # the initial value of a variable or macro consists of for it to appear in
529 # the documentation. If the initializer consists of more lines than specified
530 # here it will be hidden. Use a value of 0 to hide initializers completely.
531 # The appearance of the initializer of individual variables and macros in the
532 # documentation can be controlled using \showinitializer or \hideinitializer
533 # command in the documentation regardless of this setting.
535 MAX_INITIALIZER_LINES = 30
537 # Set the SHOW_USED_FILES tag to NO to disable the list of files generated
538 # at the bottom of the documentation of classes and structs. If set to YES the
539 # list will mention the files that were used to generate the documentation.
541 SHOW_USED_FILES = YES
543 # If the sources in your project are distributed over multiple directories
544 # then setting the SHOW_DIRECTORIES tag to YES will show the directory hierarchy
545 # in the documentation. The default is NO.
547 SHOW_DIRECTORIES = NO
549 # Set the SHOW_FILES tag to NO to disable the generation of the Files page.
550 # This will remove the Files entry from the Quick Index and from the
551 # Folder Tree View (if specified). The default is YES.
553 SHOW_FILES = YES
555 # Set the SHOW_NAMESPACES tag to NO to disable the generation of the
556 # Namespaces page.
557 # This will remove the Namespaces entry from the Quick Index
558 # and from the Folder Tree View (if specified). The default is YES.
560 SHOW_NAMESPACES = YES
562 # The FILE_VERSION_FILTER tag can be used to specify a program or script that
563 # doxygen should invoke to get the current version for each file (typically from
564 # the version control system). Doxygen will invoke the program by executing (via
565 # popen()) the command <command> <input-file>, where <command> is the value of
566 # the FILE_VERSION_FILTER tag, and <input-file> is the name of an input file
567 # provided by doxygen. Whatever the program writes to standard output
568 # is used as the file version. See the manual for examples.
570 FILE_VERSION_FILTER =
572 # The LAYOUT_FILE tag can be used to specify a layout file which will be parsed
573 # by doxygen. The layout file controls the global structure of the generated
574 # output files in an output format independent way. The create the layout file
575 # that represents doxygen's defaults, run doxygen with the -l option.
576 # You can optionally specify a file name after the option, if omitted
577 # DoxygenLayout.xml will be used as the name of the layout file.
579 LAYOUT_FILE =
581 # The CITE_BIB_FILES tag can be used to specify one or more bib files
582 # containing the references data. This must be a list of .bib files. The
583 # .bib extension is automatically appended if omitted. Using this command
584 # requires the bibtex tool to be installed. See also
585 # http://en.wikipedia.org/wiki/BibTeX for more info. For LaTeX the style
586 # of the bibliography can be controlled using LATEX_BIB_STYLE. To use this
587 # feature you need bibtex and perl available in the search path.
589 CITE_BIB_FILES =
591 #---------------------------------------------------------------------------
592 # configuration options related to warning and progress messages
593 #---------------------------------------------------------------------------
595 # The QUIET tag can be used to turn on/off the messages that are generated
596 # by doxygen. Possible values are YES and NO. If left blank NO is used.
598 QUIET = NO
600 # The WARNINGS tag can be used to turn on/off the warning messages that are
601 # generated by doxygen. Possible values are YES and NO. If left blank
602 # NO is used.
604 WARNINGS = YES
606 # If WARN_IF_UNDOCUMENTED is set to YES, then doxygen will generate warnings
607 # for undocumented members. If EXTRACT_ALL is set to YES then this flag will
608 # automatically be disabled.
610 WARN_IF_UNDOCUMENTED = YES
612 # If WARN_IF_DOC_ERROR is set to YES, doxygen will generate warnings for
613 # potential errors in the documentation, such as not documenting some
614 # parameters in a documented function, or documenting parameters that
615 # don't exist or using markup commands wrongly.
617 WARN_IF_DOC_ERROR = YES
619 # The WARN_NO_PARAMDOC option can be enabled to get warnings for
620 # functions that are documented, but have no documentation for their parameters
621 # or return value. If set to NO (the default) doxygen will only warn about
622 # wrong or incomplete parameter documentation, but not about the absence of
623 # documentation.
625 WARN_NO_PARAMDOC = NO
627 # The WARN_FORMAT tag determines the format of the warning messages that
628 # doxygen can produce. The string should contain the $file, $line, and $text
629 # tags, which will be replaced by the file and line number from which the
630 # warning originated and the warning text. Optionally the format may contain
631 # $version, which will be replaced by the version of the file (if it could
632 # be obtained via FILE_VERSION_FILTER)
634 WARN_FORMAT = "$file:$line: $text"
636 # The WARN_LOGFILE tag can be used to specify a file to which warning
637 # and error messages should be written. If left blank the output is written
638 # to stderr.
640 WARN_LOGFILE =
642 #---------------------------------------------------------------------------
643 # configuration options related to the input files
644 #---------------------------------------------------------------------------
646 # The INPUT tag can be used to specify the files and/or directories that contain
647 # documented source files. You may enter file names like "myfile.cpp" or
648 # directories like "/usr/src/myproject". Separate the files or directories
649 # with spaces.
651 INPUT = ./ticblas ./docs/doxygen
653 # This tag can be used to specify the character encoding of the source files
654 # that doxygen parses. Internally doxygen uses the UTF-8 encoding, which is
655 # also the default input encoding. Doxygen uses libiconv (or the iconv built
656 # into libc) for the transcoding. See http://www.gnu.org/software/libiconv for
657 # the list of possible encodings.
659 INPUT_ENCODING = UTF-8
661 # If the value of the INPUT tag contains directories, you can use the
662 # FILE_PATTERNS tag to specify one or more wildcard pattern (like *.cpp
663 # and *.h) to filter out the source-files in the directories. If left
664 # blank the following patterns are tested:
665 # *.c *.cc *.cxx *.cpp *.c++ *.d *.java *.ii *.ixx *.ipp *.i++ *.inl *.h *.hh
666 # *.hxx *.hpp *.h++ *.idl *.odl *.cs *.php *.php3 *.inc *.m *.mm *.dox *.py
667 # *.f90 *.f *.for *.vhd *.vhdl
669 FILE_PATTERNS = *.c *.h *.dox
671 # The RECURSIVE tag can be used to turn specify whether or not subdirectories
672 # should be searched for input files as well. Possible values are YES and NO.
673 # If left blank NO is used.
675 RECURSIVE = NO
677 # The EXCLUDE tag can be used to specify files and/or directories that should be
678 # excluded from the INPUT source files. This way you can easily exclude a
679 # subdirectory from a directory tree whose root is specified with the INPUT tag.
680 # Note that relative paths are relative to the directory from which doxygen is
681 # run.
683 EXCLUDE =
685 # The EXCLUDE_SYMLINKS tag can be used to select whether or not files or
686 # directories that are symbolic links (a Unix file system feature) are excluded
687 # from the input.
689 EXCLUDE_SYMLINKS = NO
691 # If the value of the INPUT tag contains directories, you can use the
692 # EXCLUDE_PATTERNS tag to specify one or more wildcard patterns to exclude
693 # certain files from those directories. Note that the wildcards are matched
694 # against the file with absolute path, so to exclude all test directories
695 # for example use the pattern */test/*
697 EXCLUDE_PATTERNS =
699 # The EXCLUDE_SYMBOLS tag can be used to specify one or more symbol names
700 # (namespaces, classes, functions, etc.) that should be excluded from the
701 # output. The symbol name can be a fully qualified name, a word, or if the
702 # wildcard * is used, a substring. Examples: ANamespace, AClass,
703 # AClass::ANamespace, ANamespace::*Test
705 EXCLUDE_SYMBOLS =
707 # The EXAMPLE_PATH tag can be used to specify one or more files or
708 # directories that contain example code fragments that are included (see
709 # the \include command).
711 EXAMPLE_PATH =
713 # If the value of the EXAMPLE_PATH tag contains directories, you can use the
714 # EXAMPLE_PATTERNS tag to specify one or more wildcard pattern (like *.cpp
715 # and *.h) to filter out the source-files in the directories. If left
716 # blank all files are included.
718 EXAMPLE_PATTERNS =
720 # If the EXAMPLE_RECURSIVE tag is set to YES then subdirectories will be
721 # searched for input files to be used with the \include or \dontinclude
722 # commands irrespective of the value of the RECURSIVE tag.
723 # Possible values are YES and NO. If left blank NO is used.
725 EXAMPLE_RECURSIVE = NO
727 # The IMAGE_PATH tag can be used to specify one or more files or
728 # directories that contain image that are included in the documentation (see
729 # the \image command).
731 IMAGE_PATH = ./docs/doxygen/images
733 # The INPUT_FILTER tag can be used to specify a program that doxygen should
734 # invoke to filter for each input file. Doxygen will invoke the filter program
735 # by executing (via popen()) the command <filter> <input-file>, where <filter>
736 # is the value of the INPUT_FILTER tag, and <input-file> is the name of an
737 # input file. Doxygen will then use the output that the filter program writes
738 # to standard output.
739 # If FILTER_PATTERNS is specified, this tag will be
740 # ignored.
742 INPUT_FILTER =
744 # The FILTER_PATTERNS tag can be used to specify filters on a per file pattern
745 # basis.
746 # Doxygen will compare the file name with each pattern and apply the
747 # filter if there is a match.
748 # The filters are a list of the form:
749 # pattern=filter (like *.cpp=my_cpp_filter). See INPUT_FILTER for further
750 # info on how filters are used. If FILTER_PATTERNS is empty or if
751 # non of the patterns match the file name, INPUT_FILTER is applied.
753 FILTER_PATTERNS =
755 # If the FILTER_SOURCE_FILES tag is set to YES, the input filter (if set using
756 # INPUT_FILTER) will be used to filter the input files when producing source
757 # files to browse (i.e. when SOURCE_BROWSER is set to YES).
759 FILTER_SOURCE_FILES = NO
761 # The FILTER_SOURCE_PATTERNS tag can be used to specify source filters per file
762 # pattern. A pattern will override the setting for FILTER_PATTERN (if any)
763 # and it is also possible to disable source filtering for a specific pattern
764 # using *.ext= (so without naming a filter). This option only has effect when
765 # FILTER_SOURCE_FILES is enabled.
767 FILTER_SOURCE_PATTERNS =
769 #---------------------------------------------------------------------------
770 # configuration options related to source browsing
771 #---------------------------------------------------------------------------
773 # If the SOURCE_BROWSER tag is set to YES then a list of source files will
774 # be generated. Documented entities will be cross-referenced with these sources.
775 # Note: To get rid of all source code in the generated output, make sure also
776 # VERBATIM_HEADERS is set to NO.
778 SOURCE_BROWSER = NO
780 # Setting the INLINE_SOURCES tag to YES will include the body
781 # of functions and classes directly in the documentation.
783 INLINE_SOURCES = NO
785 # Setting the STRIP_CODE_COMMENTS tag to YES (the default) will instruct
786 # doxygen to hide any special comment blocks from generated source code
787 # fragments. Normal C and C++ comments will always remain visible.
789 STRIP_CODE_COMMENTS = YES
791 # If the REFERENCED_BY_RELATION tag is set to YES
792 # then for each documented function all documented
793 # functions referencing it will be listed.
795 REFERENCED_BY_RELATION = NO
797 # If the REFERENCES_RELATION tag is set to YES
798 # then for each documented function all documented entities
799 # called/used by that function will be listed.
801 REFERENCES_RELATION = NO
803 # If the REFERENCES_LINK_SOURCE tag is set to YES (the default)
804 # and SOURCE_BROWSER tag is set to YES, then the hyperlinks from
805 # functions in REFERENCES_RELATION and REFERENCED_BY_RELATION lists will
806 # link to the source code.
807 # Otherwise they will link to the documentation.
809 REFERENCES_LINK_SOURCE = YES
811 # If the USE_HTAGS tag is set to YES then the references to source code
812 # will point to the HTML generated by the htags(1) tool instead of doxygen
813 # built-in source browser. The htags tool is part of GNU's global source
814 # tagging system (see http://www.gnu.org/software/global/global.html). You
815 # will need version 4.8.6 or higher.
817 USE_HTAGS = NO
819 # If the VERBATIM_HEADERS tag is set to YES (the default) then Doxygen
820 # will generate a verbatim copy of the header file for each class for
821 # which an include is specified. Set to NO to disable this.
823 VERBATIM_HEADERS = YES
825 #---------------------------------------------------------------------------
826 # configuration options related to the alphabetical class index
827 #---------------------------------------------------------------------------
829 # If the ALPHABETICAL_INDEX tag is set to YES, an alphabetical index
830 # of all compounds will be generated. Enable this if the project
831 # contains a lot of classes, structs, unions or interfaces.
833 ALPHABETICAL_INDEX = YES
835 # If the alphabetical index is enabled (see ALPHABETICAL_INDEX) then
836 # the COLS_IN_ALPHA_INDEX tag can be used to specify the number of columns
837 # in which this list will be split (can be a number in the range [1..20])
839 COLS_IN_ALPHA_INDEX = 5
841 # In case all classes in a project start with a common prefix, all
842 # classes will be put under the same header in the alphabetical index.
843 # The IGNORE_PREFIX tag can be used to specify one or more prefixes that
844 # should be ignored while generating the index headers.
846 IGNORE_PREFIX =
848 #---------------------------------------------------------------------------
849 # configuration options related to the HTML output
850 #---------------------------------------------------------------------------
852 # If the GENERATE_HTML tag is set to YES (the default) Doxygen will
853 # generate HTML output.
855 GENERATE_HTML = YES
857 # The HTML_OUTPUT tag is used to specify where the HTML docs will be put.
858 # If a relative path is entered the value of OUTPUT_DIRECTORY will be
859 # put in front of it. If left blank `html' will be used as the default path.
861 HTML_OUTPUT = html
863 # The HTML_FILE_EXTENSION tag can be used to specify the file extension for
864 # each generated HTML page (for example: .htm,.php,.asp). If it is left blank
865 # doxygen will generate files with .html extension.
867 HTML_FILE_EXTENSION = .html
869 # The HTML_HEADER tag can be used to specify a personal HTML header for
870 # each generated HTML page. If it is left blank doxygen will generate a
871 # standard header. Note that when using a custom header you are responsible
872 # for the proper inclusion of any scripts and style sheets that doxygen
873 # needs, which is dependent on the configuration options used.
874 # It is advised to generate a default header using "doxygen -w html
875 # header.html footer.html stylesheet.css YourConfigFile" and then modify
876 # that header. Note that the header is subject to change so you typically
877 # have to redo this when upgrading to a newer version of doxygen or when
878 # changing the value of configuration settings such as GENERATE_TREEVIEW!
880 HTML_HEADER =
882 # The HTML_FOOTER tag can be used to specify a personal HTML footer for
883 # each generated HTML page. If it is left blank doxygen will generate a
884 # standard footer.
886 HTML_FOOTER =
888 # The HTML_STYLESHEET tag can be used to specify a user-defined cascading
889 # style sheet that is used by each HTML page. It can be used to
890 # fine-tune the look of the HTML output. If the tag is left blank doxygen
891 # will generate a default style sheet. Note that doxygen will try to copy
892 # the style sheet file to the HTML output directory, so don't put your own
893 # style sheet in the HTML output directory as well, or it will be erased!
895 HTML_STYLESHEET =
897 # The HTML_EXTRA_FILES tag can be used to specify one or more extra images or
898 # other source files which should be copied to the HTML output directory. Note
899 # that these files will be copied to the base HTML output directory. Use the
900 # $relpath$ marker in the HTML_HEADER and/or HTML_FOOTER files to load these
901 # files. In the HTML_STYLESHEET file, use the file name only. Also note that
902 # the files will be copied as-is; there are no commands or markers available.
904 HTML_EXTRA_FILES =
906 # The HTML_COLORSTYLE_HUE tag controls the color of the HTML output.
907 # Doxygen will adjust the colors in the style sheet and background images
908 # according to this color. Hue is specified as an angle on a colorwheel,
909 # see http://en.wikipedia.org/wiki/Hue for more information.
910 # For instance the value 0 represents red, 60 is yellow, 120 is green,
911 # 180 is cyan, 240 is blue, 300 purple, and 360 is red again.
912 # The allowed range is 0 to 359.
914 HTML_COLORSTYLE_HUE = 220
916 # The HTML_COLORSTYLE_SAT tag controls the purity (or saturation) of
917 # the colors in the HTML output. For a value of 0 the output will use
918 # grayscales only. A value of 255 will produce the most vivid colors.
920 HTML_COLORSTYLE_SAT = 100
922 # The HTML_COLORSTYLE_GAMMA tag controls the gamma correction applied to
923 # the luminance component of the colors in the HTML output. Values below
924 # 100 gradually make the output lighter, whereas values above 100 make
925 # the output darker. The value divided by 100 is the actual gamma applied,
926 # so 80 represents a gamma of 0.8, The value 220 represents a gamma of 2.2,
927 # and 100 does not change the gamma.
929 HTML_COLORSTYLE_GAMMA = 80
931 # If the HTML_TIMESTAMP tag is set to YES then the footer of each generated HTML
932 # page will contain the date and time when the page was generated. Setting
933 # this to NO can help when comparing the output of multiple runs.
935 HTML_TIMESTAMP = YES
937 # If the HTML_ALIGN_MEMBERS tag is set to YES, the members of classes,
938 # files or namespaces will be aligned in HTML using tables. If set to
939 # NO a bullet list will be used.
941 HTML_ALIGN_MEMBERS = YES
943 # If the HTML_DYNAMIC_SECTIONS tag is set to YES then the generated HTML
944 # documentation will contain sections that can be hidden and shown after the
945 # page has loaded. For this to work a browser that supports
946 # JavaScript and DHTML is required (for instance Mozilla 1.0+, Firefox
947 # Netscape 6.0+, Internet explorer 5.0+, Konqueror, or Safari).
949 HTML_DYNAMIC_SECTIONS = NO
951 # If the GENERATE_DOCSET tag is set to YES, additional index files
952 # will be generated that can be used as input for Apple's Xcode 3
953 # integrated development environment, introduced with OSX 10.5 (Leopard).
954 # To create a documentation set, doxygen will generate a Makefile in the
955 # HTML output directory. Running make will produce the docset in that
956 # directory and running "make install" will install the docset in
957 # ~/Library/Developer/Shared/Documentation/DocSets so that Xcode will find
958 # it at startup.
959 # See http://developer.apple.com/tools/creatingdocsetswithdoxygen.html
960 # for more information.
962 GENERATE_DOCSET = NO
964 # When GENERATE_DOCSET tag is set to YES, this tag determines the name of the
965 # feed. A documentation feed provides an umbrella under which multiple
966 # documentation sets from a single provider (such as a company or product suite)
967 # can be grouped.
969 DOCSET_FEEDNAME = "Doxygen generated docs"
971 # When GENERATE_DOCSET tag is set to YES, this tag specifies a string that
972 # should uniquely identify the documentation set bundle. This should be a
973 # reverse domain-name style string, e.g. com.mycompany.MyDocSet. Doxygen
974 # will append .docset to the name.
976 DOCSET_BUNDLE_ID = org.doxygen.Project
978 # When GENERATE_PUBLISHER_ID tag specifies a string that should uniquely identify
979 # the documentation publisher. This should be a reverse domain-name style
980 # string, e.g. com.mycompany.MyDocSet.documentation.
982 DOCSET_PUBLISHER_ID = org.doxygen.Publisher
984 # The GENERATE_PUBLISHER_NAME tag identifies the documentation publisher.
986 DOCSET_PUBLISHER_NAME = Publisher
988 # If the GENERATE_HTMLHELP tag is set to YES, additional index files
989 # will be generated that can be used as input for tools like the
990 # Microsoft HTML help workshop to generate a compiled HTML help file (.chm)
991 # of the generated HTML documentation.
993 GENERATE_HTMLHELP = NO
995 # If the GENERATE_HTMLHELP tag is set to YES, the CHM_FILE tag can
996 # be used to specify the file name of the resulting .chm file. You
997 # can add a path in front of the file if the result should not be
998 # written to the html output directory.
1000 CHM_FILE =
1002 # If the GENERATE_HTMLHELP tag is set to YES, the HHC_LOCATION tag can
1003 # be used to specify the location (absolute path including file name) of
1004 # the HTML help compiler (hhc.exe). If non-empty doxygen will try to run
1005 # the HTML help compiler on the generated index.hhp.
1007 HHC_LOCATION =
1009 # If the GENERATE_HTMLHELP tag is set to YES, the GENERATE_CHI flag
1010 # controls if a separate .chi index file is generated (YES) or that
1011 # it should be included in the master .chm file (NO).
1013 GENERATE_CHI = NO
1015 # If the GENERATE_HTMLHELP tag is set to YES, the CHM_INDEX_ENCODING
1016 # is used to encode HtmlHelp index (hhk), content (hhc) and project file
1017 # content.
1019 CHM_INDEX_ENCODING =
1021 # If the GENERATE_HTMLHELP tag is set to YES, the BINARY_TOC flag
1022 # controls whether a binary table of contents is generated (YES) or a
1023 # normal table of contents (NO) in the .chm file.
1025 BINARY_TOC = NO
1027 # The TOC_EXPAND flag can be set to YES to add extra items for group members
1028 # to the contents of the HTML help documentation and to the tree view.
1030 TOC_EXPAND = NO
1032 # If the GENERATE_QHP tag is set to YES and both QHP_NAMESPACE and
1033 # QHP_VIRTUAL_FOLDER are set, an additional index file will be generated
1034 # that can be used as input for Qt's qhelpgenerator to generate a
1035 # Qt Compressed Help (.qch) of the generated HTML documentation.
1037 GENERATE_QHP = NO
1039 # If the QHG_LOCATION tag is specified, the QCH_FILE tag can
1040 # be used to specify the file name of the resulting .qch file.
1041 # The path specified is relative to the HTML output folder.
1043 QCH_FILE =
1045 # The QHP_NAMESPACE tag specifies the namespace to use when generating
1046 # Qt Help Project output. For more information please see
1047 # http://doc.trolltech.com/qthelpproject.html#namespace
1049 QHP_NAMESPACE = org.doxygen.Project
1051 # The QHP_VIRTUAL_FOLDER tag specifies the namespace to use when generating
1052 # Qt Help Project output. For more information please see
1053 # http://doc.trolltech.com/qthelpproject.html#virtual-folders
1055 QHP_VIRTUAL_FOLDER = doc
1057 # If QHP_CUST_FILTER_NAME is set, it specifies the name of a custom filter to
1058 # add. For more information please see
1059 # http://doc.trolltech.com/qthelpproject.html#custom-filters
1061 QHP_CUST_FILTER_NAME =
1063 # The QHP_CUST_FILT_ATTRS tag specifies the list of the attributes of the
1064 # custom filter to add. For more information please see
1065 # <a href="http://doc.trolltech.com/qthelpproject.html#custom-filters">
1066 # Qt Help Project / Custom Filters</a>.
1068 QHP_CUST_FILTER_ATTRS =
1070 # The QHP_SECT_FILTER_ATTRS tag specifies the list of the attributes this
1071 # project's
1072 # filter section matches.
1073 # <a href="http://doc.trolltech.com/qthelpproject.html#filter-attributes">
1074 # Qt Help Project / Filter Attributes</a>.
1076 QHP_SECT_FILTER_ATTRS =
1078 # If the GENERATE_QHP tag is set to YES, the QHG_LOCATION tag can
1079 # be used to specify the location of Qt's qhelpgenerator.
1080 # If non-empty doxygen will try to run qhelpgenerator on the generated
1081 # .qhp file.
1083 QHG_LOCATION =
1085 # If the GENERATE_ECLIPSEHELP tag is set to YES, additional index files
1086 # will be generated, which together with the HTML files, form an Eclipse help
1087 # plugin. To install this plugin and make it available under the help contents
1088 # menu in Eclipse, the contents of the directory containing the HTML and XML
1089 # files needs to be copied into the plugins directory of eclipse. The name of
1090 # the directory within the plugins directory should be the same as
1091 # the ECLIPSE_DOC_ID value. After copying Eclipse needs to be restarted before
1092 # the help appears.
1094 GENERATE_ECLIPSEHELP = NO
1096 # A unique identifier for the eclipse help plugin. When installing the plugin
1097 # the directory name containing the HTML and XML files should also have
1098 # this name.
1100 ECLIPSE_DOC_ID = org.doxygen.Project
1102 # The DISABLE_INDEX tag can be used to turn on/off the condensed index (tabs)
1103 # at top of each HTML page. The value NO (the default) enables the index and
1104 # the value YES disables it. Since the tabs have the same information as the
1105 # navigation tree you can set this option to NO if you already set
1106 # GENERATE_TREEVIEW to YES.
1108 DISABLE_INDEX = NO
1110 # The GENERATE_TREEVIEW tag is used to specify whether a tree-like index
1111 # structure should be generated to display hierarchical information.
1112 # If the tag value is set to YES, a side panel will be generated
1113 # containing a tree-like index structure (just like the one that
1114 # is generated for HTML Help). For this to work a browser that supports
1115 # JavaScript, DHTML, CSS and frames is required (i.e. any modern browser).
1116 # Windows users are probably better off using the HTML help feature.
1117 # Since the tree basically has the same information as the tab index you
1118 # could consider to set DISABLE_INDEX to NO when enabling this option.
1120 GENERATE_TREEVIEW = NO
1122 # The ENUM_VALUES_PER_LINE tag can be used to set the number of enum values
1123 # (range [0,1..20]) that doxygen will group on one line in the generated HTML
1124 # documentation. Note that a value of 0 will completely suppress the enum
1125 # values from appearing in the overview section.
1127 ENUM_VALUES_PER_LINE = 4
1129 # By enabling USE_INLINE_TREES, doxygen will generate the Groups, Directories,
1130 # and Class Hierarchy pages using a tree view instead of an ordered list.
1132 USE_INLINE_TREES = NO
1134 # If the treeview is enabled (see GENERATE_TREEVIEW) then this tag can be
1135 # used to set the initial width (in pixels) of the frame in which the tree
1136 # is shown.
1138 TREEVIEW_WIDTH = 250
1140 # When the EXT_LINKS_IN_WINDOW option is set to YES doxygen will open
1141 # links to external symbols imported via tag files in a separate window.
1143 EXT_LINKS_IN_WINDOW = NO
1145 # Use this tag to change the font size of Latex formulas included
1146 # as images in the HTML documentation. The default is 10. Note that
1147 # when you change the font size after a successful doxygen run you need
1148 # to manually remove any form_*.png images from the HTML output directory
1149 # to force them to be regenerated.
1151 FORMULA_FONTSIZE = 10
1153 # Use the FORMULA_TRANPARENT tag to determine whether or not the images
1154 # generated for formulas are transparent PNGs. Transparent PNGs are
1155 # not supported properly for IE 6.0, but are supported on all modern browsers.
1156 # Note that when changing this option you need to delete any form_*.png files
1157 # in the HTML output before the changes have effect.
1159 FORMULA_TRANSPARENT = YES
1161 # Enable the USE_MATHJAX option to render LaTeX formulas using MathJax
1162 # (see http://www.mathjax.org) which uses client side Javascript for the
1163 # rendering instead of using prerendered bitmaps. Use this if you do not
1164 # have LaTeX installed or if you want to formulas look prettier in the HTML
1165 # output. When enabled you also need to install MathJax separately and
1166 # configure the path to it using the MATHJAX_RELPATH option.
1168 USE_MATHJAX = NO
1170 # When MathJax is enabled you need to specify the location relative to the
1171 # HTML output directory using the MATHJAX_RELPATH option. The destination
1172 # directory should contain the MathJax.js script. For instance, if the mathjax
1173 # directory is located at the same level as the HTML output directory, then
1174 # MATHJAX_RELPATH should be ../mathjax. The default value points to the
1175 # mathjax.org site, so you can quickly see the result without installing
1176 # MathJax, but it is strongly recommended to install a local copy of MathJax
1177 # before deployment.
1179 MATHJAX_RELPATH = http://www.mathjax.org/mathjax
1181 # The MATHJAX_EXTENSIONS tag can be used to specify one or MathJax extension
1182 # names that should be enabled during MathJax rendering.
1184 MATHJAX_EXTENSIONS =
1186 # When the SEARCHENGINE tag is enabled doxygen will generate a search box
1187 # for the HTML output. The underlying search engine uses javascript
1188 # and DHTML and should work on any modern browser. Note that when using
1189 # HTML help (GENERATE_HTMLHELP), Qt help (GENERATE_QHP), or docsets
1190 # (GENERATE_DOCSET) there is already a search function so this one should
1191 # typically be disabled. For large projects the javascript based search engine
1192 # can be slow, then enabling SERVER_BASED_SEARCH may provide a better solution.
1194 SEARCHENGINE = YES
1196 # When the SERVER_BASED_SEARCH tag is enabled the search engine will be
1197 # implemented using a PHP enabled web server instead of at the web client
1198 # using Javascript. Doxygen will generate the search PHP script and index
1199 # file to put on the web server. The advantage of the server
1200 # based approach is that it scales better to large projects and allows
1201 # full text search. The disadvantages are that it is more difficult to setup
1202 # and does not have live searching capabilities.
1204 SERVER_BASED_SEARCH = NO
1206 #---------------------------------------------------------------------------
1207 # configuration options related to the LaTeX output
1208 #---------------------------------------------------------------------------
1210 # If the GENERATE_LATEX tag is set to YES (the default) Doxygen will
1211 # generate Latex output.
1213 GENERATE_LATEX = YES
1215 # The LATEX_OUTPUT tag is used to specify where the LaTeX docs will be put.
1216 # If a relative path is entered the value of OUTPUT_DIRECTORY will be
1217 # put in front of it. If left blank `latex' will be used as the default path.
1219 LATEX_OUTPUT = latex
1221 # The LATEX_CMD_NAME tag can be used to specify the LaTeX command name to be
1222 # invoked. If left blank `latex' will be used as the default command name.
1223 # Note that when enabling USE_PDFLATEX this option is only used for
1224 # generating bitmaps for formulas in the HTML output, but not in the
1225 # Makefile that is written to the output directory.
1227 LATEX_CMD_NAME = latex
1229 # The MAKEINDEX_CMD_NAME tag can be used to specify the command name to
1230 # generate index for LaTeX. If left blank `makeindex' will be used as the
1231 # default command name.
1233 MAKEINDEX_CMD_NAME = makeindex
1235 # If the COMPACT_LATEX tag is set to YES Doxygen generates more compact
1236 # LaTeX documents. This may be useful for small projects and may help to
1237 # save some trees in general.
1239 COMPACT_LATEX = NO
1241 # The PAPER_TYPE tag can be used to set the paper type that is used
1242 # by the printer. Possible values are: a4, letter, legal and
1243 # executive. If left blank a4wide will be used.
1245 PAPER_TYPE = a4
1247 # The EXTRA_PACKAGES tag can be to specify one or more names of LaTeX
1248 # packages that should be included in the LaTeX output.
1250 EXTRA_PACKAGES =
1252 # The LATEX_HEADER tag can be used to specify a personal LaTeX header for
1253 # the generated latex document. The header should contain everything until
1254 # the first chapter. If it is left blank doxygen will generate a
1255 # standard header. Notice: only use this tag if you know what you are doing!
1257 LATEX_HEADER =
1259 # The LATEX_FOOTER tag can be used to specify a personal LaTeX footer for
1260 # the generated latex document. The footer should contain everything after
1261 # the last chapter. If it is left blank doxygen will generate a
1262 # standard footer. Notice: only use this tag if you know what you are doing!
1264 LATEX_FOOTER =
1266 # If the PDF_HYPERLINKS tag is set to YES, the LaTeX that is generated
1267 # is prepared for conversion to pdf (using ps2pdf). The pdf file will
1268 # contain links (just like the HTML output) instead of page references
1269 # This makes the output suitable for online browsing using a pdf viewer.
1271 PDF_HYPERLINKS = YES
1273 # If the USE_PDFLATEX tag is set to YES, pdflatex will be used instead of
1274 # plain latex in the generated Makefile. Set this option to YES to get a
1275 # higher quality PDF documentation.
1277 USE_PDFLATEX = YES
1279 # If the LATEX_BATCHMODE tag is set to YES, doxygen will add the \\batchmode.
1280 # command to the generated LaTeX files. This will instruct LaTeX to keep
1281 # running if errors occur, instead of asking the user for help.
1282 # This option is also used when generating formulas in HTML.
1284 LATEX_BATCHMODE = NO
1286 # If LATEX_HIDE_INDICES is set to YES then doxygen will not
1287 # include the index chapters (such as File Index, Compound Index, etc.)
1288 # in the output.
1290 LATEX_HIDE_INDICES = NO
1292 # If LATEX_SOURCE_CODE is set to YES then doxygen will include
1293 # source code with syntax highlighting in the LaTeX output.
1294 # Note that which sources are shown also depends on other settings
1295 # such as SOURCE_BROWSER.
1297 LATEX_SOURCE_CODE = NO
1299 # The LATEX_BIB_STYLE tag can be used to specify the style to use for the
1300 # bibliography, e.g. plainnat, or ieeetr. The default style is "plain". See
1301 # http://en.wikipedia.org/wiki/BibTeX for more info.
1303 LATEX_BIB_STYLE = plain
1305 #---------------------------------------------------------------------------
1306 # configuration options related to the RTF output
1307 #---------------------------------------------------------------------------
1309 # If the GENERATE_RTF tag is set to YES Doxygen will generate RTF output
1310 # The RTF output is optimized for Word 97 and may not look very pretty with
1311 # other RTF readers or editors.
1313 GENERATE_RTF = NO
1315 # The RTF_OUTPUT tag is used to specify where the RTF docs will be put.
1316 # If a relative path is entered the value of OUTPUT_DIRECTORY will be
1317 # put in front of it. If left blank `rtf' will be used as the default path.
1319 RTF_OUTPUT = rtf
1321 # If the COMPACT_RTF tag is set to YES Doxygen generates more compact
1322 # RTF documents. This may be useful for small projects and may help to
1323 # save some trees in general.
1325 COMPACT_RTF = NO
1327 # If the RTF_HYPERLINKS tag is set to YES, the RTF that is generated
1328 # will contain hyperlink fields. The RTF file will
1329 # contain links (just like the HTML output) instead of page references.
1330 # This makes the output suitable for online browsing using WORD or other
1331 # programs which support those fields.
1332 # Note: wordpad (write) and others do not support links.
1334 RTF_HYPERLINKS = NO
1336 # Load style sheet definitions from file. Syntax is similar to doxygen's
1337 # config file, i.e. a series of assignments. You only have to provide
1338 # replacements, missing definitions are set to their default value.
1340 RTF_STYLESHEET_FILE =
1342 # Set optional variables used in the generation of an rtf document.
1343 # Syntax is similar to doxygen's config file.
1345 RTF_EXTENSIONS_FILE =
1347 #---------------------------------------------------------------------------
1348 # configuration options related to the man page output
1349 #---------------------------------------------------------------------------
1351 # If the GENERATE_MAN tag is set to YES (the default) Doxygen will
1352 # generate man pages
1354 GENERATE_MAN = NO
1356 # The MAN_OUTPUT tag is used to specify where the man pages will be put.
1357 # If a relative path is entered the value of OUTPUT_DIRECTORY will be
1358 # put in front of it. If left blank `man' will be used as the default path.
1360 MAN_OUTPUT = man
1362 # The MAN_EXTENSION tag determines the extension that is added to
1363 # the generated man pages (default is the subroutine's section .3)
1365 MAN_EXTENSION = .3
1367 # If the MAN_LINKS tag is set to YES and Doxygen generates man output,
1368 # then it will generate one additional man file for each entity
1369 # documented in the real man page(s). These additional files
1370 # only source the real man page, but without them the man command
1371 # would be unable to find the correct page. The default is NO.
1373 MAN_LINKS = NO
1375 #---------------------------------------------------------------------------
1376 # configuration options related to the XML output
1377 #---------------------------------------------------------------------------
1379 # If the GENERATE_XML tag is set to YES Doxygen will
1380 # generate an XML file that captures the structure of
1381 # the code including all documentation.
1383 GENERATE_XML = NO
1385 # The XML_OUTPUT tag is used to specify where the XML pages will be put.
1386 # If a relative path is entered the value of OUTPUT_DIRECTORY will be
1387 # put in front of it. If left blank `xml' will be used as the default path.
1389 XML_OUTPUT = xml
1391 # The XML_SCHEMA tag can be used to specify an XML schema,
1392 # which can be used by a validating XML parser to check the
1393 # syntax of the XML files.
1395 XML_SCHEMA =
1397 # The XML_DTD tag can be used to specify an XML DTD,
1398 # which can be used by a validating XML parser to check the
1399 # syntax of the XML files.
1401 XML_DTD =
1403 # If the XML_PROGRAMLISTING tag is set to YES Doxygen will
1404 # dump the program listings (including syntax highlighting
1405 # and cross-referencing information) to the XML output. Note that
1406 # enabling this will significantly increase the size of the XML output.
1408 XML_PROGRAMLISTING = YES
1410 #---------------------------------------------------------------------------
1411 # configuration options for the AutoGen Definitions output
1412 #---------------------------------------------------------------------------
1414 # If the GENERATE_AUTOGEN_DEF tag is set to YES Doxygen will
1415 # generate an AutoGen Definitions (see autogen.sf.net) file
1416 # that captures the structure of the code including all
1417 # documentation. Note that this feature is still experimental
1418 # and incomplete at the moment.
1420 GENERATE_AUTOGEN_DEF = NO
1422 #---------------------------------------------------------------------------
1423 # configuration options related to the Perl module output
1424 #---------------------------------------------------------------------------
1426 # If the GENERATE_PERLMOD tag is set to YES Doxygen will
1427 # generate a Perl module file that captures the structure of
1428 # the code including all documentation. Note that this
1429 # feature is still experimental and incomplete at the
1430 # moment.
1432 GENERATE_PERLMOD = NO
1434 # If the PERLMOD_LATEX tag is set to YES Doxygen will generate
1435 # the necessary Makefile rules, Perl scripts and LaTeX code to be able
1436 # to generate PDF and DVI output from the Perl module output.
1438 PERLMOD_LATEX = NO
1440 # If the PERLMOD_PRETTY tag is set to YES the Perl module output will be
1441 # nicely formatted so it can be parsed by a human reader.
1442 # This is useful
1443 # if you want to understand what is going on.
1444 # On the other hand, if this
1445 # tag is set to NO the size of the Perl module output will be much smaller
1446 # and Perl will parse it just the same.
1448 PERLMOD_PRETTY = YES
1450 # The names of the make variables in the generated doxyrules.make file
1451 # are prefixed with the string contained in PERLMOD_MAKEVAR_PREFIX.
1452 # This is useful so different doxyrules.make files included by the same
1453 # Makefile don't overwrite each other's variables.
1455 PERLMOD_MAKEVAR_PREFIX =
1457 #---------------------------------------------------------------------------
1458 # Configuration options related to the preprocessor
1459 #---------------------------------------------------------------------------
1461 # If the ENABLE_PREPROCESSING tag is set to YES (the default) Doxygen will
1462 # evaluate all C-preprocessor directives found in the sources and include
1463 # files.
1465 ENABLE_PREPROCESSING = YES
1467 # If the MACRO_EXPANSION tag is set to YES Doxygen will expand all macro
1468 # names in the source code. If set to NO (the default) only conditional
1469 # compilation will be performed. Macro expansion can be done in a controlled
1470 # way by setting EXPAND_ONLY_PREDEF to YES.
1472 MACRO_EXPANSION = NO
1474 # If the EXPAND_ONLY_PREDEF and MACRO_EXPANSION tags are both set to YES
1475 # then the macro expansion is limited to the macros specified with the
1476 # PREDEFINED and EXPAND_AS_DEFINED tags.
1478 EXPAND_ONLY_PREDEF = NO
1480 # If the SEARCH_INCLUDES tag is set to YES (the default) the includes files
1481 # pointed to by INCLUDE_PATH will be searched when a #include is found.
1483 SEARCH_INCLUDES = YES
1485 # The INCLUDE_PATH tag can be used to specify one or more directories that
1486 # contain include files that are not input files but should be processed by
1487 # the preprocessor.
1489 INCLUDE_PATH =
1491 # You can use the INCLUDE_FILE_PATTERNS tag to specify one or more wildcard
1492 # patterns (like *.h and *.hpp) to filter out the header-files in the
1493 # directories. If left blank, the patterns specified with FILE_PATTERNS will
1494 # be used.
1496 INCLUDE_FILE_PATTERNS =
1498 # The PREDEFINED tag can be used to specify one or more macro names that
1499 # are defined before the preprocessor is started (similar to the -D option of
1500 # gcc). The argument of the tag is a list of macros of the form: name
1501 # or name=definition (no spaces). If the definition and the = are
1502 # omitted =1 is assumed. To prevent a macro definition from being
1503 # undefined via #undef or recursively expanded use the := operator
1504 # instead of the = operator.
1506 PREDEFINED =
1508 # If the MACRO_EXPANSION and EXPAND_ONLY_PREDEF tags are set to YES then
1509 # this tag can be used to specify a list of macro names that should be expanded.
1510 # The macro definition that is found in the sources will be used.
1511 # Use the PREDEFINED tag if you want to use a different macro definition that
1512 # overrules the definition found in the source code.
1514 EXPAND_AS_DEFINED =
1516 # If the SKIP_FUNCTION_MACROS tag is set to YES (the default) then
1517 # doxygen's preprocessor will remove all references to function-like macros
1518 # that are alone on a line, have an all uppercase name, and do not end with a
1519 # semicolon, because these will confuse the parser if not removed.
1521 SKIP_FUNCTION_MACROS = YES
1523 #---------------------------------------------------------------------------
1524 # Configuration::additions related to external references
1525 #---------------------------------------------------------------------------
1527 # The TAGFILES option can be used to specify one or more tagfiles.
1528 # Optionally an initial location of the external documentation
1529 # can be added for each tagfile. The format of a tag file without
1530 # this location is as follows:
1531 #
1532 # TAGFILES = file1 file2 ...
1533 # Adding location for the tag files is done as follows:
1534 #
1535 # TAGFILES = file1=loc1 "file2 = loc2" ...
1536 # where "loc1" and "loc2" can be relative or absolute paths or
1537 # URLs. If a location is present for each tag, the installdox tool
1538 # does not have to be run to correct the links.
1539 # Note that each tag file must have a unique name
1540 # (where the name does NOT include the path)
1541 # If a tag file is not located in the directory in which doxygen
1542 # is run, you must also specify the path to the tagfile here.
1544 TAGFILES =
1546 # When a file name is specified after GENERATE_TAGFILE, doxygen will create
1547 # a tag file that is based on the input files it reads.
1549 GENERATE_TAGFILE =
1551 # If the ALLEXTERNALS tag is set to YES all external classes will be listed
1552 # in the class index. If set to NO only the inherited external classes
1553 # will be listed.
1555 ALLEXTERNALS = NO
1557 # If the EXTERNAL_GROUPS tag is set to YES all external groups will be listed
1558 # in the modules index. If set to NO, only the current project's groups will
1559 # be listed.
1561 EXTERNAL_GROUPS = YES
1563 # The PERL_PATH should be the absolute path and name of the perl script
1564 # interpreter (i.e. the result of `which perl').
1566 PERL_PATH = /usr/bin/perl
1568 #---------------------------------------------------------------------------
1569 # Configuration options related to the dot tool
1570 #---------------------------------------------------------------------------
1572 # If the CLASS_DIAGRAMS tag is set to YES (the default) Doxygen will
1573 # generate a inheritance diagram (in HTML, RTF and LaTeX) for classes with base
1574 # or super classes. Setting the tag to NO turns the diagrams off. Note that
1575 # this option also works with HAVE_DOT disabled, but it is recommended to
1576 # install and use dot, since it yields more powerful graphs.
1578 CLASS_DIAGRAMS = YES
1580 # You can define message sequence charts within doxygen comments using the \msc
1581 # command. Doxygen will then run the mscgen tool (see
1582 # http://www.mcternan.me.uk/mscgen/) to produce the chart and insert it in the
1583 # documentation. The MSCGEN_PATH tag allows you to specify the directory where
1584 # the mscgen tool resides. If left empty the tool is assumed to be found in the
1585 # default search path.
1587 MSCGEN_PATH =
1589 # If set to YES, the inheritance and collaboration graphs will hide
1590 # inheritance and usage relations if the target is undocumented
1591 # or is not a class.
1593 HIDE_UNDOC_RELATIONS = YES
1595 # If you set the HAVE_DOT tag to YES then doxygen will assume the dot tool is
1596 # available from the path. This tool is part of Graphviz, a graph visualization
1597 # toolkit from AT&T and Lucent Bell Labs. The other options in this section
1598 # have no effect if this option is set to NO (the default)
1600 HAVE_DOT = NO
1602 # The DOT_NUM_THREADS specifies the number of dot invocations doxygen is
1603 # allowed to run in parallel. When set to 0 (the default) doxygen will
1604 # base this on the number of processors available in the system. You can set it
1605 # explicitly to a value larger than 0 to get control over the balance
1606 # between CPU load and processing speed.
1608 DOT_NUM_THREADS = 0
1610 # By default doxygen will use the Helvetica font for all dot files that
1611 # doxygen generates. When you want a differently looking font you can specify
1612 # the font name using DOT_FONTNAME. You need to make sure dot is able to find
1613 # the font, which can be done by putting it in a standard location or by setting
1614 # the DOTFONTPATH environment variable or by setting DOT_FONTPATH to the
1615 # directory containing the font.
1617 DOT_FONTNAME = Helvetica
1619 # The DOT_FONTSIZE tag can be used to set the size of the font of dot graphs.
1620 # The default size is 10pt.
1622 DOT_FONTSIZE = 10
1624 # By default doxygen will tell dot to use the Helvetica font.
1625 # If you specify a different font using DOT_FONTNAME you can use DOT_FONTPATH to
1626 # set the path where dot can find it.
1628 DOT_FONTPATH =
1630 # If the CLASS_GRAPH and HAVE_DOT tags are set to YES then doxygen
1631 # will generate a graph for each documented class showing the direct and
1632 # indirect inheritance relations. Setting this tag to YES will force the
1633 # CLASS_DIAGRAMS tag to NO.
1635 CLASS_GRAPH = YES
1637 # If the COLLABORATION_GRAPH and HAVE_DOT tags are set to YES then doxygen
1638 # will generate a graph for each documented class showing the direct and
1639 # indirect implementation dependencies (inheritance, containment, and
1640 # class references variables) of the class with other documented classes.
1642 COLLABORATION_GRAPH = YES
1644 # If the GROUP_GRAPHS and HAVE_DOT tags are set to YES then doxygen
1645 # will generate a graph for groups, showing the direct groups dependencies
1647 GROUP_GRAPHS = YES
1649 # If the UML_LOOK tag is set to YES doxygen will generate inheritance and
1650 # collaboration diagrams in a style similar to the OMG's Unified Modeling
1651 # Language.
1653 UML_LOOK = NO
1655 # If set to YES, the inheritance and collaboration graphs will show the
1656 # relations between templates and their instances.
1658 TEMPLATE_RELATIONS = NO
1660 # If the ENABLE_PREPROCESSING, SEARCH_INCLUDES, INCLUDE_GRAPH, and HAVE_DOT
1661 # tags are set to YES then doxygen will generate a graph for each documented
1662 # file showing the direct and indirect include dependencies of the file with
1663 # other documented files.
1665 INCLUDE_GRAPH = YES
1667 # If the ENABLE_PREPROCESSING, SEARCH_INCLUDES, INCLUDED_BY_GRAPH, and
1668 # HAVE_DOT tags are set to YES then doxygen will generate a graph for each
1669 # documented header file showing the documented files that directly or
1670 # indirectly include this file.
1672 INCLUDED_BY_GRAPH = YES
1674 # If the CALL_GRAPH and HAVE_DOT options are set to YES then
1675 # doxygen will generate a call dependency graph for every global function
1676 # or class method. Note that enabling this option will significantly increase
1677 # the time of a run. So in most cases it will be better to enable call graphs
1678 # for selected functions only using the \callgraph command.
1680 CALL_GRAPH = NO
1682 # If the CALLER_GRAPH and HAVE_DOT tags are set to YES then
1683 # doxygen will generate a caller dependency graph for every global function
1684 # or class method. Note that enabling this option will significantly increase
1685 # the time of a run. So in most cases it will be better to enable caller
1686 # graphs for selected functions only using the \callergraph command.
1688 CALLER_GRAPH = NO
1690 # If the GRAPHICAL_HIERARCHY and HAVE_DOT tags are set to YES then doxygen
1691 # will generate a graphical hierarchy of all classes instead of a textual one.
1693 GRAPHICAL_HIERARCHY = YES
1695 # If the DIRECTORY_GRAPH, SHOW_DIRECTORIES and HAVE_DOT tags are set to YES
1696 # then doxygen will show the dependencies a directory has on other directories
1697 # in a graphical way. The dependency relations are determined by the #include
1698 # relations between the files in the directories.
1700 DIRECTORY_GRAPH = YES
1702 # The DOT_IMAGE_FORMAT tag can be used to set the image format of the images
1703 # generated by dot. Possible values are svg, png, jpg, or gif.
1704 # If left blank png will be used. If you choose svg you need to set
1705 # HTML_FILE_EXTENSION to xhtml in order to make the SVG files
1706 # visible in IE 9+ (other browsers do not have this requirement).
1708 DOT_IMAGE_FORMAT = png
1710 # If DOT_IMAGE_FORMAT is set to svg, then this option can be set to YES to
1711 # enable generation of interactive SVG images that allow zooming and panning.
1712 # Note that this requires a modern browser other than Internet Explorer.
1713 # Tested and working are Firefox, Chrome, Safari, and Opera. For IE 9+ you
1714 # need to set HTML_FILE_EXTENSION to xhtml in order to make the SVG files
1715 # visible. Older versions of IE do not have SVG support.
1717 INTERACTIVE_SVG = NO
1719 # The tag DOT_PATH can be used to specify the path where the dot tool can be
1720 # found. If left blank, it is assumed the dot tool can be found in the path.
1722 DOT_PATH =
1724 # The DOTFILE_DIRS tag can be used to specify one or more directories that
1725 # contain dot files that are included in the documentation (see the
1726 # \dotfile command).
1728 DOTFILE_DIRS =
1730 # The MSCFILE_DIRS tag can be used to specify one or more directories that
1731 # contain msc files that are included in the documentation (see the
1732 # \mscfile command).
1734 MSCFILE_DIRS =
1736 # The DOT_GRAPH_MAX_NODES tag can be used to set the maximum number of
1737 # nodes that will be shown in the graph. If the number of nodes in a graph
1738 # becomes larger than this value, doxygen will truncate the graph, which is
1739 # visualized by representing a node as a red box. Note that doxygen if the
1740 # number of direct children of the root node in a graph is already larger than
1741 # DOT_GRAPH_MAX_NODES then the graph will not be shown at all. Also note
1742 # that the size of a graph can be further restricted by MAX_DOT_GRAPH_DEPTH.
1744 DOT_GRAPH_MAX_NODES = 50
1746 # The MAX_DOT_GRAPH_DEPTH tag can be used to set the maximum depth of the
1747 # graphs generated by dot. A depth value of 3 means that only nodes reachable
1748 # from the root by following a path via at most 3 edges will be shown. Nodes
1749 # that lay further from the root node will be omitted. Note that setting this
1750 # option to 1 or 2 may greatly reduce the computation time needed for large
1751 # code bases. Also note that the size of a graph can be further restricted by
1752 # DOT_GRAPH_MAX_NODES. Using a depth of 0 means no depth restriction.
1754 MAX_DOT_GRAPH_DEPTH = 0
1756 # Set the DOT_TRANSPARENT tag to YES to generate images with a transparent
1757 # background. This is disabled by default, because dot on Windows does not
1758 # seem to support this out of the box. Warning: Depending on the platform used,
1759 # enabling this option may lead to badly anti-aliased labels on the edges of
1760 # a graph (i.e. they become hard to read).
1762 DOT_TRANSPARENT = NO
1764 # Set the DOT_MULTI_TARGETS tag to YES allow dot to generate multiple output
1765 # files in one run (i.e. multiple -o and -T options on the command line). This
1766 # makes dot run faster, but since only newer versions of dot (>1.8.10)
1767 # support this, this feature is disabled by default.
1769 DOT_MULTI_TARGETS = YES
1771 # If the GENERATE_LEGEND tag is set to YES (the default) Doxygen will
1772 # generate a legend page explaining the meaning of the various boxes and
1773 # arrows in the dot generated graphs.
1775 GENERATE_LEGEND = YES
1777 # If the DOT_CLEANUP tag is set to YES (the default) Doxygen will
1778 # remove the intermediate dot files that are used to generate
1779 # the various graphs.
1781 DOT_CLEANUP = YES