Refactored BLIS-BLAS code using LibArch API.
8 years agoAdded bli_mem_init() to level 3 facade functions. Use Perl script to generate wrapper... 1.2.0.0.3
Added bli_mem_init() to level 3 facade functions. Use Perl script to generate wrapper code.
Refactored BLIS code using LibArch API for memory transfers.
Consolidate all git repos of linalg into one.
Baseline: LINALG 1.0.0.2 which is in MCSDK-HPC drop 12.
Baseline: LINALG 1.0.0.2 which is in MCSDK-HPC drop 12.
Made changes to the Makefile so that it can be built with Yocto.
Fixed a bug (if iter==0) in tuning codes.
LINALG 1.0.0.2: Fixed BLIS hanging problem during LAPACK testing.
Updated Debian changelog.
Fixed cross compilation bug in gemm_bench.
Add installation of libelf1:i386.
Fixed makefiles to cross compile the examples on x86.
Remove IPK creation from build script.
Added release script for CM to build LINALG without building MCSDK-HPC.
Updated changelog for 1.0.0.0
Updated release note.
Modified release note.
Corrected a typo in examples/ztrmm_test.
Added release notes in docs folder.
Added gemm_bench.
Updated changelog
Added "Passed" to dgemm_test.
Added dgemm benchmarking example.
Examples improved.
Removed dependency on libatlas-base-dev.
Added what's missed for native build of DSP code.
updated for 0.7.0.0
Modified make.inc for native compilation of DSP code.
Merge branch 'master' of gitorious.design.ti.com:linearalgebra/linalg
Modified readme.txt
Added docs folder to and removed readme.txt from tar file list.
Added software manifest. Moved readme.txt to docs folder.
Added more examples. Tuning and example code clean up.
Cleaned up examples.
Added tuning for xSYRK, xTRMM, and xTRSM.
Changed example matrix sizes back to 1000.
Corrected syntax error in debian/control.
Reduced matrix sizes in examples.
Added dependencies on libatlas-base-dev
Corrected changelog
Changed OCL include path.
Updated debian/changelog.
Clean up examples eig and ludinv.
Revert to previous version.
Clean up examples code.
Remove installation of cblas.h.
Don't install cblas.h if it already exists.
Add readme to tar file list.
Added readme.txt.
Added tuning examples.
Changed debian/changelog and control.
Checked in tuning code. Cleaned up tar file list.
changed version to 0.3.0.0
clean up build scripts
Changed version number to 0.1.0.0 in changelog.
Added eigen decomposition example.
Added LUD matrix inversion example.
Test matmpy on ARM and DSP. (hard coded to test on ARM for now, due to
openCL error with HPC drop 8.)
openCL error with HPC drop 8.)
Updated matmpy example.
Enabled Launchpad build.
Removed export TI_OCL_INSTALL_DIR since it will be set by
setup_hpc_env.sh.
setup_hpc_env.sh.
Corrected a problem in copying examples.
Print out compiler commands.
Added TI_OCL_INSTALL_DIR to make.inc.
Merge branch 'master' of gitorious.design.ti.com:linearalgebra/linalg
Added linalg examples.
Fixed Debian packaging bug.
Fixed bug in Makefile.
Changed version number to 0.0.1.0.
Added Debian install and IPK generation.
Initial commit of LINALG build scripts.