This example demonstrates the usage of the FFT kernel provided with the C6x DSPLIB. The example shows: - Twiddle factor generation for the kernel - Needed scaling to get correct output - Demonstrates usage of FFT APIs Steps: 1) Load the Project using CCS V4. 2) Re-build the project. 3) Run the generated outfile. 4) Plot the output samples. 5) Compare it with reference output (refOutput_sp.jpg). Note: Please refer to CCS V4 Guide for loading, building and running projects. Link: http://processors.wiki.ti.com/index.php/CCSv4_Getting_Started_Guide