Added readme.txt on how to build DSPLIB from git.ti.com source
authorJianzhong Xu <uda0869574local@UDA0869574>
Fri, 3 Aug 2018 15:39:24 +0000 (11:39 -0400)
committerJianzhong Xu <uda0869574local@UDA0869574>
Fri, 3 Aug 2018 15:39:24 +0000 (11:39 -0400)
readme.txt [new file with mode: 0644]
ti/dsplib/docs/bundle/doxygen/release.h.xdt

diff --git a/readme.txt b/readme.txt
new file mode 100644 (file)
index 0000000..f967546
--- /dev/null
@@ -0,0 +1,44 @@
+Instructions to build DSPLIB from source:
+
+1. Clone DSPLIB from git://git.ti.com/ep-processor-libraries/dsplib.git 
+   Clone SWTOOLS from git://git.ti.com/ep-processor-libraries/swtools.git
+
+2. Make sure following Proc-SDK components are installed:
+   - SYSBIOS
+   - XDC
+   - Code Gen Tools
+   - CCS
+   - MATHLIB
+
+3. Setup following environment variables:
+export SYSBIOS_INSTALL_DIR="<COMPONENTS_INSTALLATION_ROOT>/bios_6_52_00_12"
+export XDC_INSTALL_DIR="<COMPONENTS_INSTALLATION_ROOT>/xdctools_3_50_03_33_core/"
+export XDCCGROOT="<COMPONENTS_INSTALLATION_ROOT>/ti-cgt-c6000_8.2.2"
+export CGTROOT="<COMPONENTS_INSTALLATION_ROOT>/ti-cgt-c6000_8.2.2"
+export C64PCODEGENTOOL="${CGTROOT}"
+export C674CODEGENTOOL="${CGTROOT}"
+export C66CODEGENTOOL="${CGTROOT}"
+
+export CCSVERSION="CCSV8"
+export CCS_INSTALL_DIR="<COMPONENTS_INSTALLATION_ROOT>/ccsv8"
+
+export DSPLIB_ROOT="<DSPLIB git clone root>"
+export MATHLIB_INSTALL_DIR="<COMPONENTS_INSTALLATION_ROOT>/mathlib_c66x_3_1_1_0/packages"
+
+export SWTOOLS_INSTALL_DIR="<SWTOOLS git clone root>"
+export SWTOOLS_PATH="<SWTOOLS git clone root>/ti/mas/swtools"
+export XDCBUILDCFG="${SWTOOLS_PATH}/config.bld"
+export INCDIR="${MATHLIB_INSTALL_DIR}/"
+
+export PATH="${XDC_INSTALL_DIR}:${PATH}"
+
+export XDCPATH="${XDCCGROOT}/include;${XDC_INSTALL_DIR}/packages;${SWTOOLS_INSTALL_DIR};${MATHLIB_INSTALL_DIR};${DSPLIB_ROOT};${SYSBIOS_INSTALL_DIR}/packages;/usr/share/php5;/usr/lib/php5"
+
+4. Build SWTOOLS and then DSPLIB
+   - Go to directory <SWTOOLS_PATH> and issue command "xdc"
+   - Go to directory <DSPLIB_ROOT>/ti/dsplib and issue one of following commands:
+       - xdc XDCARGS="c66x bundle"
+       - xdc XDCARGS="c674x bundle"
+       - xdc XDCARGS="c64Px bundle"
+
+
index 721441133762839567213592e1af2ef3216cb68a..ad676a6373793898fe53f105926d465f848596c2 100644 (file)
  *  </ul>
  *
  * <b> Please note that the Test Report was still based on Code Generation Tools 7.4.2. The kernel cycle numbers 
  *  </ul>
  *
  * <b> Please note that the Test Report was still based on Code Generation Tools 7.4.2. The kernel cycle numbers 
- *     were not measured in this release and may be different from prior releases. 
+ *     were not measured in this release and may be different from prior releases.</b> 
  *
  * <hr size="2" width="50%" align="left">
  *
  *
  * <hr size="2" width="50%" align="left">
  *
  *
  *  Questions regarding the `packageU` library should be directed to one of the following forums based on 
  *  the device that this library is used for:
  *
  *  Questions regarding the `packageU` library should be directed to one of the following forums based on 
  *  the device that this library is used for:
- *  <a href="http://e2e.ti.com/support/arm/sitara_arm/f/791.aspx">E2E Support Forums for AM335x, AM437x, and AM57xx
- *  <a href="http://e2e.ti.com/support/dsp/c6000_multi-core_dsps/f/639">E2E Support Forums for K2H, K2K, K2E, K2L, K2G, C665x, and C667x
- *  <a href="http://e2e.ti.com/support/dsp/omap_applications_processors/f/42">E2E Support Forums for OMAP-L13x and C674x
+ *  - <a href="http://e2e.ti.com/support/arm/sitara_arm/f/791.aspx">E2E Support Forums for AM335x, AM437x, and AM57xx</a>
+ *  - <a href="http://e2e.ti.com/support/dsp/c6000_multi-core_dsps/f/639">E2E Support Forums for K2H, K2K, K2E, K2L, K2G, C665x, and C667x</a>
+ *  - <a href="http://e2e.ti.com/support/dsp/omap_applications_processors/f/42">E2E Support Forums for OMAP-L13x and C674x</a>
  *
  *
- *  Please include the text "`packageU`" in the title and add "`DEVICES[0]`" and "`packageU`" tags to your post.
+ *  Please include the text "`packageU`" in the title and add "C66x" or "C674x" or "C64x+" tags to your post.
  *
  * <hr size="2" width="50%" align="left">
  *
  *
  * <hr size="2" width="50%" align="left">
  *