1 # Doxyfile 1.6.3
3 # This file describes the settings to be used by the documentation system
4 # doxygen (www.doxygen.org) for a project
5 #
6 # All text after a hash (#) is considered a comment and will be ignored
7 # The format is:
8 # TAG = value [value, ...]
9 # For lists items can also be appended using:
10 # TAG += value [value, ...]
11 # Values that contain spaces should be placed between quotes (" ")
13 #---------------------------------------------------------------------------
14 # Project related configuration options
15 #---------------------------------------------------------------------------
17 # This tag specifies the encoding used for all characters in the config file
18 # that follow. The default is UTF-8 which is also the encoding used for all
19 # text before the first occurrence of this tag. Doxygen uses libiconv (or the
20 # iconv built into libc) for the transcoding. See
21 # http://www.gnu.org/software/libiconv for the list of possible encodings.
23 DOXYFILE_ENCODING = UTF-8
25 # The PROJECT_NAME tag is a single word (or a sequence of words surrounded
26 # by quotes) that should identify the project.
28 PROJECT_NAME = Dual_Decode
30 # The PROJECT_NUMBER tag can be used to enter a project or revision number.
31 # This could be handy for archiving the generated documentation or
32 # if some version control system is used.
34 PROJECT_NUMBER =
36 # The OUTPUT_DIRECTORY tag is used to specify the (relative or absolute)
37 # base path where the generated documentation will be put.
38 # If a relative path is entered, it will be relative to the location
39 # where doxygen was started. If left blank the current directory will be used.
41 OUTPUT_DIRECTORY = docs
43 # If the CREATE_SUBDIRS tag is set to YES, then doxygen will create
44 # 4096 sub-directories (in 2 levels) under the output directory of each output
45 # format and will distribute the generated files over these directories.
46 # Enabling this option can be useful when feeding doxygen a huge amount of
47 # source files, where putting all generated files in the same directory would
48 # otherwise cause performance problems for the file system.
50 CREATE_SUBDIRS = NO
52 # The OUTPUT_LANGUAGE tag is used to specify the language in which all
53 # documentation generated by doxygen is written. Doxygen will use this
54 # information to generate all constant output in the proper language.
55 # The default language is English, other supported languages are:
56 # Afrikaans, Arabic, Brazilian, Catalan, Chinese, Chinese-Traditional,
57 # Croatian, Czech, Danish, Dutch, Esperanto, Farsi, Finnish, French, German,
58 # Greek, Hungarian, Italian, Japanese, Japanese-en (Japanese with English
59 # messages), Korean, Korean-en, Lithuanian, Norwegian, Macedonian, Persian,
60 # Polish, Portuguese, Romanian, Russian, Serbian, Serbian-Cyrilic, Slovak,
61 # Slovene, Spanish, Swedish, Ukrainian, and Vietnamese.
63 OUTPUT_LANGUAGE = English
65 # If the BRIEF_MEMBER_DESC tag is set to YES (the default) Doxygen will
66 # include brief member descriptions after the members that are listed in
67 # the file and class documentation (similar to JavaDoc).
68 # Set to NO to disable this.
70 BRIEF_MEMBER_DESC = YES
72 # If the REPEAT_BRIEF tag is set to YES (the default) Doxygen will prepend
73 # the brief description of a member or function before the detailed description.
74 # Note: if both HIDE_UNDOC_MEMBERS and BRIEF_MEMBER_DESC are set to NO, the
75 # brief descriptions will be completely suppressed.
77 REPEAT_BRIEF = YES
79 # This tag implements a quasi-intelligent brief description abbreviator
80 # that is used to form the text in various listings. Each string
81 # in this list, if found as the leading text of the brief description, will be
82 # stripped from the text and the result after processing the whole list, is
83 # used as the annotated text. Otherwise, the brief description is used as-is.
84 # If left blank, the following values are used ("$name" is automatically
85 # replaced with the name of the entity): "The $name class" "The $name widget"
86 # "The $name file" "is" "provides" "specifies" "contains"
87 # "represents" "a" "an" "the"
89 ABBREVIATE_BRIEF =
91 # If the ALWAYS_DETAILED_SEC and REPEAT_BRIEF tags are both set to YES then
92 # Doxygen will generate a detailed section even if there is only a brief
93 # description.
95 ALWAYS_DETAILED_SEC = NO
97 # If the INLINE_INHERITED_MEMB tag is set to YES, doxygen will show all
98 # inherited members of a class in the documentation of that class as if those
99 # members were ordinary class members. Constructors, destructors and assignment
100 # operators of the base classes will not be shown.
102 INLINE_INHERITED_MEMB = NO
104 # If the FULL_PATH_NAMES tag is set to YES then Doxygen will prepend the full
105 # path before files name in the file list and in the header files. If set
106 # to NO the shortest path that makes the file name unique will be used.
108 FULL_PATH_NAMES = YES
110 # If the FULL_PATH_NAMES tag is set to YES then the STRIP_FROM_PATH tag
111 # can be used to strip a user-defined part of the path. Stripping is
112 # only done if one of the specified strings matches the left-hand part of
113 # the path. The tag can be used to show relative paths in the file list.
114 # If left blank the directory from which doxygen is run is used as the
115 # path to strip.
117 STRIP_FROM_PATH =
119 # The STRIP_FROM_INC_PATH tag can be used to strip a user-defined part of
120 # the path mentioned in the documentation of a class, which tells
121 # the reader which header file to include in order to use a class.
122 # If left blank only the name of the header file containing the class
123 # definition is used. Otherwise one should specify the include paths that
124 # are normally passed to the compiler using the -I flag.
126 STRIP_FROM_INC_PATH =
128 # If the SHORT_NAMES tag is set to YES, doxygen will generate much shorter
129 # (but less readable) file names. This can be useful is your file systems
130 # doesn't support long names like on DOS, Mac, or CD-ROM.
132 SHORT_NAMES = NO
134 # If the JAVADOC_AUTOBRIEF tag is set to YES then Doxygen
135 # will interpret the first line (until the first dot) of a JavaDoc-style
136 # comment as the brief description. If set to NO, the JavaDoc
137 # comments will behave just like regular Qt-style comments
138 # (thus requiring an explicit @brief command for a brief description.)
140 JAVADOC_AUTOBRIEF = NO
142 # If the QT_AUTOBRIEF tag is set to YES then Doxygen will
143 # interpret the first line (until the first dot) of a Qt-style
144 # comment as the brief description. If set to NO, the comments
145 # will behave just like regular Qt-style comments (thus requiring
146 # an explicit \brief command for a brief description.)
148 QT_AUTOBRIEF = NO
150 # The MULTILINE_CPP_IS_BRIEF tag can be set to YES to make Doxygen
151 # treat a multi-line C++ special comment block (i.e. a block of //! or ///
152 # comments) as a brief description. This used to be the default behaviour.
153 # The new default is to treat a multi-line C++ comment block as a detailed
154 # description. Set this tag to YES if you prefer the old behaviour instead.
156 MULTILINE_CPP_IS_BRIEF = NO
158 # If the INHERIT_DOCS tag is set to YES (the default) then an undocumented
159 # member inherits the documentation from any documented member that it
160 # re-implements.
162 INHERIT_DOCS = YES
164 # If the SEPARATE_MEMBER_PAGES tag is set to YES, then doxygen will produce
165 # a new page for each member. If set to NO, the documentation of a member will
166 # be part of the file/class/namespace that contains it.
168 SEPARATE_MEMBER_PAGES = NO
170 # The TAB_SIZE tag can be used to set the number of spaces in a tab.
171 # Doxygen uses this value to replace tabs by spaces in code fragments.
173 TAB_SIZE = 8
175 # This tag can be used to specify a number of aliases that acts
176 # as commands in the documentation. An alias has the form "name=value".
177 # For example adding "sideeffect=\par Side Effects:\n" will allow you to
178 # put the command \sideeffect (or @sideeffect) in the documentation, which
179 # will result in a user-defined paragraph with heading "Side Effects:".
180 # You can put \n's in the value part of an alias to insert newlines.
182 ALIASES =
184 # Set the OPTIMIZE_OUTPUT_FOR_C tag to YES if your project consists of C
185 # sources only. Doxygen will then generate output that is more tailored for C.
186 # For instance, some of the names that are used will be different. The list
187 # of all members will be omitted, etc.
189 OPTIMIZE_OUTPUT_FOR_C = YES
191 # Set the OPTIMIZE_OUTPUT_JAVA tag to YES if your project consists of Java
192 # sources only. Doxygen will then generate output that is more tailored for
193 # Java. For instance, namespaces will be presented as packages, qualified
194 # scopes will look different, etc.
196 OPTIMIZE_OUTPUT_JAVA = NO
198 # Set the OPTIMIZE_FOR_FORTRAN tag to YES if your project consists of Fortran
199 # sources only. Doxygen will then generate output that is more tailored for
200 # Fortran.
202 OPTIMIZE_FOR_FORTRAN = NO
204 # Set the OPTIMIZE_OUTPUT_VHDL tag to YES if your project consists of VHDL
205 # sources. Doxygen will then generate output that is tailored for
206 # VHDL.
208 OPTIMIZE_OUTPUT_VHDL = NO
210 # Doxygen selects the parser to use depending on the extension of the files it parses.
211 # With this tag you can assign which parser to use for a given extension.
212 # Doxygen has a built-in mapping, but you can override or extend it using this tag.
213 # The format is ext=language, where ext is a file extension, and language is one of
214 # the parsers supported by doxygen: IDL, Java, Javascript, C#, C, C++, D, PHP,
215 # Objective-C, Python, Fortran, VHDL, C, C++. For instance to make doxygen treat
216 # .inc files as Fortran files (default is PHP), and .f files as C (default is Fortran),
217 # use: inc=Fortran f=C. Note that for custom extensions you also need to set FILE_PATTERNS otherwise the files are not read by doxygen.
219 EXTENSION_MAPPING =
221 # If you use STL classes (i.e. std::string, std::vector, etc.) but do not want
222 # to include (a tag file for) the STL sources as input, then you should
223 # set this tag to YES in order to let doxygen match functions declarations and
224 # definitions whose arguments contain STL classes (e.g. func(std::string); v.s.
225 # func(std::string) {}). This also make the inheritance and collaboration
226 # diagrams that involve STL classes more complete and accurate.
228 BUILTIN_STL_SUPPORT = NO
230 # If you use Microsoft's C++/CLI language, you should set this option to YES to
231 # enable parsing support.
233 CPP_CLI_SUPPORT = NO
235 # Set the SIP_SUPPORT tag to YES if your project consists of sip sources only.
236 # Doxygen will parse them like normal C++ but will assume all classes use public
237 # instead of private inheritance when no explicit protection keyword is present.
239 SIP_SUPPORT = NO
241 # For Microsoft's IDL there are propget and propput attributes to indicate getter
242 # and setter methods for a property. Setting this option to YES (the default)
243 # will make doxygen to replace the get and set methods by a property in the
244 # documentation. This will only work if the methods are indeed getting or
245 # setting a simple type. If this is not the case, or you want to show the
246 # methods anyway, you should set this option to NO.
248 IDL_PROPERTY_SUPPORT = YES
250 # If member grouping is used in the documentation and the DISTRIBUTE_GROUP_DOC
251 # tag is set to YES, then doxygen will reuse the documentation of the first
252 # member in the group (if any) for the other members of the group. By default
253 # all members of a group must be documented explicitly.
255 DISTRIBUTE_GROUP_DOC = NO
257 # Set the SUBGROUPING tag to YES (the default) to allow class member groups of
258 # the same type (for instance a group of public functions) to be put as a
259 # subgroup of that type (e.g. under the Public Functions section). Set it to
260 # NO to prevent subgrouping. Alternatively, this can be done per class using
261 # the \nosubgrouping command.
263 SUBGROUPING = YES
265 # When TYPEDEF_HIDES_STRUCT is enabled, a typedef of a struct, union, or enum
266 # is documented as struct, union, or enum with the name of the typedef. So
267 # typedef struct TypeS {} TypeT, will appear in the documentation as a struct
268 # with name TypeT. When disabled the typedef will appear as a member of a file,
269 # namespace, or class. And the struct will be named TypeS. This can typically
270 # be useful for C code in case the coding convention dictates that all compound
271 # types are typedef'ed and only the typedef is referenced, never the tag name.
273 TYPEDEF_HIDES_STRUCT = NO
275 # The SYMBOL_CACHE_SIZE determines the size of the internal cache use to
276 # determine which symbols to keep in memory and which to flush to disk.
277 # When the cache is full, less often used symbols will be written to disk.
278 # For small to medium size projects (<1000 input files) the default value is
279 # probably good enough. For larger projects a too small cache size can cause
280 # doxygen to be busy swapping symbols to and from disk most of the time
281 # causing a significant performance penality.
282 # If the system has enough physical memory increasing the cache will improve the
283 # performance by keeping more symbols in memory. Note that the value works on
284 # a logarithmic scale so increasing the size by one will rougly double the
285 # memory usage. The cache size is given by this formula:
286 # 2^(16+SYMBOL_CACHE_SIZE). The valid range is 0..9, the default is 0,
287 # corresponding to a cache size of 2^16 = 65536 symbols
289 SYMBOL_CACHE_SIZE = 0
291 #---------------------------------------------------------------------------
292 # Build related configuration options
293 #---------------------------------------------------------------------------
295 # If the EXTRACT_ALL tag is set to YES doxygen will assume all entities in
296 # documentation are documented, even if no documentation was available.
297 # Private class members and static file members will be hidden unless
298 # the EXTRACT_PRIVATE and EXTRACT_STATIC tags are set to YES
300 EXTRACT_ALL = NO
302 # If the EXTRACT_PRIVATE tag is set to YES all private members of a class
303 # will be included in the documentation.
305 EXTRACT_PRIVATE = NO
307 # If the EXTRACT_STATIC tag is set to YES all static members of a file
308 # will be included in the documentation.
310 EXTRACT_STATIC = NO
312 # If the EXTRACT_LOCAL_CLASSES tag is set to YES classes (and structs)
313 # defined locally in source files will be included in the documentation.
314 # If set to NO only classes defined in header files are included.
316 EXTRACT_LOCAL_CLASSES = YES
318 # This flag is only useful for Objective-C code. When set to YES local
319 # methods, which are defined in the implementation section but not in
320 # the interface are included in the documentation.
321 # If set to NO (the default) only methods in the interface are included.
323 EXTRACT_LOCAL_METHODS = NO
325 # If this flag is set to YES, the members of anonymous namespaces will be
326 # extracted and appear in the documentation as a namespace called
327 # 'anonymous_namespace{file}', where file will be replaced with the base
328 # name of the file that contains the anonymous namespace. By default
329 # anonymous namespace are hidden.
331 EXTRACT_ANON_NSPACES = NO
333 # If the HIDE_UNDOC_MEMBERS tag is set to YES, Doxygen will hide all
334 # undocumented members of documented classes, files or namespaces.
335 # If set to NO (the default) these members will be included in the
336 # various overviews, but no documentation section is generated.
337 # This option has no effect if EXTRACT_ALL is enabled.
339 HIDE_UNDOC_MEMBERS = NO
341 # If the HIDE_UNDOC_CLASSES tag is set to YES, Doxygen will hide all
342 # undocumented classes that are normally visible in the class hierarchy.
343 # If set to NO (the default) these classes will be included in the various
344 # overviews. This option has no effect if EXTRACT_ALL is enabled.
346 HIDE_UNDOC_CLASSES = NO
348 # If the HIDE_FRIEND_COMPOUNDS tag is set to YES, Doxygen will hide all
349 # friend (class|struct|union) declarations.
350 # If set to NO (the default) these declarations will be included in the
351 # documentation.
353 HIDE_FRIEND_COMPOUNDS = NO
355 # If the HIDE_IN_BODY_DOCS tag is set to YES, Doxygen will hide any
356 # documentation blocks found inside the body of a function.
357 # If set to NO (the default) these blocks will be appended to the
358 # function's detailed documentation block.
360 HIDE_IN_BODY_DOCS = NO
362 # The INTERNAL_DOCS tag determines if documentation
363 # that is typed after a \internal command is included. If the tag is set
364 # to NO (the default) then the documentation will be excluded.
365 # Set it to YES to include the internal documentation.
367 INTERNAL_DOCS = NO
369 # If the CASE_SENSE_NAMES tag is set to NO then Doxygen will only generate
370 # file names in lower-case letters. If set to YES upper-case letters are also
371 # allowed. This is useful if you have classes or files whose names only differ
372 # in case and if your file system supports case sensitive file names. Windows
373 # and Mac users are advised to set this option to NO.
375 CASE_SENSE_NAMES = YES
377 # If the HIDE_SCOPE_NAMES tag is set to NO (the default) then Doxygen
378 # will show members with their full class and namespace scopes in the
379 # documentation. If set to YES the scope will be hidden.
381 HIDE_SCOPE_NAMES = NO
383 # If the SHOW_INCLUDE_FILES tag is set to YES (the default) then Doxygen
384 # will put a list of the files that are included by a file in the documentation
385 # of that file.
387 SHOW_INCLUDE_FILES = YES
389 # If the FORCE_LOCAL_INCLUDES tag is set to YES then Doxygen
390 # will list include files with double quotes in the documentation
391 # rather than with sharp brackets.
393 FORCE_LOCAL_INCLUDES = NO
395 # If the INLINE_INFO tag is set to YES (the default) then a tag [inline]
396 # is inserted in the documentation for inline members.
398 INLINE_INFO = YES
400 # If the SORT_MEMBER_DOCS tag is set to YES (the default) then doxygen
401 # will sort the (detailed) documentation of file and class members
402 # alphabetically by member name. If set to NO the members will appear in
403 # declaration order.
405 SORT_MEMBER_DOCS = YES
407 # If the SORT_BRIEF_DOCS tag is set to YES then doxygen will sort the
408 # brief documentation of file, namespace and class members alphabetically
409 # by member name. If set to NO (the default) the members will appear in
410 # declaration order.
412 SORT_BRIEF_DOCS = NO
414 # If the SORT_MEMBERS_CTORS_1ST tag is set to YES then doxygen will sort the (brief and detailed) documentation of class members so that constructors and destructors are listed first. If set to NO (the default) the constructors will appear in the respective orders defined by SORT_MEMBER_DOCS and SORT_BRIEF_DOCS. This tag will be ignored for brief docs if SORT_BRIEF_DOCS is set to NO and ignored for detailed docs if SORT_MEMBER_DOCS is set to NO.
416 SORT_MEMBERS_CTORS_1ST = NO
418 # If the SORT_GROUP_NAMES tag is set to YES then doxygen will sort the
419 # hierarchy of group names into alphabetical order. If set to NO (the default)
420 # the group names will appear in their defined order.
422 SORT_GROUP_NAMES = NO
424 # If the SORT_BY_SCOPE_NAME tag is set to YES, the class list will be
425 # sorted by fully-qualified names, including namespaces. If set to
426 # NO (the default), the class list will be sorted only by class name,
427 # not including the namespace part.
428 # Note: This option is not very useful if HIDE_SCOPE_NAMES is set to YES.
429 # Note: This option applies only to the class list, not to the
430 # alphabetical list.
432 SORT_BY_SCOPE_NAME = NO
434 # The GENERATE_TODOLIST tag can be used to enable (YES) or
435 # disable (NO) the todo list. This list is created by putting \todo
436 # commands in the documentation.
438 GENERATE_TODOLIST = YES
440 # The GENERATE_TESTLIST tag can be used to enable (YES) or
441 # disable (NO) the test list. This list is created by putting \test
442 # commands in the documentation.
444 GENERATE_TESTLIST = YES
446 # The GENERATE_BUGLIST tag can be used to enable (YES) or
447 # disable (NO) the bug list. This list is created by putting \bug
448 # commands in the documentation.
450 GENERATE_BUGLIST = YES
452 # The GENERATE_DEPRECATEDLIST tag can be used to enable (YES) or
453 # disable (NO) the deprecated list. This list is created by putting
454 # \deprecated commands in the documentation.
456 GENERATE_DEPRECATEDLIST= YES
458 # The ENABLED_SECTIONS tag can be used to enable conditional
459 # documentation sections, marked by \if sectionname ... \endif.
461 ENABLED_SECTIONS =
463 # The MAX_INITIALIZER_LINES tag determines the maximum number of lines
464 # the initial value of a variable or define consists of for it to appear in
465 # the documentation. If the initializer consists of more lines than specified
466 # here it will be hidden. Use a value of 0 to hide initializers completely.
467 # The appearance of the initializer of individual variables and defines in the
468 # documentation can be controlled using \showinitializer or \hideinitializer
469 # command in the documentation regardless of this setting.
471 MAX_INITIALIZER_LINES = 30
473 # Set the SHOW_USED_FILES tag to NO to disable the list of files generated
474 # at the bottom of the documentation of classes and structs. If set to YES the
475 # list will mention the files that were used to generate the documentation.
477 SHOW_USED_FILES = YES
479 # If the sources in your project are distributed over multiple directories
480 # then setting the SHOW_DIRECTORIES tag to YES will show the directory hierarchy
481 # in the documentation. The default is NO.
483 SHOW_DIRECTORIES = NO
485 # Set the SHOW_FILES tag to NO to disable the generation of the Files page.
486 # This will remove the Files entry from the Quick Index and from the
487 # Folder Tree View (if specified). The default is YES.
489 SHOW_FILES = YES
491 # Set the SHOW_NAMESPACES tag to NO to disable the generation of the
492 # Namespaces page.
493 # This will remove the Namespaces entry from the Quick Index
494 # and from the Folder Tree View (if specified). The default is YES.
496 SHOW_NAMESPACES = YES
498 # The FILE_VERSION_FILTER tag can be used to specify a program or script that
499 # doxygen should invoke to get the current version for each file (typically from
500 # the version control system). Doxygen will invoke the program by executing (via
501 # popen()) the command <command> <input-file>, where <command> is the value of
502 # the FILE_VERSION_FILTER tag, and <input-file> is the name of an input file
503 # provided by doxygen. Whatever the program writes to standard output
504 # is used as the file version. See the manual for examples.
506 FILE_VERSION_FILTER =
508 # The LAYOUT_FILE tag can be used to specify a layout file which will be parsed by
509 # doxygen. The layout file controls the global structure of the generated output files
510 # in an output format independent way. The create the layout file that represents
511 # doxygen's defaults, run doxygen with the -l option. You can optionally specify a
512 # file name after the option, if omitted DoxygenLayout.xml will be used as the name
513 # of the layout file.
515 LAYOUT_FILE =
517 #---------------------------------------------------------------------------
518 # configuration options related to warning and progress messages
519 #---------------------------------------------------------------------------
521 # The QUIET tag can be used to turn on/off the messages that are generated
522 # by doxygen. Possible values are YES and NO. If left blank NO is used.
524 QUIET = YES
526 # The WARNINGS tag can be used to turn on/off the warning messages that are
527 # generated by doxygen. Possible values are YES and NO. If left blank
528 # NO is used.
530 WARNINGS = YES
532 # If WARN_IF_UNDOCUMENTED is set to YES, then doxygen will generate warnings
533 # for undocumented members. If EXTRACT_ALL is set to YES then this flag will
534 # automatically be disabled.
536 WARN_IF_UNDOCUMENTED = YES
538 # If WARN_IF_DOC_ERROR is set to YES, doxygen will generate warnings for
539 # potential errors in the documentation, such as not documenting some
540 # parameters in a documented function, or documenting parameters that
541 # don't exist or using markup commands wrongly.
543 WARN_IF_DOC_ERROR = YES
545 # This WARN_NO_PARAMDOC option can be abled to get warnings for
546 # functions that are documented, but have no documentation for their parameters
547 # or return value. If set to NO (the default) doxygen will only warn about
548 # wrong or incomplete parameter documentation, but not about the absence of
549 # documentation.
551 WARN_NO_PARAMDOC = NO
553 # The WARN_FORMAT tag determines the format of the warning messages that
554 # doxygen can produce. The string should contain the $file, $line, and $text
555 # tags, which will be replaced by the file and line number from which the
556 # warning originated and the warning text. Optionally the format may contain
557 # $version, which will be replaced by the version of the file (if it could
558 # be obtained via FILE_VERSION_FILTER)
560 WARN_FORMAT = "$file:$line: $text"
562 # The WARN_LOGFILE tag can be used to specify a file to which warning
563 # and error messages should be written. If left blank the output is written
564 # to stderr.
566 WARN_LOGFILE =
568 #---------------------------------------------------------------------------
569 # configuration options related to the input files
570 #---------------------------------------------------------------------------
572 # The INPUT tag can be used to specify the files and/or directories that contain
573 # documented source files. You may enter file names like "myfile.cpp" or
574 # directories like "/usr/src/myproject". Separate the files or directories
575 # with spaces.
577 INPUT = include src
579 # This tag can be used to specify the character encoding of the source files
580 # that doxygen parses. Internally doxygen uses the UTF-8 encoding, which is
581 # also the default input encoding. Doxygen uses libiconv (or the iconv built
582 # into libc) for the transcoding. See http://www.gnu.org/software/libiconv for
583 # the list of possible encodings.
585 INPUT_ENCODING = UTF-8
587 # If the value of the INPUT tag contains directories, you can use the
588 # FILE_PATTERNS tag to specify one or more wildcard pattern (like *.cpp
589 # and *.h) to filter out the source-files in the directories. If left
590 # blank the following patterns are tested:
591 # *.c *.cc *.cxx *.cpp *.c++ *.java *.ii *.ixx *.ipp *.i++ *.inl *.h *.hh *.hxx
592 # *.hpp *.h++ *.idl *.odl *.cs *.php *.php3 *.inc *.m *.mm *.py *.f90
594 FILE_PATTERNS = *.h
596 # The RECURSIVE tag can be used to turn specify whether or not subdirectories
597 # should be searched for input files as well. Possible values are YES and NO.
598 # If left blank NO is used.
600 RECURSIVE = YES
602 # The EXCLUDE tag can be used to specify files and/or directories that should
603 # excluded from the INPUT source files. This way you can easily exclude a
604 # subdirectory from a directory tree whose root is specified with the INPUT tag.
606 EXCLUDE =
608 # The EXCLUDE_SYMLINKS tag can be used select whether or not files or
609 # directories that are symbolic links (a Unix filesystem feature) are excluded
610 # from the input.
612 EXCLUDE_SYMLINKS = NO
614 # If the value of the INPUT tag contains directories, you can use the
615 # EXCLUDE_PATTERNS tag to specify one or more wildcard patterns to exclude
616 # certain files from those directories. Note that the wildcards are matched
617 # against the file with absolute path, so to exclude all test directories
618 # for example use the pattern */test/*
620 EXCLUDE_PATTERNS =
622 # The EXCLUDE_SYMBOLS tag can be used to specify one or more symbol names
623 # (namespaces, classes, functions, etc.) that should be excluded from the
624 # output. The symbol name can be a fully qualified name, a word, or if the
625 # wildcard * is used, a substring. Examples: ANamespace, AClass,
626 # AClass::ANamespace, ANamespace::*Test
628 EXCLUDE_SYMBOLS =
630 # The EXAMPLE_PATH tag can be used to specify one or more files or
631 # directories that contain example code fragments that are included (see
632 # the \include command).
634 EXAMPLE_PATH =
636 # If the value of the EXAMPLE_PATH tag contains directories, you can use the
637 # EXAMPLE_PATTERNS tag to specify one or more wildcard pattern (like *.cpp
638 # and *.h) to filter out the source-files in the directories. If left
639 # blank all files are included.
641 EXAMPLE_PATTERNS = *.c *.h
643 # If the EXAMPLE_RECURSIVE tag is set to YES then subdirectories will be
644 # searched for input files to be used with the \include or \dontinclude
645 # commands irrespective of the value of the RECURSIVE tag.
646 # Possible values are YES and NO. If left blank NO is used.
648 EXAMPLE_RECURSIVE = YES
650 # The IMAGE_PATH tag can be used to specify one or more files or
651 # directories that contain image that are included in the documentation (see
652 # the \image command).
654 IMAGE_PATH =
656 # The INPUT_FILTER tag can be used to specify a program that doxygen should
657 # invoke to filter for each input file. Doxygen will invoke the filter program
658 # by executing (via popen()) the command <filter> <input-file>, where <filter>
659 # is the value of the INPUT_FILTER tag, and <input-file> is the name of an
660 # input file. Doxygen will then use the output that the filter program writes
661 # to standard output.
662 # If FILTER_PATTERNS is specified, this tag will be
663 # ignored.
665 INPUT_FILTER =
667 # The FILTER_PATTERNS tag can be used to specify filters on a per file pattern
668 # basis.
669 # Doxygen will compare the file name with each pattern and apply the
670 # filter if there is a match.
671 # The filters are a list of the form:
672 # pattern=filter (like *.cpp=my_cpp_filter). See INPUT_FILTER for further
673 # info on how filters are used. If FILTER_PATTERNS is empty, INPUT_FILTER
674 # is applied to all files.
676 FILTER_PATTERNS =
678 # If the FILTER_SOURCE_FILES tag is set to YES, the input filter (if set using
679 # INPUT_FILTER) will be used to filter the input files when producing source
680 # files to browse (i.e. when SOURCE_BROWSER is set to YES).
682 FILTER_SOURCE_FILES = NO
684 #---------------------------------------------------------------------------
685 # configuration options related to source browsing
686 #---------------------------------------------------------------------------
688 # If the SOURCE_BROWSER tag is set to YES then a list of source files will
689 # be generated. Documented entities will be cross-referenced with these sources.
690 # Note: To get rid of all source code in the generated output, make sure also
691 # VERBATIM_HEADERS is set to NO.
693 SOURCE_BROWSER = NO
695 # Setting the INLINE_SOURCES tag to YES will include the body
696 # of functions and classes directly in the documentation.
698 INLINE_SOURCES = NO
700 # Setting the STRIP_CODE_COMMENTS tag to YES (the default) will instruct
701 # doxygen to hide any special comment blocks from generated source code
702 # fragments. Normal C and C++ comments will always remain visible.
704 STRIP_CODE_COMMENTS = YES
706 # If the REFERENCED_BY_RELATION tag is set to YES
707 # then for each documented function all documented
708 # functions referencing it will be listed.
710 REFERENCED_BY_RELATION = NO
712 # If the REFERENCES_RELATION tag is set to YES
713 # then for each documented function all documented entities
714 # called/used by that function will be listed.
716 REFERENCES_RELATION = NO
718 # If the REFERENCES_LINK_SOURCE tag is set to YES (the default)
719 # and SOURCE_BROWSER tag is set to YES, then the hyperlinks from
720 # functions in REFERENCES_RELATION and REFERENCED_BY_RELATION lists will
721 # link to the source code.
722 # Otherwise they will link to the documentation.
724 REFERENCES_LINK_SOURCE = YES
726 # If the USE_HTAGS tag is set to YES then the references to source code
727 # will point to the HTML generated by the htags(1) tool instead of doxygen
728 # built-in source browser. The htags tool is part of GNU's global source
729 # tagging system (see http://www.gnu.org/software/global/global.html). You
730 # will need version 4.8.6 or higher.
732 USE_HTAGS = NO
734 # If the VERBATIM_HEADERS tag is set to YES (the default) then Doxygen
735 # will generate a verbatim copy of the header file for each class for
736 # which an include is specified. Set to NO to disable this.
738 VERBATIM_HEADERS = YES
740 #---------------------------------------------------------------------------
741 # configuration options related to the alphabetical class index
742 #---------------------------------------------------------------------------
744 # If the ALPHABETICAL_INDEX tag is set to YES, an alphabetical index
745 # of all compounds will be generated. Enable this if the project
746 # contains a lot of classes, structs, unions or interfaces.
748 ALPHABETICAL_INDEX = NO
750 # If the alphabetical index is enabled (see ALPHABETICAL_INDEX) then
751 # the COLS_IN_ALPHA_INDEX tag can be used to specify the number of columns
752 # in which this list will be split (can be a number in the range [1..20])
754 COLS_IN_ALPHA_INDEX = 5
756 # In case all classes in a project start with a common prefix, all
757 # classes will be put under the same header in the alphabetical index.
758 # The IGNORE_PREFIX tag can be used to specify one or more prefixes that
759 # should be ignored while generating the index headers.
761 IGNORE_PREFIX =
763 #---------------------------------------------------------------------------
764 # configuration options related to the HTML output
765 #---------------------------------------------------------------------------
767 # If the GENERATE_HTML tag is set to YES (the default) Doxygen will
768 # generate HTML output.
770 GENERATE_HTML = YES
772 # The HTML_OUTPUT tag is used to specify where the HTML docs will be put.
773 # If a relative path is entered the value of OUTPUT_DIRECTORY will be
774 # put in front of it. If left blank `html' will be used as the default path.
776 HTML_OUTPUT = html
778 # The HTML_FILE_EXTENSION tag can be used to specify the file extension for
779 # each generated HTML page (for example: .htm,.php,.asp). If it is left blank
780 # doxygen will generate files with .html extension.
782 HTML_FILE_EXTENSION = .html
784 # The HTML_HEADER tag can be used to specify a personal HTML header for
785 # each generated HTML page. If it is left blank doxygen will generate a
786 # standard header.
788 HTML_HEADER =
790 # The HTML_FOOTER tag can be used to specify a personal HTML footer for
791 # each generated HTML page. If it is left blank doxygen will generate a
792 # standard footer.
794 HTML_FOOTER =
796 # The HTML_STYLESHEET tag can be used to specify a user-defined cascading
797 # style sheet that is used by each HTML page. It can be used to
798 # fine-tune the look of the HTML output. If the tag is left blank doxygen
799 # will generate a default style sheet. Note that doxygen will try to copy
800 # the style sheet file to the HTML output directory, so don't put your own
801 # stylesheet in the HTML output directory as well, or it will be erased!
803 HTML_STYLESHEET =
805 # If the HTML_TIMESTAMP tag is set to YES then the footer of each generated HTML
806 # page will contain the date and time when the page was generated. Setting
807 # this to NO can help when comparing the output of multiple runs.
809 HTML_TIMESTAMP = YES
811 # If the HTML_ALIGN_MEMBERS tag is set to YES, the members of classes,
812 # files or namespaces will be aligned in HTML using tables. If set to
813 # NO a bullet list will be used.
815 HTML_ALIGN_MEMBERS = YES
817 # If the HTML_DYNAMIC_SECTIONS tag is set to YES then the generated HTML
818 # documentation will contain sections that can be hidden and shown after the
819 # page has loaded. For this to work a browser that supports
820 # JavaScript and DHTML is required (for instance Mozilla 1.0+, Firefox
821 # Netscape 6.0+, Internet explorer 5.0+, Konqueror, or Safari).
823 HTML_DYNAMIC_SECTIONS = NO
825 # If the GENERATE_DOCSET tag is set to YES, additional index files
826 # will be generated that can be used as input for Apple's Xcode 3
827 # integrated development environment, introduced with OSX 10.5 (Leopard).
828 # To create a documentation set, doxygen will generate a Makefile in the
829 # HTML output directory. Running make will produce the docset in that
830 # directory and running "make install" will install the docset in
831 # ~/Library/Developer/Shared/Documentation/DocSets so that Xcode will find
832 # it at startup.
833 # See http://developer.apple.com/tools/creatingdocsetswithdoxygen.html for more information.
835 GENERATE_DOCSET = NO
837 # When GENERATE_DOCSET tag is set to YES, this tag determines the name of the
838 # feed. A documentation feed provides an umbrella under which multiple
839 # documentation sets from a single provider (such as a company or product suite)
840 # can be grouped.
842 DOCSET_FEEDNAME = "Doxygen generated docs"
844 # When GENERATE_DOCSET tag is set to YES, this tag specifies a string that
845 # should uniquely identify the documentation set bundle. This should be a
846 # reverse domain-name style string, e.g. com.mycompany.MyDocSet. Doxygen
847 # will append .docset to the name.
849 DOCSET_BUNDLE_ID = org.doxygen.Project
851 # If the GENERATE_HTMLHELP tag is set to YES, additional index files
852 # will be generated that can be used as input for tools like the
853 # Microsoft HTML help workshop to generate a compiled HTML help file (.chm)
854 # of the generated HTML documentation.
856 GENERATE_HTMLHELP = NO
858 # If the GENERATE_HTMLHELP tag is set to YES, the CHM_FILE tag can
859 # be used to specify the file name of the resulting .chm file. You
860 # can add a path in front of the file if the result should not be
861 # written to the html output directory.
863 CHM_FILE =
865 # If the GENERATE_HTMLHELP tag is set to YES, the HHC_LOCATION tag can
866 # be used to specify the location (absolute path including file name) of
867 # the HTML help compiler (hhc.exe). If non-empty doxygen will try to run
868 # the HTML help compiler on the generated index.hhp.
870 HHC_LOCATION =
872 # If the GENERATE_HTMLHELP tag is set to YES, the GENERATE_CHI flag
873 # controls if a separate .chi index file is generated (YES) or that
874 # it should be included in the master .chm file (NO).
876 GENERATE_CHI = NO
878 # If the GENERATE_HTMLHELP tag is set to YES, the CHM_INDEX_ENCODING
879 # is used to encode HtmlHelp index (hhk), content (hhc) and project file
880 # content.
882 CHM_INDEX_ENCODING =
884 # If the GENERATE_HTMLHELP tag is set to YES, the BINARY_TOC flag
885 # controls whether a binary table of contents is generated (YES) or a
886 # normal table of contents (NO) in the .chm file.
888 BINARY_TOC = NO
890 # The TOC_EXPAND flag can be set to YES to add extra items for group members
891 # to the contents of the HTML help documentation and to the tree view.
893 TOC_EXPAND = NO
895 # If the GENERATE_QHP tag is set to YES and both QHP_NAMESPACE and QHP_VIRTUAL_FOLDER
896 # are set, an additional index file will be generated that can be used as input for
897 # Qt's qhelpgenerator to generate a Qt Compressed Help (.qch) of the generated
898 # HTML documentation.
900 GENERATE_QHP = NO
902 # If the QHG_LOCATION tag is specified, the QCH_FILE tag can
903 # be used to specify the file name of the resulting .qch file.
904 # The path specified is relative to the HTML output folder.
906 QCH_FILE =
908 # The QHP_NAMESPACE tag specifies the namespace to use when generating
909 # Qt Help Project output. For more information please see
910 # http://doc.trolltech.com/qthelpproject.html#namespace
912 QHP_NAMESPACE = org.doxygen.Project
914 # The QHP_VIRTUAL_FOLDER tag specifies the namespace to use when generating
915 # Qt Help Project output. For more information please see
916 # http://doc.trolltech.com/qthelpproject.html#virtual-folders
918 QHP_VIRTUAL_FOLDER = doc
920 # If QHP_CUST_FILTER_NAME is set, it specifies the name of a custom filter to add.
921 # For more information please see
922 # http://doc.trolltech.com/qthelpproject.html#custom-filters
924 QHP_CUST_FILTER_NAME =
926 # The QHP_CUST_FILT_ATTRS tag specifies the list of the attributes of the custom filter to add.For more information please see
927 # <a href="http://doc.trolltech.com/qthelpproject.html#custom-filters">Qt Help Project / Custom Filters</a>.
929 QHP_CUST_FILTER_ATTRS =
931 # The QHP_SECT_FILTER_ATTRS tag specifies the list of the attributes this project's
932 # filter section matches.
933 # <a href="http://doc.trolltech.com/qthelpproject.html#filter-attributes">Qt Help Project / Filter Attributes</a>.
935 QHP_SECT_FILTER_ATTRS =
937 # If the GENERATE_QHP tag is set to YES, the QHG_LOCATION tag can
938 # be used to specify the location of Qt's qhelpgenerator.
939 # If non-empty doxygen will try to run qhelpgenerator on the generated
940 # .qhp file.
942 QHG_LOCATION =
944 # If the GENERATE_ECLIPSEHELP tag is set to YES, additional index files
945 # will be generated, which together with the HTML files, form an Eclipse help
946 # plugin. To install this plugin and make it available under the help contents
947 # menu in Eclipse, the contents of the directory containing the HTML and XML
948 # files needs to be copied into the plugins directory of eclipse. The name of
949 # the directory within the plugins directory should be the same as
950 # the ECLIPSE_DOC_ID value. After copying Eclipse needs to be restarted before the help appears.
952 GENERATE_ECLIPSEHELP = NO
954 # A unique identifier for the eclipse help plugin. When installing the plugin
955 # the directory name containing the HTML and XML files should also have
956 # this name.
958 ECLIPSE_DOC_ID = org.doxygen.Project
960 # The DISABLE_INDEX tag can be used to turn on/off the condensed index at
961 # top of each HTML page. The value NO (the default) enables the index and
962 # the value YES disables it.
964 DISABLE_INDEX = NO
966 # This tag can be used to set the number of enum values (range [1..20])
967 # that doxygen will group on one line in the generated HTML documentation.
969 ENUM_VALUES_PER_LINE = 4
971 # The GENERATE_TREEVIEW tag is used to specify whether a tree-like index
972 # structure should be generated to display hierarchical information.
973 # If the tag value is set to YES, a side panel will be generated
974 # containing a tree-like index structure (just like the one that
975 # is generated for HTML Help). For this to work a browser that supports
976 # JavaScript, DHTML, CSS and frames is required (i.e. any modern browser).
977 # Windows users are probably better off using the HTML help feature.
979 GENERATE_TREEVIEW = NO
981 # By enabling USE_INLINE_TREES, doxygen will generate the Groups, Directories,
982 # and Class Hierarchy pages using a tree view instead of an ordered list.
984 USE_INLINE_TREES = NO
986 # If the treeview is enabled (see GENERATE_TREEVIEW) then this tag can be
987 # used to set the initial width (in pixels) of the frame in which the tree
988 # is shown.
990 TREEVIEW_WIDTH = 250
992 # Use this tag to change the font size of Latex formulas included
993 # as images in the HTML documentation. The default is 10. Note that
994 # when you change the font size after a successful doxygen run you need
995 # to manually remove any form_*.png images from the HTML output directory
996 # to force them to be regenerated.
998 FORMULA_FONTSIZE = 10
1000 # When the SEARCHENGINE tag is enabled doxygen will generate a search box for the HTML output. The underlying search engine uses javascript
1001 # and DHTML and should work on any modern browser. Note that when using HTML help (GENERATE_HTMLHELP), Qt help (GENERATE_QHP), or docsets (GENERATE_DOCSET) there is already a search function so this one should
1002 # typically be disabled. For large projects the javascript based search engine
1003 # can be slow, then enabling SERVER_BASED_SEARCH may provide a better solution.
1005 SEARCHENGINE = YES
1007 # When the SERVER_BASED_SEARCH tag is enabled the search engine will be implemented using a PHP enabled web server instead of at the web client using Javascript. Doxygen will generate the search PHP script and index
1008 # file to put on the web server. The advantage of the server based approach is that it scales better to large projects and allows full text search. The disadvances is that it is more difficult to setup
1009 # and does not have live searching capabilities.
1011 SERVER_BASED_SEARCH = NO
1013 #---------------------------------------------------------------------------
1014 # configuration options related to the LaTeX output
1015 #---------------------------------------------------------------------------
1017 # If the GENERATE_LATEX tag is set to YES (the default) Doxygen will
1018 # generate Latex output.
1020 GENERATE_LATEX = NO
1022 # The LATEX_OUTPUT tag is used to specify where the LaTeX docs will be put.
1023 # If a relative path is entered the value of OUTPUT_DIRECTORY will be
1024 # put in front of it. If left blank `latex' will be used as the default path.
1026 LATEX_OUTPUT = latex
1028 # The LATEX_CMD_NAME tag can be used to specify the LaTeX command name to be
1029 # invoked. If left blank `latex' will be used as the default command name.
1030 # Note that when enabling USE_PDFLATEX this option is only used for
1031 # generating bitmaps for formulas in the HTML output, but not in the
1032 # Makefile that is written to the output directory.
1034 LATEX_CMD_NAME = latex
1036 # The MAKEINDEX_CMD_NAME tag can be used to specify the command name to
1037 # generate index for LaTeX. If left blank `makeindex' will be used as the
1038 # default command name.
1040 MAKEINDEX_CMD_NAME = makeindex
1042 # If the COMPACT_LATEX tag is set to YES Doxygen generates more compact
1043 # LaTeX documents. This may be useful for small projects and may help to
1044 # save some trees in general.
1046 COMPACT_LATEX = NO
1048 # The PAPER_TYPE tag can be used to set the paper type that is used
1049 # by the printer. Possible values are: a4, a4wide, letter, legal and
1050 # executive. If left blank a4wide will be used.
1052 PAPER_TYPE = a4wide
1054 # The EXTRA_PACKAGES tag can be to specify one or more names of LaTeX
1055 # packages that should be included in the LaTeX output.
1057 EXTRA_PACKAGES =
1059 # The LATEX_HEADER tag can be used to specify a personal LaTeX header for
1060 # the generated latex document. The header should contain everything until
1061 # the first chapter. If it is left blank doxygen will generate a
1062 # standard header. Notice: only use this tag if you know what you are doing!
1064 LATEX_HEADER =
1066 # If the PDF_HYPERLINKS tag is set to YES, the LaTeX that is generated
1067 # is prepared for conversion to pdf (using ps2pdf). The pdf file will
1068 # contain links (just like the HTML output) instead of page references
1069 # This makes the output suitable for online browsing using a pdf viewer.
1071 PDF_HYPERLINKS = YES
1073 # If the USE_PDFLATEX tag is set to YES, pdflatex will be used instead of
1074 # plain latex in the generated Makefile. Set this option to YES to get a
1075 # higher quality PDF documentation.
1077 USE_PDFLATEX = YES
1079 # If the LATEX_BATCHMODE tag is set to YES, doxygen will add the \\batchmode.
1080 # command to the generated LaTeX files. This will instruct LaTeX to keep
1081 # running if errors occur, instead of asking the user for help.
1082 # This option is also used when generating formulas in HTML.
1084 LATEX_BATCHMODE = NO
1086 # If LATEX_HIDE_INDICES is set to YES then doxygen will not
1087 # include the index chapters (such as File Index, Compound Index, etc.)
1088 # in the output.
1090 LATEX_HIDE_INDICES = NO
1092 # If LATEX_SOURCE_CODE is set to YES then doxygen will include source code with syntax highlighting in the LaTeX output. Note that which sources are shown also depends on other settings such as SOURCE_BROWSER.
1094 LATEX_SOURCE_CODE = NO
1096 #---------------------------------------------------------------------------
1097 # configuration options related to the RTF output
1098 #---------------------------------------------------------------------------
1100 # If the GENERATE_RTF tag is set to YES Doxygen will generate RTF output
1101 # The RTF output is optimized for Word 97 and may not look very pretty with
1102 # other RTF readers or editors.
1104 GENERATE_RTF = NO
1106 # The RTF_OUTPUT tag is used to specify where the RTF docs will be put.
1107 # If a relative path is entered the value of OUTPUT_DIRECTORY will be
1108 # put in front of it. If left blank `rtf' will be used as the default path.
1110 RTF_OUTPUT = rtf
1112 # If the COMPACT_RTF tag is set to YES Doxygen generates more compact
1113 # RTF documents. This may be useful for small projects and may help to
1114 # save some trees in general.
1116 COMPACT_RTF = NO
1118 # If the RTF_HYPERLINKS tag is set to YES, the RTF that is generated
1119 # will contain hyperlink fields. The RTF file will
1120 # contain links (just like the HTML output) instead of page references.
1121 # This makes the output suitable for online browsing using WORD or other
1122 # programs which support those fields.
1123 # Note: wordpad (write) and others do not support links.
1125 RTF_HYPERLINKS = NO
1127 # Load stylesheet definitions from file. Syntax is similar to doxygen's
1128 # config file, i.e. a series of assignments. You only have to provide
1129 # replacements, missing definitions are set to their default value.
1131 RTF_STYLESHEET_FILE =
1133 # Set optional variables used in the generation of an rtf document.
1134 # Syntax is similar to doxygen's config file.
1136 RTF_EXTENSIONS_FILE =
1138 #---------------------------------------------------------------------------
1139 # configuration options related to the man page output
1140 #---------------------------------------------------------------------------
1142 # If the GENERATE_MAN tag is set to YES (the default) Doxygen will
1143 # generate man pages
1145 GENERATE_MAN = NO
1147 # The MAN_OUTPUT tag is used to specify where the man pages will be put.
1148 # If a relative path is entered the value of OUTPUT_DIRECTORY will be
1149 # put in front of it. If left blank `man' will be used as the default path.
1151 MAN_OUTPUT = man
1153 # The MAN_EXTENSION tag determines the extension that is added to
1154 # the generated man pages (default is the subroutine's section .3)
1156 MAN_EXTENSION = .3
1158 # If the MAN_LINKS tag is set to YES and Doxygen generates man output,
1159 # then it will generate one additional man file for each entity
1160 # documented in the real man page(s). These additional files
1161 # only source the real man page, but without them the man command
1162 # would be unable to find the correct page. The default is NO.
1164 MAN_LINKS = NO
1166 #---------------------------------------------------------------------------
1167 # configuration options related to the XML output
1168 #---------------------------------------------------------------------------
1170 # If the GENERATE_XML tag is set to YES Doxygen will
1171 # generate an XML file that captures the structure of
1172 # the code including all documentation.
1174 GENERATE_XML = NO
1176 # The XML_OUTPUT tag is used to specify where the XML pages will be put.
1177 # If a relative path is entered the value of OUTPUT_DIRECTORY will be
1178 # put in front of it. If left blank `xml' will be used as the default path.
1180 XML_OUTPUT = xml
1182 # The XML_SCHEMA tag can be used to specify an XML schema,
1183 # which can be used by a validating XML parser to check the
1184 # syntax of the XML files.
1186 XML_SCHEMA =
1188 # The XML_DTD tag can be used to specify an XML DTD,
1189 # which can be used by a validating XML parser to check the
1190 # syntax of the XML files.
1192 XML_DTD =
1194 # If the XML_PROGRAMLISTING tag is set to YES Doxygen will
1195 # dump the program listings (including syntax highlighting
1196 # and cross-referencing information) to the XML output. Note that
1197 # enabling this will significantly increase the size of the XML output.
1199 XML_PROGRAMLISTING = YES
1201 #---------------------------------------------------------------------------
1202 # configuration options for the AutoGen Definitions output
1203 #---------------------------------------------------------------------------
1205 # If the GENERATE_AUTOGEN_DEF tag is set to YES Doxygen will
1206 # generate an AutoGen Definitions (see autogen.sf.net) file
1207 # that captures the structure of the code including all
1208 # documentation. Note that this feature is still experimental
1209 # and incomplete at the moment.
1211 GENERATE_AUTOGEN_DEF = NO
1213 #---------------------------------------------------------------------------
1214 # configuration options related to the Perl module output
1215 #---------------------------------------------------------------------------
1217 # If the GENERATE_PERLMOD tag is set to YES Doxygen will
1218 # generate a Perl module file that captures the structure of
1219 # the code including all documentation. Note that this
1220 # feature is still experimental and incomplete at the
1221 # moment.
1223 GENERATE_PERLMOD = NO
1225 # If the PERLMOD_LATEX tag is set to YES Doxygen will generate
1226 # the necessary Makefile rules, Perl scripts and LaTeX code to be able
1227 # to generate PDF and DVI output from the Perl module output.
1229 PERLMOD_LATEX = NO
1231 # If the PERLMOD_PRETTY tag is set to YES the Perl module output will be
1232 # nicely formatted so it can be parsed by a human reader.
1233 # This is useful
1234 # if you want to understand what is going on.
1235 # On the other hand, if this
1236 # tag is set to NO the size of the Perl module output will be much smaller
1237 # and Perl will parse it just the same.
1239 PERLMOD_PRETTY = YES
1241 # The names of the make variables in the generated doxyrules.make file
1242 # are prefixed with the string contained in PERLMOD_MAKEVAR_PREFIX.
1243 # This is useful so different doxyrules.make files included by the same
1244 # Makefile don't overwrite each other's variables.
1246 PERLMOD_MAKEVAR_PREFIX =
1248 #---------------------------------------------------------------------------
1249 # Configuration options related to the preprocessor
1250 #---------------------------------------------------------------------------
1252 # If the ENABLE_PREPROCESSING tag is set to YES (the default) Doxygen will
1253 # evaluate all C-preprocessor directives found in the sources and include
1254 # files.
1256 ENABLE_PREPROCESSING = YES
1258 # If the MACRO_EXPANSION tag is set to YES Doxygen will expand all macro
1259 # names in the source code. If set to NO (the default) only conditional
1260 # compilation will be performed. Macro expansion can be done in a controlled
1261 # way by setting EXPAND_ONLY_PREDEF to YES.
1263 MACRO_EXPANSION = NO
1265 # If the EXPAND_ONLY_PREDEF and MACRO_EXPANSION tags are both set to YES
1266 # then the macro expansion is limited to the macros specified with the
1267 # PREDEFINED and EXPAND_AS_DEFINED tags.
1269 EXPAND_ONLY_PREDEF = NO
1271 # If the SEARCH_INCLUDES tag is set to YES (the default) the includes files
1272 # in the INCLUDE_PATH (see below) will be search if a #include is found.
1274 SEARCH_INCLUDES = YES
1276 # The INCLUDE_PATH tag can be used to specify one or more directories that
1277 # contain include files that are not input files but should be processed by
1278 # the preprocessor.
1280 INCLUDE_PATH =
1282 # You can use the INCLUDE_FILE_PATTERNS tag to specify one or more wildcard
1283 # patterns (like *.h and *.hpp) to filter out the header-files in the
1284 # directories. If left blank, the patterns specified with FILE_PATTERNS will
1285 # be used.
1287 INCLUDE_FILE_PATTERNS =
1289 # The PREDEFINED tag can be used to specify one or more macro names that
1290 # are defined before the preprocessor is started (similar to the -D option of
1291 # gcc). The argument of the tag is a list of macros of the form: name
1292 # or name=definition (no spaces). If the definition and the = are
1293 # omitted =1 is assumed. To prevent a macro definition from being
1294 # undefined via #undef or recursively expanded use the := operator
1295 # instead of the = operator.
1297 PREDEFINED =
1299 # If the MACRO_EXPANSION and EXPAND_ONLY_PREDEF tags are set to YES then
1300 # this tag can be used to specify a list of macro names that should be expanded.
1301 # The macro definition that is found in the sources will be used.
1302 # Use the PREDEFINED tag if you want to use a different macro definition.
1304 EXPAND_AS_DEFINED =
1306 # If the SKIP_FUNCTION_MACROS tag is set to YES (the default) then
1307 # doxygen's preprocessor will remove all function-like macros that are alone
1308 # on a line, have an all uppercase name, and do not end with a semicolon. Such
1309 # function macros are typically used for boiler-plate code, and will confuse
1310 # the parser if not removed.
1312 SKIP_FUNCTION_MACROS = YES
1314 #---------------------------------------------------------------------------
1315 # Configuration::additions related to external references
1316 #---------------------------------------------------------------------------
1318 # The TAGFILES option can be used to specify one or more tagfiles.
1319 # Optionally an initial location of the external documentation
1320 # can be added for each tagfile. The format of a tag file without
1321 # this location is as follows:
1322 #
1323 # TAGFILES = file1 file2 ...
1324 # Adding location for the tag files is done as follows:
1325 #
1326 # TAGFILES = file1=loc1 "file2 = loc2" ...
1327 # where "loc1" and "loc2" can be relative or absolute paths or
1328 # URLs. If a location is present for each tag, the installdox tool
1329 # does not have to be run to correct the links.
1330 # Note that each tag file must have a unique name
1331 # (where the name does NOT include the path)
1332 # If a tag file is not located in the directory in which doxygen
1333 # is run, you must also specify the path to the tagfile here.
1335 TAGFILES =
1337 # When a file name is specified after GENERATE_TAGFILE, doxygen will create
1338 # a tag file that is based on the input files it reads.
1340 GENERATE_TAGFILE = docs/dual_decode.tag
1342 # If the ALLEXTERNALS tag is set to YES all external classes will be listed
1343 # in the class index. If set to NO only the inherited external classes
1344 # will be listed.
1346 ALLEXTERNALS = NO
1348 # If the EXTERNAL_GROUPS tag is set to YES all external groups will be listed
1349 # in the modules index. If set to NO, only the current project's groups will
1350 # be listed.
1352 EXTERNAL_GROUPS = YES
1354 # The PERL_PATH should be the absolute path and name of the perl script
1355 # interpreter (i.e. the result of `which perl').
1357 PERL_PATH = /usr/bin/perl
1359 #---------------------------------------------------------------------------
1360 # Configuration options related to the dot tool
1361 #---------------------------------------------------------------------------
1363 # If the CLASS_DIAGRAMS tag is set to YES (the default) Doxygen will
1364 # generate a inheritance diagram (in HTML, RTF and LaTeX) for classes with base
1365 # or super classes. Setting the tag to NO turns the diagrams off. Note that
1366 # this option is superseded by the HAVE_DOT option below. This is only a
1367 # fallback. It is recommended to install and use dot, since it yields more
1368 # powerful graphs.
1370 CLASS_DIAGRAMS = YES
1372 # You can define message sequence charts within doxygen comments using the \msc
1373 # command. Doxygen will then run the mscgen tool (see
1374 # http://www.mcternan.me.uk/mscgen/) to produce the chart and insert it in the
1375 # documentation. The MSCGEN_PATH tag allows you to specify the directory where
1376 # the mscgen tool resides. If left empty the tool is assumed to be found in the
1377 # default search path.
1379 MSCGEN_PATH =
1381 # If set to YES, the inheritance and collaboration graphs will hide
1382 # inheritance and usage relations if the target is undocumented
1383 # or is not a class.
1385 HIDE_UNDOC_RELATIONS = YES
1387 # If you set the HAVE_DOT tag to YES then doxygen will assume the dot tool is
1388 # available from the path. This tool is part of Graphviz, a graph visualization
1389 # toolkit from AT&T and Lucent Bell Labs. The other options in this section
1390 # have no effect if this option is set to NO (the default)
1392 HAVE_DOT = NO
1394 # By default doxygen will write a font called FreeSans.ttf to the output
1395 # directory and reference it in all dot files that doxygen generates. This
1396 # font does not include all possible unicode characters however, so when you need
1397 # these (or just want a differently looking font) you can specify the font name
1398 # using DOT_FONTNAME. You need need to make sure dot is able to find the font,
1399 # which can be done by putting it in a standard location or by setting the
1400 # DOTFONTPATH environment variable or by setting DOT_FONTPATH to the directory
1401 # containing the font.
1403 DOT_FONTNAME = FreeSans
1405 # The DOT_FONTSIZE tag can be used to set the size of the font of dot graphs.
1406 # The default size is 10pt.
1408 DOT_FONTSIZE = 10
1410 # By default doxygen will tell dot to use the output directory to look for the
1411 # FreeSans.ttf font (which doxygen will put there itself). If you specify a
1412 # different font using DOT_FONTNAME you can set the path where dot
1413 # can find it using this tag.
1415 DOT_FONTPATH =
1417 # If the CLASS_GRAPH and HAVE_DOT tags are set to YES then doxygen
1418 # will generate a graph for each documented class showing the direct and
1419 # indirect inheritance relations. Setting this tag to YES will force the
1420 # the CLASS_DIAGRAMS tag to NO.
1422 CLASS_GRAPH = YES
1424 # If the COLLABORATION_GRAPH and HAVE_DOT tags are set to YES then doxygen
1425 # will generate a graph for each documented class showing the direct and
1426 # indirect implementation dependencies (inheritance, containment, and
1427 # class references variables) of the class with other documented classes.
1429 COLLABORATION_GRAPH = YES
1431 # If the GROUP_GRAPHS and HAVE_DOT tags are set to YES then doxygen
1432 # will generate a graph for groups, showing the direct groups dependencies
1434 GROUP_GRAPHS = YES
1436 # If the UML_LOOK tag is set to YES doxygen will generate inheritance and
1437 # collaboration diagrams in a style similar to the OMG's Unified Modeling
1438 # Language.
1440 UML_LOOK = NO
1442 # If set to YES, the inheritance and collaboration graphs will show the
1443 # relations between templates and their instances.
1445 TEMPLATE_RELATIONS = NO
1447 # If the ENABLE_PREPROCESSING, SEARCH_INCLUDES, INCLUDE_GRAPH, and HAVE_DOT
1448 # tags are set to YES then doxygen will generate a graph for each documented
1449 # file showing the direct and indirect include dependencies of the file with
1450 # other documented files.
1452 INCLUDE_GRAPH = YES
1454 # If the ENABLE_PREPROCESSING, SEARCH_INCLUDES, INCLUDED_BY_GRAPH, and
1455 # HAVE_DOT tags are set to YES then doxygen will generate a graph for each
1456 # documented header file showing the documented files that directly or
1457 # indirectly include this file.
1459 INCLUDED_BY_GRAPH = YES
1461 # If the CALL_GRAPH and HAVE_DOT options are set to YES then
1462 # doxygen will generate a call dependency graph for every global function
1463 # or class method. Note that enabling this option will significantly increase
1464 # the time of a run. So in most cases it will be better to enable call graphs
1465 # for selected functions only using the \callgraph command.
1467 CALL_GRAPH = NO
1469 # If the CALLER_GRAPH and HAVE_DOT tags are set to YES then
1470 # doxygen will generate a caller dependency graph for every global function
1471 # or class method. Note that enabling this option will significantly increase
1472 # the time of a run. So in most cases it will be better to enable caller
1473 # graphs for selected functions only using the \callergraph command.
1475 CALLER_GRAPH = NO
1477 # If the GRAPHICAL_HIERARCHY and HAVE_DOT tags are set to YES then doxygen
1478 # will graphical hierarchy of all classes instead of a textual one.
1480 GRAPHICAL_HIERARCHY = YES
1482 # If the DIRECTORY_GRAPH, SHOW_DIRECTORIES and HAVE_DOT tags are set to YES
1483 # then doxygen will show the dependencies a directory has on other directories
1484 # in a graphical way. The dependency relations are determined by the #include
1485 # relations between the files in the directories.
1487 DIRECTORY_GRAPH = YES
1489 # The DOT_IMAGE_FORMAT tag can be used to set the image format of the images
1490 # generated by dot. Possible values are png, jpg, or gif
1491 # If left blank png will be used.
1493 DOT_IMAGE_FORMAT = png
1495 # The tag DOT_PATH can be used to specify the path where the dot tool can be
1496 # found. If left blank, it is assumed the dot tool can be found in the path.
1498 DOT_PATH =
1500 # The DOTFILE_DIRS tag can be used to specify one or more directories that
1501 # contain dot files that are included in the documentation (see the
1502 # \dotfile command).
1504 DOTFILE_DIRS =
1506 # The DOT_GRAPH_MAX_NODES tag can be used to set the maximum number of
1507 # nodes that will be shown in the graph. If the number of nodes in a graph
1508 # becomes larger than this value, doxygen will truncate the graph, which is
1509 # visualized by representing a node as a red box. Note that doxygen if the
1510 # number of direct children of the root node in a graph is already larger than
1511 # DOT_GRAPH_MAX_NODES then the graph will not be shown at all. Also note
1512 # that the size of a graph can be further restricted by MAX_DOT_GRAPH_DEPTH.
1514 DOT_GRAPH_MAX_NODES = 50
1516 # The MAX_DOT_GRAPH_DEPTH tag can be used to set the maximum depth of the
1517 # graphs generated by dot. A depth value of 3 means that only nodes reachable
1518 # from the root by following a path via at most 3 edges will be shown. Nodes
1519 # that lay further from the root node will be omitted. Note that setting this
1520 # option to 1 or 2 may greatly reduce the computation time needed for large
1521 # code bases. Also note that the size of a graph can be further restricted by
1522 # DOT_GRAPH_MAX_NODES. Using a depth of 0 means no depth restriction.
1524 MAX_DOT_GRAPH_DEPTH = 0
1526 # Set the DOT_TRANSPARENT tag to YES to generate images with a transparent
1527 # background. This is disabled by default, because dot on Windows does not
1528 # seem to support this out of the box. Warning: Depending on the platform used,
1529 # enabling this option may lead to badly anti-aliased labels on the edges of
1530 # a graph (i.e. they become hard to read).
1532 DOT_TRANSPARENT = NO
1534 # Set the DOT_MULTI_TARGETS tag to YES allow dot to generate multiple output
1535 # files in one run (i.e. multiple -o and -T options on the command line). This
1536 # makes dot run faster, but since only newer versions of dot (>1.8.10)
1537 # support this, this feature is disabled by default.
1539 DOT_MULTI_TARGETS = YES
1541 # If the GENERATE_LEGEND tag is set to YES (the default) Doxygen will
1542 # generate a legend page explaining the meaning of the various boxes and
1543 # arrows in the dot generated graphs.
1545 GENERATE_LEGEND = YES
1547 # If the DOT_CLEANUP tag is set to YES (the default) Doxygen will
1548 # remove the intermediate dot files that are used to generate
1549 # the various graphs.
1551 DOT_CLEANUP = YES