arm: Remove unused relocate_code() parameters Commit e05e5de7fae5bec79617e113916dac6631251156 made the 2 1st parameters of ARM's relocate_code() useless since it moved the code handling them to crt0.S. So, drop these parameters. Signed-off-by: Benoît Thébaudeau <benoit.thebaudeau@advansee.com>
arm: relocate_code(): Use __image_copy_end for end of relocation Use __image_copy_end instead of __bss_start for the end of the image to relocate. This is the same as commit 033ca72, but applied to all ARM start.S. This is a more appropriate symbol naming for an image copy & relocate feature, and this also saves a useless copy of data put between __image_copy_end and __bss_start in linker scripts (e.g. relocation information, or MMU initialization tables used only before jumping to the relocated image). Signed-off-by: Benoît Thébaudeau <benoit.thebaudeau@advansee.com>
arm: relocate_code(): Remove useless relocation offset computation Signed-off-by: Benoît Thébaudeau <benoit.thebaudeau@advansee.com>
arm: relocate_code() is no longer noreturn Commit e05e5de7fae5bec79617e113916dac6631251156 made ARM's relocate_code() return to its caller, but it did not update its declaration accordingly. Fixing this function declaration fixes dropped C code following calls to relocate_code(). Signed-off-by: Benoît Thébaudeau <benoit.thebaudeau@advansee.com>
arm: start.S: Fix _TEXT_BASE for SPL _TEXT_BASE must be set to CONFIG_SPL_TEXT_BASE for generic SPL, and to CONFIG_SYS_TEXT_BASE for non-SPL builds. Signed-off-by: Benoît Thébaudeau <benoit.thebaudeau@advansee.com> Reviewed-by: Tom Rini <trini@ti.com>
Replace __bss_end__ with __bss_end Note this is a tree-wide change affecting multiple architectures. At present we use __bss_start, but mostly __bss_end__. This seems inconsistent and in a number of places __bss_end is used instead. Change to use __bss_end for the BSS end symbol throughout U-Boot. This makes it possible to use the asm-generic/sections.h file on all archs. Signed-off-by: Simon Glass <sjg@chromium.org>
arm: remove useless code in start.S files Remove code such as unneeded includes or labels. These removals have no functional effect. Signed-off-by: Albert ARIBAUD <albert.u.boot@aribaud.net>
arm: move C runtime setup code in crt0.S Move all the C runtime setup code from every start.S in arch/arm into arch/arm/lib/crt0.S. This covers the code sequence from setting up the initial stack to calling into board_init_r(). Also, rewrite the C runtime setup and make functions board_init_*() and relocate_code() behave according to normal C semantics (no jumping across the C stack any more, etc). Some SPL targets had to be touched because they use start.S explicitly or for some reason; the relevant maintainers and custodians are cc:ed. Signed-off-by: Albert ARIBAUD <albert.u.boot@aribaud.net>
arm: Fixed the offset for the no relocation. When the u-boot address of destination equal to __start, no relocation. relocation offset(r9) = 0. Signed-off-by: Zhong Hongbo <bocui107@gmail.com> Tested-by: Stefano Babic <sbabic@denx.de>
arm: Fix to mistake clean the memory space In currently, when __bss_start is equal to __bss_end__, The bss loop will clear all the things in memory space. But just only when __bss_end__ greater than __bss_start__, we do the clear bss section operation. Signed-off-by: Zhong Hongbo <bocui107@gmail.com> Acked-by: Andreas Bießmann <andreas.devel@googlemail.com>
led: remove camel casing of led identifiers globally Result of running the following command to address Wolfgang's comment about camel case: for file in `find . | grep '\.[chS]$'`; do perl -i -pe 's/(green|yellow|red|blue)_LED_(on|off)/$1_led_$2/g' $file; done Discussion: http://patchwork.ozlabs.org/patch/84988/ Signed-off-by: Jason Kridner <jkridner@beagleboard.org> Signed-off-by: Joel A Fernandes <agnel.joel@gmail.com> Signed-off-by: Sandeep Paulraj <s-paulraj@ti.com>
Convert ISO-8859 files to UTF-8 There was a mix of UTF-8 and ISO-8859 files in the U-Boot source tree, which could cause issues with the patchwork review system. This commit converts all ISO-8859 files to UTF-8. Signed-off-by: Albert ARIBAUD <albert.u.boot@aribaud.net>
replace CONFIG_PRELOADER with CONFIG_SPL_BUILD replace all occurences of CONFIG_PRELOADER with CONFIG_SPL_BUILD Signed-off-by: Aneesh V <aneesh@ti.com>
arm: fix incorrect monitor protection region in FLASH Monitor protection region in FLASH did not cover .rel.dyn and .dynsym sections, because it uses __bss_start to compute monitor_flash_len. Use _end instead. Add _end to linker scripts for end of u-boot image Add _end_ofs to all the start.S. Signed-off-by: Po-Yu Chuang <ratbert@faraday-tech.com>
rename _end to __bss_end__ Currently, _end is used for end of BSS section. We want _end to mean end of u-boot image, so we rename _end to __bss_end__ first. Signed-off-by: Po-Yu Chuang <ratbert@faraday-tech.com>
ARM: */start.S: code cleanup Remove the useless code from start.S Signed-off-by: Jason Liu <r64343@freescale.com> Tested-by: Andreas Bießmann <andreas.devel@googlemail.com>
ARM: */start.S: use canonical asm syntax Make code build with older tool chains. Signed-off-by: Wolfgang Denk <wd@denx.de>
arm: fixloop(): do not use r8 for relocation r8 is used for global_data and should therefore be left alone! For C code the compiler flag --fixed-r8 does the job, but in assembler we need to be aware of that fact. Signed-off-by: Andreas Bießmann <andreas.devel@googlemail.com>
arm: relocate_code(): do not set register useless In case we are still at relocation target address before relocation we do not need to load the registers needed for relocation. We should instead skip the whole relocation part and jump over to clear_bss immediately. Signed-off-by: Andreas Bießmann <andreas.devel@googlemail.com>
arm: copy_loop(): use scratch register This patch uses r1 as scratch register for copy_loop(). Therefore we do not longer need r7 for the storage of relocate_code()'s 'addr_moni' (the destination address of relocation). Therefore r7 can be used later on for other purposes. Signed-off-by: Andreas Bießmann <andreas.devel@googlemail.com>