ARM: OMAP4/5: Make OMAPx_SRAM_SCRATCH_ defines common These defines are same across OMAP4/5. So move them to omap_common.h. This is required for the patches that follow. Signed-off-by: Sricharan R <r.sricharan@ti.com>
arm: omap4: Fix SDRAM AUTO DETECTION Commit "8602114 omap: emif: configure emif only when required" breaks SDRAM_AUTO_DETECTION. The issue is dmm_init() depends on emif_sizes[](SDRAM Auto detection) done in do_sdram_init(). The above commit moves dmm_init() above do_sdram_init() because of which dmm_init() uses uninitialized emif_sizes[]. So instead of using global emif_sizes[], get sdram details locally and calculate emif sizes. Reported-by: Michael Cashwell <mboards@prograde.net> Signed-off-by: Lokesh Vutla <lokeshvutla@ti.com>
omap5: emif: Add emif/ddr configurations required for omap5 evm Add the emif configurations required for omap5 soc.Add the correct ddr part configurations required for omap5 evm board. EDB8164B3PH from ELPIDA is the part used on the board. Also changes are done to retain some part of the code common for OMAP4/5 and keep only the remaining in the Soc specific directories. Signed-off-by: sricharan <r.sricharan@ti.com> Signed-off-by: Sandeep Paulraj <s-paulraj@ti.com>
omap4: make omap4 code common for future reuse Much of omap4 soc support code can be reused for omap5. Move them to the omap-common directory to facilitate this. Signed-off-by: sricharan <r.sricharan@ti.com> Signed-off-by: Sandeep Paulraj <s-paulraj@ti.com>
omap4: IO settings Tuning some IO settings for better performance and power. And consolidate all such IO settings at one place. Signed-off-by: Aneesh V <aneesh@ti.com> Signed-off-by: Sandeep Paulraj <s-paulraj@ti.com>
omap4: make SDRAM init work for ES1.0 silicon SDRAM init was not working on ES1.0 due to a programming error. A pointer that was passed by value to a function was set in function emif_get_device_details(), but the effect wouldn't be seen in the calling function. The issue came out while testing for ES1.0 because ES1.0 doesn't have any SDRAM chips connected to CS1 Signed-off-by: Aneesh V <aneesh@ti.com> Signed-off-by: Sandeep Paulraj <s-paulraj@ti.com>
omap4: sdram init changes for omap4460 Signed-off-by: Aneesh V <aneesh@ti.com> Signed-off-by: Sandeep Paulraj <s-paulraj@ti.com>
omap4: automatic sdram detection Identify SDRAM devices connected to EMIF automatically: LPDDR2 devices have some Mode Registers that provide details about the device such as the type, density, bus width etc. EMIF has the capability to read these registers. If there are no devices connected to a given chip-select reading mode registers will return junk values. After reading as many such registers as possible and matching with expected ranges of values the driver can identify if there is a device connected to the respective CS. If we identify that a device is connected the values read give us complete details about the device. This along with the base AC timings specified by JESD209-2 allows us to do a complete automatic initialization of SDRAM that works on all boards. Please note that the default AC timings specified by JESD209-2 will be safe for all devices but not necessarily optimal. However, for the Elpida devices used on Panda and SDP the default timings are both safe and optimal. Signed-off-by: Aneesh V <aneesh@ti.com> Signed-off-by: Sandeep Paulraj <s-paulraj@ti.com>
omap4: calculate EMIF register values Calculate EMIF register values based on AC timing parameters from the SDRAM datasheet and the DDR frequency rather than using the hard-coded values. For a new board the user doen't have to go through the tedious process of calculating the register values. Instead, just provide the AC timings from the device data sheet as input and the driver will automatically calculate the register values. Signed-off-by: Aneesh V <aneesh@ti.com> Signed-off-by: Sandeep Paulraj <s-paulraj@ti.com>
omap4: add sdram init support Add support for the SDRAM controller (EMIF). Signed-off-by: Aneesh V <aneesh@ti.com> Signed-off-by: Sandeep Paulraj <s-paulraj@ti.com>