ARM: DRA7xx: EMIF: Change settings required for EVM board DRA7 EVM board has the below configuration. Adding the settings for the same here. 2Gb_1_35V_DDR3L part * 2 on EMIF1 2Gb_1_35V_DDR3L part * 4 on EMIF2 Signed-off-by: Sricharan R <r.sricharan@ti.com> Signed-off-by: Lokesh Vutla <lokeshvutla@ti.com>
ARM: DRA7xx: Do not enable srcomp for DRA7xx Soc's Slew rate compensation cells are not present for DRA7xx Soc's. So return from function srcomp_enable() if soc is not OMAP54xx. Signed-off-by: Lokesh Vutla <lokeshvutla@ti.com>
ARM: OMAP4/5: Make OMAPx_SRAM_SCRATCH_ defines common These defines are same across OMAP4/5. So move them to omap_common.h. This is required for the patches that follow. Signed-off-by: Sricharan R <r.sricharan@ti.com>
ARM: OMAP5: Fix warm reset with USB cable connected Warm reset on OMAP5 freezes when USB cable is connected. Fix requires PRM_RSTTIME.RSTTIME1 to be programmed with the time for which reset should be held low for the voltages and the oscillator to reach stable state. There are 3 parameters to be considered for calculating the time, which are mostly board and PMIC dependent. -1- Time taken by the Oscillator to shut + restart -2- PMIC OTP times -3- Voltage rail ramp times, which inturn depends on the PMIC slew rate and value of the voltage ramp needed. In order to keep the code in u-boot simple, have a way for boards to specify a pre computed time directly using the 'CONFIG_OMAP_PLATFORM_RESET_TIME_MAX_USEC' option. If boards fail to specify the time, use a default as specified by 'CONFIG_DEFAULT_OMAP_RESET_TIME_MAX_USEC' instead. Using the default value translates into some ~22ms and should work in all cases. However in order to avoid this large delay hiding other bugs, its recommended that all boards look at their respective data sheets and specify a pre computed and optimal value using 'CONFIG_OMAP_PLATFORM_RESET_TIME_MAX_USEC' In order to help future board additions to compute this config option value, add a README at doc/README.omap-reset-time which explains how to compute the value. Also update the toplevel README with the additional option and pointers to doc/README.omap-reset-time. Signed-off-by: Lokesh Vutla <lokeshvutla@ti.com> [rnayak@ti.com: Updated changelog and added the README] Signed-off-by: Rajendra Nayak <rnayak@ti.com>
arm: dra7xx: Add silicon id support for DRA752 soc Adding CPU detection support for the DRA752 ES1.0 soc. Signed-off-by: Lokesh Vutla <lokeshvutla@ti.com> Signed-off-by: R Sricharan <r.sricharan@ti.com> Reviewed-by: Tom Rini <trini@ti.com>
arm: dra7xx: clock: Add the prcm changes PRCM register addresses are changed from OMAP5 ES2.0 to DRA7XX. So adding the necessary register changes for DRA7XX socs. Signed-off-by: Lokesh Vutla <lokeshvutla@ti.com> Signed-off-by: R Sricharan <r.sricharan@ti.com>
ARM: OMAP5: srcomp: enable slew rate compensation cells after powerup After power-up SRCOMP cells are by-passed by default in OMAP5. Software has to enable these SRCOMP sells. For ES2: All 5 SRCOMP cells needs to be enabled. For ES1: Only 4 SRCOMP cells in core power domain are enabled. The 1 in wkup domain is not enabled because smart i/os of wkup domain work with default compensation code. Signed-off-by: R Sricharan <r.sricharan@ti.com> Signed-off-by: Lokesh Vutla <lokeshvutla@ti.com> Reviewed-by: Tom Rini <trini@ti.com> Cc: Tom Rini <trini@ti.com>
ARM: OMAP5: Add silicon id support for ES2.0 revision. Adding the CPU detection suport for OMAP5430 and OMAP5432 ES2.0 SOCs. Signed-off-by: R Sricharan <r.sricharan@ti.com> Cc: Tom Rini <trini@ti.com> Cc: Nishanth Menon <nm@ti.com>
ARM: OMAP5: Clean up iosettings code There is some code duplication in the ddr io settings code. This is avoided by moving the data to a Soc specific place and letting the code generic. This avoids unnessecary code addition for future socs. Signed-off-by: Lokesh Vutla <lokeshvutla@ti.com> Reviewed-by: Tom Rini <trini@ti.com>
ARM: OMAP4+: Make control module register structure generic A seperate omap_sys_ctrl_regs structure is defined for omap4 & 5. If there is any change in control module for any of the ES versions, a new structure needs to be created. In order to remove this dependency, making the register structure generic for all the omap4+ boards. Signed-off-by: R Sricharan <r.sricharan@ti.com> Signed-off-by: Lokesh Vutla <lokeshvutla@ti.com> Reviewed-by: Tom Rini <trini@ti.com>
ARM: OMAP4+: emif: Detect SDRAM from SDRAM config register Now SDRAM initialization is done on the basis of omap revision. Instead this should be done on basis of SDRAM type read from EMIF_SDRAM_CONFIG register. This will be helpful to avoid unnessecary cpu checks for new boards Signed-off-by: R Sricharan <r.sricharan@ti.com> Signed-off-by: Lokesh Vutla <lokeshvutla@ti.com> Reviewed-by: Tom Rini <trini@ti.com>
OMAP5: EMIF: Add support for DDR3 device In OMAP5432 EMIF controlller supports DDR3 device. This patch adds support for ddr3 device intialization and configuration. Initialization sequence is done as specified in JEDEC specs. This also adds support for ddr3 leveling. Signed-off-by: Lokesh Vutla <lokeshvutla@ti.com>
OMAP5: Configure the io settings for omap5432 uevm board This patch adds the IO settings required for OMAP5432 uevm's DDR3 pads Signed-off-by: Lokesh Vutla <lokeshvutla@ti.com>
OMAP5: ADD chip detection for OMAP5432 SOC This patch adds chip detection for OMAP5432 Signed-off-by: Lokesh Vutla <lokeshvutla@ti.com>
OMAP5: reset: Use cold reset in case of 5430ES1.0 Warm reset is not functional in case of omap5430ES1.0. So override the weak reset_cpu function to use cold reset instead. Signed-off-by: R Sricharan <r.sricharan@ti.com>
OMAP4/5: Make the sysctrl structure common Make the sysctrl structure common, so that it can be used in generic functions across socs. Also change the base address of the system control module, to include all the registers and not simply the io regs. Signed-off-by: R Sricharan <r.sricharan@ti.com>
OMAP4/5: Make the silicon revision variable common. The different silicon revision variable names was defined for OMAP4 and OMAP5 socs. Making the variable common so that some code can be made generic. Signed-off-by: R Sricharan <r.sricharan@ti.com>
OMAP5: hwinit: Add the missing break statement The break statement is missing in init_omap_revision function, resulting in a wrong revision identification. So fixing this. Signed-off-by: R Sricharan <r.sricharan@ti.com>
OMAP5: io: Configure the io settings for omap5430 sevm board. The control module provides options to set various signal integrity parameters like the output impedance, slew rate, load capacitance for different pad groups. Configure these as required for the omap5430 sevm board. Signed-off-by: R Sricharan <r.sricharan@ti.com>
omap5: Add minimal support for omap5430. This patch adds the minimal support for OMAP5. The platform and machine specific headers and sources updated for OMAP5430. OMAP5430 is Texas Instrument's SOC based on ARM Cortex-A15 SMP architecture. It's a dual core SOC with GIC used for interrupt handling and SCU for cache coherency. Also moved some part of code from the basic platform support that can be made common for OMAP4/5. Rest is kept out seperately. The same approach is followed for clocks and emif support in the subsequent patches. Signed-off-by: sricharan <r.sricharan@ti.com> Signed-off-by: Sandeep Paulraj <s-paulraj@ti.com>