1 #
2 # (C) Copyright 2000-2012
3 # Wolfgang Denk, DENX Software Engineering, wd@denx.de.
4 #
5 # See file CREDITS for list of people who contributed to this
6 # project.
7 #
8 # This program is free software; you can redistribute it and/or
9 # modify it under the terms of the GNU General Public License as
10 # published by the Free Software Foundatio; either version 2 of
11 # the License, or (at your option) any later version.
12 #
13 # This program is distributed in the hope that it will be useful,
14 # but WITHOUT ANY WARRANTY; without even the implied warranty of
15 # MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
16 # GNU General Public License for more details.
17 #
18 # You should have received a copy of the GNU General Public License
19 # along with this program; if not, write to the Free Software
20 # Foundation, Inc., 59 Temple Place, Suite 330, Boston,
21 # MA 02111-1307 USA
22 #
24 VERSION = 2013
25 PATCHLEVEL = 04
26 SUBLEVEL =
27 EXTRAVERSION = -rc1
28 ifneq "$(SUBLEVEL)" ""
29 U_BOOT_VERSION = $(VERSION).$(PATCHLEVEL).$(SUBLEVEL)$(EXTRAVERSION)
30 else
31 U_BOOT_VERSION = $(VERSION).$(PATCHLEVEL)$(EXTRAVERSION)
32 endif
33 TIMESTAMP_FILE = $(obj)include/generated/timestamp_autogenerated.h
34 VERSION_FILE = $(obj)include/generated/version_autogenerated.h
36 HOSTARCH := $(shell uname -m | \
37 sed -e s/i.86/x86/ \
38 -e s/sun4u/sparc64/ \
39 -e s/arm.*/arm/ \
40 -e s/sa110/arm/ \
41 -e s/ppc64/powerpc/ \
42 -e s/ppc/powerpc/ \
43 -e s/macppc/powerpc/\
44 -e s/sh.*/sh/)
46 HOSTOS := $(shell uname -s | tr '[:upper:]' '[:lower:]' | \
47 sed -e 's/\(cygwin\).*/cygwin/')
49 export HOSTARCH HOSTOS
51 # Deal with colliding definitions from tcsh etc.
52 VENDOR=
54 #########################################################################
55 # Allow for silent builds
56 ifeq (,$(findstring s,$(MAKEFLAGS)))
57 XECHO = echo
58 else
59 XECHO = :
60 endif
62 #########################################################################
63 #
64 # U-boot build supports producing a object files to the separate external
65 # directory. Two use cases are supported:
66 #
67 # 1) Add O= to the make command line
68 # 'make O=/tmp/build all'
69 #
70 # 2) Set environement variable BUILD_DIR to point to the desired location
71 # 'export BUILD_DIR=/tmp/build'
72 # 'make'
73 #
74 # The second approach can also be used with a MAKEALL script
75 # 'export BUILD_DIR=/tmp/build'
76 # './MAKEALL'
77 #
78 # Command line 'O=' setting overrides BUILD_DIR environent variable.
79 #
80 # When none of the above methods is used the local build is performed and
81 # the object files are placed in the source directory.
82 #
84 ifdef O
85 ifeq ("$(origin O)", "command line")
86 BUILD_DIR := $(O)
87 endif
88 endif
90 # Call a source code checker (by default, "sparse") as part of the
91 # C compilation.
92 #
93 # Use 'make C=1' to enable checking of re-compiled files.
94 #
95 # See the linux kernel file "Documentation/sparse.txt" for more details,
96 # including where to get the "sparse" utility.
98 ifdef C
99 ifeq ("$(origin C)", "command line")
100 CHECKSRC := $(C)
101 endif
102 endif
103 ifndef CHECKSRC
104 CHECKSRC = 0
105 endif
106 export CHECKSRC
108 ifneq ($(BUILD_DIR),)
109 saved-output := $(BUILD_DIR)
111 # Attempt to create a output directory.
112 $(shell [ -d ${BUILD_DIR} ] || mkdir -p ${BUILD_DIR})
114 # Verify if it was successful.
115 BUILD_DIR := $(shell cd $(BUILD_DIR) && /bin/pwd)
116 $(if $(BUILD_DIR),,$(error output directory "$(saved-output)" does not exist))
117 endif # ifneq ($(BUILD_DIR),)
119 OBJTREE := $(if $(BUILD_DIR),$(BUILD_DIR),$(CURDIR))
120 SPLTREE := $(OBJTREE)/spl
121 SRCTREE := $(CURDIR)
122 TOPDIR := $(SRCTREE)
123 LNDIR := $(OBJTREE)
124 export TOPDIR SRCTREE OBJTREE SPLTREE
126 MKCONFIG := $(SRCTREE)/mkconfig
127 export MKCONFIG
129 ifneq ($(OBJTREE),$(SRCTREE))
130 REMOTE_BUILD := 1
131 export REMOTE_BUILD
132 endif
134 # $(obj) and (src) are defined in config.mk but here in main Makefile
135 # we also need them before config.mk is included which is the case for
136 # some targets like unconfig, clean, clobber, distclean, etc.
137 ifneq ($(OBJTREE),$(SRCTREE))
138 obj := $(OBJTREE)/
139 src := $(SRCTREE)/
140 else
141 obj :=
142 src :=
143 endif
144 export obj src
146 # Make sure CDPATH settings don't interfere
147 unexport CDPATH
149 #########################################################################
151 # The "tools" are needed early, so put this first
152 # Don't include stuff already done in $(LIBS)
153 # The "examples" conditionally depend on U-Boot (say, when USE_PRIVATE_LIBGCC
154 # is "yes"), so compile examples after U-Boot is compiled.
155 SUBDIR_TOOLS = tools
156 SUBDIR_EXAMPLES = examples/standalone examples/api
157 SUBDIRS = $(SUBDIR_TOOLS)
159 .PHONY : $(SUBDIRS) $(VERSION_FILE) $(TIMESTAMP_FILE)
161 ifeq ($(obj)include/config.mk,$(wildcard $(obj)include/config.mk))
163 # Include autoconf.mk before config.mk so that the config options are available
164 # to all top level build files. We need the dummy all: target to prevent the
165 # dependency target in autoconf.mk.dep from being the default.
166 all:
167 sinclude $(obj)include/autoconf.mk.dep
168 sinclude $(obj)include/autoconf.mk
170 ifndef CONFIG_SANDBOX
171 SUBDIRS += $(SUBDIR_EXAMPLES)
172 endif
174 # load ARCH, BOARD, and CPU configuration
175 include $(obj)include/config.mk
176 export ARCH CPU BOARD VENDOR SOC
178 # set default to nothing for native builds
179 ifeq ($(HOSTARCH),$(ARCH))
180 CROSS_COMPILE ?=
181 endif
183 # load other configuration
184 include $(TOPDIR)/config.mk
186 # If board code explicitly specified LDSCRIPT or CONFIG_SYS_LDSCRIPT, use
187 # that (or fail if absent). Otherwise, search for a linker script in a
188 # standard location.
190 LDSCRIPT_MAKEFILE_DIR = $(dir $(LDSCRIPT))
192 ifndef LDSCRIPT
193 #LDSCRIPT := $(TOPDIR)/board/$(BOARDDIR)/u-boot.lds.debug
194 ifdef CONFIG_SYS_LDSCRIPT
195 # need to strip off double quotes
196 LDSCRIPT := $(subst ",,$(CONFIG_SYS_LDSCRIPT))
197 endif
198 endif
200 # If there is no specified link script, we look in a number of places for it
201 ifndef LDSCRIPT
202 ifeq ($(CONFIG_NAND_U_BOOT),y)
203 LDSCRIPT := $(TOPDIR)/board/$(BOARDDIR)/u-boot-nand.lds
204 ifeq ($(wildcard $(LDSCRIPT)),)
205 LDSCRIPT := $(TOPDIR)/$(CPUDIR)/u-boot-nand.lds
206 endif
207 endif
208 ifeq ($(wildcard $(LDSCRIPT)),)
209 LDSCRIPT := $(TOPDIR)/board/$(BOARDDIR)/u-boot.lds
210 endif
211 ifeq ($(wildcard $(LDSCRIPT)),)
212 LDSCRIPT := $(TOPDIR)/$(CPUDIR)/u-boot.lds
213 endif
214 ifeq ($(wildcard $(LDSCRIPT)),)
215 LDSCRIPT := $(TOPDIR)/arch/$(ARCH)/cpu/u-boot.lds
216 # We don't expect a Makefile here
217 LDSCRIPT_MAKEFILE_DIR =
218 endif
219 ifeq ($(wildcard $(LDSCRIPT)),)
220 $(error could not find linker script)
221 endif
222 endif
224 #########################################################################
225 # U-Boot objects....order is important (i.e. start must be first)
227 OBJS = $(CPUDIR)/start.o
228 ifeq ($(CPU),ppc4xx)
229 OBJS += $(CPUDIR)/resetvec.o
230 endif
231 ifeq ($(CPU),mpc85xx)
232 OBJS += $(CPUDIR)/resetvec.o
233 endif
235 OBJS := $(addprefix $(obj),$(OBJS))
237 HAVE_VENDOR_COMMON_LIB = $(if $(wildcard board/$(VENDOR)/common/Makefile),y,n)
239 LIBS-y += lib/libgeneric.o
240 LIBS-y += lib/lzma/liblzma.o
241 LIBS-y += lib/lzo/liblzo.o
242 LIBS-y += lib/zlib/libz.o
243 LIBS-$(CONFIG_TIZEN) += lib/tizen/libtizen.o
244 LIBS-$(HAVE_VENDOR_COMMON_LIB) += board/$(VENDOR)/common/lib$(VENDOR).o
245 LIBS-y += $(CPUDIR)/lib$(CPU).o
246 ifdef SOC
247 LIBS-y += $(CPUDIR)/$(SOC)/lib$(SOC).o
248 endif
249 ifeq ($(CPU),ixp)
250 LIBS-y += drivers/net/npe/libnpe.o
251 endif
252 LIBS-$(CONFIG_OF_EMBED) += dts/libdts.o
253 LIBS-y += arch/$(ARCH)/lib/lib$(ARCH).o
254 LIBS-y += fs/libfs.o \
255 fs/cbfs/libcbfs.o \
256 fs/cramfs/libcramfs.o \
257 fs/ext4/libext4fs.o \
258 fs/fat/libfat.o \
259 fs/fdos/libfdos.o \
260 fs/jffs2/libjffs2.o \
261 fs/reiserfs/libreiserfs.o \
262 fs/sandbox/libsandboxfs.o \
263 fs/ubifs/libubifs.o \
264 fs/yaffs2/libyaffs2.o \
265 fs/zfs/libzfs.o
266 LIBS-y += net/libnet.o
267 LIBS-y += disk/libdisk.o
268 LIBS-y += drivers/bios_emulator/libatibiosemu.o
269 LIBS-y += drivers/block/libblock.o
270 LIBS-$(CONFIG_BOOTCOUNT_LIMIT) += drivers/bootcount/libbootcount.o
271 LIBS-y += drivers/crypto/libcrypto.o
272 LIBS-y += drivers/dma/libdma.o
273 LIBS-y += drivers/fpga/libfpga.o
274 LIBS-y += drivers/gpio/libgpio.o
275 LIBS-y += drivers/hwmon/libhwmon.o
276 LIBS-y += drivers/i2c/libi2c.o
277 LIBS-y += drivers/input/libinput.o
278 LIBS-y += drivers/misc/libmisc.o
279 LIBS-y += drivers/mmc/libmmc.o
280 LIBS-y += drivers/mtd/libmtd.o
281 LIBS-y += drivers/mtd/nand/libnand.o
282 LIBS-y += drivers/mtd/onenand/libonenand.o
283 LIBS-y += drivers/mtd/ubi/libubi.o
284 LIBS-y += drivers/mtd/spi/libspi_flash.o
285 LIBS-y += drivers/net/libnet.o
286 LIBS-y += drivers/net/phy/libphy.o
287 LIBS-y += drivers/pci/libpci.o
288 LIBS-y += drivers/pcmcia/libpcmcia.o
289 LIBS-y += drivers/power/libpower.o \
290 drivers/power/fuel_gauge/libfuel_gauge.o \
291 drivers/power/pmic/libpmic.o \
292 drivers/power/battery/libbattery.o
293 LIBS-y += drivers/spi/libspi.o
294 LIBS-y += drivers/dfu/libdfu.o
295 ifeq ($(CPU),mpc83xx)
296 LIBS-y += drivers/qe/libqe.o
297 LIBS-y += arch/powerpc/cpu/mpc8xxx/ddr/libddr.o
298 LIBS-y += arch/powerpc/cpu/mpc8xxx/lib8xxx.o
299 endif
300 ifeq ($(CPU),mpc85xx)
301 LIBS-y += drivers/qe/libqe.o
302 LIBS-y += drivers/net/fm/libfm.o
303 LIBS-y += arch/powerpc/cpu/mpc8xxx/ddr/libddr.o
304 LIBS-y += arch/powerpc/cpu/mpc8xxx/lib8xxx.o
305 endif
306 ifeq ($(CPU),mpc86xx)
307 LIBS-y += arch/powerpc/cpu/mpc8xxx/ddr/libddr.o
308 LIBS-y += arch/powerpc/cpu/mpc8xxx/lib8xxx.o
309 endif
310 LIBS-y += drivers/rtc/librtc.o
311 LIBS-y += drivers/serial/libserial.o
312 LIBS-y += drivers/sound/libsound.o
313 LIBS-$(CONFIG_GENERIC_LPC_TPM) += drivers/tpm/libtpm.o
314 LIBS-y += drivers/twserial/libtws.o
315 LIBS-y += drivers/usb/eth/libusb_eth.o
316 LIBS-y += drivers/usb/gadget/libusb_gadget.o
317 LIBS-y += drivers/usb/host/libusb_host.o
318 LIBS-y += drivers/usb/musb/libusb_musb.o
319 LIBS-y += drivers/usb/musb-new/libusb_musb-new.o
320 LIBS-y += drivers/usb/phy/libusb_phy.o
321 LIBS-y += drivers/usb/ulpi/libusb_ulpi.o
322 LIBS-y += drivers/video/libvideo.o
323 LIBS-y += drivers/watchdog/libwatchdog.o
324 LIBS-y += common/libcommon.o
325 LIBS-y += lib/libfdt/libfdt.o
326 LIBS-y += api/libapi.o
327 LIBS-y += post/libpost.o
328 LIBS-y += test/libtest.o
330 ifneq ($(CONFIG_AM33XX)$(CONFIG_OMAP34XX)$(CONFIG_OMAP44XX)$(CONFIG_OMAP54XX)$(CONFIG_TI814X),)
331 LIBS-y += $(CPUDIR)/omap-common/libomap-common.o
332 endif
334 ifneq (,$(filter $(SOC), mx25 mx27 mx5 mx6 mx31 mx35))
335 LIBS-y += arch/$(ARCH)/imx-common/libimx-common.o
336 endif
338 ifeq ($(SOC),s5pc1xx)
339 LIBS-y += $(CPUDIR)/s5p-common/libs5p-common.o
340 endif
341 ifeq ($(SOC),exynos)
342 LIBS-y += $(CPUDIR)/s5p-common/libs5p-common.o
343 endif
344 ifneq ($(CONFIG_TEGRA),)
345 LIBS-y += arch/$(ARCH)/cpu/$(SOC)-common/lib$(SOC)-common.o
346 LIBS-y += arch/$(ARCH)/cpu/tegra-common/libcputegra-common.o
347 LIBS-y += $(CPUDIR)/tegra-common/libtegra-common.o
348 endif
350 LIBS := $(addprefix $(obj),$(sort $(LIBS-y)))
351 .PHONY : $(LIBS)
353 LIBBOARD = board/$(BOARDDIR)/lib$(BOARD).o
354 LIBBOARD := $(addprefix $(obj),$(LIBBOARD))
356 # Add GCC lib
357 ifdef USE_PRIVATE_LIBGCC
358 ifeq ("$(USE_PRIVATE_LIBGCC)", "yes")
359 PLATFORM_LIBGCC = $(OBJTREE)/arch/$(ARCH)/lib/libgcc.o
360 else
361 PLATFORM_LIBGCC = -L $(USE_PRIVATE_LIBGCC) -lgcc
362 endif
363 else
364 PLATFORM_LIBGCC := -L $(shell dirname `$(CC) $(CFLAGS) -print-libgcc-file-name`) -lgcc
365 endif
366 PLATFORM_LIBS += $(PLATFORM_LIBGCC)
367 export PLATFORM_LIBS
369 # Special flags for CPP when processing the linker script.
370 # Pass the version down so we can handle backwards compatibility
371 # on the fly.
372 LDPPFLAGS += \
373 -include $(TOPDIR)/include/u-boot/u-boot.lds.h \
374 -DCPUDIR=$(CPUDIR) \
375 $(shell $(LD) --version | \
376 sed -ne 's/GNU ld version \([0-9][0-9]*\)\.\([0-9][0-9]*\).*/-DLD_MAJOR=\1 -DLD_MINOR=\2/p')
378 __OBJS := $(subst $(obj),,$(OBJS))
379 __LIBS := $(subst $(obj),,$(LIBS)) $(subst $(obj),,$(LIBBOARD))
381 #########################################################################
382 #########################################################################
384 ifneq ($(CONFIG_BOARD_SIZE_LIMIT),)
385 BOARD_SIZE_CHECK = \
386 @actual=`wc -c $@ | awk '{print $$1}'`; \
387 limit=`printf "%d" $(CONFIG_BOARD_SIZE_LIMIT)`; \
388 if test $$actual -gt $$limit; then \
389 echo "$@ exceeds file size limit:" >&2 ; \
390 echo " limit: $$limit bytes" >&2 ; \
391 echo " actual: $$actual bytes" >&2 ; \
392 echo " excess: $$((actual - limit)) bytes" >&2; \
393 exit 1; \
394 fi
395 else
396 BOARD_SIZE_CHECK =
397 endif
399 # Always append ALL so that arch config.mk's can add custom ones
400 ALL-y += $(obj)u-boot.srec $(obj)u-boot.bin $(obj)System.map
402 ALL-$(CONFIG_NAND_U_BOOT) += $(obj)u-boot-nand.bin
403 ALL-$(CONFIG_ONENAND_U_BOOT) += $(obj)u-boot-onenand.bin
404 ALL-$(CONFIG_SPL) += $(obj)spl/u-boot-spl.bin
405 ALL-$(CONFIG_SPL) += $(obj)$(subst ",,$(CONFIG_SPL_TARGET))
406 ALL-$(CONFIG_OF_SEPARATE) += $(obj)u-boot.dtb $(obj)u-boot-dtb.bin
408 # enable combined SPL/u-boot/dtb rules for tegra
409 ifneq ($(CONFIG_TEGRA),)
410 ifeq ($(CONFIG_OF_SEPARATE),y)
411 ALL-y += $(obj)u-boot-dtb-tegra.bin
412 else
413 ALL-y += $(obj)u-boot-nodtb-tegra.bin
414 endif
415 endif
417 all: $(ALL-y) $(SUBDIR_EXAMPLES)
419 $(obj)u-boot.dtb: $(obj)u-boot
420 $(MAKE) -C dts binary
421 mv $(obj)dts/dt.dtb $@
423 $(obj)u-boot-dtb.bin: $(obj)u-boot.bin $(obj)u-boot.dtb
424 cat $^ >$@
426 $(obj)u-boot.hex: $(obj)u-boot
427 $(OBJCOPY) ${OBJCFLAGS} -O ihex $< $@
429 $(obj)u-boot.srec: $(obj)u-boot
430 $(OBJCOPY) -O srec $< $@
432 $(obj)u-boot.bin: $(obj)u-boot
433 $(OBJCOPY) ${OBJCFLAGS} -O binary $< $@
434 $(BOARD_SIZE_CHECK)
436 $(obj)u-boot.ldr: $(obj)u-boot
437 $(CREATE_LDR_ENV)
438 $(LDR) -T $(CONFIG_BFIN_CPU) -c $@ $< $(LDR_FLAGS)
439 $(BOARD_SIZE_CHECK)
441 $(obj)u-boot.ldr.hex: $(obj)u-boot.ldr
442 $(OBJCOPY) ${OBJCFLAGS} -O ihex $< $@ -I binary
444 $(obj)u-boot.ldr.srec: $(obj)u-boot.ldr
445 $(OBJCOPY) ${OBJCFLAGS} -O srec $< $@ -I binary
447 #
448 # U-Boot entry point, needed for booting of full-blown U-Boot
449 # from the SPL U-Boot version.
450 #
451 ifndef CONFIG_SYS_UBOOT_START
452 CONFIG_SYS_UBOOT_START := 0
453 endif
455 $(obj)u-boot.img: $(obj)u-boot.bin
456 $(obj)tools/mkimage -A $(ARCH) -T firmware -C none \
457 -O u-boot -a $(CONFIG_SYS_TEXT_BASE) \
458 -e $(CONFIG_SYS_UBOOT_START) \
459 -n $(shell sed -n -e 's/.*U_BOOT_VERSION//p' $(VERSION_FILE) | \
460 sed -e 's/"[ ]*$$/ for $(BOARD) board"/') \
461 -d $< $@
463 $(obj)u-boot.imx: $(obj)u-boot.bin depend
464 $(MAKE) -C $(SRCTREE)/arch/arm/imx-common $(OBJTREE)/u-boot.imx
466 $(obj)u-boot.kwb: $(obj)u-boot.bin
467 $(obj)tools/mkimage -n $(CONFIG_SYS_KWD_CONFIG) -T kwbimage \
468 -a $(CONFIG_SYS_TEXT_BASE) -e $(CONFIG_SYS_TEXT_BASE) -d $< $@
470 $(obj)u-boot.pbl: $(obj)u-boot.bin
471 $(obj)tools/mkimage -n $(CONFIG_PBLRCW_CONFIG) \
472 -R $(CONFIG_PBLPBI_CONFIG) -T pblimage \
473 -d $< $@
475 $(obj)u-boot.sha1: $(obj)u-boot.bin
476 $(obj)tools/ubsha1 $(obj)u-boot.bin
478 $(obj)u-boot.dis: $(obj)u-boot
479 $(OBJDUMP) -d $< > $@
483 $(obj)u-boot-with-spl.bin: $(obj)spl/u-boot-spl.bin $(obj)u-boot.bin
484 $(OBJCOPY) ${OBJCFLAGS} --pad-to=$(CONFIG_SPL_PAD_TO) \
485 -I binary -O binary $< $(obj)spl/u-boot-spl-pad.bin
486 cat $(obj)spl/u-boot-spl-pad.bin $(obj)u-boot.bin > $@
487 rm $(obj)spl/u-boot-spl-pad.bin
489 $(obj)u-boot-with-spl.imx: $(obj)spl/u-boot-spl.bin $(obj)u-boot.bin
490 $(MAKE) -C $(SRCTREE)/arch/arm/imx-common \
491 $(OBJTREE)/u-boot-with-spl.imx
493 $(obj)u-boot-with-nand-spl.imx: $(obj)spl/u-boot-spl.bin $(obj)u-boot.bin
494 $(MAKE) -C $(SRCTREE)/arch/arm/imx-common \
495 $(OBJTREE)/u-boot-with-nand-spl.imx
497 $(obj)u-boot.ubl: $(obj)u-boot-with-spl.bin
498 $(obj)tools/mkimage -n $(UBL_CONFIG) -T ublimage \
499 -e $(CONFIG_SYS_TEXT_BASE) -d $< $(obj)u-boot.ubl
501 $(obj)u-boot.ais: $(obj)spl/u-boot-spl.bin $(obj)u-boot.img
502 $(obj)tools/mkimage -s -n $(if $(CONFIG_AIS_CONFIG_FILE),$(CONFIG_AIS_CONFIG_FILE),"/dev/null") \
503 -T aisimage \
504 -e $(CONFIG_SPL_TEXT_BASE) \
505 -d $(obj)spl/u-boot-spl.bin \
506 $(obj)spl/u-boot-spl.ais
507 $(OBJCOPY) ${OBJCFLAGS} -I binary \
508 --pad-to=$(CONFIG_SPL_MAX_SIZE) -O binary \
509 $(obj)spl/u-boot-spl.ais $(obj)spl/u-boot-spl-pad.ais
510 cat $(obj)spl/u-boot-spl-pad.ais $(obj)u-boot.img > \
511 $(obj)u-boot.ais
513 # Specify the target for use in elftosb call
514 ELFTOSB_TARGET-$(CONFIG_MX23) = imx23
515 ELFTOSB_TARGET-$(CONFIG_MX28) = imx28
517 $(obj)u-boot.sb: $(obj)u-boot.bin $(obj)spl/u-boot-spl.bin
518 elftosb -zf $(ELFTOSB_TARGET-y) -c $(TOPDIR)/$(CPUDIR)/$(SOC)/u-boot-$(ELFTOSB_TARGET-y).bd \
519 -o $(obj)u-boot.sb
521 # On x600 (SPEAr600) U-Boot is appended to U-Boot SPL.
522 # Both images are created using mkimage (crc etc), so that the ROM
523 # bootloader can check its integrity. Padding needs to be done to the
524 # SPL image (with mkimage header) and not the binary. Otherwise the resulting image
525 # which is loaded/copied by the ROM bootloader to SRAM doesn't fit.
526 # The resulting image containing both U-Boot images is called u-boot.spr
527 $(obj)u-boot.spr: $(obj)u-boot.img $(obj)spl/u-boot-spl.bin
528 $(obj)tools/mkimage -A $(ARCH) -T firmware -C none \
529 -a $(CONFIG_SPL_TEXT_BASE) -e $(CONFIG_SPL_TEXT_BASE) -n XLOADER \
530 -d $(obj)spl/u-boot-spl.bin $(obj)spl/u-boot-spl.img
531 tr "\000" "\377" < /dev/zero | dd ibs=1 count=$(CONFIG_SPL_PAD_TO) \
532 of=$(obj)spl/u-boot-spl-pad.img 2>/dev/null
533 dd if=$(obj)spl/u-boot-spl.img of=$(obj)spl/u-boot-spl-pad.img \
534 conv=notrunc 2>/dev/null
535 cat $(obj)spl/u-boot-spl-pad.img $(obj)u-boot.img > $@
537 ifneq ($(CONFIG_TEGRA),)
538 ifeq ($(CONFIG_OF_SEPARATE),y)
539 nodtb=dtb
540 dtbfile=$(obj)u-boot.dtb
541 else
542 nodtb=nodtb
543 dtbfile=
544 endif
546 $(obj)u-boot-$(nodtb)-tegra.bin: $(obj)spl/u-boot-spl.bin $(obj)u-boot.bin $(dtbfile)
547 $(OBJCOPY) ${OBJCFLAGS} --pad-to=$(CONFIG_SYS_TEXT_BASE) -O binary $(obj)spl/u-boot-spl $(obj)spl/u-boot-spl-pad.bin
548 cat $(obj)spl/u-boot-spl-pad.bin $(obj)u-boot.bin $(dtbfile) > $@
549 rm $(obj)spl/u-boot-spl-pad.bin
550 endif
552 $(obj)u-boot-img.bin: $(obj)spl/u-boot-spl.bin $(obj)u-boot.img
553 cat $(obj)spl/u-boot-spl.bin $(obj)u-boot.img > $@
555 ifeq ($(CONFIG_SANDBOX),y)
556 GEN_UBOOT = \
557 cd $(LNDIR) && $(CC) $(SYMS) -T $(obj)u-boot.lds \
558 -Wl,--start-group $(__LIBS) -Wl,--end-group \
559 $(PLATFORM_LIBS) -Wl,-Map -Wl,u-boot.map -o u-boot
560 else
561 GEN_UBOOT = \
562 cd $(LNDIR) && $(LD) $(LDFLAGS) $(LDFLAGS_$(@F)) \
563 $(__OBJS) \
564 --start-group $(__LIBS) --end-group $(PLATFORM_LIBS) \
565 -Map u-boot.map -o u-boot
566 endif
568 $(obj)u-boot: depend \
569 $(SUBDIR_TOOLS) $(OBJS) $(LIBBOARD) $(LIBS) $(LDSCRIPT) $(obj)u-boot.lds
570 $(GEN_UBOOT)
571 ifeq ($(CONFIG_KALLSYMS),y)
572 smap=`$(call SYSTEM_MAP,$(obj)u-boot) | \
573 awk '$$2 ~ /[tTwW]/ {printf $$1 $$3 "\\\\000"}'` ; \
574 $(CC) $(CFLAGS) -DSYSTEM_MAP="\"$${smap}\"" \
575 -c common/system_map.c -o $(obj)common/system_map.o
576 $(GEN_UBOOT) $(obj)common/system_map.o
577 endif
579 $(OBJS): depend
580 $(MAKE) -C $(CPUDIR) $(if $(REMOTE_BUILD),$@,$(notdir $@))
582 $(LIBS): depend $(SUBDIR_TOOLS)
583 $(MAKE) -C $(dir $(subst $(obj),,$@))
585 $(LIBBOARD): depend $(LIBS)
586 $(MAKE) -C $(dir $(subst $(obj),,$@))
588 $(SUBDIRS): depend
589 $(MAKE) -C $@ all
591 $(SUBDIR_EXAMPLES): $(obj)u-boot
593 $(LDSCRIPT): depend
594 $(MAKE) -C $(dir $@) $(notdir $@)
596 $(obj)u-boot.lds: $(LDSCRIPT)
597 $(CPP) $(CPPFLAGS) $(LDPPFLAGS) -ansi -D__ASSEMBLY__ -P - <$< >$@
599 nand_spl: $(TIMESTAMP_FILE) $(VERSION_FILE) depend
600 $(MAKE) -C nand_spl/board/$(BOARDDIR) all
602 $(obj)u-boot-nand.bin: nand_spl $(obj)u-boot.bin
603 cat $(obj)nand_spl/u-boot-spl-16k.bin $(obj)u-boot.bin > $(obj)u-boot-nand.bin
605 $(obj)spl/u-boot-spl.bin: $(SUBDIR_TOOLS) depend
606 $(MAKE) -C spl all
608 updater:
609 $(MAKE) -C tools/updater all
611 # Explicitly make _depend in subdirs containing multiple targets to prevent
612 # parallel sub-makes creating .depend files simultaneously.
613 depend dep: $(TIMESTAMP_FILE) $(VERSION_FILE) \
614 $(obj)include/autoconf.mk \
615 $(obj)include/generated/generic-asm-offsets.h \
616 $(obj)include/generated/asm-offsets.h
617 for dir in $(SUBDIRS) $(CPUDIR) $(LDSCRIPT_MAKEFILE_DIR) ; do \
618 $(MAKE) -C $$dir _depend ; done
620 TAG_SUBDIRS = $(SUBDIRS)
621 TAG_SUBDIRS += $(dir $(__LIBS))
622 TAG_SUBDIRS += include
624 FIND := find
625 FINDFLAGS := -L
627 checkstack:
628 $(CROSS_COMPILE)objdump -d $(obj)u-boot \
629 `$(FIND) $(obj) -name u-boot-spl -print` | \
630 perl $(src)tools/checkstack.pl $(ARCH)
632 tags ctags:
633 ctags -w -o $(obj)ctags `$(FIND) $(FINDFLAGS) $(TAG_SUBDIRS) \
634 -name '*.[chS]' -print`
636 etags:
637 etags -a -o $(obj)etags `$(FIND) $(FINDFLAGS) $(TAG_SUBDIRS) \
638 -name '*.[chS]' -print`
639 cscope:
640 $(FIND) $(FINDFLAGS) $(TAG_SUBDIRS) -name '*.[chS]' -print > \
641 cscope.files
642 cscope -b -q -k
644 SYSTEM_MAP = \
645 $(NM) $1 | \
646 grep -v '\(compiled\)\|\(\.o$$\)\|\( [aUw] \)\|\(\.\.ng$$\)\|\(LASH[RL]DI\)' | \
647 LC_ALL=C sort
648 $(obj)System.map: $(obj)u-boot
649 @$(call SYSTEM_MAP,$<) > $(obj)System.map
651 checkthumb:
652 @if test $(call cc-version) -lt 0404; then \
653 echo -n '*** Your GCC does not produce working '; \
654 echo 'binaries in THUMB mode.'; \
655 echo '*** Your board is configured for THUMB mode.'; \
656 false; \
657 fi
659 # GCC 3.x is reported to have problems generating the type of relocation
660 # that U-Boot wants.
661 # See http://lists.denx.de/pipermail/u-boot/2012-September/135156.html
662 checkgcc4:
663 @if test $(call cc-version) -lt 0400; then \
664 echo -n '*** Your GCC is too old, please upgrade to GCC 4.x or newer'; \
665 false; \
666 fi
668 #
669 # Auto-generate the autoconf.mk file (which is included by all makefiles)
670 #
671 # This target actually generates 2 files; autoconf.mk and autoconf.mk.dep.
672 # the dep file is only include in this top level makefile to determine when
673 # to regenerate the autoconf.mk file.
674 $(obj)include/autoconf.mk.dep: $(obj)include/config.h include/common.h
675 @$(XECHO) Generating $@ ; \
676 set -e ; \
677 : Generate the dependancies ; \
678 $(CC) -x c -DDO_DEPS_ONLY -M $(CFLAGS) $(CPPFLAGS) \
679 -MQ $(obj)include/autoconf.mk include/common.h > $@
681 $(obj)include/autoconf.mk: $(obj)include/config.h
682 @$(XECHO) Generating $@ ; \
683 set -e ; \
684 : Extract the config macros ; \
685 $(CPP) $(CFLAGS) -DDO_DEPS_ONLY -dM include/common.h | \
686 sed -n -f tools/scripts/define2mk.sed > $@.tmp && \
687 mv $@.tmp $@
689 $(obj)include/generated/generic-asm-offsets.h: $(obj)include/autoconf.mk.dep \
690 $(obj)lib/asm-offsets.s
691 @$(XECHO) Generating $@
692 tools/scripts/make-asm-offsets $(obj)lib/asm-offsets.s $@
694 $(obj)lib/asm-offsets.s: $(obj)include/autoconf.mk.dep \
695 $(src)lib/asm-offsets.c
696 @mkdir -p $(obj)lib
697 $(CC) -DDO_DEPS_ONLY \
698 $(CFLAGS) $(CFLAGS_$(BCURDIR)/$(@F)) $(CFLAGS_$(BCURDIR)) \
699 -o $@ $(src)lib/asm-offsets.c -c -S
701 $(obj)include/generated/asm-offsets.h: $(obj)include/autoconf.mk.dep \
702 $(obj)$(CPUDIR)/$(SOC)/asm-offsets.s
703 @$(XECHO) Generating $@
704 tools/scripts/make-asm-offsets $(obj)$(CPUDIR)/$(SOC)/asm-offsets.s $@
706 $(obj)$(CPUDIR)/$(SOC)/asm-offsets.s: $(obj)include/autoconf.mk.dep
707 @mkdir -p $(obj)$(CPUDIR)/$(SOC)
708 if [ -f $(src)$(CPUDIR)/$(SOC)/asm-offsets.c ];then \
709 $(CC) -DDO_DEPS_ONLY \
710 $(CFLAGS) $(CFLAGS_$(BCURDIR)/$(@F)) $(CFLAGS_$(BCURDIR)) \
711 -o $@ $(src)$(CPUDIR)/$(SOC)/asm-offsets.c -c -S; \
712 else \
713 touch $@; \
714 fi
716 #########################################################################
717 else # !config.mk
718 all $(obj)u-boot.hex $(obj)u-boot.srec $(obj)u-boot.bin \
719 $(obj)u-boot.img $(obj)u-boot.dis $(obj)u-boot \
720 $(filter-out tools,$(SUBDIRS)) \
721 updater depend dep tags ctags etags cscope $(obj)System.map:
722 @echo "System not configured - see README" >&2
723 @ exit 1
725 tools: $(VERSION_FILE) $(TIMESTAMP_FILE)
726 $(MAKE) -C $@ all
727 endif # config.mk
729 $(VERSION_FILE):
730 @mkdir -p $(dir $(VERSION_FILE))
731 @( localvers='$(shell $(TOPDIR)/tools/setlocalversion $(TOPDIR))' ; \
732 printf '#define PLAIN_VERSION "%s%s"\n' \
733 "$(U_BOOT_VERSION)" "$${localvers}" ; \
734 printf '#define U_BOOT_VERSION "U-Boot %s%s"\n' \
735 "$(U_BOOT_VERSION)" "$${localvers}" ; \
736 ) > $@.tmp
737 @( printf '#define CC_VERSION_STRING "%s"\n' \
738 '$(shell $(CC) --version | head -n 1)' )>> $@.tmp
739 @( printf '#define LD_VERSION_STRING "%s"\n' \
740 '$(shell $(LD) -v | head -n 1)' )>> $@.tmp
741 @cmp -s $@ $@.tmp && rm -f $@.tmp || mv -f $@.tmp $@
743 $(TIMESTAMP_FILE):
744 @mkdir -p $(dir $(TIMESTAMP_FILE))
745 @LC_ALL=C date +'#define U_BOOT_DATE "%b %d %C%y"' > $@.tmp
746 @LC_ALL=C date +'#define U_BOOT_TIME "%T"' >> $@.tmp
747 @cmp -s $@ $@.tmp && rm -f $@.tmp || mv -f $@.tmp $@
749 easylogo env gdb:
750 $(MAKE) -C tools/$@ all MTD_VERSION=${MTD_VERSION}
751 gdbtools: gdb
753 xmldocs pdfdocs psdocs htmldocs mandocs: tools/kernel-doc/docproc
754 $(MAKE) U_BOOT_VERSION=$(U_BOOT_VERSION) -C doc/DocBook/ $@
756 tools-all: easylogo env gdb $(VERSION_FILE) $(TIMESTAMP_FILE)
757 $(MAKE) -C tools HOST_TOOLS_ALL=y
759 .PHONY : CHANGELOG
760 CHANGELOG:
761 git log --no-merges U-Boot-1_1_5.. | \
762 unexpand -a | sed -e 's/\s\s*$$//' > $@
764 include/license.h: tools/bin2header COPYING
765 cat COPYING | gzip -9 -c | ./tools/bin2header license_gzip > include/license.h
766 #########################################################################
768 unconfig:
769 @rm -f $(obj)include/config.h $(obj)include/config.mk \
770 $(obj)board/*/config.tmp $(obj)board/*/*/config.tmp \
771 $(obj)include/autoconf.mk $(obj)include/autoconf.mk.dep
773 %_config:: unconfig
774 @$(MKCONFIG) -A $(@:_config=)
776 sinclude $(obj).boards.depend
777 $(obj).boards.depend: boards.cfg
778 @awk '(NF && $$1 !~ /^#/) { print $$1 ": " $$1 "_config; $$(MAKE)" }' $< > $@
780 #
781 # Functions to generate common board directory names
782 #
783 lcname = $(shell echo $(1) | sed -e 's/\(.*\)_config/\L\1/')
784 ucname = $(shell echo $(1) | sed -e 's/\(.*\)_config/\U\1/')
786 #########################################################################
787 #########################################################################
789 clean:
790 @rm -f $(obj)examples/standalone/82559_eeprom \
791 $(obj)examples/standalone/atmel_df_pow2 \
792 $(obj)examples/standalone/eepro100_eeprom \
793 $(obj)examples/standalone/hello_world \
794 $(obj)examples/standalone/interrupt \
795 $(obj)examples/standalone/mem_to_mem_idma2intr \
796 $(obj)examples/standalone/sched \
797 $(obj)examples/standalone/smc911{11,x}_eeprom \
798 $(obj)examples/standalone/test_burst \
799 $(obj)examples/standalone/timer
800 @rm -f $(obj)examples/api/demo{,.bin}
801 @rm -f $(obj)tools/bmp_logo $(obj)tools/easylogo/easylogo \
802 $(obj)tools/env/{fw_printenv,fw_setenv} \
803 $(obj)tools/envcrc \
804 $(obj)tools/gdb/{astest,gdbcont,gdbsend} \
805 $(obj)tools/gen_eth_addr $(obj)tools/img2srec \
806 $(obj)tools/mk{env,}image $(obj)tools/mpc86x_clk \
807 $(obj)tools/mk{smdk5250,}spl \
808 $(obj)tools/mxsboot \
809 $(obj)tools/ncb $(obj)tools/ubsha1 \
810 $(obj)tools/kernel-doc/docproc
811 @rm -f $(obj)board/cray/L1/{bootscript.c,bootscript.image} \
812 $(obj)board/matrix_vision/*/bootscript.img \
813 $(obj)board/voiceblue/eeprom \
814 $(obj)u-boot.lds \
815 $(obj)arch/blackfin/cpu/bootrom-asm-offsets.[chs] \
816 $(obj)arch/blackfin/cpu/init.{lds,elf}
817 @rm -f $(obj)include/bmp_logo.h
818 @rm -f $(obj)include/bmp_logo_data.h
819 @rm -f $(obj)lib/asm-offsets.s
820 @rm -f $(obj)include/generated/asm-offsets.h
821 @rm -f $(obj)$(CPUDIR)/$(SOC)/asm-offsets.s
822 @rm -f $(TIMESTAMP_FILE) $(VERSION_FILE)
823 @$(MAKE) -s -C doc/DocBook/ cleandocs
824 @find $(OBJTREE) -type f \
825 \( -name 'core' -o -name '*.bak' -o -name '*~' -o -name '*.su' \
826 -o -name '*.o' -o -name '*.a' -o -name '*.exe' \
827 -o -name '*.cfgtmp' \) -print \
828 | xargs rm -f
830 # Removes everything not needed for testing u-boot
831 tidy: clean
832 @find $(OBJTREE) -type f \( -name '*.depend*' \) -print | xargs rm -f
834 clobber: tidy
835 @find $(OBJTREE) -type f \( -name '*.srec' \
836 -o -name '*.bin' -o -name u-boot.img \) \
837 -print0 | xargs -0 rm -f
838 @rm -f $(OBJS) $(obj)*.bak $(obj)ctags $(obj)etags $(obj)TAGS \
839 $(obj)cscope.* $(obj)*.*~
840 @rm -f $(obj)u-boot $(obj)u-boot.map $(obj)u-boot.hex $(ALL-y)
841 @rm -f $(obj)u-boot.kwb
842 @rm -f $(obj)u-boot.pbl
843 @rm -f $(obj)u-boot.imx
844 @rm -f $(obj)u-boot-with-spl.imx
845 @rm -f $(obj)u-boot-with-nand-spl.imx
846 @rm -f $(obj)u-boot.ubl
847 @rm -f $(obj)u-boot.ais
848 @rm -f $(obj)u-boot.dtb
849 @rm -f $(obj)u-boot.sb
850 @rm -f $(obj)u-boot.spr
851 @rm -f $(obj)nand_spl/{u-boot.{lds,lst},System.map}
852 @rm -f $(obj)nand_spl/{u-boot-nand_spl.lds,u-boot-spl,u-boot-spl.map}
853 @rm -f $(obj)spl/{u-boot-spl,u-boot-spl.bin,u-boot-spl.map}
854 @rm -f $(obj)spl/u-boot-spl.lds
855 @rm -f $(obj)MLO MLO.byteswap
856 @rm -f $(obj)SPL
857 @rm -f $(obj)tools/xway-swap-bytes
858 @rm -f $(obj)arch/powerpc/cpu/mpc824x/bedbug_603e.c
859 @rm -f $(obj)arch/powerpc/cpu/mpc83xx/ddr-gen?.c
860 @rm -fr $(obj)include/asm/proc $(obj)include/asm/arch $(obj)include/asm
861 @rm -fr $(obj)include/generated
862 @[ ! -d $(obj)nand_spl ] || find $(obj)nand_spl -name "*" -type l -print | xargs rm -f
863 @rm -f $(obj)dts/*.tmp
864 @rm -f $(obj)spl/u-boot-spl{,-pad}.ais
866 mrproper \
867 distclean: clobber unconfig
868 ifneq ($(OBJTREE),$(SRCTREE))
869 rm -rf $(obj)*
870 endif
872 backup:
873 F=`basename $(TOPDIR)` ; cd .. ; \
874 gtar --force-local -zcvf `LC_ALL=C date "+$$F-%Y-%m-%d-%T.tar.gz"` $$F
876 #########################################################################