]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/glsdk-u-boot.git/blob - Makefile
sandbox: Add basic test for command execution
[glsdk/glsdk-u-boot.git] / Makefile
1 #
2 # (C) Copyright 2000-2012
3 # Wolfgang Denk, DENX Software Engineering, wd@denx.de.
4 #
5 # See file CREDITS for list of people who contributed to this
6 # project.
7 #
8 # This program is free software; you can redistribute it and/or
9 # modify it under the terms of the GNU General Public License as
10 # published by the Free Software Foundatio; either version 2 of
11 # the License, or (at your option) any later version.
12 #
13 # This program is distributed in the hope that it will be useful,
14 # but WITHOUT ANY WARRANTY; without even the implied warranty of
15 # MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
16 # GNU General Public License for more details.
17 #
18 # You should have received a copy of the GNU General Public License
19 # along with this program; if not, write to the Free Software
20 # Foundation, Inc., 59 Temple Place, Suite 330, Boston,
21 # MA 02111-1307 USA
22 #
24 VERSION = 2012
25 PATCHLEVEL = 07
26 SUBLEVEL =
27 EXTRAVERSION =
28 ifneq "$(SUBLEVEL)" ""
29 U_BOOT_VERSION = $(VERSION).$(PATCHLEVEL).$(SUBLEVEL)$(EXTRAVERSION)
30 else
31 U_BOOT_VERSION = $(VERSION).$(PATCHLEVEL)$(EXTRAVERSION)
32 endif
33 TIMESTAMP_FILE = $(obj)include/generated/timestamp_autogenerated.h
34 VERSION_FILE = $(obj)include/generated/version_autogenerated.h
36 HOSTARCH := $(shell uname -m | \
37         sed -e s/i.86/x86/ \
38             -e s/sun4u/sparc64/ \
39             -e s/arm.*/arm/ \
40             -e s/sa110/arm/ \
41             -e s/ppc64/powerpc/ \
42             -e s/ppc/powerpc/ \
43             -e s/macppc/powerpc/\
44             -e s/sh.*/sh/)
46 HOSTOS := $(shell uname -s | tr '[:upper:]' '[:lower:]' | \
47             sed -e 's/\(cygwin\).*/cygwin/')
49 # Set shell to bash if possible, otherwise fall back to sh
50 SHELL := $(shell if [ -x "$$BASH" ]; then echo $$BASH; \
51         else if [ -x /bin/bash ]; then echo /bin/bash; \
52         else echo sh; fi; fi)
54 export  HOSTARCH HOSTOS SHELL
56 # Deal with colliding definitions from tcsh etc.
57 VENDOR=
59 #########################################################################
60 # Allow for silent builds
61 ifeq (,$(findstring s,$(MAKEFLAGS)))
62 XECHO = echo
63 else
64 XECHO = :
65 endif
67 #########################################################################
68 #
69 # U-boot build supports producing a object files to the separate external
70 # directory. Two use cases are supported:
71 #
72 # 1) Add O= to the make command line
73 # 'make O=/tmp/build all'
74 #
75 # 2) Set environement variable BUILD_DIR to point to the desired location
76 # 'export BUILD_DIR=/tmp/build'
77 # 'make'
78 #
79 # The second approach can also be used with a MAKEALL script
80 # 'export BUILD_DIR=/tmp/build'
81 # './MAKEALL'
82 #
83 # Command line 'O=' setting overrides BUILD_DIR environent variable.
84 #
85 # When none of the above methods is used the local build is performed and
86 # the object files are placed in the source directory.
87 #
89 ifdef O
90 ifeq ("$(origin O)", "command line")
91 BUILD_DIR := $(O)
92 endif
93 endif
95 ifneq ($(BUILD_DIR),)
96 saved-output := $(BUILD_DIR)
98 # Attempt to create a output directory.
99 $(shell [ -d ${BUILD_DIR} ] || mkdir -p ${BUILD_DIR})
101 # Verify if it was successful.
102 BUILD_DIR := $(shell cd $(BUILD_DIR) && /bin/pwd)
103 $(if $(BUILD_DIR),,$(error output directory "$(saved-output)" does not exist))
104 endif # ifneq ($(BUILD_DIR),)
106 OBJTREE         := $(if $(BUILD_DIR),$(BUILD_DIR),$(CURDIR))
107 SPLTREE         := $(OBJTREE)/spl
108 SRCTREE         := $(CURDIR)
109 TOPDIR          := $(SRCTREE)
110 LNDIR           := $(OBJTREE)
111 export  TOPDIR SRCTREE OBJTREE SPLTREE
113 MKCONFIG        := $(SRCTREE)/mkconfig
114 export MKCONFIG
116 ifneq ($(OBJTREE),$(SRCTREE))
117 REMOTE_BUILD    := 1
118 export REMOTE_BUILD
119 endif
121 # $(obj) and (src) are defined in config.mk but here in main Makefile
122 # we also need them before config.mk is included which is the case for
123 # some targets like unconfig, clean, clobber, distclean, etc.
124 ifneq ($(OBJTREE),$(SRCTREE))
125 obj := $(OBJTREE)/
126 src := $(SRCTREE)/
127 else
128 obj :=
129 src :=
130 endif
131 export obj src
133 # Make sure CDPATH settings don't interfere
134 unexport CDPATH
136 #########################################################################
138 # The "tools" are needed early, so put this first
139 # Don't include stuff already done in $(LIBS)
140 # The "examples" conditionally depend on U-Boot (say, when USE_PRIVATE_LIBGCC
141 # is "yes"), so compile examples after U-Boot is compiled.
142 SUBDIR_TOOLS = tools
143 SUBDIR_EXAMPLES = examples/standalone examples/api
144 SUBDIRS = $(SUBDIR_TOOLS)
146 .PHONY : $(SUBDIRS) $(VERSION_FILE) $(TIMESTAMP_FILE)
148 ifeq ($(obj)include/config.mk,$(wildcard $(obj)include/config.mk))
150 # Include autoconf.mk before config.mk so that the config options are available
151 # to all top level build files.  We need the dummy all: target to prevent the
152 # dependency target in autoconf.mk.dep from being the default.
153 all:
154 sinclude $(obj)include/autoconf.mk.dep
155 sinclude $(obj)include/autoconf.mk
157 ifndef CONFIG_SANDBOX
158 SUBDIRS += $(SUBDIR_EXAMPLES)
159 endif
161 # load ARCH, BOARD, and CPU configuration
162 include $(obj)include/config.mk
163 export  ARCH CPU BOARD VENDOR SOC
165 # set default to nothing for native builds
166 ifeq ($(HOSTARCH),$(ARCH))
167 CROSS_COMPILE ?=
168 endif
170 # load other configuration
171 include $(TOPDIR)/config.mk
173 # If board code explicitly specified LDSCRIPT or CONFIG_SYS_LDSCRIPT, use
174 # that (or fail if absent).  Otherwise, search for a linker script in a
175 # standard location.
177 LDSCRIPT_MAKEFILE_DIR = $(dir $(LDSCRIPT))
179 ifndef LDSCRIPT
180         #LDSCRIPT := $(TOPDIR)/board/$(BOARDDIR)/u-boot.lds.debug
181         ifdef CONFIG_SYS_LDSCRIPT
182                 # need to strip off double quotes
183                 LDSCRIPT := $(subst ",,$(CONFIG_SYS_LDSCRIPT))
184         endif
185 endif
187 # If there is no specified link script, we look in a number of places for it
188 ifndef LDSCRIPT
189         ifeq ($(CONFIG_NAND_U_BOOT),y)
190                 LDSCRIPT := $(TOPDIR)/board/$(BOARDDIR)/u-boot-nand.lds
191                 ifeq ($(wildcard $(LDSCRIPT)),)
192                         LDSCRIPT := $(TOPDIR)/$(CPUDIR)/u-boot-nand.lds
193                 endif
194         endif
195         ifeq ($(wildcard $(LDSCRIPT)),)
196                 LDSCRIPT := $(TOPDIR)/board/$(BOARDDIR)/u-boot.lds
197         endif
198         ifeq ($(wildcard $(LDSCRIPT)),)
199                 LDSCRIPT := $(TOPDIR)/$(CPUDIR)/u-boot.lds
200         endif
201         ifeq ($(wildcard $(LDSCRIPT)),)
202                 LDSCRIPT := $(TOPDIR)/arch/$(ARCH)/cpu/u-boot.lds
203                 # We don't expect a Makefile here
204                 LDSCRIPT_MAKEFILE_DIR =
205         endif
206         ifeq ($(wildcard $(LDSCRIPT)),)
207 $(error could not find linker script)
208         endif
209 endif
211 #########################################################################
212 # U-Boot objects....order is important (i.e. start must be first)
214 OBJS  = $(CPUDIR)/start.o
215 ifeq ($(CPU),x86)
216 OBJS += $(CPUDIR)/start16.o
217 OBJS += $(CPUDIR)/resetvec.o
218 endif
219 ifeq ($(CPU),ppc4xx)
220 OBJS += $(CPUDIR)/resetvec.o
221 endif
222 ifeq ($(CPU),mpc85xx)
223 OBJS += $(CPUDIR)/resetvec.o
224 endif
226 OBJS := $(addprefix $(obj),$(OBJS))
228 LIBS  = lib/libgeneric.o
229 LIBS += lib/lzma/liblzma.o
230 LIBS += lib/lzo/liblzo.o
231 LIBS += lib/zlib/libz.o
232 ifeq ($(CONFIG_TIZEN),y)
233 LIBS += lib/tizen/libtizen.o
234 endif
235 LIBS += $(shell if [ -f board/$(VENDOR)/common/Makefile ]; then echo \
236         "board/$(VENDOR)/common/lib$(VENDOR).o"; fi)
237 LIBS += $(CPUDIR)/lib$(CPU).o
238 ifdef SOC
239 LIBS += $(CPUDIR)/$(SOC)/lib$(SOC).o
240 endif
241 ifeq ($(CPU),ixp)
242 LIBS += arch/arm/cpu/ixp/npe/libnpe.o
243 endif
244 ifeq ($(CONFIG_OF_EMBED),y)
245 LIBS += dts/libdts.o
246 endif
247 LIBS += arch/$(ARCH)/lib/lib$(ARCH).o
248 LIBS += fs/cramfs/libcramfs.o fs/fat/libfat.o fs/fdos/libfdos.o fs/jffs2/libjffs2.o \
249         fs/reiserfs/libreiserfs.o fs/ext2/libext2fs.o fs/yaffs2/libyaffs2.o \
250         fs/ubifs/libubifs.o
251 LIBS += net/libnet.o
252 LIBS += disk/libdisk.o
253 LIBS += drivers/bios_emulator/libatibiosemu.o
254 LIBS += drivers/block/libblock.o
255 LIBS += drivers/dma/libdma.o
256 LIBS += drivers/fpga/libfpga.o
257 LIBS += drivers/gpio/libgpio.o
258 LIBS += drivers/hwmon/libhwmon.o
259 LIBS += drivers/i2c/libi2c.o
260 LIBS += drivers/input/libinput.o
261 LIBS += drivers/misc/libmisc.o
262 LIBS += drivers/mmc/libmmc.o
263 LIBS += drivers/mtd/libmtd.o
264 LIBS += drivers/mtd/nand/libnand.o
265 LIBS += drivers/mtd/onenand/libonenand.o
266 LIBS += drivers/mtd/ubi/libubi.o
267 LIBS += drivers/mtd/spi/libspi_flash.o
268 LIBS += drivers/net/libnet.o
269 LIBS += drivers/net/phy/libphy.o
270 LIBS += drivers/pci/libpci.o
271 LIBS += drivers/pcmcia/libpcmcia.o
272 LIBS += drivers/power/libpower.o
273 LIBS += drivers/spi/libspi.o
274 ifeq ($(CPU),mpc83xx)
275 LIBS += drivers/qe/libqe.o
276 LIBS += arch/powerpc/cpu/mpc8xxx/ddr/libddr.o
277 LIBS += arch/powerpc/cpu/mpc8xxx/lib8xxx.o
278 endif
279 ifeq ($(CPU),mpc85xx)
280 LIBS += drivers/qe/libqe.o
281 LIBS += drivers/net/fm/libfm.o
282 LIBS += arch/powerpc/cpu/mpc8xxx/ddr/libddr.o
283 LIBS += arch/powerpc/cpu/mpc8xxx/lib8xxx.o
284 endif
285 ifeq ($(CPU),mpc86xx)
286 LIBS += arch/powerpc/cpu/mpc8xxx/ddr/libddr.o
287 LIBS += arch/powerpc/cpu/mpc8xxx/lib8xxx.o
288 endif
289 LIBS += drivers/rtc/librtc.o
290 LIBS += drivers/serial/libserial.o
291 ifeq ($(CONFIG_GENERIC_LPC_TPM),y)
292 LIBS += drivers/tpm/libtpm.o
293 endif
294 LIBS += drivers/twserial/libtws.o
295 LIBS += drivers/usb/eth/libusb_eth.o
296 LIBS += drivers/usb/gadget/libusb_gadget.o
297 LIBS += drivers/usb/host/libusb_host.o
298 LIBS += drivers/usb/musb/libusb_musb.o
299 LIBS += drivers/usb/phy/libusb_phy.o
300 LIBS += drivers/usb/ulpi/libusb_ulpi.o
301 LIBS += drivers/video/libvideo.o
302 LIBS += drivers/watchdog/libwatchdog.o
303 LIBS += common/libcommon.o
304 LIBS += lib/libfdt/libfdt.o
305 LIBS += api/libapi.o
306 LIBS += post/libpost.o
307 LIBS += test/libtest.o
309 ifneq ($(CONFIG_AM33XX)$(CONFIG_OMAP34XX)$(CONFIG_OMAP44XX)$(CONFIG_OMAP54XX),)
310 LIBS += $(CPUDIR)/omap-common/libomap-common.o
311 endif
313 ifeq ($(SOC),mx5)
314 LIBS += $(CPUDIR)/imx-common/libimx-common.o
315 endif
316 ifeq ($(SOC),mx6)
317 LIBS += $(CPUDIR)/imx-common/libimx-common.o
318 endif
320 ifeq ($(SOC),s5pc1xx)
321 LIBS += $(CPUDIR)/s5p-common/libs5p-common.o
322 endif
323 ifeq ($(SOC),exynos)
324 LIBS += $(CPUDIR)/s5p-common/libs5p-common.o
325 endif
327 LIBS := $(addprefix $(obj),$(sort $(LIBS)))
328 .PHONY : $(LIBS)
330 LIBBOARD = board/$(BOARDDIR)/lib$(BOARD).o
331 LIBBOARD := $(addprefix $(obj),$(LIBBOARD))
333 # Add GCC lib
334 ifdef USE_PRIVATE_LIBGCC
335 ifeq ("$(USE_PRIVATE_LIBGCC)", "yes")
336 PLATFORM_LIBGCC = $(OBJTREE)/arch/$(ARCH)/lib/libgcc.o
337 else
338 PLATFORM_LIBGCC = -L $(USE_PRIVATE_LIBGCC) -lgcc
339 endif
340 else
341 PLATFORM_LIBGCC := -L $(shell dirname `$(CC) $(CFLAGS) -print-libgcc-file-name`) -lgcc
342 endif
343 PLATFORM_LIBS += $(PLATFORM_LIBGCC)
344 export PLATFORM_LIBS
346 # Special flags for CPP when processing the linker script.
347 # Pass the version down so we can handle backwards compatibility
348 # on the fly.
349 LDPPFLAGS += \
350         -include $(TOPDIR)/include/u-boot/u-boot.lds.h \
351         -DCPUDIR=$(CPUDIR) \
352         $(shell $(LD) --version | \
353           sed -ne 's/GNU ld version \([0-9][0-9]*\)\.\([0-9][0-9]*\).*/-DLD_MAJOR=\1 -DLD_MINOR=\2/p')
355 __OBJS := $(subst $(obj),,$(OBJS))
356 __LIBS := $(subst $(obj),,$(LIBS)) $(subst $(obj),,$(LIBBOARD))
358 #########################################################################
359 #########################################################################
361 ifneq ($(CONFIG_BOARD_SIZE_LIMIT),)
362 BOARD_SIZE_CHECK = \
363         @actual=`wc -c $@ | awk '{print $$1}'`; \
364         limit=$(CONFIG_BOARD_SIZE_LIMIT); \
365         if test $$actual -gt $$limit; then \
366                 echo "$@ exceeds file size limit:"; \
367                 echo "  limit:  $$limit bytes"; \
368                 echo "  actual: $$actual bytes"; \
369                 echo "  excess: $$((actual - limit)) bytes"; \
370                 exit 1; \
371         fi
372 else
373 BOARD_SIZE_CHECK =
374 endif
376 # Always append ALL so that arch config.mk's can add custom ones
377 ALL-y += $(obj)u-boot.srec $(obj)u-boot.bin $(obj)System.map
379 ALL-$(CONFIG_NAND_U_BOOT) += $(obj)u-boot-nand.bin
380 ALL-$(CONFIG_ONENAND_U_BOOT) += $(obj)u-boot-onenand.bin
381 ONENAND_BIN ?= $(obj)onenand_ipl/onenand-ipl-2k.bin
382 ALL-$(CONFIG_SPL) += $(obj)spl/u-boot-spl.bin
383 ALL-$(CONFIG_OF_SEPARATE) += $(obj)u-boot.dtb $(obj)u-boot-dtb.bin
385 all:            $(ALL-y) $(SUBDIR_EXAMPLES)
387 $(obj)u-boot.dtb:       $(obj)u-boot
388                 $(MAKE) -C dts binary
389                 mv $(obj)dts/dt.dtb $@
391 $(obj)u-boot-dtb.bin:   $(obj)u-boot.bin $(obj)u-boot.dtb
392                 cat $^ >$@
394 $(obj)u-boot.hex:       $(obj)u-boot
395                 $(OBJCOPY) ${OBJCFLAGS} -O ihex $< $@
397 $(obj)u-boot.srec:      $(obj)u-boot
398                 $(OBJCOPY) -O srec $< $@
400 $(obj)u-boot.bin:       $(obj)u-boot
401                 $(OBJCOPY) ${OBJCFLAGS} -O binary $< $@
402                 $(BOARD_SIZE_CHECK)
404 $(obj)u-boot.ldr:       $(obj)u-boot
405                 $(CREATE_LDR_ENV)
406                 $(LDR) -T $(CONFIG_BFIN_CPU) -c $@ $< $(LDR_FLAGS)
407                 $(BOARD_SIZE_CHECK)
409 $(obj)u-boot.ldr.hex:   $(obj)u-boot.ldr
410                 $(OBJCOPY) ${OBJCFLAGS} -O ihex $< $@ -I binary
412 $(obj)u-boot.ldr.srec:  $(obj)u-boot.ldr
413                 $(OBJCOPY) ${OBJCFLAGS} -O srec $< $@ -I binary
415 $(obj)u-boot.img:       $(obj)u-boot.bin
416                 $(obj)tools/mkimage -A $(ARCH) -T firmware -C none \
417                 -O u-boot -a $(CONFIG_SYS_TEXT_BASE) -e 0 \
418                 -n $(shell sed -n -e 's/.*U_BOOT_VERSION//p' $(VERSION_FILE) | \
419                         sed -e 's/"[     ]*$$/ for $(BOARD) board"/') \
420                 -d $< $@
422 $(obj)u-boot.imx:       $(obj)u-boot.bin
423                 $(obj)tools/mkimage -n  $(CONFIG_IMX_CONFIG) -T imximage \
424                 -e $(CONFIG_SYS_TEXT_BASE) -d $< $@
426 $(obj)u-boot.kwb:       $(obj)u-boot.bin
427                 $(obj)tools/mkimage -n $(CONFIG_SYS_KWD_CONFIG) -T kwbimage \
428                 -a $(CONFIG_SYS_TEXT_BASE) -e $(CONFIG_SYS_TEXT_BASE) -d $< $@
430 $(obj)u-boot.sha1:      $(obj)u-boot.bin
431                 $(obj)tools/ubsha1 $(obj)u-boot.bin
433 $(obj)u-boot.dis:       $(obj)u-boot
434                 $(OBJDUMP) -d $< > $@
436 $(obj)u-boot.ubl:       $(obj)spl/u-boot-spl.bin $(obj)u-boot.bin
437                 $(OBJCOPY) ${OBJCFLAGS} --pad-to=$(PAD_TO) -O binary $(obj)spl/u-boot-spl $(obj)spl/u-boot-spl-pad.bin
438                 cat $(obj)spl/u-boot-spl-pad.bin $(obj)u-boot.bin > $(obj)u-boot-ubl.bin
439                 $(obj)tools/mkimage -n $(UBL_CONFIG) -T ublimage \
440                 -e $(CONFIG_SYS_TEXT_BASE) -d $(obj)u-boot-ubl.bin $(obj)u-boot.ubl
441                 rm $(obj)u-boot-ubl.bin
442                 rm $(obj)spl/u-boot-spl-pad.bin
444 $(obj)u-boot.ais:       $(obj)spl/u-boot-spl.bin $(obj)u-boot.bin
445                 $(obj)tools/mkimage -s -n /dev/null -T aisimage \
446                         -e $(CONFIG_SPL_TEXT_BASE) \
447                         -d $(obj)spl/u-boot-spl.bin \
448                         $(obj)spl/u-boot-spl.ais
449                 $(OBJCOPY) ${OBJCFLAGS} -I binary \
450                         --pad-to=$(CONFIG_SPL_MAX_SIZE) -O binary \
451                         $(obj)spl/u-boot-spl.ais $(obj)spl/u-boot-spl-pad.ais
452                 cat $(obj)spl/u-boot-spl-pad.ais $(obj)u-boot.bin > \
453                         $(obj)u-boot.ais
454                 rm $(obj)spl/u-boot-spl{,-pad}.ais
456 $(obj)u-boot.sb:       $(obj)u-boot.bin $(obj)spl/u-boot-spl.bin
457                 elftosb -zdf imx28 -c $(TOPDIR)/board/$(BOARDDIR)/u-boot.bd \
458                         -o $(obj)u-boot.sb
460 # On x600 (SPEAr600) U-Boot is appended to U-Boot SPL.
461 # Both images are created using mkimage (crc etc), so that the ROM
462 # bootloader can check its integrity. Padding needs to be done to the
463 # SPL image (with mkimage header) and not the binary. Otherwise the resulting image
464 # which is loaded/copied by the ROM bootloader to SRAM doesn't fit.
465 # The resulting image containing both U-Boot images is called u-boot.spr
466 $(obj)u-boot.spr:       $(obj)u-boot.img $(obj)spl/u-boot-spl.bin
467                 $(obj)tools/mkimage -A $(ARCH) -T firmware -C none \
468                 -a $(CONFIG_SPL_TEXT_BASE) -e $(CONFIG_SPL_TEXT_BASE) -n XLOADER \
469                 -d $(obj)spl/u-boot-spl.bin $(obj)spl/u-boot-spl.img
470                 tr "\000" "\377" < /dev/zero | dd ibs=1 count=$(CONFIG_SPL_PAD_TO) \
471                         of=$(obj)spl/u-boot-spl-pad.img 2>/dev/null
472                 dd if=$(obj)spl/u-boot-spl.img of=$(obj)spl/u-boot-spl-pad.img \
473                         conv=notrunc 2>/dev/null
474                 cat $(obj)spl/u-boot-spl-pad.img $(obj)u-boot.img > $@
476 ifeq ($(CONFIG_SANDBOX),y)
477 GEN_UBOOT = \
478                 cd $(LNDIR) && $(CC) $(SYMS) -T $(obj)u-boot.lds \
479                         -Wl,--start-group $(__LIBS) -Wl,--end-group \
480                         $(PLATFORM_LIBS) -Wl,-Map -Wl,u-boot.map -o u-boot
481 else
482 GEN_UBOOT = \
483                 UNDEF_SYM=`$(OBJDUMP) -x $(LIBBOARD) $(LIBS) | \
484                 sed  -n -e 's/.*\($(SYM_PREFIX)__u_boot_cmd_.*\)/-u\1/p'|sort|uniq`;\
485                 cd $(LNDIR) && $(LD) $(LDFLAGS) $(LDFLAGS_$(@F)) $$UNDEF_SYM $(__OBJS) \
486                         --start-group $(__LIBS) --end-group $(PLATFORM_LIBS) \
487                         -Map u-boot.map -o u-boot
488 endif
490 $(obj)u-boot:   depend \
491                 $(SUBDIR_TOOLS) $(OBJS) $(LIBBOARD) $(LIBS) $(LDSCRIPT) $(obj)u-boot.lds
492                 $(GEN_UBOOT)
493 ifeq ($(CONFIG_KALLSYMS),y)
494                 smap=`$(call SYSTEM_MAP,u-boot) | \
495                         awk '$$2 ~ /[tTwW]/ {printf $$1 $$3 "\\\\000"}'` ; \
496                 $(CC) $(CFLAGS) -DSYSTEM_MAP="\"$${smap}\"" \
497                         -c common/system_map.c -o $(obj)common/system_map.o
498                 $(GEN_UBOOT) $(obj)common/system_map.o
499 endif
501 $(OBJS):        depend
502                 $(MAKE) -C $(CPUDIR) $(if $(REMOTE_BUILD),$@,$(notdir $@))
504 $(LIBS):        depend $(SUBDIR_TOOLS)
505                 $(MAKE) -C $(dir $(subst $(obj),,$@))
507 $(LIBBOARD):    depend $(LIBS)
508                 $(MAKE) -C $(dir $(subst $(obj),,$@))
510 $(SUBDIRS):     depend
511                 $(MAKE) -C $@ all
513 $(SUBDIR_EXAMPLES): $(obj)u-boot
515 $(LDSCRIPT):    depend
516                 $(MAKE) -C $(dir $@) $(notdir $@)
518 $(obj)u-boot.lds: $(LDSCRIPT)
519                 $(CPP) $(CPPFLAGS) $(LDPPFLAGS) -ansi -D__ASSEMBLY__ -P - <$^ >$@
521 nand_spl:       $(TIMESTAMP_FILE) $(VERSION_FILE) depend
522                 $(MAKE) -C nand_spl/board/$(BOARDDIR) all
524 $(obj)u-boot-nand.bin:  nand_spl $(obj)u-boot.bin
525                 cat $(obj)nand_spl/u-boot-spl-16k.bin $(obj)u-boot.bin > $(obj)u-boot-nand.bin
527 onenand_ipl:    $(TIMESTAMP_FILE) $(VERSION_FILE) $(obj)include/autoconf.mk
528                 $(MAKE) -C onenand_ipl/board/$(BOARDDIR) all
530 $(obj)u-boot-onenand.bin:       onenand_ipl $(obj)u-boot.bin
531                 cat $(ONENAND_BIN) $(obj)u-boot.bin > $(obj)u-boot-onenand.bin
533 $(obj)spl/u-boot-spl.bin:       $(SUBDIR_TOOLS) depend
534                 $(MAKE) -C spl all
536 updater:
537                 $(MAKE) -C tools/updater all
539 # Explicitly make _depend in subdirs containing multiple targets to prevent
540 # parallel sub-makes creating .depend files simultaneously.
541 depend dep:     $(TIMESTAMP_FILE) $(VERSION_FILE) \
542                 $(obj)include/autoconf.mk \
543                 $(obj)include/generated/generic-asm-offsets.h \
544                 $(obj)include/generated/asm-offsets.h
545                 for dir in $(SUBDIRS) $(CPUDIR) $(LDSCRIPT_MAKEFILE_DIR) ; do \
546                         $(MAKE) -C $$dir _depend ; done
548 TAG_SUBDIRS = $(SUBDIRS)
549 TAG_SUBDIRS += $(dir $(__LIBS))
550 TAG_SUBDIRS += include
552 FIND := find
553 FINDFLAGS := -L
555 checkstack:
556                 $(CROSS_COMPILE)objdump -d $(obj)u-boot \
557                         `$(FIND) $(obj) -name u-boot-spl -print` | \
558                         perl $(src)tools/checkstack.pl $(ARCH)
560 tags ctags:
561                 ctags -w -o $(obj)ctags `$(FIND) $(FINDFLAGS) $(TAG_SUBDIRS) \
562                                                 -name '*.[chS]' -print`
564 etags:
565                 etags -a -o $(obj)etags `$(FIND) $(FINDFLAGS) $(TAG_SUBDIRS) \
566                                                 -name '*.[chS]' -print`
567 cscope:
568                 $(FIND) $(FINDFLAGS) $(TAG_SUBDIRS) -name '*.[chS]' -print > \
569                                                 cscope.files
570                 cscope -b -q -k
572 SYSTEM_MAP = \
573                 $(NM) $1 | \
574                 grep -v '\(compiled\)\|\(\.o$$\)\|\( [aUw] \)\|\(\.\.ng$$\)\|\(LASH[RL]DI\)' | \
575                 LC_ALL=C sort
576 $(obj)System.map:       $(obj)u-boot
577                 @$(call SYSTEM_MAP,$<) > $(obj)System.map
579 checkthumb:
580         @if test $(call cc-version) -lt 0404; then \
581                 echo -n '*** Your GCC does not produce working '; \
582                 echo 'binaries in THUMB mode.'; \
583                 echo '*** Your board is configured for THUMB mode.'; \
584                 false; \
585         fi
587 # Auto-generate the autoconf.mk file (which is included by all makefiles)
589 # This target actually generates 2 files; autoconf.mk and autoconf.mk.dep.
590 # the dep file is only include in this top level makefile to determine when
591 # to regenerate the autoconf.mk file.
592 $(obj)include/autoconf.mk.dep: $(obj)include/config.h include/common.h
593         @$(XECHO) Generating $@ ; \
594         set -e ; \
595         : Generate the dependancies ; \
596         $(CC) -x c -DDO_DEPS_ONLY -M $(CFLAGS) $(CPPFLAGS) \
597                 -MQ $(obj)include/autoconf.mk include/common.h > $@
599 $(obj)include/autoconf.mk: $(obj)include/config.h
600         @$(XECHO) Generating $@ ; \
601         set -e ; \
602         : Extract the config macros ; \
603         $(CPP) $(CFLAGS) -DDO_DEPS_ONLY -dM include/common.h | \
604                 sed -n -f tools/scripts/define2mk.sed > $@.tmp && \
605         mv $@.tmp $@
607 $(obj)include/generated/generic-asm-offsets.h:  $(obj)include/autoconf.mk.dep \
608         $(obj)lib/asm-offsets.s
609         @$(XECHO) Generating $@
610         tools/scripts/make-asm-offsets $(obj)lib/asm-offsets.s $@
612 $(obj)lib/asm-offsets.s:        $(obj)include/autoconf.mk.dep \
613         $(src)lib/asm-offsets.c
614         @mkdir -p $(obj)lib
615         $(CC) -DDO_DEPS_ONLY \
616                 $(CFLAGS) $(CFLAGS_$(BCURDIR)/$(@F)) $(CFLAGS_$(BCURDIR)) \
617                 -o $@ $(src)lib/asm-offsets.c -c -S
619 $(obj)include/generated/asm-offsets.h:  $(obj)include/autoconf.mk.dep \
620         $(obj)$(CPUDIR)/$(SOC)/asm-offsets.s
621         @$(XECHO) Generating $@
622         tools/scripts/make-asm-offsets $(obj)$(CPUDIR)/$(SOC)/asm-offsets.s $@
624 $(obj)$(CPUDIR)/$(SOC)/asm-offsets.s:   $(obj)include/autoconf.mk.dep
625         @mkdir -p $(obj)$(CPUDIR)/$(SOC)
626         if [ -f $(src)$(CPUDIR)/$(SOC)/asm-offsets.c ];then \
627                 $(CC) -DDO_DEPS_ONLY \
628                 $(CFLAGS) $(CFLAGS_$(BCURDIR)/$(@F)) $(CFLAGS_$(BCURDIR)) \
629                         -o $@ $(src)$(CPUDIR)/$(SOC)/asm-offsets.c -c -S; \
630         else \
631                 touch $@; \
632         fi
634 #########################################################################
635 else    # !config.mk
636 all $(obj)u-boot.hex $(obj)u-boot.srec $(obj)u-boot.bin \
637 $(obj)u-boot.img $(obj)u-boot.dis $(obj)u-boot \
638 $(filter-out tools,$(SUBDIRS)) \
639 updater depend dep tags ctags etags cscope $(obj)System.map:
640         @echo "System not configured - see README" >&2
641         @ exit 1
643 tools: $(VERSION_FILE) $(TIMESTAMP_FILE)
644         $(MAKE) -C $@ all
645 endif   # config.mk
647 $(VERSION_FILE):
648                 @mkdir -p $(dir $(VERSION_FILE))
649                 @( localvers='$(shell $(TOPDIR)/tools/setlocalversion $(TOPDIR))' ; \
650                    printf '#define PLAIN_VERSION "%s%s"\n' \
651                         "$(U_BOOT_VERSION)" "$${localvers}" ; \
652                    printf '#define U_BOOT_VERSION "U-Boot %s%s"\n' \
653                         "$(U_BOOT_VERSION)" "$${localvers}" ; \
654                 ) > $@.tmp
655                 @( printf '#define CC_VERSION_STRING "%s"\n' \
656                  '$(shell $(CC) --version | head -n 1)' )>>  $@.tmp
657                 @( printf '#define LD_VERSION_STRING "%s"\n' \
658                  '$(shell $(LD) -v | head -n 1)' )>>  $@.tmp
659                 @cmp -s $@ $@.tmp && rm -f $@.tmp || mv -f $@.tmp $@
661 $(TIMESTAMP_FILE):
662                 @mkdir -p $(dir $(TIMESTAMP_FILE))
663                 @LC_ALL=C date +'#define U_BOOT_DATE "%b %d %C%y"' > $@.tmp
664                 @LC_ALL=C date +'#define U_BOOT_TIME "%T"' >> $@.tmp
665                 @cmp -s $@ $@.tmp && rm -f $@.tmp || mv -f $@.tmp $@
667 easylogo env gdb:
668         $(MAKE) -C tools/$@ all MTD_VERSION=${MTD_VERSION}
669 gdbtools: gdb
671 tools-all: easylogo env gdb $(VERSION_FILE) $(TIMESTAMP_FILE)
672         $(MAKE) -C tools HOST_TOOLS_ALL=y
674 .PHONY : CHANGELOG
675 CHANGELOG:
676         git log --no-merges U-Boot-1_1_5.. | \
677         unexpand -a | sed -e 's/\s\s*$$//' > $@
679 include/license.h: tools/bin2header COPYING
680         cat COPYING | gzip -9 -c | ./tools/bin2header license_gzip > include/license.h
681 #########################################################################
683 unconfig:
684         @rm -f $(obj)include/config.h $(obj)include/config.mk \
685                 $(obj)board/*/config.tmp $(obj)board/*/*/config.tmp \
686                 $(obj)include/autoconf.mk $(obj)include/autoconf.mk.dep
688 %_config::      unconfig
689         @$(MKCONFIG) -A $(@:_config=)
691 sinclude $(obj).boards.depend
692 $(obj).boards.depend:   boards.cfg
693         @awk '(NF && $$1 !~ /^#/) { print $$1 ": " $$1 "_config; $$(MAKE)" }' $< > $@
696 # Functions to generate common board directory names
698 lcname  = $(shell echo $(1) | sed -e 's/\(.*\)_config/\L\1/')
699 ucname  = $(shell echo $(1) | sed -e 's/\(.*\)_config/\U\1/')
701 #========================================================================
702 # ARM
703 #========================================================================
705 SX1_stdout_serial_config \
706 SX1_config:             unconfig
707         @mkdir -p $(obj)include
708         @if [ "$(findstring _stdout_serial_, $@)" ] ; then \
709                 echo "#undef CONFIG_STDOUT_USBTTY" >> $(obj)include/config.h ; \
710         else \
711                 echo "#define CONFIG_STDOUT_USBTTY" >> $(obj)include/config.h ; \
712         fi;
713         @$(MKCONFIG) -n $@ SX1 arm arm925t sx1
715 #########################################################################
716 ## ARM1176 Systems
717 #########################################################################
718 smdk6400_noUSB_config   \
719 smdk6400_config :       unconfig
720         @mkdir -p $(obj)include $(obj)board/samsung/smdk6400
721         @mkdir -p $(obj)nand_spl/board/samsung/smdk6400
722         @echo "#define CONFIG_NAND_U_BOOT" > $(obj)include/config.h
723         @echo "CONFIG_NAND_U_BOOT = y" >> $(obj)include/config.mk
724         @if [ -z "$(findstring smdk6400_noUSB_config,$@)" ]; then                       \
725                 echo "RAM_TEXT = 0x57e00000" >> $(obj)board/samsung/smdk6400/config.tmp;\
726         else                                                                            \
727                 echo "RAM_TEXT = 0xc7e00000" >> $(obj)board/samsung/smdk6400/config.tmp;\
728         fi
729         @$(MKCONFIG) smdk6400 arm arm1176 smdk6400 samsung s3c64xx
730         @echo "CONFIG_NAND_U_BOOT = y" >> $(obj)include/config.mk
732 #########################################################################
733 #########################################################################
735 clean:
736         @rm -f $(obj)examples/standalone/82559_eeprom                     \
737                $(obj)examples/standalone/atmel_df_pow2                    \
738                $(obj)examples/standalone/eepro100_eeprom                  \
739                $(obj)examples/standalone/hello_world                      \
740                $(obj)examples/standalone/interrupt                        \
741                $(obj)examples/standalone/mem_to_mem_idma2intr             \
742                $(obj)examples/standalone/sched                            \
743                $(obj)examples/standalone/smc911{11,x}_eeprom              \
744                $(obj)examples/standalone/test_burst                       \
745                $(obj)examples/standalone/timer
746         @rm -f $(obj)examples/api/demo{,.bin}
747         @rm -f $(obj)tools/bmp_logo        $(obj)tools/easylogo/easylogo  \
748                $(obj)tools/env/{fw_printenv,fw_setenv}                    \
749                $(obj)tools/envcrc                                         \
750                $(obj)tools/gdb/{astest,gdbcont,gdbsend}                   \
751                $(obj)tools/gen_eth_addr    $(obj)tools/img2srec           \
752                $(obj)tools/mk{env,}image   $(obj)tools/mpc86x_clk         \
753                $(obj)tools/mk{smdk5250,}spl                               \
754                $(obj)tools/ncb             $(obj)tools/ubsha1
755         @rm -f $(obj)board/cray/L1/{bootscript.c,bootscript.image}        \
756                $(obj)board/matrix_vision/*/bootscript.img                 \
757                $(obj)board/voiceblue/eeprom                               \
758                $(obj)u-boot.lds                                           \
759                $(obj)arch/blackfin/cpu/bootrom-asm-offsets.[chs]          \
760                $(obj)arch/blackfin/cpu/init.{lds,elf}
761         @rm -f $(obj)include/bmp_logo.h
762         @rm -f $(obj)include/bmp_logo_data.h
763         @rm -f $(obj)lib/asm-offsets.s
764         @rm -f $(obj)include/generated/asm-offsets.h
765         @rm -f $(obj)$(CPUDIR)/$(SOC)/asm-offsets.s
766         @rm -f $(obj)nand_spl/{u-boot.lds,u-boot-nand_spl.lds,u-boot-spl,u-boot-spl.map,System.map}
767         @rm -f $(obj)onenand_ipl/onenand-{ipl,ipl.bin,ipl.map}
768         @rm -f $(ONENAND_BIN)
769         @rm -f $(obj)onenand_ipl/u-boot.lds
770         @rm -f $(obj)spl/{u-boot-spl,u-boot-spl.bin,u-boot-spl.lds,u-boot-spl.map}
771         @rm -f $(obj)MLO
772         @rm -f $(TIMESTAMP_FILE) $(VERSION_FILE)
773         @find $(OBJTREE) -type f \
774                 \( -name 'core' -o -name '*.bak' -o -name '*~' -o -name '*.su' \
775                 -o -name '*.o'  -o -name '*.a' -o -name '*.exe' \) -print \
776                 | xargs rm -f
778 # Removes everything not needed for testing u-boot
779 tidy:   clean
780         @find $(OBJTREE) -type f \( -name '*.depend*' \) -print | xargs rm -f
782 clobber:        tidy
783         @find $(OBJTREE) -type f \( -name '*.srec' \
784                 -o -name '*.bin' -o -name u-boot.img \) \
785                 -print0 | xargs -0 rm -f
786         @rm -f $(OBJS) $(obj)*.bak $(obj)ctags $(obj)etags $(obj)TAGS \
787                 $(obj)cscope.* $(obj)*.*~
788         @rm -f $(obj)u-boot $(obj)u-boot.map $(obj)u-boot.hex $(ALL-y)
789         @rm -f $(obj)u-boot.kwb
790         @rm -f $(obj)u-boot.imx
791         @rm -f $(obj)u-boot.ubl
792         @rm -f $(obj)u-boot.ais
793         @rm -f $(obj)u-boot.dtb
794         @rm -f $(obj)u-boot.sb
795         @rm -f $(obj)u-boot.spr
796         @rm -f $(obj)tools/xway-swap-bytes
797         @rm -f $(obj)arch/powerpc/cpu/mpc824x/bedbug_603e.c
798         @rm -f $(obj)arch/powerpc/cpu/mpc83xx/ddr-gen?.c
799         @rm -fr $(obj)include/asm/proc $(obj)include/asm/arch $(obj)include/asm
800         @rm -fr $(obj)include/generated
801         @[ ! -d $(obj)nand_spl ] || find $(obj)nand_spl -name "*" -type l -print | xargs rm -f
802         @[ ! -d $(obj)onenand_ipl ] || find $(obj)onenand_ipl -name "*" -type l -print | xargs rm -f
803         @rm -f $(obj)dts/*.tmp
805 mrproper \
806 distclean:      clobber unconfig
807 ifneq ($(OBJTREE),$(SRCTREE))
808         rm -rf $(obj)*
809 endif
811 backup:
812         F=`basename $(TOPDIR)` ; cd .. ; \
813         gtar --force-local -zcvf `LC_ALL=C date "+$$F-%Y-%m-%d-%T.tar.gz"` $$F
815 #########################################################################