]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/glsdk-u-boot.git/blob - api/api.c
rename CFG_ENV macros to CONFIG_ENV
[glsdk/glsdk-u-boot.git] / api / api.c
1 /*
2  * (C) Copyright 2007 Semihalf
3  *
4  * Written by: Rafal Jaworowski <raj@semihalf.com>
5  *
6  * See file CREDITS for list of people who contributed to this
7  * project.
8  *
9  * This program is free software; you can redistribute it and/or
10  * modify it under the terms of the GNU General Public License as
11  * published by the Free Software Foundation; either version 2 of
12  * the License, or (at your option) any later version.
13  *
14  * This program is distributed in the hope that it will be useful,
15  * but WITHOUT ANY WARRANTY; without even the implied warranty of
16  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
17  * GNU General Public License for more details.
18  *
19  * You should have received a copy of the GNU General Public License
20  * along with this program; if not, write to the Free Software
21  * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
22  * MA 02111-1307 USA
23  *
24  */
26 #include <config.h>
28 #if defined(CONFIG_API)
30 #include <command.h>
31 #include <common.h>
32 #include <malloc.h>
33 #include <environment.h>
34 #include <linux/types.h>
35 #include <api_public.h>
37 #include "api_private.h"
39 #define DEBUG
40 #undef DEBUG
42 /* U-Boot routines needed */
43 extern int do_reset (cmd_tbl_t *cmdtp, int flag, int argc, char *argv[]);
45 /*****************************************************************************
46  *
47  * This is the API core.
48  *
49  * API_ functions are part of U-Boot code and constitute the lowest level
50  * calls:
51  *
52  *  - they know what values they need as arguments
53  *  - their direct return value pertains to the API_ "shell" itself (0 on
54  *    success, some error code otherwise)
55  *  - if the call returns a value it is buried within arguments
56  *
57  ****************************************************************************/
59 #ifdef DEBUG
60 #define debugf(fmt, args...) do { printf("%s(): ", __func__); printf(fmt, ##args); } while (0)
61 #else
62 #define debugf(fmt, args...)
63 #endif
65 typedef int (*cfp_t)(va_list argp);
67 static int calls_no;
69 /*
70  * pseudo signature:
71  *
72  * int API_getc(int *c)
73  */
74 static int API_getc(va_list ap)
75 {
76         int *c;
78         if ((c = (int *)va_arg(ap, u_int32_t)) == NULL)
79                 return API_EINVAL;
81         *c = getc();
82         return 0;
83 }
85 /*
86  * pseudo signature:
87  *
88  * int API_tstc(int *c)
89  */
90 static int API_tstc(va_list ap)
91 {
92         int *t;
94         if ((t = (int *)va_arg(ap, u_int32_t)) == NULL)
95                 return API_EINVAL;
97         *t = tstc();
98         return 0;
99 }
101 /*
102  * pseudo signature:
103  *
104  * int API_putc(char *ch)
105  */
106 static int API_putc(va_list ap)
108         char *c;
110         if ((c = (char *)va_arg(ap, u_int32_t)) == NULL)
111                 return API_EINVAL;
113         putc(*c);
114         return 0;
117 /*
118  * pseudo signature:
119  *
120  * int API_puts(char **s)
121  */
122 static int API_puts(va_list ap)
124         char *s;
126         if ((s = (char *)va_arg(ap, u_int32_t)) == NULL)
127                 return API_EINVAL;
129         puts(s);
130         return 0;
133 /*
134  * pseudo signature:
135  *
136  * int API_reset(void)
137  */
138 static int API_reset(va_list ap)
140         do_reset(NULL, 0, 0, NULL);
142         /* NOT REACHED */
143         return 0;
146 /*
147  * pseudo signature:
148  *
149  * int API_get_sys_info(struct sys_info *si)
150  *
151  * fill out the sys_info struct containing selected parameters about the
152  * machine
153  */
154 static int API_get_sys_info(va_list ap)
156         struct sys_info *si;
158         si = (struct sys_info *)va_arg(ap, u_int32_t);
159         if (si == NULL)
160                 return API_ENOMEM;
162         return (platform_sys_info(si)) ? 0 : API_ENODEV;
165 /*
166  * pseudo signature:
167  *
168  * int API_udelay(unsigned long *udelay)
169  */
170 static int API_udelay(va_list ap)
172         unsigned long *d;
174         if ((d = (unsigned long *)va_arg(ap, u_int32_t)) == NULL)
175                 return API_EINVAL;
177         udelay(*d);
178         return 0;
181 /*
182  * pseudo signature:
183  *
184  * int API_get_timer(unsigned long *current, unsigned long *base)
185  */
186 static int API_get_timer(va_list ap)
188         unsigned long *base, *cur;
190         cur = (unsigned long *)va_arg(ap, u_int32_t);
191         if (cur == NULL)
192                 return API_EINVAL;
194         base = (unsigned long *)va_arg(ap, u_int32_t);
195         if (base == NULL)
196                 return API_EINVAL;
198         *cur = get_timer(*base);
199         return 0;
203 /*****************************************************************************
204  *
205  * pseudo signature:
206  *
207  * int API_dev_enum(struct device_info *)
208  *
209  *
210  * cookies uniqely identify the previously enumerated device instance and
211  * provide a hint for what to inspect in current enum iteration:
212  *
213  *   - net: &eth_device struct address from list pointed to by eth_devices
214  *
215  *   - storage: block_dev_desc_t struct address from &ide_dev_desc[n],
216  *     &scsi_dev_desc[n] and similar tables
217  *
218  ****************************************************************************/
220 static int API_dev_enum(va_list ap)
222         struct device_info *di;
224         /* arg is ptr to the device_info struct we are going to fill out */
225         di = (struct device_info *)va_arg(ap, u_int32_t);
226         if (di == NULL)
227                 return API_EINVAL;
229         if (di->cookie == NULL) {
230                 /* start over - clean up enumeration */
231                 dev_enum_reset();       /* XXX shouldn't the name contain 'stor'? */
232                 debugf("RESTART ENUM\n");
234                 /* net device enumeration first */
235                 if (dev_enum_net(di))
236                         return 0;
237         }
239         /*
240          * The hidden assumption is there can only be one active network
241          * device and it is identified upon enumeration (re)start, so there's
242          * no point in trying to find network devices in other cases than the
243          * (re)start and hence the 'next' device can only be storage
244          */
245         if (!dev_enum_storage(di))
246                 /* make sure we mark there are no more devices */
247                 di->cookie = NULL;
249         return 0;
253 static int API_dev_open(va_list ap)
255         struct device_info *di;
256         int err = 0;
258         /* arg is ptr to the device_info struct */
259         di = (struct device_info *)va_arg(ap, u_int32_t);
260         if (di == NULL)
261                 return API_EINVAL;
263         /* Allow only one consumer of the device at a time */
264         if (di->state == DEV_STA_OPEN)
265                 return API_EBUSY;
267         if (di->cookie == NULL)
268                 return API_ENODEV;
270         if (di->type & DEV_TYP_STOR)
271                 err = dev_open_stor(di->cookie);
273         else if (di->type & DEV_TYP_NET)
274                 err = dev_open_net(di->cookie);
275         else
276                 err = API_ENODEV;
278         if (!err)
279                 di->state = DEV_STA_OPEN;
281         return err;
285 static int API_dev_close(va_list ap)
287         struct device_info *di;
288         int err = 0;
290         /* arg is ptr to the device_info struct */
291         di = (struct device_info *)va_arg(ap, u_int32_t);
292         if (di == NULL)
293                 return API_EINVAL;
295         if (di->state == DEV_STA_CLOSED)
296                 return 0;
298         if (di->cookie == NULL)
299                 return API_ENODEV;
301         if (di->type & DEV_TYP_STOR)
302                 err = dev_close_stor(di->cookie);
304         else if (di->type & DEV_TYP_NET)
305                 err = dev_close_net(di->cookie);
306         else
307                 /*
308                  * In case of unknown device we cannot change its state, so
309                  * only return error code
310                  */
311                 err = API_ENODEV;
313         if (!err)
314                 di->state = DEV_STA_CLOSED;
316         return err;
320 /*
321  * Notice: this is for sending network packets only, as U-Boot does not
322  * support writing to storage at the moment (12.2007)
323  *
324  * pseudo signature:
325  *
326  * int API_dev_write(
327  *      struct device_info *di,
328  *      void *buf,
329  *      int *len
330  * )
331  *
332  * buf: ptr to buffer from where to get the data to send
333  *
334  * len: length of packet to be sent (in bytes)
335  *
336  */
337 static int API_dev_write(va_list ap)
339         struct device_info *di;
340         void *buf;
341         int *len;
342         int err = 0;
344         /* 1. arg is ptr to the device_info struct */
345         di = (struct device_info *)va_arg(ap, u_int32_t);
346         if (di == NULL)
347                 return API_EINVAL;
349         /* XXX should we check if device is open? i.e. the ->state ? */
351         if (di->cookie == NULL)
352                 return API_ENODEV;
354         /* 2. arg is ptr to buffer from where to get data to write */
355         buf = (void *)va_arg(ap, u_int32_t);
356         if (buf == NULL)
357                 return API_EINVAL;
359         /* 3. arg is length of buffer */
360         len = (int *)va_arg(ap, u_int32_t);
361         if (len == NULL)
362                 return API_EINVAL;
363         if (*len <= 0)
364                 return API_EINVAL;
366         if (di->type & DEV_TYP_STOR)
367                 /*
368                  * write to storage is currently not supported by U-Boot:
369                  * no storage device implements block_write() method
370                  */
371                 return API_ENODEV;
373         else if (di->type & DEV_TYP_NET)
374                 err = dev_write_net(di->cookie, buf, *len);
375         else
376                 err = API_ENODEV;
378         return err;
382 /*
383  * pseudo signature:
384  *
385  * int API_dev_read(
386  *      struct device_info *di,
387  *      void *buf,
388  *      size_t *len,
389  *      unsigned long *start
390  *      size_t *act_len
391  * )
392  *
393  * buf: ptr to buffer where to put the read data
394  *
395  * len: ptr to length to be read
396  *      - network: len of packet to read (in bytes)
397  *      - storage: # of blocks to read (can vary in size depending on define)
398  *
399  * start: ptr to start block (only used for storage devices, ignored for
400  *        network)
401  *
402  * act_len: ptr to where to put the len actually read
403  */
404 static int API_dev_read(va_list ap)
406         struct device_info *di;
407         void *buf;
408         lbasize_t *len_stor, *act_len_stor;
409         lbastart_t *start;
410         int *len_net, *act_len_net;
412         /* 1. arg is ptr to the device_info struct */
413         di = (struct device_info *)va_arg(ap, u_int32_t);
414         if (di == NULL)
415                 return API_EINVAL;
417         /* XXX should we check if device is open? i.e. the ->state ? */
419         if (di->cookie == NULL)
420                 return API_ENODEV;
422         /* 2. arg is ptr to buffer from where to put the read data */
423         buf = (void *)va_arg(ap, u_int32_t);
424         if (buf == NULL)
425                 return API_EINVAL;
427         if (di->type & DEV_TYP_STOR) {
428                 /* 3. arg - ptr to var with # of blocks to read */
429                 len_stor = (lbasize_t *)va_arg(ap, u_int32_t);
430                 if (!len_stor)
431                         return API_EINVAL;
432                 if (*len_stor <= 0)
433                         return API_EINVAL;
435                 /* 4. arg - ptr to var with start block */
436                 start = (lbastart_t *)va_arg(ap, u_int32_t);
438                 /* 5. arg - ptr to var where to put the len actually read */
439                 act_len_stor = (lbasize_t *)va_arg(ap, u_int32_t);
440                 if (!act_len_stor)
441                         return API_EINVAL;
443                 *act_len_stor = dev_read_stor(di->cookie, buf, *len_stor, *start);
445         } else if (di->type & DEV_TYP_NET) {
447                 /* 3. arg points to the var with length of packet to read */
448                 len_net = (int *)va_arg(ap, u_int32_t);
449                 if (!len_net)
450                         return API_EINVAL;
451                 if (*len_net <= 0)
452                         return API_EINVAL;
454                 /* 4. - ptr to var where to put the len actually read */
455                 act_len_net = (int *)va_arg(ap, u_int32_t);
456                 if (!act_len_net)
457                         return API_EINVAL;
459                 *act_len_net = dev_read_net(di->cookie, buf, *len_net);
461         } else
462                 return API_ENODEV;
464         return 0;
468 /*
469  * pseudo signature:
470  *
471  * int API_env_get(const char *name, char **value)
472  *
473  * name: ptr to name of env var
474  */
475 static int API_env_get(va_list ap)
477         char *name, **value;
479         if ((name = (char *)va_arg(ap, u_int32_t)) == NULL)
480                 return API_EINVAL;
481         if ((value = (char **)va_arg(ap, u_int32_t)) == NULL)
482                 return API_EINVAL;
484         *value = getenv(name);
486         return 0;
489 /*
490  * pseudo signature:
491  *
492  * int API_env_set(const char *name, const char *value)
493  *
494  * name: ptr to name of env var
495  *
496  * value: ptr to value to be set
497  */
498 static int API_env_set(va_list ap)
500         char *name, *value;
502         if ((name = (char *)va_arg(ap, u_int32_t)) == NULL)
503                 return API_EINVAL;
504         if ((value = (char *)va_arg(ap, u_int32_t)) == NULL)
505                 return API_EINVAL;
507         setenv(name, value);
509         return 0;
512 /*
513  * pseudo signature:
514  *
515  * int API_env_enum(const char *last, char **next)
516  *
517  * last: ptr to name of env var found in last iteration
518  */
519 static int API_env_enum(va_list ap)
521         int i, n;
522         char *last, **next;
524         last = (char *)va_arg(ap, u_int32_t);
526         if ((next = (char **)va_arg(ap, u_int32_t)) == NULL)
527                 return API_EINVAL;
529         if (last == NULL)
530                 /* start over */
531                 *next = ((char *)env_get_addr(0));
532         else {
533                 *next = last;
535                 for (i = 0; env_get_char(i) != '\0'; i = n + 1) {
536                         for (n = i; env_get_char(n) != '\0'; ++n) {
537                                 if (n >= CONFIG_ENV_SIZE) {
538                                         /* XXX shouldn't we set *next = NULL?? */
539                                         return 0;
540                                 }
541                         }
543                         if (envmatch((uchar *)last, i) < 0)
544                                 continue;
546                         /* try to get next name */
547                         i = n + 1;
548                         if (env_get_char(i) == '\0') {
549                                 /* no more left */
550                                 *next = NULL;
551                                 return 0;
552                         }
554                         *next = ((char *)env_get_addr(i));
555                         return 0;
556                 }
557         }
559         return 0;
562 static cfp_t calls_table[API_MAXCALL] = { NULL, };
564 /*
565  * The main syscall entry point - this is not reentrant, only one call is
566  * serviced until finished.
567  *
568  * e.g. syscall(1, int *, u_int32_t, u_int32_t, u_int32_t, u_int32_t);
569  *
570  * call:        syscall number
571  *
572  * retval:      points to the return value placeholder, this is the place the
573  *              syscall puts its return value, if NULL the caller does not
574  *              expect a return value
575  *
576  * ...          syscall arguments (variable number)
577  *
578  * returns:     0 if the call not found, 1 if serviced
579  */
580 int syscall(int call, int *retval, ...)
582         va_list ap;
583         int rv;
585         if (call < 0 || call >= calls_no) {
586                 debugf("invalid call #%d\n", call);
587                 return 0;
588         }
590         if (calls_table[call] == NULL) {
591                 debugf("syscall #%d does not have a handler\n", call);
592                 return 0;
593         }
595         va_start(ap, retval);
596         rv = calls_table[call](ap);
597         if (retval != NULL)
598                 *retval = rv;
600         return 1;
603 void api_init(void)
605         struct api_signature *sig = NULL;
607         /* TODO put this into linker set one day... */
608         calls_table[API_RSVD] = NULL;
609         calls_table[API_GETC] = &API_getc;
610         calls_table[API_PUTC] = &API_putc;
611         calls_table[API_TSTC] = &API_tstc;
612         calls_table[API_PUTS] = &API_puts;
613         calls_table[API_RESET] = &API_reset;
614         calls_table[API_GET_SYS_INFO] = &API_get_sys_info;
615         calls_table[API_UDELAY] = &API_udelay;
616         calls_table[API_GET_TIMER] = &API_get_timer;
617         calls_table[API_DEV_ENUM] = &API_dev_enum;
618         calls_table[API_DEV_OPEN] = &API_dev_open;
619         calls_table[API_DEV_CLOSE] = &API_dev_close;
620         calls_table[API_DEV_READ] = &API_dev_read;
621         calls_table[API_DEV_WRITE] = &API_dev_write;
622         calls_table[API_ENV_GET] = &API_env_get;
623         calls_table[API_ENV_SET] = &API_env_set;
624         calls_table[API_ENV_ENUM] = &API_env_enum;
625         calls_no = API_MAXCALL;
627         debugf("API initialized with %d calls\n", calls_no);
629         dev_stor_init();
631         /*
632          * Produce the signature so the API consumers can find it
633          */
634         sig = malloc(sizeof(struct api_signature));
635         if (sig == NULL) {
636                 printf("API: could not allocate memory for the signature!\n");
637                 return;
638         }
640         debugf("API sig @ 0x%08x\n", sig);
641         memcpy(sig->magic, API_SIG_MAGIC, 8);
642         sig->version = API_SIG_VERSION;
643         sig->syscall = &syscall;
644         sig->checksum = 0;
645         sig->checksum = crc32(0, (unsigned char *)sig,
646                               sizeof(struct api_signature));
647         debugf("syscall entry: 0x%08x\n", sig->syscall);
650 void platform_set_mr(struct sys_info *si, unsigned long start, unsigned long size,
651                         int flags)
653         int i;
655         if (!si->mr || !size || (flags == 0))
656                 return;
658         /* find free slot */
659         for (i = 0; i < si->mr_no; i++)
660                 if (si->mr[i].flags == 0) {
661                         /* insert new mem region */
662                         si->mr[i].start = start;
663                         si->mr[i].size = size;
664                         si->mr[i].flags = flags;
665                         return;
666                 }
669 #endif /* CONFIG_API */