1 /*
2 * (C) Copyright 2007 Semihalf
3 *
4 * Written by: Rafal Jaworowski <raj@semihalf.com>
5 *
6 * See file CREDITS for list of people who contributed to this
7 * project.
8 *
9 * This program is free software; you can redistribute it and/or
10 * modify it under the terms of the GNU General Public License as
11 * published by the Free Software Foundation; either version 2 of
12 * the License, or (at your option) any later version.
13 *
14 * This program is distributed in the hope that it will be useful,
15 * but WITHOUT ANY WARRANTY; without even the implied warranty of
16 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
17 * GNU General Public License for more details.
18 *
19 * You should have received a copy of the GNU General Public License
20 * along with this program; if not, write to the Free Software
21 * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
22 * MA 02111-1307 USA
23 *
24 */
26 #include <config.h>
28 #if defined(CONFIG_API)
30 #include <command.h>
31 #include <common.h>
32 #include <malloc.h>
33 #include <linux/types.h>
34 #include <api_public.h>
36 #include "api_private.h"
38 #define DEBUG
39 #undef DEBUG
41 /* U-Boot routines needed */
42 extern int do_reset (cmd_tbl_t *cmdtp, int flag, int argc, char *argv[]);
43 extern uchar (*env_get_char)(int);
44 extern uchar *env_get_addr(int);
46 /*****************************************************************************
47 *
48 * This is the API core.
49 *
50 * API_ functions are part of U-Boot code and constitute the lowest level
51 * calls:
52 *
53 * - they know what values they need as arguments
54 * - their direct return value pertains to the API_ "shell" itself (0 on
55 * success, some error code otherwise)
56 * - if the call returns a value it is buried within arguments
57 *
58 ****************************************************************************/
60 #ifdef DEBUG
61 #define debugf(fmt, args...) do { printf("%s(): ", __func__); printf(fmt, ##args); } while (0)
62 #else
63 #define debugf(fmt, args...)
64 #endif
66 typedef int (*cfp_t)(va_list argp);
68 static int calls_no;
70 /*
71 * pseudo signature:
72 *
73 * int API_getc(int *c)
74 */
75 static int API_getc(va_list ap)
76 {
77 int *c;
79 if ((c = (int *)va_arg(ap, u_int32_t)) == NULL)
80 return API_EINVAL;
82 *c = getc();
83 return 0;
84 }
86 /*
87 * pseudo signature:
88 *
89 * int API_tstc(int *c)
90 */
91 static int API_tstc(va_list ap)
92 {
93 int *t;
95 if ((t = (int *)va_arg(ap, u_int32_t)) == NULL)
96 return API_EINVAL;
98 *t = tstc();
99 return 0;
100 }
102 /*
103 * pseudo signature:
104 *
105 * int API_putc(char *ch)
106 */
107 static int API_putc(va_list ap)
108 {
109 char *c;
111 if ((c = (char *)va_arg(ap, u_int32_t)) == NULL)
112 return API_EINVAL;
114 putc(*c);
115 return 0;
116 }
118 /*
119 * pseudo signature:
120 *
121 * int API_puts(char **s)
122 */
123 static int API_puts(va_list ap)
124 {
125 char *s;
127 if ((s = (char *)va_arg(ap, u_int32_t)) == NULL)
128 return API_EINVAL;
130 puts(s);
131 return 0;
132 }
134 /*
135 * pseudo signature:
136 *
137 * int API_reset(void)
138 */
139 static int API_reset(va_list ap)
140 {
141 do_reset(NULL, 0, 0, NULL);
143 /* NOT REACHED */
144 return 0;
145 }
147 /*
148 * pseudo signature:
149 *
150 * int API_get_sys_info(struct sys_info *si)
151 *
152 * fill out the sys_info struct containing selected parameters about the
153 * machine
154 */
155 static int API_get_sys_info(va_list ap)
156 {
157 struct sys_info *si;
159 si = (struct sys_info *)va_arg(ap, u_int32_t);
160 if (si == NULL)
161 return API_ENOMEM;
163 return (platform_sys_info(si)) ? 0 : API_ENODEV;
164 }
166 /*
167 * pseudo signature:
168 *
169 * int API_udelay(unsigned long *udelay)
170 */
171 static int API_udelay(va_list ap)
172 {
173 unsigned long *d;
175 if ((d = (unsigned long *)va_arg(ap, u_int32_t)) == NULL)
176 return API_EINVAL;
178 udelay(*d);
179 return 0;
180 }
182 /*
183 * pseudo signature:
184 *
185 * int API_get_timer(unsigned long *current, unsigned long *base)
186 */
187 static int API_get_timer(va_list ap)
188 {
189 unsigned long *base, *cur;
191 cur = (unsigned long *)va_arg(ap, u_int32_t);
192 if (cur == NULL)
193 return API_EINVAL;
195 base = (unsigned long *)va_arg(ap, u_int32_t);
196 if (base == NULL)
197 return API_EINVAL;
199 *cur = get_timer(*base);
200 return 0;
201 }
204 /*****************************************************************************
205 *
206 * pseudo signature:
207 *
208 * int API_dev_enum(struct device_info *)
209 *
210 *
211 * cookies uniqely identify the previously enumerated device instance and
212 * provide a hint for what to inspect in current enum iteration:
213 *
214 * - net: ð_device struct address from list pointed to by eth_devices
215 *
216 * - storage: block_dev_desc_t struct address from &ide_dev_desc[n],
217 * &scsi_dev_desc[n] and similar tables
218 *
219 ****************************************************************************/
221 static int API_dev_enum(va_list ap)
222 {
223 struct device_info *di;
225 /* arg is ptr to the device_info struct we are going to fill out */
226 di = (struct device_info *)va_arg(ap, u_int32_t);
227 if (di == NULL)
228 return API_EINVAL;
230 if (di->cookie == NULL) {
231 /* start over - clean up enumeration */
232 dev_enum_reset(); /* XXX shouldn't the name contain 'stor'? */
233 debugf("RESTART ENUM\n");
235 /* net device enumeration first */
236 if (dev_enum_net(di))
237 return 0;
238 }
240 /*
241 * The hidden assumption is there can only be one active network
242 * device and it is identified upon enumeration (re)start, so there's
243 * no point in trying to find network devices in other cases than the
244 * (re)start and hence the 'next' device can only be storage
245 */
246 if (!dev_enum_storage(di))
247 /* make sure we mark there are no more devices */
248 di->cookie = NULL;
250 return 0;
251 }
254 static int API_dev_open(va_list ap)
255 {
256 struct device_info *di;
257 int err = 0;
259 /* arg is ptr to the device_info struct */
260 di = (struct device_info *)va_arg(ap, u_int32_t);
261 if (di == NULL)
262 return API_EINVAL;
264 /* Allow only one consumer of the device at a time */
265 if (di->state == DEV_STA_OPEN)
266 return API_EBUSY;
268 if (di->cookie == NULL)
269 return API_ENODEV;
271 if (di->type & DEV_TYP_STOR)
272 err = dev_open_stor(di->cookie);
274 else if (di->type & DEV_TYP_NET)
275 err = dev_open_net(di->cookie);
276 else
277 err = API_ENODEV;
279 if (!err)
280 di->state = DEV_STA_OPEN;
282 return err;
283 }
286 static int API_dev_close(va_list ap)
287 {
288 struct device_info *di;
289 int err = 0;
291 /* arg is ptr to the device_info struct */
292 di = (struct device_info *)va_arg(ap, u_int32_t);
293 if (di == NULL)
294 return API_EINVAL;
296 if (di->state == DEV_STA_CLOSED)
297 return 0;
299 if (di->cookie == NULL)
300 return API_ENODEV;
302 if (di->type & DEV_TYP_STOR)
303 err = dev_close_stor(di->cookie);
305 else if (di->type & DEV_TYP_NET)
306 err = dev_close_net(di->cookie);
307 else
308 /*
309 * In case of unknown device we cannot change its state, so
310 * only return error code
311 */
312 err = API_ENODEV;
314 if (!err)
315 di->state = DEV_STA_CLOSED;
317 return err;
318 }
321 /*
322 * Notice: this is for sending network packets only, as U-Boot does not
323 * support writing to storage at the moment (12.2007)
324 *
325 * pseudo signature:
326 *
327 * int API_dev_write(
328 * struct device_info *di,
329 * void *buf,
330 * int *len
331 * )
332 *
333 * buf: ptr to buffer from where to get the data to send
334 *
335 * len: length of packet to be sent (in bytes)
336 *
337 */
338 static int API_dev_write(va_list ap)
339 {
340 struct device_info *di;
341 void *buf;
342 int *len;
343 int err = 0;
345 /* 1. arg is ptr to the device_info struct */
346 di = (struct device_info *)va_arg(ap, u_int32_t);
347 if (di == NULL)
348 return API_EINVAL;
350 /* XXX should we check if device is open? i.e. the ->state ? */
352 if (di->cookie == NULL)
353 return API_ENODEV;
355 /* 2. arg is ptr to buffer from where to get data to write */
356 buf = (void *)va_arg(ap, u_int32_t);
357 if (buf == NULL)
358 return API_EINVAL;
360 /* 3. arg is length of buffer */
361 len = (int *)va_arg(ap, u_int32_t);
362 if (len == NULL)
363 return API_EINVAL;
364 if (*len <= 0)
365 return API_EINVAL;
367 if (di->type & DEV_TYP_STOR)
368 /*
369 * write to storage is currently not supported by U-Boot:
370 * no storage device implements block_write() method
371 */
372 return API_ENODEV;
374 else if (di->type & DEV_TYP_NET)
375 err = dev_write_net(di->cookie, buf, *len);
376 else
377 err = API_ENODEV;
379 return err;
380 }
383 /*
384 * pseudo signature:
385 *
386 * int API_dev_read(
387 * struct device_info *di,
388 * void *buf,
389 * size_t *len,
390 * unsigned long *start
391 * size_t *act_len
392 * )
393 *
394 * buf: ptr to buffer where to put the read data
395 *
396 * len: ptr to length to be read
397 * - network: len of packet to read (in bytes)
398 * - storage: # of blocks to read (can vary in size depending on define)
399 *
400 * start: ptr to start block (only used for storage devices, ignored for
401 * network)
402 *
403 * act_len: ptr to where to put the len actually read
404 */
405 static int API_dev_read(va_list ap)
406 {
407 struct device_info *di;
408 void *buf;
409 lbasize_t *len_stor, *act_len_stor;
410 lbastart_t *start;
411 int *len_net, *act_len_net;
413 /* 1. arg is ptr to the device_info struct */
414 di = (struct device_info *)va_arg(ap, u_int32_t);
415 if (di == NULL)
416 return API_EINVAL;
418 /* XXX should we check if device is open? i.e. the ->state ? */
420 if (di->cookie == NULL)
421 return API_ENODEV;
423 /* 2. arg is ptr to buffer from where to put the read data */
424 buf = (void *)va_arg(ap, u_int32_t);
425 if (buf == NULL)
426 return API_EINVAL;
428 if (di->type & DEV_TYP_STOR) {
429 /* 3. arg - ptr to var with # of blocks to read */
430 len_stor = (lbasize_t *)va_arg(ap, u_int32_t);
431 if (!len_stor)
432 return API_EINVAL;
433 if (*len_stor <= 0)
434 return API_EINVAL;
436 /* 4. arg - ptr to var with start block */
437 start = (lbastart_t *)va_arg(ap, u_int32_t);
439 /* 5. arg - ptr to var where to put the len actually read */
440 act_len_stor = (lbasize_t *)va_arg(ap, u_int32_t);
441 if (!act_len_stor)
442 return API_EINVAL;
444 *act_len_stor = dev_read_stor(di->cookie, buf, *len_stor, *start);
446 } else if (di->type & DEV_TYP_NET) {
448 /* 3. arg points to the var with length of packet to read */
449 len_net = (int *)va_arg(ap, u_int32_t);
450 if (!len_net)
451 return API_EINVAL;
452 if (*len_net <= 0)
453 return API_EINVAL;
455 /* 4. - ptr to var where to put the len actually read */
456 act_len_net = (int *)va_arg(ap, u_int32_t);
457 if (!act_len_net)
458 return API_EINVAL;
460 *act_len_net = dev_read_net(di->cookie, buf, *len_net);
462 } else
463 return API_ENODEV;
465 return 0;
466 }
469 /*
470 * pseudo signature:
471 *
472 * int API_env_get(const char *name, char **value)
473 *
474 * name: ptr to name of env var
475 */
476 static int API_env_get(va_list ap)
477 {
478 char *name, **value;
480 if ((name = (char *)va_arg(ap, u_int32_t)) == NULL)
481 return API_EINVAL;
482 if ((value = (char **)va_arg(ap, u_int32_t)) == NULL)
483 return API_EINVAL;
485 *value = getenv(name);
487 return 0;
488 }
490 /*
491 * pseudo signature:
492 *
493 * int API_env_set(const char *name, const char *value)
494 *
495 * name: ptr to name of env var
496 *
497 * value: ptr to value to be set
498 */
499 static int API_env_set(va_list ap)
500 {
501 char *name, *value;
503 if ((name = (char *)va_arg(ap, u_int32_t)) == NULL)
504 return API_EINVAL;
505 if ((value = (char *)va_arg(ap, u_int32_t)) == NULL)
506 return API_EINVAL;
508 setenv(name, value);
510 return 0;
511 }
513 /*
514 * pseudo signature:
515 *
516 * int API_env_enum(const char *last, char **next)
517 *
518 * last: ptr to name of env var found in last iteration
519 */
520 static int API_env_enum(va_list ap)
521 {
522 int i, n;
523 char *last, **next;
525 last = (char *)va_arg(ap, u_int32_t);
527 if ((next = (char **)va_arg(ap, u_int32_t)) == NULL)
528 return API_EINVAL;
530 if (last == NULL)
531 /* start over */
532 *next = ((char *)env_get_addr(0));
533 else {
534 *next = last;
536 for (i = 0; env_get_char(i) != '\0'; i = n + 1) {
537 for (n = i; env_get_char(n) != '\0'; ++n) {
538 if (n >= CFG_ENV_SIZE) {
539 /* XXX shouldn't we set *next = NULL?? */
540 return 0;
541 }
542 }
544 if (envmatch((uchar *)last, i) < 0)
545 continue;
547 /* try to get next name */
548 i = n + 1;
549 if (env_get_char(i) == '\0') {
550 /* no more left */
551 *next = NULL;
552 return 0;
553 }
555 *next = ((char *)env_get_addr(i));
556 return 0;
557 }
558 }
560 return 0;
561 }
563 static cfp_t calls_table[API_MAXCALL] = { NULL, };
565 /*
566 * The main syscall entry point - this is not reentrant, only one call is
567 * serviced until finished.
568 *
569 * e.g. syscall(1, int *, u_int32_t, u_int32_t, u_int32_t, u_int32_t);
570 *
571 * call: syscall number
572 *
573 * retval: points to the return value placeholder, this is the place the
574 * syscall puts its return value, if NULL the caller does not
575 * expect a return value
576 *
577 * ... syscall arguments (variable number)
578 *
579 * returns: 0 if the call not found, 1 if serviced
580 */
581 int syscall(int call, int *retval, ...)
582 {
583 va_list ap;
584 int rv;
586 if (call < 0 || call >= calls_no || calls_table[call] == NULL) {
587 debugf("invalid call #%d\n", call);
588 return 0;
589 }
591 if (calls_table[call] == NULL) {
592 debugf("syscall #%d does not have a handler\n", call);
593 return 0;
594 }
596 va_start(ap, retval);
597 rv = calls_table[call](ap);
598 if (retval != NULL)
599 *retval = rv;
601 return 1;
602 }
604 void api_init(void)
605 {
606 struct api_signature *sig = NULL;
608 /* TODO put this into linker set one day... */
609 calls_table[API_RSVD] = NULL;
610 calls_table[API_GETC] = &API_getc;
611 calls_table[API_PUTC] = &API_putc;
612 calls_table[API_TSTC] = &API_tstc;
613 calls_table[API_PUTS] = &API_puts;
614 calls_table[API_RESET] = &API_reset;
615 calls_table[API_GET_SYS_INFO] = &API_get_sys_info;
616 calls_table[API_UDELAY] = &API_udelay;
617 calls_table[API_GET_TIMER] = &API_get_timer;
618 calls_table[API_DEV_ENUM] = &API_dev_enum;
619 calls_table[API_DEV_OPEN] = &API_dev_open;
620 calls_table[API_DEV_CLOSE] = &API_dev_close;
621 calls_table[API_DEV_READ] = &API_dev_read;
622 calls_table[API_DEV_WRITE] = &API_dev_write;
623 calls_table[API_ENV_GET] = &API_env_get;
624 calls_table[API_ENV_SET] = &API_env_set;
625 calls_table[API_ENV_ENUM] = &API_env_enum;
626 calls_no = API_MAXCALL;
628 debugf("API initialized with %d calls\n", calls_no);
630 dev_stor_init();
632 /*
633 * Produce the signature so the API consumers can find it
634 */
635 sig = malloc(sizeof(struct api_signature));
636 if (sig == NULL) {
637 printf("API: could not allocate memory for the signature!\n");
638 return;
639 }
641 debugf("API sig @ 0x%08x\n", sig);
642 memcpy(sig->magic, API_SIG_MAGIC, 8);
643 sig->version = API_SIG_VERSION;
644 sig->syscall = &syscall;
645 sig->checksum = 0;
646 sig->checksum = crc32(0, (unsigned char *)sig,
647 sizeof(struct api_signature));
648 debugf("syscall entry: 0x%08x\n", sig->syscall);
649 }
651 void platform_set_mr(struct sys_info *si, unsigned long start, unsigned long size,
652 int flags)
653 {
654 int i;
656 if (!si->mr || !size || (flags == 0))
657 return;
659 /* find free slot */
660 for (i = 0; i < si->mr_no; i++)
661 if (si->mr[i].flags == 0) {
662 /* insert new mem region */
663 si->mr[i].start = start;
664 si->mr[i].size = size;
665 si->mr[i].flags = flags;
666 return;
667 }
668 }
670 #endif /* CONFIG_API */