HACK: ARM: DRA7xx: Add VPE crossbar setting
[glsdk/glsdk-u-boot.git] / api / api_net.c
1 /*
2  * (C) Copyright 2007 Semihalf
3  *
4  * Written by: Rafal Jaworowski <raj@semihalf.com>
5  *
6  * See file CREDITS for list of people who contributed to this
7  * project.
8  *
9  * This program is free software; you can redistribute it and/or
10  * modify it under the terms of the GNU General Public License as
11  * published by the Free Software Foundation; either version 2 of
12  * the License, or (at your option) any later version.
13  *
14  * This program is distributed in the hope that it will be useful,
15  * but WITHOUT ANY WARRANTY; without even the implied warranty of
16  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
17  * GNU General Public License for more details.
18  *
19  * You should have received a copy of the GNU General Public License
20  * along with this program; if not, write to the Free Software
21  * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
22  * MA 02111-1307 USA
23  *
24  */
26 #include <config.h>
27 #include <common.h>
28 #include <net.h>
29 #include <linux/types.h>
30 #include <api_public.h>
32 DECLARE_GLOBAL_DATA_PTR;
34 #define DEBUG
35 #undef DEBUG
37 #ifdef DEBUG
38 #define debugf(fmt, args...) do { printf("%s(): ", __func__); printf(fmt, ##args); } while (0)
39 #else
40 #define debugf(fmt, args...)
41 #endif
43 #define errf(fmt, args...) do { printf("ERROR @ %s(): ", __func__); printf(fmt, ##args); } while (0)
46 static int dev_valid_net(void *cookie)
47 {
48         return ((void *)eth_get_dev() == cookie) ? 1 : 0;
49 }
51 int dev_open_net(void *cookie)
52 {
53         if (!dev_valid_net(cookie))
54                 return API_ENODEV;
56         if (eth_init(gd->bd) < 0)
57                 return API_EIO;
59         return 0;
60 }
62 int dev_close_net(void *cookie)
63 {
64         if (!dev_valid_net(cookie))
65                 return API_ENODEV;
67         eth_halt();
68         return 0;
69 }
71 /*
72  * There can only be one active eth interface at a time - use what is
73  * currently set to eth_current
74  */
75 int dev_enum_net(struct device_info *di)
76 {
77         struct eth_device *eth_current = eth_get_dev();
79         di->type = DEV_TYP_NET;
80         di->cookie = (void *)eth_current;
81         if (di->cookie == NULL)
82                 return 0;
84         memcpy(di->di_net.hwaddr, eth_current->enetaddr, 6);
86         debugf("device found, returning cookie 0x%08x\n",
87                 (u_int32_t)di->cookie);
89         return 1;
90 }
92 int dev_write_net(void *cookie, void *buf, int len)
93 {
94         /* XXX verify that cookie points to a valid net device??? */
96         return eth_send(buf, len);
97 }
99 int dev_read_net(void *cookie, void *buf, int len)
101         /* XXX verify that cookie points to a valid net device??? */
103         return eth_receive(buf, len);