HACK: ARM: DRA7xx: Add VPE crossbar setting
[glsdk/glsdk-u-boot.git] / api / api_private.h
1 /*
2  * (C) Copyright 2007 Semihalf
3  *
4  * Written by: Rafal Jaworowski <raj@semihalf.com>
5  *
6  * See file CREDITS for list of people who contributed to this
7  * project.
8  *
9  * This program is free software; you can redistribute it and/or
10  * modify it under the terms of the GNU General Public License as
11  * published by the Free Software Foundation; either version 2 of
12  * the License, or (at your option) any later version.
13  *
14  * This program is distributed in the hope that it will be useful,
15  * but WITHOUT ANY WARRANTY; without even the implied warranty of
16  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
17  * GNU General Public License for more details.
18  *
19  * You should have received a copy of the GNU General Public License
20  * along with this program; if not, write to the Free Software
21  * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
22  * MA 02111-1307 USA
23  *
24  */
26 #ifndef _API_PRIVATE_H_
27 #define _API_PRIVATE_H_
29 void    api_init(void);
30 void    platform_set_mr(struct sys_info *, unsigned long, unsigned long, int);
31 int     platform_sys_info(struct sys_info *);
33 void    dev_enum_reset(void);
34 int     dev_enum_storage(struct device_info *);
35 int     dev_enum_net(struct device_info *);
37 int     dev_open_stor(void *);
38 int     dev_open_net(void *);
39 int     dev_close_stor(void *);
40 int     dev_close_net(void *);
42 lbasize_t       dev_read_stor(void *, void *, lbasize_t, lbastart_t);
43 int             dev_read_net(void *, void *, int);
44 int             dev_write_net(void *, void *, int);
46 void dev_stor_init(void);
48 int display_get_info(int type, struct display_info *di);
49 int display_draw_bitmap(ulong bitmap, int x, int y);
50 void display_clear(void);
52 #endif /* _API_PRIVATE_H_ */