1 /*
2 * (C) Copyright 2010-2011
3 * NVIDIA Corporation <www.nvidia.com>
4 *
5 * See file CREDITS for list of people who contributed to this
6 * project.
7 *
8 * This program is free software; you can redistribute it and/or
9 * modify it under the terms of the GNU General Public License as
10 * published by the Free Software Foundation; either version 2 of
11 * the License, or (at your option) any later version.
12 *
13 * This program is distributed in the hope that it will be useful,
14 * but WITHOUT ANY WARRANTY; without even the implied warranty of
15 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
16 * GNU General Public License for more details.
17 *
18 * You should have received a copy of the GNU General Public License
19 * along with this program; if not, write to the Free Software
20 * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
21 * MA 02111-1307 USA
22 */
23 #include <asm/types.h>
25 /* Stabilization delays, in usec */
26 #define PLL_STABILIZATION_DELAY (300)
27 #define IO_STABILIZATION_DELAY (1000)
29 #define NVBL_PLLP_KHZ (216000)
31 #define PLLX_ENABLED (1 << 30)
32 #define CCLK_BURST_POLICY 0x20008888
33 #define SUPER_CCLK_DIVIDER 0x80000000
35 /* Calculate clock fractional divider value from ref and target frequencies */
36 #define CLK_DIVIDER(REF, FREQ) ((((REF) * 2) / FREQ) - 2)
38 /* Calculate clock frequency value from reference and clock divider value */
39 #define CLK_FREQUENCY(REF, REG) (((REF) * 2) / (REG + 2))
41 /* AVP/CPU ID */
42 #define PG_UP_TAG_0_PID_CPU 0x55555555 /* CPU aka "a9" aka "mpcore" */
43 #define PG_UP_TAG_0 0x0
45 #define CORESIGHT_UNLOCK 0xC5ACCE55;
47 /* AP20-Specific Base Addresses */
49 /* AP20 Base physical address of SDRAM. */
50 #define AP20_BASE_PA_SDRAM 0x00000000
51 /* AP20 Base physical address of internal SRAM. */
52 #define AP20_BASE_PA_SRAM 0x40000000
53 /* AP20 Size of internal SRAM (256KB). */
54 #define AP20_BASE_PA_SRAM_SIZE 0x00040000
55 /* AP20 Base physical address of flash. */
56 #define AP20_BASE_PA_NOR_FLASH 0xD0000000
57 /* AP20 Base physical address of boot information table. */
58 #define AP20_BASE_PA_BOOT_INFO AP20_BASE_PA_SRAM
60 /*
61 * Super-temporary stacks for EXTREMELY early startup. The values chosen for
62 * these addresses must be valid on ALL SOCs because this value is used before
63 * we are able to differentiate between the SOC types.
64 *
65 * NOTE: The since CPU's stack will eventually be moved from IRAM to SDRAM, its
66 * stack is placed below the AVP stack. Once the CPU stack has been moved,
67 * the AVP is free to use the IRAM the CPU stack previously occupied if
68 * it should need to do so.
69 *
70 * NOTE: In multi-processor CPU complex configurations, each processor will have
71 * its own stack of size CPU_EARLY_BOOT_STACK_SIZE. CPU 0 will have a
72 * limit of CPU_EARLY_BOOT_STACK_LIMIT. Each successive CPU will have a
73 * stack limit that is CPU_EARLY_BOOT_STACK_SIZE less then the previous
74 * CPU.
75 */
77 /* Common AVP early boot stack limit */
78 #define AVP_EARLY_BOOT_STACK_LIMIT \
79 (AP20_BASE_PA_SRAM + (AP20_BASE_PA_SRAM_SIZE/2))
80 /* Common AVP early boot stack size */
81 #define AVP_EARLY_BOOT_STACK_SIZE 0x1000
82 /* Common CPU early boot stack limit */
83 #define CPU_EARLY_BOOT_STACK_LIMIT \
84 (AVP_EARLY_BOOT_STACK_LIMIT - AVP_EARLY_BOOT_STACK_SIZE)
85 /* Common CPU early boot stack size */
86 #define CPU_EARLY_BOOT_STACK_SIZE 0x1000
88 #define EXCEP_VECTOR_CPU_RESET_VECTOR (NV_PA_EVP_BASE + 0x100)
89 #define CSITE_CPU_DBG0_LAR (NV_PA_CSITE_BASE + 0x10FB0)
90 #define CSITE_CPU_DBG1_LAR (NV_PA_CSITE_BASE + 0x12FB0)
92 #define FLOW_CTLR_HALT_COP_EVENTS (NV_PA_FLOW_BASE + 4)
93 #define FLOW_MODE_STOP 2
94 #define HALT_COP_EVENT_JTAG (1 << 28)
95 #define HALT_COP_EVENT_IRQ_1 (1 << 11)
96 #define HALT_COP_EVENT_FIQ_1 (1 << 9)
98 void start_cpu(u32 reset_vector);
99 int ap20_cpu_is_cortexa9(void);
100 void halt_avp(void) __attribute__ ((noreturn));