]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/glsdk-u-boot.git/blob - arch/arm/cpu/arm720t/tegra-common/cpu.h
Merge branch 'master' of git://git.denx.de/u-boot
[glsdk/glsdk-u-boot.git] / arch / arm / cpu / arm720t / tegra-common / cpu.h
1 /*
2  * (C) Copyright 2010-2011
3  * NVIDIA Corporation <www.nvidia.com>
4  *
5  * See file CREDITS for list of people who contributed to this
6  * project.
7  *
8  * This program is free software; you can redistribute it and/or
9  * modify it under the terms of the GNU General Public License as
10  * published by the Free Software Foundation; either version 2 of
11  * the License, or (at your option) any later version.
12  *
13  * This program is distributed in the hope that it will be useful,
14  * but WITHOUT ANY WARRANTY; without even the implied warranty of
15  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
16  * GNU General Public License for more details.
17  *
18  * You should have received a copy of the GNU General Public License
19  * along with this program; if not, write to the Free Software
20  * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
21  * MA 02111-1307 USA
22  */
23 #include <asm/types.h>
25 /* Stabilization delays, in usec */
26 #define PLL_STABILIZATION_DELAY (300)
27 #define IO_STABILIZATION_DELAY  (1000)
29 #define NVBL_PLLP_KHZ   (216000)
31 #define PLLX_ENABLED            (1 << 30)
32 #define CCLK_BURST_POLICY       0x20008888
33 #define SUPER_CCLK_DIVIDER      0x80000000
35 /* Calculate clock fractional divider value from ref and target frequencies */
36 #define CLK_DIVIDER(REF, FREQ)  ((((REF) * 2) / FREQ) - 2)
38 /* Calculate clock frequency value from reference and clock divider value */
39 #define CLK_FREQUENCY(REF, REG)  (((REF) * 2) / (REG + 2))
41 /* AVP/CPU ID */
42 #define PG_UP_TAG_0_PID_CPU     0x55555555      /* CPU aka "a9" aka "mpcore" */
43 #define PG_UP_TAG_0             0x0
45 #define CORESIGHT_UNLOCK        0xC5ACCE55;
47 /* AP20-Specific Base Addresses */
49 /* AP20 Base physical address of SDRAM. */
50 #define AP20_BASE_PA_SDRAM      0x00000000
51 /* AP20 Base physical address of internal SRAM. */
52 #define AP20_BASE_PA_SRAM       0x40000000
53 /* AP20 Size of internal SRAM (256KB). */
54 #define AP20_BASE_PA_SRAM_SIZE  0x00040000
55 /* AP20 Base physical address of flash. */
56 #define AP20_BASE_PA_NOR_FLASH  0xD0000000
57 /* AP20 Base physical address of boot information table. */
58 #define AP20_BASE_PA_BOOT_INFO  AP20_BASE_PA_SRAM
60 /*
61  * Super-temporary stacks for EXTREMELY early startup. The values chosen for
62  * these addresses must be valid on ALL SOCs because this value is used before
63  * we are able to differentiate between the SOC types.
64  *
65  * NOTE: The since CPU's stack will eventually be moved from IRAM to SDRAM, its
66  *       stack is placed below the AVP stack. Once the CPU stack has been moved,
67  *       the AVP is free to use the IRAM the CPU stack previously occupied if
68  *       it should need to do so.
69  *
70  * NOTE: In multi-processor CPU complex configurations, each processor will have
71  *       its own stack of size CPU_EARLY_BOOT_STACK_SIZE. CPU 0 will have a
72  *       limit of CPU_EARLY_BOOT_STACK_LIMIT. Each successive CPU will have a
73  *       stack limit that is CPU_EARLY_BOOT_STACK_SIZE less then the previous
74  *       CPU.
75  */
77 /* Common AVP early boot stack limit */
78 #define AVP_EARLY_BOOT_STACK_LIMIT      \
79         (AP20_BASE_PA_SRAM + (AP20_BASE_PA_SRAM_SIZE/2))
80 /* Common AVP early boot stack size */
81 #define AVP_EARLY_BOOT_STACK_SIZE       0x1000
82 /* Common CPU early boot stack limit */
83 #define CPU_EARLY_BOOT_STACK_LIMIT      \
84         (AVP_EARLY_BOOT_STACK_LIMIT - AVP_EARLY_BOOT_STACK_SIZE)
85 /* Common CPU early boot stack size */
86 #define CPU_EARLY_BOOT_STACK_SIZE       0x1000
88 #define EXCEP_VECTOR_CPU_RESET_VECTOR   (NV_PA_EVP_BASE + 0x100)
89 #define CSITE_CPU_DBG0_LAR              (NV_PA_CSITE_BASE + 0x10FB0)
90 #define CSITE_CPU_DBG1_LAR              (NV_PA_CSITE_BASE + 0x12FB0)
92 #define FLOW_CTLR_HALT_COP_EVENTS       (NV_PA_FLOW_BASE + 4)
93 #define FLOW_MODE_STOP                  2
94 #define HALT_COP_EVENT_JTAG             (1 << 28)
95 #define HALT_COP_EVENT_IRQ_1            (1 << 11)
96 #define HALT_COP_EVENT_FIQ_1            (1 << 9)
98 void start_cpu(u32 reset_vector);
99 int ap20_cpu_is_cortexa9(void);
100 void halt_avp(void)  __attribute__ ((noreturn));