]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/glsdk-u-boot.git/blob - arch/arm/cpu/arm720t/tegra30/cpu.c
Merge branch 'next' of git://git.denx.de/u-boot-mips
[glsdk/glsdk-u-boot.git] / arch / arm / cpu / arm720t / tegra30 / cpu.c
1 /*
2  * Copyright (c) 2010-2012, NVIDIA CORPORATION.  All rights reserved.
3  *
4  * This program is free software; you can redistribute it and/or modify it
5  * under the terms and conditions of the GNU General Public License,
6  * version 2, as published by the Free Software Foundation.
7  *
8  * This program is distributed in the hope it will be useful, but WITHOUT
9  * ANY WARRANTY; without even the implied warranty of MERCHANTABILITY or
10  * FITNESS FOR A PARTICULAR PURPOSE.  See the GNU General Public License for
11  * more details.
12  *
13  * You should have received a copy of the GNU General Public License
14  * along with this program.  If not, see <http://www.gnu.org/licenses/>.
15  */
17 #include <common.h>
18 #include <asm/io.h>
19 #include <asm/arch/clock.h>
20 #include <asm/arch/flow.h>
21 #include <asm/arch/tegra.h>
22 #include <asm/arch-tegra/clk_rst.h>
23 #include <asm/arch-tegra/pmc.h>
24 #include <asm/arch-tegra/tegra_i2c.h>
25 #include "../tegra-common/cpu.h"
27 /* Tegra30-specific CPU init code */
28 void tegra_i2c_ll_write_addr(uint addr, uint config)
29 {
30         struct i2c_ctlr *reg = (struct i2c_ctlr *)TEGRA_DVC_BASE;
32         writel(addr, &reg->cmd_addr0);
33         writel(config, &reg->cnfg);
34 }
36 void tegra_i2c_ll_write_data(uint data, uint config)
37 {
38         struct i2c_ctlr *reg = (struct i2c_ctlr *)TEGRA_DVC_BASE;
40         writel(data, &reg->cmd_data1);
41         writel(config, &reg->cnfg);
42 }
44 #define TPS65911_I2C_ADDR               0x5A
45 #define TPS65911_VDDCTRL_OP_REG         0x28
46 #define TPS65911_VDDCTRL_SR_REG         0x27
47 #define TPS65911_VDDCTRL_OP_DATA        (0x2300 | TPS65911_VDDCTRL_OP_REG)
48 #define TPS65911_VDDCTRL_SR_DATA        (0x0100 | TPS65911_VDDCTRL_SR_REG)
49 #define I2C_SEND_2_BYTES                0x0A02
51 static void enable_cpu_power_rail(void)
52 {
53         struct pmc_ctlr *pmc = (struct pmc_ctlr *)NV_PA_PMC_BASE;
54         u32 reg;
56         debug("enable_cpu_power_rail entry\n");
57         reg = readl(&pmc->pmc_cntrl);
58         reg |= CPUPWRREQ_OE;
59         writel(reg, &pmc->pmc_cntrl);
61         /*
62          * Bring up CPU VDD via the TPS65911x PMIC on the DVC I2C bus.
63          * First set VDD to 1.4V, then enable the VDD regulator.
64          */
65         tegra_i2c_ll_write_addr(TPS65911_I2C_ADDR, 2);
66         tegra_i2c_ll_write_data(TPS65911_VDDCTRL_OP_DATA, I2C_SEND_2_BYTES);
67         udelay(1000);
68         tegra_i2c_ll_write_data(TPS65911_VDDCTRL_SR_DATA, I2C_SEND_2_BYTES);
69         udelay(10 * 1000);
70 }
72 /**
73  * The T30 requires some special clock initialization, including setting up
74  * the dvc i2c, turning on mselect and selecting the G CPU cluster
75  */
76 void t30_init_clocks(void)
77 {
78         struct clk_rst_ctlr *clkrst =
79                         (struct clk_rst_ctlr *)NV_PA_CLK_RST_BASE;
80         struct flow_ctlr *flow = (struct flow_ctlr *)NV_PA_FLOW_BASE;
81         u32 val;
83         debug("t30_init_clocks entry\n");
84         /* Set active CPU cluster to G */
85         clrbits_le32(flow->cluster_control, 1 << 0);
87         /*
88          * Switch system clock to PLLP_OUT4 (108 MHz), AVP will now run
89          * at 108 MHz. This is glitch free as only the source is changed, no
90          * special precaution needed.
91          */
92         val = (SCLK_SOURCE_PLLP_OUT4 << SCLK_SWAKEUP_FIQ_SOURCE_SHIFT) |
93                 (SCLK_SOURCE_PLLP_OUT4 << SCLK_SWAKEUP_IRQ_SOURCE_SHIFT) |
94                 (SCLK_SOURCE_PLLP_OUT4 << SCLK_SWAKEUP_RUN_SOURCE_SHIFT) |
95                 (SCLK_SOURCE_PLLP_OUT4 << SCLK_SWAKEUP_IDLE_SOURCE_SHIFT) |
96                 (SCLK_SYS_STATE_RUN << SCLK_SYS_STATE_SHIFT);
97         writel(val, &clkrst->crc_sclk_brst_pol);
99         writel(SUPER_SCLK_ENB_MASK, &clkrst->crc_super_sclk_div);
101         val = (0 << CLK_SYS_RATE_HCLK_DISABLE_SHIFT) |
102                 (1 << CLK_SYS_RATE_AHB_RATE_SHIFT) |
103                 (0 << CLK_SYS_RATE_PCLK_DISABLE_SHIFT) |
104                 (0 << CLK_SYS_RATE_APB_RATE_SHIFT);
105         writel(val, &clkrst->crc_clk_sys_rate);
107         /* Put i2c, mselect in reset and enable clocks */
108         reset_set_enable(PERIPH_ID_DVC_I2C, 1);
109         clock_set_enable(PERIPH_ID_DVC_I2C, 1);
110         reset_set_enable(PERIPH_ID_MSELECT, 1);
111         clock_set_enable(PERIPH_ID_MSELECT, 1);
113         /* Switch MSELECT clock to PLLP (00) */
114         clock_ll_set_source(PERIPH_ID_MSELECT, 0);
116         /*
117          * Our high-level clock routines are not available prior to
118          * relocation. We use the low-level functions which require a
119          * hard-coded divisor. Use CLK_M with divide by (n + 1 = 17)
120          */
121         clock_ll_set_source_divisor(PERIPH_ID_DVC_I2C, 3, 16);
123         /*
124          * Give clocks time to stabilize, then take i2c and mselect out of
125          * reset
126          */
127         udelay(1000);
128         reset_set_enable(PERIPH_ID_DVC_I2C, 0);
129         reset_set_enable(PERIPH_ID_MSELECT, 0);
132 static void set_cpu_running(int run)
134         struct flow_ctlr *flow = (struct flow_ctlr *)NV_PA_FLOW_BASE;
136         debug("set_cpu_running entry, run = %d\n", run);
137         writel(run ? FLOW_MODE_NONE : FLOW_MODE_STOP, &flow->halt_cpu_events);
140 void start_cpu(u32 reset_vector)
142         debug("start_cpu entry, reset_vector = %x\n", reset_vector);
143         t30_init_clocks();
145         /* Enable VDD_CPU */
146         enable_cpu_power_rail();
148         set_cpu_running(0);
150         /* Hold the CPUs in reset */
151         reset_A9_cpu(1);
153         /* Disable the CPU clock */
154         enable_cpu_clock(0);
156         /* Enable CoreSight */
157         clock_enable_coresight(1);
159         /*
160          * Set the entry point for CPU execution from reset,
161          *  if it's a non-zero value.
162          */
163         if (reset_vector)
164                 writel(reset_vector, EXCEP_VECTOR_CPU_RESET_VECTOR);
166         /* Enable the CPU clock */
167         enable_cpu_clock(1);
169         /* If the CPU doesn't already have power, power it up */
170         powerup_cpu();
172         /* Take the CPU out of reset */
173         reset_A9_cpu(0);
175         set_cpu_running(1);