]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/glsdk-u-boot.git/blob - arch/arm/cpu/arm926ejs/at91/at91sam9x5_devices.c
am335x: add initial AM335x IDK board support
[glsdk/glsdk-u-boot.git] / arch / arm / cpu / arm926ejs / at91 / at91sam9x5_devices.c
1 /*
2  * Copyright (C) 2012 Atmel Corporation
3  *
4  * See file CREDITS for list of people who contributed to this
5  * project.
6  *
7  * This program is free software; you can redistribute it and/or
8  * modify it under the terms of the GNU General Public License as
9  * published by the Free Software Foundation; either version 2 of
10  * the License, or (at your option) any later version.
11  *
12  * This program is distributed in the hope that it will be useful,
13  * but WITHOUT ANY WARRANTY; without even the implied warranty of
14  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
15  * GNU General Public License for more details.
16  *
17  * You should have received a copy of the GNU General Public License
18  * along with this program; if not, write to the Free Software
19  * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
20  * MA 02111-1307 USA
21  */
23 #include <common.h>
24 #include <asm/arch/at91_common.h>
25 #include <asm/arch/at91_pmc.h>
26 #include <asm/arch/gpio.h>
27 #include <asm/io.h>
29 unsigned int get_chip_id(void)
30 {
31         /* The 0x40 is the offset of cidr in DBGU */
32         return readl(ATMEL_BASE_DBGU + 0x40) & ~ARCH_ID_VERSION_MASK;
33 }
35 unsigned int get_extension_chip_id(void)
36 {
37         /* The 0x44 is the offset of exid in DBGU */
38         return readl(ATMEL_BASE_DBGU + 0x44);
39 }
41 unsigned int has_emac1()
42 {
43         return cpu_is_at91sam9x25();
44 }
46 unsigned int has_emac0()
47 {
48         return !(cpu_is_at91sam9g15());
49 }
51 unsigned int has_lcdc()
52 {
53         return cpu_is_at91sam9g15() || cpu_is_at91sam9g35()
54                 || cpu_is_at91sam9x35();
55 }
57 char *get_cpu_name()
58 {
59         unsigned int extension_id = get_extension_chip_id();
61         if (cpu_is_at91sam9x5()) {
62                 switch (extension_id) {
63                 case ARCH_EXID_AT91SAM9G15:
64                         return CONFIG_SYS_AT91_G15_CPU_NAME;
65                 case ARCH_EXID_AT91SAM9G25:
66                         return CONFIG_SYS_AT91_G25_CPU_NAME;
67                 case ARCH_EXID_AT91SAM9G35:
68                         return CONFIG_SYS_AT91_G35_CPU_NAME;
69                 case ARCH_EXID_AT91SAM9X25:
70                         return CONFIG_SYS_AT91_X25_CPU_NAME;
71                 case ARCH_EXID_AT91SAM9X35:
72                         return CONFIG_SYS_AT91_X35_CPU_NAME;
73                 default:
74                         return CONFIG_SYS_AT91_UNKNOWN_CPU;
75                 }
76         } else {
77                 return CONFIG_SYS_AT91_UNKNOWN_CPU;
78         }
79 }
81 void at91_seriald_hw_init(void)
82 {
83         at91_pmc_t *pmc = (at91_pmc_t *) ATMEL_BASE_PMC;
85         at91_set_a_periph(AT91_PIO_PORTA, 9, 0);        /* DRXD */
86         at91_set_a_periph(AT91_PIO_PORTA, 10, 1);       /* DTXD */
88         writel(1 << ATMEL_ID_SYS, &pmc->pcer);
89 }
91 void at91_serial0_hw_init(void)
92 {
93         at91_pmc_t *pmc = (at91_pmc_t *) ATMEL_BASE_PMC;
95         at91_set_a_periph(AT91_PIO_PORTA, 0, 1);        /* TXD */
96         at91_set_a_periph(AT91_PIO_PORTA, 1, 0);        /* RXD */
98         writel(1 << ATMEL_ID_USART0, &pmc->pcer);
99 }
101 void at91_serial1_hw_init(void)
103         at91_pmc_t *pmc = (at91_pmc_t *) ATMEL_BASE_PMC;
105         at91_set_a_periph(AT91_PIO_PORTA, 5, 1);        /* TXD */
106         at91_set_a_periph(AT91_PIO_PORTA, 6, 0);        /* RXD */
108         writel(1 << ATMEL_ID_USART1, &pmc->pcer);
111 void at91_serial2_hw_init(void)
113         at91_pmc_t *pmc = (at91_pmc_t *) ATMEL_BASE_PMC;
115         at91_set_a_periph(AT91_PIO_PORTA, 7, 1);        /* TXD */
116         at91_set_a_periph(AT91_PIO_PORTA, 8, 0);        /* RXD */
118         writel(1 << ATMEL_ID_USART2, &pmc->pcer);
121 #ifdef CONFIG_ATMEL_SPI
122 void at91_spi0_hw_init(unsigned long cs_mask)
124         at91_pmc_t *pmc = (at91_pmc_t *) ATMEL_BASE_PMC;
126         at91_set_a_periph(AT91_PIO_PORTA, 11, 0);       /* SPI0_MISO */
127         at91_set_a_periph(AT91_PIO_PORTA, 12, 0);       /* SPI0_MOSI */
128         at91_set_a_periph(AT91_PIO_PORTA, 13, 0);       /* SPI0_SPCK */
130         /* Enable clock */
131         writel(1 << ATMEL_ID_SPI0, &pmc->pcer);
133         if (cs_mask & (1 << 0))
134                 at91_set_a_periph(AT91_PIO_PORTA, 14, 0);
135         if (cs_mask & (1 << 1))
136                 at91_set_b_periph(AT91_PIO_PORTA, 7, 0);
137         if (cs_mask & (1 << 2))
138                 at91_set_b_periph(AT91_PIO_PORTA, 1, 0);
139         if (cs_mask & (1 << 3))
140                 at91_set_b_periph(AT91_PIO_PORTB, 3, 0);
141         if (cs_mask & (1 << 4))
142                 at91_set_pio_output(AT91_PIO_PORTA, 14, 0);
143         if (cs_mask & (1 << 5))
144                 at91_set_pio_output(AT91_PIO_PORTA, 7, 0);
145         if (cs_mask & (1 << 6))
146                 at91_set_pio_output(AT91_PIO_PORTA, 1, 0);
147         if (cs_mask & (1 << 7))
148                 at91_set_pio_output(AT91_PIO_PORTB, 3, 0);
151 void at91_spi1_hw_init(unsigned long cs_mask)
153         at91_pmc_t *pmc = (at91_pmc_t *) ATMEL_BASE_PMC;
155         at91_set_b_periph(AT91_PIO_PORTA, 21, 0);       /* SPI1_MISO */
156         at91_set_b_periph(AT91_PIO_PORTA, 22, 0);       /* SPI1_MOSI */
157         at91_set_b_periph(AT91_PIO_PORTA, 23, 0);       /* SPI1_SPCK */
159         /* Enable clock */
160         writel(1 << ATMEL_ID_SPI1, &pmc->pcer);
162         if (cs_mask & (1 << 0))
163                 at91_set_b_periph(AT91_PIO_PORTA, 8, 0);
164         if (cs_mask & (1 << 1))
165                 at91_set_b_periph(AT91_PIO_PORTA, 0, 0);
166         if (cs_mask & (1 << 2))
167                 at91_set_b_periph(AT91_PIO_PORTA, 31, 0);
168         if (cs_mask & (1 << 3))
169                 at91_set_b_periph(AT91_PIO_PORTA, 30, 0);
170         if (cs_mask & (1 << 4))
171                 at91_set_pio_output(AT91_PIO_PORTA, 8, 0);
172         if (cs_mask & (1 << 5))
173                 at91_set_pio_output(AT91_PIO_PORTA, 0, 0);
174         if (cs_mask & (1 << 6))
175                 at91_set_pio_output(AT91_PIO_PORTA, 31, 0);
176         if (cs_mask & (1 << 7))
177                 at91_set_pio_output(AT91_PIO_PORTA, 30, 0);
179 #endif
181 #ifdef CONFIG_MACB
182 void at91_macb_hw_init(void)
184         at91_pmc_t *pmc = (at91_pmc_t *) ATMEL_BASE_PMC;
186         if (has_emac0()) {
187                 /* Enable EMAC0 clock */
188                 writel(1 << ATMEL_ID_EMAC0, &pmc->pcer);
189                 /* EMAC0 pins setup */
190                 at91_set_a_periph(AT91_PIO_PORTB, 4, 0);        /* ETXCK */
191                 at91_set_a_periph(AT91_PIO_PORTB, 3, 0);        /* ERXDV */
192                 at91_set_a_periph(AT91_PIO_PORTB, 0, 0);        /* ERX0 */
193                 at91_set_a_periph(AT91_PIO_PORTB, 1, 0);        /* ERX1 */
194                 at91_set_a_periph(AT91_PIO_PORTB, 2, 0);        /* ERXER */
195                 at91_set_a_periph(AT91_PIO_PORTB, 7, 0);        /* ETXEN */
196                 at91_set_a_periph(AT91_PIO_PORTB, 9, 0);        /* ETX0 */
197                 at91_set_a_periph(AT91_PIO_PORTB, 10, 0);       /* ETX1 */
198                 at91_set_a_periph(AT91_PIO_PORTB, 5, 0);        /* EMDIO */
199                 at91_set_a_periph(AT91_PIO_PORTB, 6, 0);        /* EMDC */
200         }
202         if (has_emac1()) {
203                 /* Enable EMAC1 clock */
204                 writel(1 << ATMEL_ID_EMAC1, &pmc->pcer);
205                 /* EMAC1 pins setup */
206                 at91_set_b_periph(AT91_PIO_PORTC, 29, 0);       /* ETXCK */
207                 at91_set_b_periph(AT91_PIO_PORTC, 28, 0);       /* ECRSDV */
208                 at91_set_b_periph(AT91_PIO_PORTC, 20, 0);       /* ERXO */
209                 at91_set_b_periph(AT91_PIO_PORTC, 21, 0);       /* ERX1 */
210                 at91_set_b_periph(AT91_PIO_PORTC, 16, 0);       /* ERXER */
211                 at91_set_b_periph(AT91_PIO_PORTC, 27, 0);       /* ETXEN */
212                 at91_set_b_periph(AT91_PIO_PORTC, 18, 0);       /* ETX0 */
213                 at91_set_b_periph(AT91_PIO_PORTC, 19, 0);       /* ETX1 */
214                 at91_set_b_periph(AT91_PIO_PORTC, 31, 0);       /* EMDIO */
215                 at91_set_b_periph(AT91_PIO_PORTC, 30, 0);       /* EMDC */
216         }
218 #ifndef CONFIG_RMII
219         /* Only emac0 support MII */
220         if (has_emac0()) {
221                 at91_set_b_periph(AT91_PIO_PORTB, 16, 0);       /* ECRS */
222                 at91_set_b_periph(AT91_PIO_PORTB, 17, 0);       /* ECOL */
223                 at91_set_b_periph(AT91_PIO_PORTB, 13, 0);       /* ERX2 */
224                 at91_set_b_periph(AT91_PIO_PORTB, 14, 0);       /* ERX3 */
225                 at91_set_b_periph(AT91_PIO_PORTB, 15, 0);       /* ERXCK */
226                 at91_set_b_periph(AT91_PIO_PORTB, 11, 0);       /* ETX2 */
227                 at91_set_b_periph(AT91_PIO_PORTB, 12, 0);       /* ETX3 */
228                 at91_set_b_periph(AT91_PIO_PORTB, 8, 0);        /* ETXER */
229         }
230 #endif
232 #endif