1 /*
2 * Copyright (C) 2012 Atmel Corporation
3 *
4 * See file CREDITS for list of people who contributed to this
5 * project.
6 *
7 * This program is free software; you can redistribute it and/or
8 * modify it under the terms of the GNU General Public License as
9 * published by the Free Software Foundation; either version 2 of
10 * the License, or (at your option) any later version.
11 *
12 * This program is distributed in the hope that it will be useful,
13 * but WITHOUT ANY WARRANTY; without even the implied warranty of
14 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
15 * GNU General Public License for more details.
16 *
17 * You should have received a copy of the GNU General Public License
18 * along with this program; if not, write to the Free Software
19 * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
20 * MA 02111-1307 USA
21 */
23 #include <common.h>
24 #include <asm/arch/at91_common.h>
25 #include <asm/arch/at91_pmc.h>
26 #include <asm/arch/gpio.h>
27 #include <asm/io.h>
29 unsigned int get_chip_id(void)
30 {
31 /* The 0x40 is the offset of cidr in DBGU */
32 return readl(ATMEL_BASE_DBGU + 0x40) & ~ARCH_ID_VERSION_MASK;
33 }
35 unsigned int get_extension_chip_id(void)
36 {
37 /* The 0x44 is the offset of exid in DBGU */
38 return readl(ATMEL_BASE_DBGU + 0x44);
39 }
41 unsigned int has_emac1()
42 {
43 return cpu_is_at91sam9x25();
44 }
46 unsigned int has_emac0()
47 {
48 return !(cpu_is_at91sam9g15());
49 }
51 unsigned int has_lcdc()
52 {
53 return cpu_is_at91sam9g15() || cpu_is_at91sam9g35()
54 || cpu_is_at91sam9x35();
55 }
57 char *get_cpu_name()
58 {
59 unsigned int extension_id = get_extension_chip_id();
61 if (cpu_is_at91sam9x5()) {
62 switch (extension_id) {
63 case ARCH_EXID_AT91SAM9G15:
64 return CONFIG_SYS_AT91_G15_CPU_NAME;
65 case ARCH_EXID_AT91SAM9G25:
66 return CONFIG_SYS_AT91_G25_CPU_NAME;
67 case ARCH_EXID_AT91SAM9G35:
68 return CONFIG_SYS_AT91_G35_CPU_NAME;
69 case ARCH_EXID_AT91SAM9X25:
70 return CONFIG_SYS_AT91_X25_CPU_NAME;
71 case ARCH_EXID_AT91SAM9X35:
72 return CONFIG_SYS_AT91_X35_CPU_NAME;
73 default:
74 return CONFIG_SYS_AT91_UNKNOWN_CPU;
75 }
76 } else {
77 return CONFIG_SYS_AT91_UNKNOWN_CPU;
78 }
79 }
81 void at91_seriald_hw_init(void)
82 {
83 at91_pmc_t *pmc = (at91_pmc_t *) ATMEL_BASE_PMC;
85 at91_set_a_periph(AT91_PIO_PORTA, 9, 0); /* DRXD */
86 at91_set_a_periph(AT91_PIO_PORTA, 10, 1); /* DTXD */
88 writel(1 << ATMEL_ID_SYS, &pmc->pcer);
89 }
91 void at91_serial0_hw_init(void)
92 {
93 at91_pmc_t *pmc = (at91_pmc_t *) ATMEL_BASE_PMC;
95 at91_set_a_periph(AT91_PIO_PORTA, 0, 1); /* TXD */
96 at91_set_a_periph(AT91_PIO_PORTA, 1, 0); /* RXD */
98 writel(1 << ATMEL_ID_USART0, &pmc->pcer);
99 }
101 void at91_serial1_hw_init(void)
102 {
103 at91_pmc_t *pmc = (at91_pmc_t *) ATMEL_BASE_PMC;
105 at91_set_a_periph(AT91_PIO_PORTA, 5, 1); /* TXD */
106 at91_set_a_periph(AT91_PIO_PORTA, 6, 0); /* RXD */
108 writel(1 << ATMEL_ID_USART1, &pmc->pcer);
109 }
111 void at91_serial2_hw_init(void)
112 {
113 at91_pmc_t *pmc = (at91_pmc_t *) ATMEL_BASE_PMC;
115 at91_set_a_periph(AT91_PIO_PORTA, 7, 1); /* TXD */
116 at91_set_a_periph(AT91_PIO_PORTA, 8, 0); /* RXD */
118 writel(1 << ATMEL_ID_USART2, &pmc->pcer);
119 }
121 void at91_mci_hw_init(void)
122 {
123 /* Initialize the MCI0 */
124 at91_set_a_periph(AT91_PIO_PORTA, 17, 1); /* MCCK */
125 at91_set_a_periph(AT91_PIO_PORTA, 16, 1); /* MCCDA */
126 at91_set_a_periph(AT91_PIO_PORTA, 15, 1); /* MCDA0 */
127 at91_set_a_periph(AT91_PIO_PORTA, 18, 1); /* MCDA1 */
128 at91_set_a_periph(AT91_PIO_PORTA, 19, 1); /* MCDA2 */
129 at91_set_a_periph(AT91_PIO_PORTA, 20, 1); /* MCDA3 */
131 /* Enable clock for MCI0 */
132 struct at91_pmc *pmc = (struct at91_pmc *)ATMEL_BASE_PMC;
133 writel(1 << ATMEL_ID_HSMCI0, &pmc->pcer);
134 }
136 #ifdef CONFIG_ATMEL_SPI
137 void at91_spi0_hw_init(unsigned long cs_mask)
138 {
139 at91_pmc_t *pmc = (at91_pmc_t *) ATMEL_BASE_PMC;
141 at91_set_a_periph(AT91_PIO_PORTA, 11, 0); /* SPI0_MISO */
142 at91_set_a_periph(AT91_PIO_PORTA, 12, 0); /* SPI0_MOSI */
143 at91_set_a_periph(AT91_PIO_PORTA, 13, 0); /* SPI0_SPCK */
145 /* Enable clock */
146 writel(1 << ATMEL_ID_SPI0, &pmc->pcer);
148 if (cs_mask & (1 << 0))
149 at91_set_a_periph(AT91_PIO_PORTA, 14, 0);
150 if (cs_mask & (1 << 1))
151 at91_set_b_periph(AT91_PIO_PORTA, 7, 0);
152 if (cs_mask & (1 << 2))
153 at91_set_b_periph(AT91_PIO_PORTA, 1, 0);
154 if (cs_mask & (1 << 3))
155 at91_set_b_periph(AT91_PIO_PORTB, 3, 0);
156 if (cs_mask & (1 << 4))
157 at91_set_pio_output(AT91_PIO_PORTA, 14, 0);
158 if (cs_mask & (1 << 5))
159 at91_set_pio_output(AT91_PIO_PORTA, 7, 0);
160 if (cs_mask & (1 << 6))
161 at91_set_pio_output(AT91_PIO_PORTA, 1, 0);
162 if (cs_mask & (1 << 7))
163 at91_set_pio_output(AT91_PIO_PORTB, 3, 0);
164 }
166 void at91_spi1_hw_init(unsigned long cs_mask)
167 {
168 at91_pmc_t *pmc = (at91_pmc_t *) ATMEL_BASE_PMC;
170 at91_set_b_periph(AT91_PIO_PORTA, 21, 0); /* SPI1_MISO */
171 at91_set_b_periph(AT91_PIO_PORTA, 22, 0); /* SPI1_MOSI */
172 at91_set_b_periph(AT91_PIO_PORTA, 23, 0); /* SPI1_SPCK */
174 /* Enable clock */
175 writel(1 << ATMEL_ID_SPI1, &pmc->pcer);
177 if (cs_mask & (1 << 0))
178 at91_set_b_periph(AT91_PIO_PORTA, 8, 0);
179 if (cs_mask & (1 << 1))
180 at91_set_b_periph(AT91_PIO_PORTA, 0, 0);
181 if (cs_mask & (1 << 2))
182 at91_set_b_periph(AT91_PIO_PORTA, 31, 0);
183 if (cs_mask & (1 << 3))
184 at91_set_b_periph(AT91_PIO_PORTA, 30, 0);
185 if (cs_mask & (1 << 4))
186 at91_set_pio_output(AT91_PIO_PORTA, 8, 0);
187 if (cs_mask & (1 << 5))
188 at91_set_pio_output(AT91_PIO_PORTA, 0, 0);
189 if (cs_mask & (1 << 6))
190 at91_set_pio_output(AT91_PIO_PORTA, 31, 0);
191 if (cs_mask & (1 << 7))
192 at91_set_pio_output(AT91_PIO_PORTA, 30, 0);
193 }
194 #endif
196 #ifdef CONFIG_MACB
197 void at91_macb_hw_init(void)
198 {
199 at91_pmc_t *pmc = (at91_pmc_t *) ATMEL_BASE_PMC;
201 if (has_emac0()) {
202 /* Enable EMAC0 clock */
203 writel(1 << ATMEL_ID_EMAC0, &pmc->pcer);
204 /* EMAC0 pins setup */
205 at91_set_a_periph(AT91_PIO_PORTB, 4, 0); /* ETXCK */
206 at91_set_a_periph(AT91_PIO_PORTB, 3, 0); /* ERXDV */
207 at91_set_a_periph(AT91_PIO_PORTB, 0, 0); /* ERX0 */
208 at91_set_a_periph(AT91_PIO_PORTB, 1, 0); /* ERX1 */
209 at91_set_a_periph(AT91_PIO_PORTB, 2, 0); /* ERXER */
210 at91_set_a_periph(AT91_PIO_PORTB, 7, 0); /* ETXEN */
211 at91_set_a_periph(AT91_PIO_PORTB, 9, 0); /* ETX0 */
212 at91_set_a_periph(AT91_PIO_PORTB, 10, 0); /* ETX1 */
213 at91_set_a_periph(AT91_PIO_PORTB, 5, 0); /* EMDIO */
214 at91_set_a_periph(AT91_PIO_PORTB, 6, 0); /* EMDC */
215 }
217 if (has_emac1()) {
218 /* Enable EMAC1 clock */
219 writel(1 << ATMEL_ID_EMAC1, &pmc->pcer);
220 /* EMAC1 pins setup */
221 at91_set_b_periph(AT91_PIO_PORTC, 29, 0); /* ETXCK */
222 at91_set_b_periph(AT91_PIO_PORTC, 28, 0); /* ECRSDV */
223 at91_set_b_periph(AT91_PIO_PORTC, 20, 0); /* ERXO */
224 at91_set_b_periph(AT91_PIO_PORTC, 21, 0); /* ERX1 */
225 at91_set_b_periph(AT91_PIO_PORTC, 16, 0); /* ERXER */
226 at91_set_b_periph(AT91_PIO_PORTC, 27, 0); /* ETXEN */
227 at91_set_b_periph(AT91_PIO_PORTC, 18, 0); /* ETX0 */
228 at91_set_b_periph(AT91_PIO_PORTC, 19, 0); /* ETX1 */
229 at91_set_b_periph(AT91_PIO_PORTC, 31, 0); /* EMDIO */
230 at91_set_b_periph(AT91_PIO_PORTC, 30, 0); /* EMDC */
231 }
233 #ifndef CONFIG_RMII
234 /* Only emac0 support MII */
235 if (has_emac0()) {
236 at91_set_b_periph(AT91_PIO_PORTB, 16, 0); /* ECRS */
237 at91_set_b_periph(AT91_PIO_PORTB, 17, 0); /* ECOL */
238 at91_set_b_periph(AT91_PIO_PORTB, 13, 0); /* ERX2 */
239 at91_set_b_periph(AT91_PIO_PORTB, 14, 0); /* ERX3 */
240 at91_set_b_periph(AT91_PIO_PORTB, 15, 0); /* ERXCK */
241 at91_set_b_periph(AT91_PIO_PORTB, 11, 0); /* ETX2 */
242 at91_set_b_periph(AT91_PIO_PORTB, 12, 0); /* ETX3 */
243 at91_set_b_periph(AT91_PIO_PORTB, 8, 0); /* ETXER */
244 }
245 #endif
246 }
247 #endif