]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/glsdk-u-boot.git/blob - arch/arm/cpu/arm926ejs/start.S
Merge branch 'at91' of git://git.denx.de/u-boot-atmel
[glsdk/glsdk-u-boot.git] / arch / arm / cpu / arm926ejs / start.S
1 /*
2  *  armboot - Startup Code for ARM926EJS CPU-core
3  *
4  *  Copyright (c) 2003  Texas Instruments
5  *
6  *  ----- Adapted for OMAP1610 OMAP730 from ARM925t code ------
7  *
8  *  Copyright (c) 2001  Marius Gröger <mag@sysgo.de>
9  *  Copyright (c) 2002  Alex Züpke <azu@sysgo.de>
10  *  Copyright (c) 2002  Gary Jennejohn <garyj@denx.de>
11  *  Copyright (c) 2003  Richard Woodruff <r-woodruff2@ti.com>
12  *  Copyright (c) 2003  Kshitij <kshitij@ti.com>
13  *  Copyright (c) 2010  Albert Aribaud <albert.aribaud@free.fr>
14  *
15  * See file CREDITS for list of people who contributed to this
16  * project.
17  *
18  * This program is free software; you can redistribute it and/or
19  * modify it under the terms of the GNU General Public License as
20  * published by the Free Software Foundation; either version 2 of
21  * the License, or (at your option) any later version.
22  *
23  * This program is distributed in the hope that it will be useful,
24  * but WITHOUT ANY WARRANTY; without even the implied warranty of
25  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
26  * GNU General Public License for more details.
27  *
28  * You should have received a copy of the GNU General Public License
29  * along with this program; if not, write to the Free Software
30  * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
31  * MA 02111-1307 USA
32  */
35 #include <config.h>
36 #include <common.h>
37 #include <version.h>
39 #if defined(CONFIG_OMAP1610)
40 #include <./configs/omap1510.h>
41 #elif defined(CONFIG_OMAP730)
42 #include <./configs/omap730.h>
43 #endif
45 /*
46  *************************************************************************
47  *
48  * Jump vector table as in table 3.1 in [1]
49  *
50  *************************************************************************
51  */
54 .globl _start
55 _start:
56         b       reset
57 #ifdef CONFIG_PRELOADER
58 /* No exception handlers in preloader */
59         ldr     pc, _hang
60         ldr     pc, _hang
61         ldr     pc, _hang
62         ldr     pc, _hang
63         ldr     pc, _hang
64         ldr     pc, _hang
65         ldr     pc, _hang
67 _hang:
68         .word   do_hang
69 /* pad to 64 byte boundary */
70         .word   0x12345678
71         .word   0x12345678
72         .word   0x12345678
73         .word   0x12345678
74         .word   0x12345678
75         .word   0x12345678
76         .word   0x12345678
77 #else
78         ldr     pc, _undefined_instruction
79         ldr     pc, _software_interrupt
80         ldr     pc, _prefetch_abort
81         ldr     pc, _data_abort
82         ldr     pc, _not_used
83         ldr     pc, _irq
84         ldr     pc, _fiq
86 _undefined_instruction:
87         .word undefined_instruction
88 _software_interrupt:
89         .word software_interrupt
90 _prefetch_abort:
91         .word prefetch_abort
92 _data_abort:
93         .word data_abort
94 _not_used:
95         .word not_used
96 _irq:
97         .word irq
98 _fiq:
99         .word fiq
101 #endif  /* CONFIG_PRELOADER */
102         .balignl 16,0xdeadbeef
105 /*
106  *************************************************************************
107  *
108  * Startup Code (reset vector)
109  *
110  * do important init only if we don't start from memory!
111  * setup Memory and board specific bits prior to relocation.
112  * relocate armboot to ram
113  * setup stack
114  *
115  *************************************************************************
116  */
118 .globl _TEXT_BASE
119 _TEXT_BASE:
120         .word   CONFIG_SYS_TEXT_BASE
122 /*
123  * These are defined in the board-specific linker script.
124  * Subtracting _start from them lets the linker put their
125  * relative position in the executable instead of leaving
126  * them null.
127  */
128 .globl _bss_start_ofs
129 _bss_start_ofs:
130         .word __bss_start - _start
132 .globl _bss_end_ofs
133 _bss_end_ofs:
134         .word _end - _start
136 #ifdef CONFIG_USE_IRQ
137 /* IRQ stack memory (calculated at run-time) */
138 .globl IRQ_STACK_START
139 IRQ_STACK_START:
140         .word   0x0badc0de
142 /* IRQ stack memory (calculated at run-time) */
143 .globl FIQ_STACK_START
144 FIQ_STACK_START:
145         .word 0x0badc0de
146 #endif
148 #if !defined(CONFIG_SYS_ARM_WITHOUT_RELOC)
149 /* IRQ stack memory (calculated at run-time) + 8 bytes */
150 .globl IRQ_STACK_START_IN
151 IRQ_STACK_START_IN:
152         .word   0x0badc0de
154 /*
155  * the actual reset code
156  */
158 reset:
159         /*
160          * set the cpu to SVC32 mode
161          */
162         mrs     r0,cpsr
163         bic     r0,r0,#0x1f
164         orr     r0,r0,#0xd3
165         msr     cpsr,r0
167         /*
168          * we do sys-critical inits only at reboot,
169          * not when booting from ram!
170          */
171 #ifndef CONFIG_SKIP_LOWLEVEL_INIT
172         bl      cpu_init_crit
173 #endif
175 /* Set stackpointer in internal RAM to call board_init_f */
176 call_board_init_f:
177         ldr     sp, =(CONFIG_SYS_INIT_SP_ADDR)
178         ldr     r0,=0x00000000
179         bl      board_init_f
181 /*------------------------------------------------------------------------------*/
183 /*
184  * void relocate_code (addr_sp, gd, addr_moni)
185  *
186  * This "function" does not return, instead it continues in RAM
187  * after relocating the monitor code.
188  *
189  */
190         .globl  relocate_code
191 relocate_code:
192         mov     r4, r0  /* save addr_sp */
193         mov     r5, r1  /* save addr of gd */
194         mov     r6, r2  /* save addr of destination */
195         mov     r7, r2  /* save addr of destination */
197         /* Set up the stack                                                 */
198 stack_setup:
199         mov     sp, r4
201         adr     r0, _start
202         ldr     r2, _TEXT_BASE
203         ldr     r3, _bss_start_ofs
204         add     r2, r0, r3              /* r2 <- source end address         */
205         cmp     r0, r6
206         beq     clear_bss
208 #ifndef CONFIG_SKIP_RELOCATE_UBOOT
209 copy_loop:
210         ldmia   r0!, {r9-r10}           /* copy from source address [r0]    */
211         stmia   r6!, {r9-r10}           /* copy to   target address [r1]    */
212         cmp     r0, r2                  /* until source end address [r2]    */
213         blo     copy_loop
215 #ifndef CONFIG_PRELOADER
216         /*
217          * fix .rel.dyn relocations
218          */
219         ldr     r0, _TEXT_BASE          /* r0 <- Text base */
220         sub     r9, r7, r0              /* r9 <- relocation offset */
221         ldr     r10, _dynsym_start_ofs  /* r10 <- sym table ofs */
222         add     r10, r10, r0            /* r10 <- sym table in FLASH */
223         ldr     r2, _rel_dyn_start_ofs  /* r2 <- rel dyn start ofs */
224         add     r2, r2, r0              /* r2 <- rel dyn start in FLASH */
225         ldr     r3, _rel_dyn_end_ofs    /* r3 <- rel dyn end ofs */
226         add     r3, r3, r0              /* r3 <- rel dyn end in FLASH */
227 fixloop:
228         ldr     r0, [r2]        /* r0 <- location to fix up, IN FLASH! */
229         add     r0, r9          /* r0 <- location to fix up in RAM */
230         ldr     r1, [r2, #4]
231         and     r8, r1, #0xff
232         cmp     r8, #23         /* relative fixup? */
233         beq     fixrel
234         cmp     r8, #2          /* absolute fixup? */
235         beq     fixabs
236         /* ignore unknown type of fixup */
237         b       fixnext
238 fixabs:
239         /* absolute fix: set location to (offset) symbol value */
240         mov     r1, r1, LSR #4          /* r1 <- symbol index in .dynsym */
241         add     r1, r10, r1             /* r1 <- address of symbol in table */
242         ldr     r1, [r1, #4]            /* r1 <- symbol value */
243         add     r1, r9                  /* r1 <- relocated sym addr */
244         b       fixnext
245 fixrel:
246         /* relative fix: increase location by offset */
247         ldr     r1, [r0]
248         add     r1, r1, r9
249 fixnext:
250         str     r1, [r0]
251         add     r2, r2, #8      /* each rel.dyn entry is 8 bytes */
252         cmp     r2, r3
253         blo     fixloop
254 #endif
255 #endif  /* #ifndef CONFIG_SKIP_RELOCATE_UBOOT */
257 clear_bss:
258 #ifndef CONFIG_PRELOADER
259         ldr     r0, _bss_start_ofs
260         ldr     r1, _bss_end_ofs
261         ldr     r3, _TEXT_BASE          /* Text base */
262         mov     r4, r7                  /* reloc addr */
263         add     r0, r0, r4
264         add     r1, r1, r4
265         mov     r2, #0x00000000         /* clear                            */
267 clbss_l:str     r2, [r0]                /* clear loop...                    */
268         add     r0, r0, #4
269         cmp     r0, r1
270         bne     clbss_l
272         bl coloured_LED_init
273         bl red_LED_on
274 #endif
276 /*
277  * We are done. Do not return, instead branch to second part of board
278  * initialization, now running from RAM.
279  */
280 #ifdef CONFIG_NAND_SPL
281         ldr     r0, _nand_boot_ofs
282         mov     pc, r0
284 _nand_boot_ofs:
285         .word nand_boot
286 #else
287         ldr     r0, _board_init_r_ofs
288         adr     r1, _start
289         add     r0, r0, r1
290         add     lr, r0, r9
291         /* setup parameters for board_init_r */
292         mov     r0, r5          /* gd_t */
293         mov     r1, r7          /* dest_addr */
294         /* jump to it ... */
295         mov     pc, lr
297 _board_init_r_ofs:
298         .word board_init_r - _start
299 #endif
301 _rel_dyn_start_ofs:
302         .word __rel_dyn_start - _start
303 _rel_dyn_end_ofs:
304         .word __rel_dyn_end - _start
305 _dynsym_start_ofs:
306         .word __dynsym_start - _start
308 #else /* #if !defined(CONFIG_SYS_ARM_WITHOUT_RELOC) */
309 /*
310  * the actual reset code
311  */
313 reset:
314         /*
315          * set the cpu to SVC32 mode
316          */
317         mrs     r0,cpsr
318         bic     r0,r0,#0x1f
319         orr     r0,r0,#0xd3
320         msr     cpsr,r0
322         /*
323          * we do sys-critical inits only at reboot,
324          * not when booting from ram!
325          */
326 #ifndef CONFIG_SKIP_LOWLEVEL_INIT
327         bl      cpu_init_crit
328 #endif
330 #ifndef CONFIG_SKIP_RELOCATE_UBOOT
331 relocate:                               /* relocate U-Boot to RAM           */
332         adr     r0, _start              /* r0 <- current position of code   */
333         ldr     r1, _TEXT_BASE          /* test if we run from flash or RAM */
334         cmp     r0, r1                  /* don't reloc during debug         */
335         beq     stack_setup
336         ldr     r3, _bss_start_ofs      /* r3 <- _bss_start - _start        */
337         add     r2, r0, r3              /* r2 <- source end address         */
339 copy_loop:
340         ldmia   r0!, {r3-r10}           /* copy from source address [r0]    */
341         stmia   r1!, {r3-r10}           /* copy to   target address [r1]    */
342         cmp     r0, r2                  /* until source end address [r2]    */
343         blo     copy_loop
344 #endif  /* CONFIG_SKIP_RELOCATE_UBOOT */
346         /* Set up the stack                                                 */
347 stack_setup:
348         ldr     r0, _TEXT_BASE          /* upper 128 KiB: relocated uboot   */
349         sub     sp, r0, #128            /* leave 32 words for abort-stack   */
350 #ifndef CONFIG_PRELOADER
351         sub     r0, r0, #CONFIG_SYS_MALLOC_LEN  /* malloc area                      */
352         sub     r0, r0, #CONFIG_SYS_GBL_DATA_SIZE /* bdinfo                        */
353 #ifdef CONFIG_USE_IRQ
354         sub     r0, r0, #(CONFIG_STACKSIZE_IRQ+CONFIG_STACKSIZE_FIQ)
355 #endif
356 #endif /* CONFIG_PRELOADER */
357         sub     sp, r0, #12             /* leave 3 words for abort-stack    */
358         bic     sp, sp, #7              /* 8-byte alignment for ABI compliance */
360 clear_bss:
361         adr     r2, _start
362         ldr     r0, _bss_start_ofs      /* find start of bss segment        */
363         add     r0, r0, r2
364         ldr     r1, _bss_end_ofs        /* stop here                        */
365         add     r1, r1, r2
366         mov     r2, #0x00000000         /* clear                            */
368 #ifndef CONFIG_PRELOADER
369 clbss_l:str     r2, [r0]                /* clear loop...                    */
370         add     r0, r0, #4
371         cmp     r0, r1
372         blo     clbss_l
374         bl coloured_LED_init
375         bl red_LED_on
376 #endif /* CONFIG_PRELOADER */
378         ldr     r0, _start_armboot_ofs
379         adr     r1, _start
380         add     r0, r0, r1
381         ldr     pc, r0
383 _start_armboot_ofs:
384 #ifdef CONFIG_NAND_SPL
385         .word nand_boot - _start
386 #else
387         .word start_armboot - _start
388 #endif /* CONFIG_NAND_SPL */
389 #endif /* #if !defined(CONFIG_SYS_ARM_WITHOUT_RELOC) */
391 /*
392  *************************************************************************
393  *
394  * CPU_init_critical registers
395  *
396  * setup important registers
397  * setup memory timing
398  *
399  *************************************************************************
400  */
401 #ifndef CONFIG_SKIP_LOWLEVEL_INIT
402 cpu_init_crit:
403         /*
404          * flush v4 I/D caches
405          */
406         mov     r0, #0
407         mcr     p15, 0, r0, c7, c7, 0   /* flush v3/v4 cache */
408         mcr     p15, 0, r0, c8, c7, 0   /* flush v4 TLB */
410         /*
411          * disable MMU stuff and caches
412          */
413         mrc     p15, 0, r0, c1, c0, 0
414         bic     r0, r0, #0x00002300     /* clear bits 13, 9:8 (--V- --RS) */
415         bic     r0, r0, #0x00000087     /* clear bits 7, 2:0 (B--- -CAM) */
416         orr     r0, r0, #0x00000002     /* set bit 2 (A) Align */
417         orr     r0, r0, #0x00001000     /* set bit 12 (I) I-Cache */
418         mcr     p15, 0, r0, c1, c0, 0
420         /*
421          * Go setup Memory and board specific bits prior to relocation.
422          */
423         mov     ip, lr          /* perserve link reg across call */
424         bl      lowlevel_init   /* go setup pll,mux,memory */
425         mov     lr, ip          /* restore link */
426         mov     pc, lr          /* back to my caller */
427 #endif /* CONFIG_SKIP_LOWLEVEL_INIT */
429 #ifndef CONFIG_PRELOADER
430 /*
431  *************************************************************************
432  *
433  * Interrupt handling
434  *
435  *************************************************************************
436  */
439 @ IRQ stack frame.
441 #define S_FRAME_SIZE    72
443 #define S_OLD_R0        68
444 #define S_PSR           64
445 #define S_PC            60
446 #define S_LR            56
447 #define S_SP            52
449 #define S_IP            48
450 #define S_FP            44
451 #define S_R10           40
452 #define S_R9            36
453 #define S_R8            32
454 #define S_R7            28
455 #define S_R6            24
456 #define S_R5            20
457 #define S_R4            16
458 #define S_R3            12
459 #define S_R2            8
460 #define S_R1            4
461 #define S_R0            0
463 #define MODE_SVC 0x13
464 #define I_BIT    0x80
466 /*
467  * use bad_save_user_regs for abort/prefetch/undef/swi ...
468  * use irq_save_user_regs / irq_restore_user_regs for IRQ/FIQ handling
469  */
471         .macro  bad_save_user_regs
472         @ carve out a frame on current user stack
473         sub     sp, sp, #S_FRAME_SIZE
474         stmia   sp, {r0 - r12}  @ Save user registers (now in svc mode) r0-r12
475 #if defined(CONFIG_SYS_ARM_WITHOUT_RELOC)
476         adr     r2, _start
477         sub     r2, r2, #(CONFIG_STACKSIZE+CONFIG_SYS_MALLOC_LEN)
478         sub     r2, r2, #(CONFIG_SYS_GBL_DATA_SIZE+8)  @ set base 2 words into abort stack
479 #else
480         ldr     r2, IRQ_STACK_START_IN
481 #endif
482         @ get values for "aborted" pc and cpsr (into parm regs)
483         ldmia   r2, {r2 - r3}
484         add     r0, sp, #S_FRAME_SIZE           @ grab pointer to old stack
485         add     r5, sp, #S_SP
486         mov     r1, lr
487         stmia   r5, {r0 - r3}   @ save sp_SVC, lr_SVC, pc, cpsr
488         mov     r0, sp          @ save current stack into r0 (param register)
489         .endm
491         .macro  irq_save_user_regs
492         sub     sp, sp, #S_FRAME_SIZE
493         stmia   sp, {r0 - r12}                  @ Calling r0-r12
494         @ !!!! R8 NEEDS to be saved !!!! a reserved stack spot would be good.
495         add     r8, sp, #S_PC
496         stmdb   r8, {sp, lr}^           @ Calling SP, LR
497         str     lr, [r8, #0]            @ Save calling PC
498         mrs     r6, spsr
499         str     r6, [r8, #4]            @ Save CPSR
500         str     r0, [r8, #8]            @ Save OLD_R0
501         mov     r0, sp
502         .endm
504         .macro  irq_restore_user_regs
505         ldmia   sp, {r0 - lr}^                  @ Calling r0 - lr
506         mov     r0, r0
507         ldr     lr, [sp, #S_PC]                 @ Get PC
508         add     sp, sp, #S_FRAME_SIZE
509         subs    pc, lr, #4              @ return & move spsr_svc into cpsr
510         .endm
512         .macro get_bad_stack
513 #if defined(CONFIG_SYS_ARM_WITHOUT_RELOC)
514         adr     r13, _start             @ setup our mode stack
515         sub     r13, r13, #(CONFIG_STACKSIZE+CONFIG_SYS_MALLOC_LEN)
516         sub     r13, r13, #(CONFIG_SYS_GBL_DATA_SIZE+8) @ reserved a couple spots in abort stack
517 #else
518         ldr     r13, IRQ_STACK_START_IN         @ setup our mode stack
519 #endif
521         str     lr, [r13]       @ save caller lr in position 0 of saved stack
522         mrs     lr, spsr        @ get the spsr
523         str     lr, [r13, #4]   @ save spsr in position 1 of saved stack
524         mov     r13, #MODE_SVC  @ prepare SVC-Mode
525         @ msr   spsr_c, r13
526         msr     spsr, r13       @ switch modes, make sure moves will execute
527         mov     lr, pc          @ capture return pc
528         movs    pc, lr          @ jump to next instruction & switch modes.
529         .endm
531         .macro get_irq_stack                    @ setup IRQ stack
532         ldr     sp, IRQ_STACK_START
533         .endm
535         .macro get_fiq_stack                    @ setup FIQ stack
536         ldr     sp, FIQ_STACK_START
537         .endm
538 #endif  /* CONFIG_PRELOADER */
540 /*
541  * exception handlers
542  */
543 #ifdef CONFIG_PRELOADER
544         .align  5
545 do_hang:
546         ldr     sp, _TEXT_BASE                  /* switch to abort stack */
547 1:
548         bl      1b                              /* hang and never return */
549 #else   /* !CONFIG_PRELOADER */
550         .align  5
551 undefined_instruction:
552         get_bad_stack
553         bad_save_user_regs
554         bl      do_undefined_instruction
556         .align  5
557 software_interrupt:
558         get_bad_stack
559         bad_save_user_regs
560         bl      do_software_interrupt
562         .align  5
563 prefetch_abort:
564         get_bad_stack
565         bad_save_user_regs
566         bl      do_prefetch_abort
568         .align  5
569 data_abort:
570         get_bad_stack
571         bad_save_user_regs
572         bl      do_data_abort
574         .align  5
575 not_used:
576         get_bad_stack
577         bad_save_user_regs
578         bl      do_not_used
580 #ifdef CONFIG_USE_IRQ
582         .align  5
583 irq:
584         get_irq_stack
585         irq_save_user_regs
586         bl      do_irq
587         irq_restore_user_regs
589         .align  5
590 fiq:
591         get_fiq_stack
592         /* someone ought to write a more effiction fiq_save_user_regs */
593         irq_save_user_regs
594         bl      do_fiq
595         irq_restore_user_regs
597 #else
599         .align  5
600 irq:
601         get_bad_stack
602         bad_save_user_regs
603         bl      do_irq
605         .align  5
606 fiq:
607         get_bad_stack
608         bad_save_user_regs
609         bl      do_fiq
611 #endif
612 #endif  /* CONFIG_PRELOADER */