ARM: OMAP4/5: clocks: Add the required OPP settings as per the latest addendum
[glsdk/glsdk-u-boot.git] / arch / arm / cpu / armv7 / omap-common / clocks-common.c
1 /*
2  *
3  * Clock initialization for OMAP4
4  *
5  * (C) Copyright 2010
6  * Texas Instruments, <www.ti.com>
7  *
8  * Aneesh V <aneesh@ti.com>
9  *
10  * Based on previous work by:
11  *      Santosh Shilimkar <santosh.shilimkar@ti.com>
12  *      Rajendra Nayak <rnayak@ti.com>
13  *
14  * See file CREDITS for list of people who contributed to this
15  * project.
16  *
17  * This program is free software; you can redistribute it and/or
18  * modify it under the terms of the GNU General Public License as
19  * published by the Free Software Foundation; either version 2 of
20  * the License, or (at your option) any later version.
21  *
22  * This program is distributed in the hope that it will be useful,
23  * but WITHOUT ANY WARRANTY; without even the implied warranty of
24  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
25  * GNU General Public License for more details.
26  *
27  * You should have received a copy of the GNU General Public License
28  * along with this program; if not, write to the Free Software
29  * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
30  * MA 02111-1307 USA
31  */
32 #include <common.h>
33 #include <asm/omap_common.h>
34 #include <asm/gpio.h>
35 #include <asm/arch/clocks.h>
36 #include <asm/arch/sys_proto.h>
37 #include <asm/utils.h>
38 #include <asm/omap_gpio.h>
39 #include <asm/emif.h>
41 #ifndef CONFIG_SPL_BUILD
42 /*
43  * printing to console doesn't work unless
44  * this code is executed from SPL
45  */
46 #define printf(fmt, args...)
47 #define puts(s)
48 #endif
50 const u32 sys_clk_array[8] = {
51         12000000,              /* 12 MHz */
52         13000000,              /* 13 MHz */
53         16800000,              /* 16.8 MHz */
54         19200000,              /* 19.2 MHz */
55         26000000,              /* 26 MHz */
56         27000000,              /* 27 MHz */
57         38400000,              /* 38.4 MHz */
58 };
60 static inline u32 __get_sys_clk_index(void)
61 {
62         u32 ind;
63         /*
64          * For ES1 the ROM code calibration of sys clock is not reliable
65          * due to hw issue. So, use hard-coded value. If this value is not
66          * correct for any board over-ride this function in board file
67          * From ES2.0 onwards you will get this information from
68          * CM_SYS_CLKSEL
69          */
70         if (omap_revision() == OMAP4430_ES1_0)
71                 ind = OMAP_SYS_CLK_IND_38_4_MHZ;
72         else {
73                 /* SYS_CLKSEL - 1 to match the dpll param array indices */
74                 ind = (readl((*prcm)->cm_sys_clksel) &
75                         CM_SYS_CLKSEL_SYS_CLKSEL_MASK) - 1;
76         }
77         return ind;
78 }
80 u32 get_sys_clk_index(void)
81         __attribute__ ((weak, alias("__get_sys_clk_index")));
83 u32 get_sys_clk_freq(void)
84 {
85         u8 index = get_sys_clk_index();
86         return sys_clk_array[index];
87 }
89 void setup_post_dividers(u32 const base, const struct dpll_params *params)
90 {
91         struct dpll_regs *const dpll_regs = (struct dpll_regs *)base;
93         /* Setup post-dividers */
94         if (params->m2 >= 0)
95                 writel(params->m2, &dpll_regs->cm_div_m2_dpll);
96         if (params->m3 >= 0)
97                 writel(params->m3, &dpll_regs->cm_div_m3_dpll);
98         if (params->m4_h11 >= 0)
99                 writel(params->m4_h11, &dpll_regs->cm_div_m4_h11_dpll);
100         if (params->m5_h12 >= 0)
101                 writel(params->m5_h12, &dpll_regs->cm_div_m5_h12_dpll);
102         if (params->m6_h13 >= 0)
103                 writel(params->m6_h13, &dpll_regs->cm_div_m6_h13_dpll);
104         if (params->m7_h14 >= 0)
105                 writel(params->m7_h14, &dpll_regs->cm_div_m7_h14_dpll);
106         if (params->h21 >= 0)
107                 writel(params->h21, &dpll_regs->cm_div_h21_dpll);
108         if (params->h22 >= 0)
109                 writel(params->h22, &dpll_regs->cm_div_h22_dpll);
110         if (params->h23 >= 0)
111                 writel(params->h23, &dpll_regs->cm_div_h23_dpll);
112         if (params->h24 >= 0)
113                 writel(params->h24, &dpll_regs->cm_div_h24_dpll);
116 static inline void do_bypass_dpll(u32 const base)
118         struct dpll_regs *dpll_regs = (struct dpll_regs *)base;
120         clrsetbits_le32(&dpll_regs->cm_clkmode_dpll,
121                         CM_CLKMODE_DPLL_DPLL_EN_MASK,
122                         DPLL_EN_FAST_RELOCK_BYPASS <<
123                         CM_CLKMODE_DPLL_EN_SHIFT);
126 static inline void wait_for_bypass(u32 const base)
128         struct dpll_regs *const dpll_regs = (struct dpll_regs *)base;
130         if (!wait_on_value(ST_DPLL_CLK_MASK, 0, &dpll_regs->cm_idlest_dpll,
131                                 LDELAY)) {
132                 printf("Bypassing DPLL failed %x\n", base);
133         }
136 static inline void do_lock_dpll(u32 const base)
138         struct dpll_regs *const dpll_regs = (struct dpll_regs *)base;
140         clrsetbits_le32(&dpll_regs->cm_clkmode_dpll,
141                       CM_CLKMODE_DPLL_DPLL_EN_MASK,
142                       DPLL_EN_LOCK << CM_CLKMODE_DPLL_EN_SHIFT);
145 static inline void wait_for_lock(u32 const base)
147         struct dpll_regs *const dpll_regs = (struct dpll_regs *)base;
149         if (!wait_on_value(ST_DPLL_CLK_MASK, ST_DPLL_CLK_MASK,
150                 &dpll_regs->cm_idlest_dpll, LDELAY)) {
151                 printf("DPLL locking failed for %x\n", base);
152                 hang();
153         }
156 inline u32 check_for_lock(u32 const base)
158         struct dpll_regs *const dpll_regs = (struct dpll_regs *)base;
159         u32 lock = readl(&dpll_regs->cm_idlest_dpll) & ST_DPLL_CLK_MASK;
161         return lock;
164 const struct dpll_params *get_mpu_dpll_params(struct dplls const *dpll_data)
166         u32 sysclk_ind = get_sys_clk_index();
167         return &dpll_data->mpu[sysclk_ind];
170 const struct dpll_params *get_core_dpll_params(struct dplls const *dpll_data)
172         u32 sysclk_ind = get_sys_clk_index();
173         return &dpll_data->core[sysclk_ind];
176 const struct dpll_params *get_per_dpll_params(struct dplls const *dpll_data)
178         u32 sysclk_ind = get_sys_clk_index();
179         return &dpll_data->per[sysclk_ind];
182 const struct dpll_params *get_iva_dpll_params(struct dplls const *dpll_data)
184         u32 sysclk_ind = get_sys_clk_index();
185         return &dpll_data->iva[sysclk_ind];
188 const struct dpll_params *get_usb_dpll_params(struct dplls const *dpll_data)
190         u32 sysclk_ind = get_sys_clk_index();
191         return &dpll_data->usb[sysclk_ind];
194 const struct dpll_params *get_abe_dpll_params(struct dplls const *dpll_data)
196 #ifdef CONFIG_SYS_OMAP_ABE_SYSCK
197         u32 sysclk_ind = get_sys_clk_index();
198         return &dpll_data->abe[sysclk_ind];
199 #else
200         return dpll_data->abe;
201 #endif
204 static void do_setup_dpll(u32 const base, const struct dpll_params *params,
205                                 u8 lock, char *dpll)
207         u32 temp, M, N;
208         struct dpll_regs *const dpll_regs = (struct dpll_regs *)base;
210         temp = readl(&dpll_regs->cm_clksel_dpll);
212         if (check_for_lock(base)) {
213                 /*
214                  * The Dpll has already been locked by rom code using CH.
215                  * Check if M,N are matching with Ideal nominal opp values.
216                  * If matches, skip the rest otherwise relock.
217                  */
218                 M = (temp & CM_CLKSEL_DPLL_M_MASK) >> CM_CLKSEL_DPLL_M_SHIFT;
219                 N = (temp & CM_CLKSEL_DPLL_N_MASK) >> CM_CLKSEL_DPLL_N_SHIFT;
220                 if ((M != (params->m)) || (N != (params->n))) {
221                         debug("\n %s Dpll locked, but not for ideal M = %d,"
222                                 "N = %d values, current values are M = %d,"
223                                 "N= %d" , dpll, params->m, params->n,
224                                 M, N);
225                 } else {
226                         /* Dpll locked with ideal values for nominal opps. */
227                         debug("\n %s Dpll already locked with ideal"
228                                                 "nominal opp values", dpll);
229                         goto setup_post_dividers;
230                 }
231         }
233         bypass_dpll(base);
235         /* Set M & N */
236         temp &= ~CM_CLKSEL_DPLL_M_MASK;
237         temp |= (params->m << CM_CLKSEL_DPLL_M_SHIFT) & CM_CLKSEL_DPLL_M_MASK;
239         temp &= ~CM_CLKSEL_DPLL_N_MASK;
240         temp |= (params->n << CM_CLKSEL_DPLL_N_SHIFT) & CM_CLKSEL_DPLL_N_MASK;
242         writel(temp, &dpll_regs->cm_clksel_dpll);
244         /* Lock */
245         if (lock)
246                 do_lock_dpll(base);
248 setup_post_dividers:
249         setup_post_dividers(base, params);
251         /* Wait till the DPLL locks */
252         if (lock)
253                 wait_for_lock(base);
256 u32 omap_ddr_clk(void)
258         u32 ddr_clk, sys_clk_khz, omap_rev, divider;
259         const struct dpll_params *core_dpll_params;
261         omap_rev = omap_revision();
262         sys_clk_khz = get_sys_clk_freq() / 1000;
264         core_dpll_params = get_core_dpll_params(*dplls_data);
266         debug("sys_clk %d\n ", sys_clk_khz * 1000);
268         /* Find Core DPLL locked frequency first */
269         ddr_clk = sys_clk_khz * 2 * core_dpll_params->m /
270                         (core_dpll_params->n + 1);
272         if (omap_rev < OMAP5430_ES1_0) {
273                 /*
274                  * DDR frequency is PHY_ROOT_CLK/2
275                  * PHY_ROOT_CLK = Fdpll/2/M2
276                  */
277                 divider = 4;
278         } else {
279                 /*
280                  * DDR frequency is PHY_ROOT_CLK
281                  * PHY_ROOT_CLK = Fdpll/2/M2
282                  */
283                 divider = 2;
284         }
286         ddr_clk = ddr_clk / divider / core_dpll_params->m2;
287         ddr_clk *= 1000;        /* convert to Hz */
288         debug("ddr_clk %d\n ", ddr_clk);
290         return ddr_clk;
293 /*
294  * Lock MPU dpll
295  *
296  * Resulting MPU frequencies:
297  * 4430 ES1.0   : 600 MHz
298  * 4430 ES2.x   : 792 MHz (OPP Turbo)
299  * 4460         : 920 MHz (OPP Turbo) - DCC disabled
300  */
301 void configure_mpu_dpll(void)
303         const struct dpll_params *params;
304         struct dpll_regs *mpu_dpll_regs;
305         u32 omap_rev;
306         omap_rev = omap_revision();
308         /*
309          * DCC and clock divider settings for 4460.
310          * DCC is required, if more than a certain frequency is required.
311          * For, 4460 > 1GHZ.
312          *     5430 > 1.4GHZ.
313          */
314         if ((omap_rev >= OMAP4460_ES1_0) && (omap_rev < OMAP5430_ES1_0)) {
315                 mpu_dpll_regs =
316                         (struct dpll_regs *)((*prcm)->cm_clkmode_dpll_mpu);
317                 bypass_dpll((*prcm)->cm_clkmode_dpll_mpu);
318                 clrbits_le32((*prcm)->cm_mpu_mpu_clkctrl,
319                         MPU_CLKCTRL_CLKSEL_EMIF_DIV_MODE_MASK);
320                 setbits_le32((*prcm)->cm_mpu_mpu_clkctrl,
321                         MPU_CLKCTRL_CLKSEL_ABE_DIV_MODE_MASK);
322                 clrbits_le32(&mpu_dpll_regs->cm_clksel_dpll,
323                         CM_CLKSEL_DCC_EN_MASK);
324         }
326         params = get_mpu_dpll_params(*dplls_data);
328         do_setup_dpll((*prcm)->cm_clkmode_dpll_mpu, params, DPLL_LOCK, "mpu");
329         debug("MPU DPLL locked\n");
332 #ifdef CONFIG_USB_EHCI_OMAP
333 static void setup_usb_dpll(void)
335         const struct dpll_params *params;
336         u32 sys_clk_khz, sd_div, num, den;
338         sys_clk_khz = get_sys_clk_freq() / 1000;
339         /*
340          * USB:
341          * USB dpll is J-type. Need to set DPLL_SD_DIV for jitter correction
342          * DPLL_SD_DIV = CEILING ([DPLL_MULT/(DPLL_DIV+1)]* CLKINP / 250)
343          *      - where CLKINP is sys_clk in MHz
344          * Use CLKINP in KHz and adjust the denominator accordingly so
345          * that we have enough accuracy and at the same time no overflow
346          */
347         params = get_usb_dpll_params(*dplls_data);
348         num = params->m * sys_clk_khz;
349         den = (params->n + 1) * 250 * 1000;
350         num += den - 1;
351         sd_div = num / den;
352         clrsetbits_le32((*prcm)->cm_clksel_dpll_usb,
353                         CM_CLKSEL_DPLL_DPLL_SD_DIV_MASK,
354                         sd_div << CM_CLKSEL_DPLL_DPLL_SD_DIV_SHIFT);
356         /* Now setup the dpll with the regular function */
357         do_setup_dpll((*prcm)->cm_clkmode_dpll_usb, params, DPLL_LOCK, "usb");
359 #endif
361 static void setup_dplls(void)
363         u32 temp;
364         const struct dpll_params *params;
366         debug("setup_dplls\n");
368         /* CORE dpll */
369         params = get_core_dpll_params(*dplls_data);     /* default - safest */
370         /*
371          * Do not lock the core DPLL now. Just set it up.
372          * Core DPLL will be locked after setting up EMIF
373          * using the FREQ_UPDATE method(freq_update_core())
374          */
375         if (emif_sdram_type() == EMIF_SDRAM_TYPE_LPDDR2)
376                 do_setup_dpll((*prcm)->cm_clkmode_dpll_core, params,
377                                                         DPLL_NO_LOCK, "core");
378         else
379                 do_setup_dpll((*prcm)->cm_clkmode_dpll_core, params,
380                                                         DPLL_LOCK, "core");
381         /* Set the ratios for CORE_CLK, L3_CLK, L4_CLK */
382         temp = (CLKSEL_CORE_X2_DIV_1 << CLKSEL_CORE_SHIFT) |
383             (CLKSEL_L3_CORE_DIV_2 << CLKSEL_L3_SHIFT) |
384             (CLKSEL_L4_L3_DIV_2 << CLKSEL_L4_SHIFT);
385         writel(temp, (*prcm)->cm_clksel_core);
386         debug("Core DPLL configured\n");
388         /* lock PER dpll */
389         params = get_per_dpll_params(*dplls_data);
390         do_setup_dpll((*prcm)->cm_clkmode_dpll_per,
391                         params, DPLL_LOCK, "per");
392         debug("PER DPLL locked\n");
394         /* MPU dpll */
395         configure_mpu_dpll();
397 #ifdef CONFIG_USB_EHCI_OMAP
398         setup_usb_dpll();
399 #endif
402 #ifdef CONFIG_SYS_CLOCKS_ENABLE_ALL
403 static void setup_non_essential_dplls(void)
405         u32 abe_ref_clk;
406         const struct dpll_params *params;
408         /* IVA */
409         clrsetbits_le32((*prcm)->cm_bypclk_dpll_iva,
410                 CM_BYPCLK_DPLL_IVA_CLKSEL_MASK, DPLL_IVA_CLKSEL_CORE_X2_DIV_2);
412         params = get_iva_dpll_params(*dplls_data);
413         do_setup_dpll((*prcm)->cm_clkmode_dpll_iva, params, DPLL_LOCK, "iva");
415         /* Configure ABE dpll */
416         params = get_abe_dpll_params(*dplls_data);
417 #ifdef CONFIG_SYS_OMAP_ABE_SYSCK
418         abe_ref_clk = CM_ABE_PLL_REF_CLKSEL_CLKSEL_SYSCLK;
419 #else
420         abe_ref_clk = CM_ABE_PLL_REF_CLKSEL_CLKSEL_32KCLK;
421         /*
422          * We need to enable some additional options to achieve
423          * 196.608MHz from 32768 Hz
424          */
425         setbits_le32((*prcm)->cm_clkmode_dpll_abe,
426                         CM_CLKMODE_DPLL_DRIFTGUARD_EN_MASK|
427                         CM_CLKMODE_DPLL_RELOCK_RAMP_EN_MASK|
428                         CM_CLKMODE_DPLL_LPMODE_EN_MASK|
429                         CM_CLKMODE_DPLL_REGM4XEN_MASK);
430         /* Spend 4 REFCLK cycles at each stage */
431         clrsetbits_le32((*prcm)->cm_clkmode_dpll_abe,
432                         CM_CLKMODE_DPLL_RAMP_RATE_MASK,
433                         1 << CM_CLKMODE_DPLL_RAMP_RATE_SHIFT);
434 #endif
436         /* Select the right reference clk */
437         clrsetbits_le32((*prcm)->cm_abe_pll_ref_clksel,
438                         CM_ABE_PLL_REF_CLKSEL_CLKSEL_MASK,
439                         abe_ref_clk << CM_ABE_PLL_REF_CLKSEL_CLKSEL_SHIFT);
440         /* Lock the dpll */
441         do_setup_dpll((*prcm)->cm_clkmode_dpll_abe, params, DPLL_LOCK, "abe");
443 #endif
445 u32 get_offset_code(u32 volt_offset, struct pmic_data *pmic)
447         u32 offset_code;
449         volt_offset -= pmic->base_offset;
451         offset_code = (volt_offset + pmic->step - 1) / pmic->step;
453         /*
454          * Offset codes 1-6 all give the base voltage in Palmas
455          * Offset code 0 switches OFF the SMPS
456          */
457         return offset_code + pmic->start_code;
460 void do_scale_vcore(u32 vcore_reg, u32 volt_mv, struct pmic_data *pmic)
462         u32 offset_code;
463         u32 offset = volt_mv;
464         int ret = 0;
466         /* See if we can first get the GPIO if needed */
467         if (pmic->gpio_en)
468                 ret = gpio_request(pmic->gpio, "PMIC_GPIO");
470         if (ret < 0) {
471                 printf("%s: gpio %d request failed %d\n", __func__,
472                                                         pmic->gpio, ret);
473                 return;
474         }
476         /* Pull the GPIO low to select SET0 register, while we program SET1 */
477         if (pmic->gpio_en)
478                 gpio_direction_output(pmic->gpio, 0);
480         /* convert to uV for better accuracy in the calculations */
481         offset *= 1000;
483         offset_code = get_offset_code(offset, pmic);
485         debug("do_scale_vcore: volt - %d offset_code - 0x%x\n", volt_mv,
486                 offset_code);
488         if (omap_vc_bypass_send_value(SMPS_I2C_SLAVE_ADDR,
489                                 vcore_reg, offset_code))
490                 printf("Scaling voltage failed for 0x%x\n", vcore_reg);
492         if (pmic->gpio_en)
493                 gpio_direction_output(pmic->gpio, 1);
496 /*
497  * Setup the voltages for vdd_mpu, vdd_core, and vdd_iva
498  * We set the maximum voltages allowed here because Smart-Reflex is not
499  * enabled in bootloader. Voltage initialization in the kernel will set
500  * these to the nominal values after enabling Smart-Reflex
501  */
502 void scale_vcores(struct vcores_data const *vcores)
504         omap_vc_init(PRM_VC_I2C_CHANNEL_FREQ_KHZ);
506         do_scale_vcore(vcores->core.addr, vcores->core.value,
507                                           vcores->core.pmic);
509         do_scale_vcore(vcores->mpu.addr, vcores->mpu.value,
510                                           vcores->mpu.pmic);
512         do_scale_vcore(vcores->mm.addr, vcores->mm.value,
513                                           vcores->mm.pmic);
515          if (emif_sdram_type() == EMIF_SDRAM_TYPE_DDR3) {
516                 /* Configure LDO SRAM "magic" bits */
517                 writel(2, (*prcm)->prm_sldo_core_setup);
518                 writel(2, (*prcm)->prm_sldo_mpu_setup);
519                 writel(2, (*prcm)->prm_sldo_mm_setup);
520         }
523 static inline void enable_clock_domain(u32 const clkctrl_reg, u32 enable_mode)
525         clrsetbits_le32(clkctrl_reg, CD_CLKCTRL_CLKTRCTRL_MASK,
526                         enable_mode << CD_CLKCTRL_CLKTRCTRL_SHIFT);
527         debug("Enable clock domain - %x\n", clkctrl_reg);
530 static inline void wait_for_clk_enable(u32 clkctrl_addr)
532         u32 clkctrl, idlest = MODULE_CLKCTRL_IDLEST_DISABLED;
533         u32 bound = LDELAY;
535         while ((idlest == MODULE_CLKCTRL_IDLEST_DISABLED) ||
536                 (idlest == MODULE_CLKCTRL_IDLEST_TRANSITIONING)) {
538                 clkctrl = readl(clkctrl_addr);
539                 idlest = (clkctrl & MODULE_CLKCTRL_IDLEST_MASK) >>
540                          MODULE_CLKCTRL_IDLEST_SHIFT;
541                 if (--bound == 0) {
542                         printf("Clock enable failed for 0x%x idlest 0x%x\n",
543                                 clkctrl_addr, clkctrl);
544                         return;
545                 }
546         }
549 static inline void enable_clock_module(u32 const clkctrl_addr, u32 enable_mode,
550                                 u32 wait_for_enable)
552         clrsetbits_le32(clkctrl_addr, MODULE_CLKCTRL_MODULEMODE_MASK,
553                         enable_mode << MODULE_CLKCTRL_MODULEMODE_SHIFT);
554         debug("Enable clock module - %x\n", clkctrl_addr);
555         if (wait_for_enable)
556                 wait_for_clk_enable(clkctrl_addr);
559 void freq_update_core(void)
561         u32 freq_config1 = 0;
562         const struct dpll_params *core_dpll_params;
563         u32 omap_rev = omap_revision();
565         core_dpll_params = get_core_dpll_params(*dplls_data);
566         /* Put EMIF clock domain in sw wakeup mode */
567         enable_clock_domain((*prcm)->cm_memif_clkstctrl,
568                                 CD_CLKCTRL_CLKTRCTRL_SW_WKUP);
569         wait_for_clk_enable((*prcm)->cm_memif_emif_1_clkctrl);
570         wait_for_clk_enable((*prcm)->cm_memif_emif_2_clkctrl);
572         freq_config1 = SHADOW_FREQ_CONFIG1_FREQ_UPDATE_MASK |
573             SHADOW_FREQ_CONFIG1_DLL_RESET_MASK;
575         freq_config1 |= (DPLL_EN_LOCK << SHADOW_FREQ_CONFIG1_DPLL_EN_SHIFT) &
576                                 SHADOW_FREQ_CONFIG1_DPLL_EN_MASK;
578         freq_config1 |= (core_dpll_params->m2 <<
579                         SHADOW_FREQ_CONFIG1_M2_DIV_SHIFT) &
580                         SHADOW_FREQ_CONFIG1_M2_DIV_MASK;
582         writel(freq_config1, (*prcm)->cm_shadow_freq_config1);
583         if (!wait_on_value(SHADOW_FREQ_CONFIG1_FREQ_UPDATE_MASK, 0,
584                         (u32 *) (*prcm)->cm_shadow_freq_config1, LDELAY)) {
585                 puts("FREQ UPDATE procedure failed!!");
586                 hang();
587         }
589         /*
590          * Putting EMIF in HW_AUTO is seen to be causing issues with
591          * EMIF clocks and the master DLL. Put EMIF in SW_WKUP
592          * in OMAP5430 ES1.0 silicon
593          */
594         if (omap_rev != OMAP5430_ES1_0) {
595                 /* Put EMIF clock domain back in hw auto mode */
596                 enable_clock_domain((*prcm)->cm_memif_clkstctrl,
597                                         CD_CLKCTRL_CLKTRCTRL_HW_AUTO);
598                 wait_for_clk_enable((*prcm)->cm_memif_emif_1_clkctrl);
599                 wait_for_clk_enable((*prcm)->cm_memif_emif_2_clkctrl);
600         }
603 void bypass_dpll(u32 const base)
605         do_bypass_dpll(base);
606         wait_for_bypass(base);
609 void lock_dpll(u32 const base)
611         do_lock_dpll(base);
612         wait_for_lock(base);
615 void setup_clocks_for_console(void)
617         /* Do not add any spl_debug prints in this function */
618         clrsetbits_le32((*prcm)->cm_l4per_clkstctrl, CD_CLKCTRL_CLKTRCTRL_MASK,
619                         CD_CLKCTRL_CLKTRCTRL_SW_WKUP <<
620                         CD_CLKCTRL_CLKTRCTRL_SHIFT);
622         /* Enable all UARTs - console will be on one of them */
623         clrsetbits_le32((*prcm)->cm_l4per_uart1_clkctrl,
624                         MODULE_CLKCTRL_MODULEMODE_MASK,
625                         MODULE_CLKCTRL_MODULEMODE_SW_EXPLICIT_EN <<
626                         MODULE_CLKCTRL_MODULEMODE_SHIFT);
628         clrsetbits_le32((*prcm)->cm_l4per_uart2_clkctrl,
629                         MODULE_CLKCTRL_MODULEMODE_MASK,
630                         MODULE_CLKCTRL_MODULEMODE_SW_EXPLICIT_EN <<
631                         MODULE_CLKCTRL_MODULEMODE_SHIFT);
633         clrsetbits_le32((*prcm)->cm_l4per_uart3_clkctrl,
634                         MODULE_CLKCTRL_MODULEMODE_MASK,
635                         MODULE_CLKCTRL_MODULEMODE_SW_EXPLICIT_EN <<
636                         MODULE_CLKCTRL_MODULEMODE_SHIFT);
638         clrsetbits_le32((*prcm)->cm_l4per_uart3_clkctrl,
639                         MODULE_CLKCTRL_MODULEMODE_MASK,
640                         MODULE_CLKCTRL_MODULEMODE_SW_EXPLICIT_EN <<
641                         MODULE_CLKCTRL_MODULEMODE_SHIFT);
643         clrsetbits_le32((*prcm)->cm_l4per_clkstctrl, CD_CLKCTRL_CLKTRCTRL_MASK,
644                         CD_CLKCTRL_CLKTRCTRL_HW_AUTO <<
645                         CD_CLKCTRL_CLKTRCTRL_SHIFT);
648 void do_enable_clocks(u32 const *clk_domains,
649                             u32 const *clk_modules_hw_auto,
650                             u32 const *clk_modules_explicit_en,
651                             u8 wait_for_enable)
653         u32 i, max = 100;
655         /* Put the clock domains in SW_WKUP mode */
656         for (i = 0; (i < max) && clk_domains[i]; i++) {
657                 enable_clock_domain(clk_domains[i],
658                                     CD_CLKCTRL_CLKTRCTRL_SW_WKUP);
659         }
661         /* Clock modules that need to be put in HW_AUTO */
662         for (i = 0; (i < max) && clk_modules_hw_auto[i]; i++) {
663                 enable_clock_module(clk_modules_hw_auto[i],
664                                     MODULE_CLKCTRL_MODULEMODE_HW_AUTO,
665                                     wait_for_enable);
666         };
668         /* Clock modules that need to be put in SW_EXPLICIT_EN mode */
669         for (i = 0; (i < max) && clk_modules_explicit_en[i]; i++) {
670                 enable_clock_module(clk_modules_explicit_en[i],
671                                     MODULE_CLKCTRL_MODULEMODE_SW_EXPLICIT_EN,
672                                     wait_for_enable);
673         };
675         /* Put the clock domains in HW_AUTO mode now */
676         for (i = 0; (i < max) && clk_domains[i]; i++) {
677                 enable_clock_domain(clk_domains[i],
678                                     CD_CLKCTRL_CLKTRCTRL_HW_AUTO);
679         }
682 void prcm_init(void)
684         switch (omap_hw_init_context()) {
685         case OMAP_INIT_CONTEXT_SPL:
686         case OMAP_INIT_CONTEXT_UBOOT_FROM_NOR:
687         case OMAP_INIT_CONTEXT_UBOOT_AFTER_CH:
688                 enable_basic_clocks();
689                 scale_vcores(*omap_vcores);
690                 setup_dplls();
691 #ifdef CONFIG_SYS_CLOCKS_ENABLE_ALL
692                 setup_non_essential_dplls();
693                 enable_non_essential_clocks();
694 #endif
695                 break;
696         default:
697                 break;
698         }
700         if (OMAP_INIT_CONTEXT_SPL != omap_hw_init_context())
701                 enable_basic_uboot_clocks();