ARM: OMAP4+: Cleanup emif specific files
[glsdk/glsdk-u-boot.git] / arch / arm / cpu / armv7 / omap-common / emif-common.c
1 /*
2  * EMIF programming
3  *
4  * (C) Copyright 2010
5  * Texas Instruments, <www.ti.com>
6  *
7  * Aneesh V <aneesh@ti.com>
8  *
9  * See file CREDITS for list of people who contributed to this
10  * project.
11  *
12  * This program is free software; you can redistribute it and/or
13  * modify it under the terms of the GNU General Public License as
14  * published by the Free Software Foundation; either version 2 of
15  * the License, or (at your option) any later version.
16  *
17  * This program is distributed in the hope that it will be useful,
18  * but WITHOUT ANY WARRANTY; without even the implied warranty of
19  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
20  * GNU General Public License for more details.
21  *
22  * You should have received a copy of the GNU General Public License
23  * along with this program; if not, write to the Free Software
24  * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
25  * MA 02111-1307 USA
26  */
28 #include <common.h>
29 #include <asm/emif.h>
30 #include <asm/arch/clocks.h>
31 #include <asm/arch/sys_proto.h>
32 #include <asm/omap_common.h>
33 #include <asm/utils.h>
34 #include <linux/compiler.h>
36 static int emif1_enabled = -1, emif2_enabled = -1;
38 void set_lpmode_selfrefresh(u32 base)
39 {
40         struct emif_reg_struct *emif = (struct emif_reg_struct *)base;
41         u32 reg;
43         reg = readl(&emif->emif_pwr_mgmt_ctrl);
44         reg &= ~EMIF_REG_LP_MODE_MASK;
45         reg |= LP_MODE_SELF_REFRESH << EMIF_REG_LP_MODE_SHIFT;
46         reg &= ~EMIF_REG_SR_TIM_MASK;
47         writel(reg, &emif->emif_pwr_mgmt_ctrl);
49         /* dummy read for the new SR_TIM to be loaded */
50         readl(&emif->emif_pwr_mgmt_ctrl);
51 }
53 void force_emif_self_refresh()
54 {
55         set_lpmode_selfrefresh(EMIF1_BASE);
56         set_lpmode_selfrefresh(EMIF2_BASE);
57 }
59 inline u32 emif_num(u32 base)
60 {
61         if (base == EMIF1_BASE)
62                 return 1;
63         else if (base == EMIF2_BASE)
64                 return 2;
65         else
66                 return 0;
67 }
69 /*
70  * Get SDRAM type connected to EMIF.
71  * Assuming similar SDRAM parts are connected to both EMIF's
72  * which is typically the case. So it is sufficient to get
73  * SDRAM type from EMIF1.
74  */
75 u32 emif_sdram_type()
76 {
77         struct emif_reg_struct *emif = (struct emif_reg_struct *)EMIF1_BASE;
79         return (readl(&emif->emif_sdram_config) &
80                 EMIF_REG_SDRAM_TYPE_MASK) >> EMIF_REG_SDRAM_TYPE_SHIFT;
81 }
83 static inline u32 get_mr(u32 base, u32 cs, u32 mr_addr)
84 {
85         u32 mr;
86         struct emif_reg_struct *emif = (struct emif_reg_struct *)base;
88         mr_addr |= cs << EMIF_REG_CS_SHIFT;
89         writel(mr_addr, &emif->emif_lpddr2_mode_reg_cfg);
90         if (omap_revision() == OMAP4430_ES2_0)
91                 mr = readl(&emif->emif_lpddr2_mode_reg_data_es2);
92         else
93                 mr = readl(&emif->emif_lpddr2_mode_reg_data);
94         debug("get_mr: EMIF%d cs %d mr %08x val 0x%x\n", emif_num(base),
95               cs, mr_addr, mr);
96         if (((mr & 0x0000ff00) >>  8) == (mr & 0xff) &&
97             ((mr & 0x00ff0000) >> 16) == (mr & 0xff) &&
98             ((mr & 0xff000000) >> 24) == (mr & 0xff))
99                 return mr & 0xff;
100         else
101                 return mr;
104 static inline void set_mr(u32 base, u32 cs, u32 mr_addr, u32 mr_val)
106         struct emif_reg_struct *emif = (struct emif_reg_struct *)base;
108         mr_addr |= cs << EMIF_REG_CS_SHIFT;
109         writel(mr_addr, &emif->emif_lpddr2_mode_reg_cfg);
110         writel(mr_val, &emif->emif_lpddr2_mode_reg_data);
113 void emif_reset_phy(u32 base)
115         struct emif_reg_struct *emif = (struct emif_reg_struct *)base;
116         u32 iodft;
118         iodft = readl(&emif->emif_iodft_tlgc);
119         iodft |= EMIF_REG_RESET_PHY_MASK;
120         writel(iodft, &emif->emif_iodft_tlgc);
123 static void do_lpddr2_init(u32 base, u32 cs)
125         u32 mr_addr;
126         const struct lpddr2_mr_regs *mr_regs;
128         get_lpddr2_mr_regs(&mr_regs);
129         /* Wait till device auto initialization is complete */
130         while (get_mr(base, cs, LPDDR2_MR0) & LPDDR2_MR0_DAI_MASK)
131                 ;
132         set_mr(base, cs, LPDDR2_MR10, mr_regs->mr10);
133         /*
134          * tZQINIT = 1 us
135          * Enough loops assuming a maximum of 2GHz
136          */
138         sdelay(2000);
140         set_mr(base, cs, LPDDR2_MR1, mr_regs->mr1);
141         set_mr(base, cs, LPDDR2_MR16, mr_regs->mr16);
143         /*
144          * Enable refresh along with writing MR2
145          * Encoding of RL in MR2 is (RL - 2)
146          */
147         mr_addr = LPDDR2_MR2 | EMIF_REG_REFRESH_EN_MASK;
148         set_mr(base, cs, mr_addr, mr_regs->mr2);
150         if (mr_regs->mr3 > 0)
151                 set_mr(base, cs, LPDDR2_MR3, mr_regs->mr3);
154 static void lpddr2_init(u32 base, const struct emif_regs *regs)
156         struct emif_reg_struct *emif = (struct emif_reg_struct *)base;
158         /* Not NVM */
159         clrbits_le32(&emif->emif_lpddr2_nvm_config, EMIF_REG_CS1NVMEN_MASK);
161         /*
162          * Keep REG_INITREF_DIS = 1 to prevent re-initialization of SDRAM
163          * when EMIF_SDRAM_CONFIG register is written
164          */
165         setbits_le32(&emif->emif_sdram_ref_ctrl, EMIF_REG_INITREF_DIS_MASK);
167         /*
168          * Set the SDRAM_CONFIG and PHY_CTRL for the
169          * un-locked frequency & default RL
170          */
171         writel(regs->sdram_config_init, &emif->emif_sdram_config);
172         writel(regs->emif_ddr_phy_ctlr_1, &emif->emif_ddr_phy_ctrl_1);
174         do_ext_phy_settings(base, regs);
176         do_lpddr2_init(base, CS0);
177         if (regs->sdram_config & EMIF_REG_EBANK_MASK)
178                 do_lpddr2_init(base, CS1);
180         writel(regs->sdram_config, &emif->emif_sdram_config);
181         writel(regs->emif_ddr_phy_ctlr_1, &emif->emif_ddr_phy_ctrl_1);
183         /* Enable refresh now */
184         clrbits_le32(&emif->emif_sdram_ref_ctrl, EMIF_REG_INITREF_DIS_MASK);
186         }
188 __weak void do_ext_phy_settings(u32 base, const struct emif_regs *regs)
192 void emif_update_timings(u32 base, const struct emif_regs *regs)
194         struct emif_reg_struct *emif = (struct emif_reg_struct *)base;
196         writel(regs->ref_ctrl, &emif->emif_sdram_ref_ctrl_shdw);
197         writel(regs->sdram_tim1, &emif->emif_sdram_tim_1_shdw);
198         writel(regs->sdram_tim2, &emif->emif_sdram_tim_2_shdw);
199         writel(regs->sdram_tim3, &emif->emif_sdram_tim_3_shdw);
200         if (omap_revision() == OMAP4430_ES1_0) {
201                 /* ES1 bug EMIF should be in force idle during freq_update */
202                 writel(0, &emif->emif_pwr_mgmt_ctrl);
203         } else {
204                 writel(EMIF_PWR_MGMT_CTRL, &emif->emif_pwr_mgmt_ctrl);
205                 writel(EMIF_PWR_MGMT_CTRL_SHDW, &emif->emif_pwr_mgmt_ctrl_shdw);
206         }
207         writel(regs->read_idle_ctrl, &emif->emif_read_idlectrl_shdw);
208         writel(regs->zq_config, &emif->emif_zq_config);
209         writel(regs->temp_alert_config, &emif->emif_temp_alert_config);
210         writel(regs->emif_ddr_phy_ctlr_1, &emif->emif_ddr_phy_ctrl_1_shdw);
212         if (omap_revision() >= OMAP5430_ES1_0) {
213                 writel(EMIF_L3_CONFIG_VAL_SYS_10_MPU_5_LL_0,
214                         &emif->emif_l3_config);
215         } else if (omap_revision() >= OMAP4460_ES1_0) {
216                 writel(EMIF_L3_CONFIG_VAL_SYS_10_MPU_3_LL_0,
217                         &emif->emif_l3_config);
218         } else {
219                 writel(EMIF_L3_CONFIG_VAL_SYS_10_LL_0,
220                         &emif->emif_l3_config);
221         }
224 static void ddr3_leveling(u32 base, const struct emif_regs *regs)
226         struct emif_reg_struct *emif = (struct emif_reg_struct *)base;
228         /* keep sdram in self-refresh */
229         writel(((LP_MODE_SELF_REFRESH << EMIF_REG_LP_MODE_SHIFT)
230                 & EMIF_REG_LP_MODE_MASK), &emif->emif_pwr_mgmt_ctrl);
231         __udelay(130);
233         /*
234          * Set invert_clkout (if activated)--DDR_PHYCTRL_1
235          * Invert clock adds an additional half cycle delay on the command
236          * interface.  The additional half cycle, is usually meant to enable
237          * leveling in the situation that DQS is later than CK on the board.It
238          * also helps provide some additional margin for leveling.
239          */
240         writel(regs->emif_ddr_phy_ctlr_1, &emif->emif_ddr_phy_ctrl_1);
241         writel(regs->emif_ddr_phy_ctlr_1, &emif->emif_ddr_phy_ctrl_1_shdw);
242         __udelay(130);
244         writel(((LP_MODE_DISABLE << EMIF_REG_LP_MODE_SHIFT)
245                 & EMIF_REG_LP_MODE_MASK), &emif->emif_pwr_mgmt_ctrl);
247         /* Launch Full leveling */
248         writel(DDR3_FULL_LVL, &emif->emif_rd_wr_lvl_ctl);
250         /* Wait till full leveling is complete */
251         readl(&emif->emif_rd_wr_lvl_ctl);
252         __udelay(130);
254         /* Read data eye leveling no of samples */
255         config_data_eye_leveling_samples(base);
257         /* Launch 8 incremental WR_LVL- to compensate for PHY limitation */
258         writel(0x2 << EMIF_REG_WRLVLINC_INT_SHIFT, &emif->emif_rd_wr_lvl_ctl);
259         __udelay(130);
261         /* Launch Incremental leveling */
262         writel(DDR3_INC_LVL, &emif->emif_rd_wr_lvl_ctl);
263         __udelay(130);
266 static void ddr3_init(u32 base, const struct emif_regs *regs)
268         struct emif_reg_struct *emif = (struct emif_reg_struct *)base;
270         /*
271          * Set SDRAM_CONFIG and PHY control registers to locked frequency
272          * and RL =7. As the default values of the Mode Registers are not
273          * defined, contents of mode Registers must be fully initialized.
274          * H/W takes care of this initialization
275          */
276         writel(regs->sdram_config_init, &emif->emif_sdram_config);
278         writel(regs->emif_ddr_phy_ctlr_1_init, &emif->emif_ddr_phy_ctrl_1);
280         /* Update timing registers */
281         writel(regs->sdram_tim1, &emif->emif_sdram_tim_1);
282         writel(regs->sdram_tim2, &emif->emif_sdram_tim_2);
283         writel(regs->sdram_tim3, &emif->emif_sdram_tim_3);
285         writel(regs->ref_ctrl, &emif->emif_sdram_ref_ctrl);
286         writel(regs->read_idle_ctrl, &emif->emif_read_idlectrl);
288         do_ext_phy_settings(base, regs);
290         /* enable leveling */
291         writel(regs->emif_rd_wr_lvl_rmp_ctl, &emif->emif_rd_wr_lvl_rmp_ctl);
293         ddr3_leveling(base, regs);
296 #ifndef CONFIG_SYS_EMIF_PRECALCULATED_TIMING_REGS
297 #define print_timing_reg(reg) debug(#reg" - 0x%08x\n", (reg))
299 /*
300  * Organization and refresh requirements for LPDDR2 devices of different
301  * types and densities. Derived from JESD209-2 section 2.4
302  */
303 const struct lpddr2_addressing addressing_table[] = {
304         /* Banks tREFIx10     rowx32,rowx16      colx32,colx16  density */
305         {BANKS4, T_REFI_15_6, {ROW_12, ROW_12}, {COL_7, COL_8} },/*64M */
306         {BANKS4, T_REFI_15_6, {ROW_12, ROW_12}, {COL_8, COL_9} },/*128M */
307         {BANKS4, T_REFI_7_8, {ROW_13, ROW_13}, {COL_8, COL_9} },/*256M */
308         {BANKS4, T_REFI_7_8, {ROW_13, ROW_13}, {COL_9, COL_10} },/*512M */
309         {BANKS8, T_REFI_7_8, {ROW_13, ROW_13}, {COL_9, COL_10} },/*1GS4 */
310         {BANKS8, T_REFI_3_9, {ROW_14, ROW_14}, {COL_9, COL_10} },/*2GS4 */
311         {BANKS8, T_REFI_3_9, {ROW_14, ROW_14}, {COL_10, COL_11} },/*4G */
312         {BANKS8, T_REFI_3_9, {ROW_15, ROW_15}, {COL_10, COL_11} },/*8G */
313         {BANKS4, T_REFI_7_8, {ROW_14, ROW_14}, {COL_9, COL_10} },/*1GS2 */
314         {BANKS4, T_REFI_3_9, {ROW_15, ROW_15}, {COL_9, COL_10} },/*2GS2 */
315 };
317 static const u32 lpddr2_density_2_size_in_mbytes[] = {
318         8,                      /* 64Mb */
319         16,                     /* 128Mb */
320         32,                     /* 256Mb */
321         64,                     /* 512Mb */
322         128,                    /* 1Gb   */
323         256,                    /* 2Gb   */
324         512,                    /* 4Gb   */
325         1024,                   /* 8Gb   */
326         2048,                   /* 16Gb  */
327         4096                    /* 32Gb  */
328 };
330 /*
331  * Calculate the period of DDR clock from frequency value and set the
332  * denominator and numerator in global variables for easy access later
333  */
334 static void set_ddr_clk_period(u32 freq)
336         /*
337          * period = 1/freq
338          * period_in_ns = 10^9/freq
339          */
340         *T_num = 1000000000;
341         *T_den = freq;
342         cancel_out(T_num, T_den, 200);
346 /*
347  * Convert time in nano seconds to number of cycles of DDR clock
348  */
349 static inline u32 ns_2_cycles(u32 ns)
351         return ((ns * (*T_den)) + (*T_num) - 1) / (*T_num);
354 /*
355  * ns_2_cycles with the difference that the time passed is 2 times the actual
356  * value(to avoid fractions). The cycles returned is for the original value of
357  * the timing parameter
358  */
359 static inline u32 ns_x2_2_cycles(u32 ns)
361         return ((ns * (*T_den)) + (*T_num) * 2 - 1) / ((*T_num) * 2);
364 /*
365  * Find addressing table index based on the device's type(S2 or S4) and
366  * density
367  */
368 s8 addressing_table_index(u8 type, u8 density, u8 width)
370         u8 index;
371         if ((density > LPDDR2_DENSITY_8Gb) || (width == LPDDR2_IO_WIDTH_8))
372                 return -1;
374         /*
375          * Look at the way ADDR_TABLE_INDEX* values have been defined
376          * in emif.h compared to LPDDR2_DENSITY_* values
377          * The table is layed out in the increasing order of density
378          * (ignoring type). The exceptions 1GS2 and 2GS2 have been placed
379          * at the end
380          */
381         if ((type == LPDDR2_TYPE_S2) && (density == LPDDR2_DENSITY_1Gb))
382                 index = ADDR_TABLE_INDEX1GS2;
383         else if ((type == LPDDR2_TYPE_S2) && (density == LPDDR2_DENSITY_2Gb))
384                 index = ADDR_TABLE_INDEX2GS2;
385         else
386                 index = density;
388         debug("emif: addressing table index %d\n", index);
390         return index;
393 /*
394  * Find the the right timing table from the array of timing
395  * tables of the device using DDR clock frequency
396  */
397 static const struct lpddr2_ac_timings *get_timings_table(const struct
398                         lpddr2_ac_timings const *const *device_timings,
399                         u32 freq)
401         u32 i, temp, freq_nearest;
402         const struct lpddr2_ac_timings *timings = 0;
404         emif_assert(freq <= MAX_LPDDR2_FREQ);
405         emif_assert(device_timings);
407         /*
408          * Start with the maximum allowed frequency - that is always safe
409          */
410         freq_nearest = MAX_LPDDR2_FREQ;
411         /*
412          * Find the timings table that has the max frequency value:
413          *   i.  Above or equal to the DDR frequency - safe
414          *   ii. The lowest that satisfies condition (i) - optimal
415          */
416         for (i = 0; (i < MAX_NUM_SPEEDBINS) && device_timings[i]; i++) {
417                 temp = device_timings[i]->max_freq;
418                 if ((temp >= freq) && (temp <= freq_nearest)) {
419                         freq_nearest = temp;
420                         timings = device_timings[i];
421                 }
422         }
423         debug("emif: timings table: %d\n", freq_nearest);
424         return timings;
427 /*
428  * Finds the value of emif_sdram_config_reg
429  * All parameters are programmed based on the device on CS0.
430  * If there is a device on CS1, it will be same as that on CS0 or
431  * it will be NVM. We don't support NVM yet.
432  * If cs1_device pointer is NULL it is assumed that there is no device
433  * on CS1
434  */
435 static u32 get_sdram_config_reg(const struct lpddr2_device_details *cs0_device,
436                                 const struct lpddr2_device_details *cs1_device,
437                                 const struct lpddr2_addressing *addressing,
438                                 u8 RL)
440         u32 config_reg = 0;
442         config_reg |=  (cs0_device->type + 4) << EMIF_REG_SDRAM_TYPE_SHIFT;
443         config_reg |=  EMIF_INTERLEAVING_POLICY_MAX_INTERLEAVING <<
444                         EMIF_REG_IBANK_POS_SHIFT;
446         config_reg |= cs0_device->io_width << EMIF_REG_NARROW_MODE_SHIFT;
448         config_reg |= RL << EMIF_REG_CL_SHIFT;
450         config_reg |= addressing->row_sz[cs0_device->io_width] <<
451                         EMIF_REG_ROWSIZE_SHIFT;
453         config_reg |= addressing->num_banks << EMIF_REG_IBANK_SHIFT;
455         config_reg |= (cs1_device ? EBANK_CS1_EN : EBANK_CS1_DIS) <<
456                         EMIF_REG_EBANK_SHIFT;
458         config_reg |= addressing->col_sz[cs0_device->io_width] <<
459                         EMIF_REG_PAGESIZE_SHIFT;
461         return config_reg;
464 static u32 get_sdram_ref_ctrl(u32 freq,
465                               const struct lpddr2_addressing *addressing)
467         u32 ref_ctrl = 0, val = 0, freq_khz;
468         freq_khz = freq / 1000;
469         /*
470          * refresh rate to be set is 'tREFI * freq in MHz
471          * division by 10000 to account for khz and x10 in t_REFI_us_x10
472          */
473         val = addressing->t_REFI_us_x10 * freq_khz / 10000;
474         ref_ctrl |= val << EMIF_REG_REFRESH_RATE_SHIFT;
476         return ref_ctrl;
479 static u32 get_sdram_tim_1_reg(const struct lpddr2_ac_timings *timings,
480                                const struct lpddr2_min_tck *min_tck,
481                                const struct lpddr2_addressing *addressing)
483         u32 tim1 = 0, val = 0;
484         val = max(min_tck->tWTR, ns_x2_2_cycles(timings->tWTRx2)) - 1;
485         tim1 |= val << EMIF_REG_T_WTR_SHIFT;
487         if (addressing->num_banks == BANKS8)
488                 val = (timings->tFAW * (*T_den) + 4 * (*T_num) - 1) /
489                                                         (4 * (*T_num)) - 1;
490         else
491                 val = max(min_tck->tRRD, ns_2_cycles(timings->tRRD)) - 1;
493         tim1 |= val << EMIF_REG_T_RRD_SHIFT;
495         val = ns_2_cycles(timings->tRASmin + timings->tRPab) - 1;
496         tim1 |= val << EMIF_REG_T_RC_SHIFT;
498         val = max(min_tck->tRAS_MIN, ns_2_cycles(timings->tRASmin)) - 1;
499         tim1 |= val << EMIF_REG_T_RAS_SHIFT;
501         val = max(min_tck->tWR, ns_2_cycles(timings->tWR)) - 1;
502         tim1 |= val << EMIF_REG_T_WR_SHIFT;
504         val = max(min_tck->tRCD, ns_2_cycles(timings->tRCD)) - 1;
505         tim1 |= val << EMIF_REG_T_RCD_SHIFT;
507         val = max(min_tck->tRP_AB, ns_2_cycles(timings->tRPab)) - 1;
508         tim1 |= val << EMIF_REG_T_RP_SHIFT;
510         return tim1;
513 static u32 get_sdram_tim_2_reg(const struct lpddr2_ac_timings *timings,
514                                const struct lpddr2_min_tck *min_tck)
516         u32 tim2 = 0, val = 0;
517         val = max(min_tck->tCKE, timings->tCKE) - 1;
518         tim2 |= val << EMIF_REG_T_CKE_SHIFT;
520         val = max(min_tck->tRTP, ns_x2_2_cycles(timings->tRTPx2)) - 1;
521         tim2 |= val << EMIF_REG_T_RTP_SHIFT;
523         /*
524          * tXSRD = tRFCab + 10 ns. XSRD and XSNR should have the
525          * same value
526          */
527         val = ns_2_cycles(timings->tXSR) - 1;
528         tim2 |= val << EMIF_REG_T_XSRD_SHIFT;
529         tim2 |= val << EMIF_REG_T_XSNR_SHIFT;
531         val = max(min_tck->tXP, ns_x2_2_cycles(timings->tXPx2)) - 1;
532         tim2 |= val << EMIF_REG_T_XP_SHIFT;
534         return tim2;
537 static u32 get_sdram_tim_3_reg(const struct lpddr2_ac_timings *timings,
538                                const struct lpddr2_min_tck *min_tck,
539                                const struct lpddr2_addressing *addressing)
541         u32 tim3 = 0, val = 0;
542         val = min(timings->tRASmax * 10 / addressing->t_REFI_us_x10 - 1, 0xF);
543         tim3 |= val << EMIF_REG_T_RAS_MAX_SHIFT;
545         val = ns_2_cycles(timings->tRFCab) - 1;
546         tim3 |= val << EMIF_REG_T_RFC_SHIFT;
548         val = ns_x2_2_cycles(timings->tDQSCKMAXx2) - 1;
549         tim3 |= val << EMIF_REG_T_TDQSCKMAX_SHIFT;
551         val = ns_2_cycles(timings->tZQCS) - 1;
552         tim3 |= val << EMIF_REG_ZQ_ZQCS_SHIFT;
554         val = max(min_tck->tCKESR, ns_2_cycles(timings->tCKESR)) - 1;
555         tim3 |= val << EMIF_REG_T_CKESR_SHIFT;
557         return tim3;
560 static u32 get_zq_config_reg(const struct lpddr2_device_details *cs1_device,
561                              const struct lpddr2_addressing *addressing,
562                              u8 volt_ramp)
564         u32 zq = 0, val = 0;
565         if (volt_ramp)
566                 val =
567                     EMIF_ZQCS_INTERVAL_DVFS_IN_US * 10 /
568                     addressing->t_REFI_us_x10;
569         else
570                 val =
571                     EMIF_ZQCS_INTERVAL_NORMAL_IN_US * 10 /
572                     addressing->t_REFI_us_x10;
573         zq |= val << EMIF_REG_ZQ_REFINTERVAL_SHIFT;
575         zq |= (REG_ZQ_ZQCL_MULT - 1) << EMIF_REG_ZQ_ZQCL_MULT_SHIFT;
577         zq |= (REG_ZQ_ZQINIT_MULT - 1) << EMIF_REG_ZQ_ZQINIT_MULT_SHIFT;
579         zq |= REG_ZQ_SFEXITEN_ENABLE << EMIF_REG_ZQ_SFEXITEN_SHIFT;
581         /*
582          * Assuming that two chipselects have a single calibration resistor
583          * If there are indeed two calibration resistors, then this flag should
584          * be enabled to take advantage of dual calibration feature.
585          * This data should ideally come from board files. But considering
586          * that none of the boards today have calibration resistors per CS,
587          * it would be an unnecessary overhead.
588          */
589         zq |= REG_ZQ_DUALCALEN_DISABLE << EMIF_REG_ZQ_DUALCALEN_SHIFT;
591         zq |= REG_ZQ_CS0EN_ENABLE << EMIF_REG_ZQ_CS0EN_SHIFT;
593         zq |= (cs1_device ? 1 : 0) << EMIF_REG_ZQ_CS1EN_SHIFT;
595         return zq;
598 static u32 get_temp_alert_config(const struct lpddr2_device_details *cs1_device,
599                                  const struct lpddr2_addressing *addressing,
600                                  u8 is_derated)
602         u32 alert = 0, interval;
603         interval =
604             TEMP_ALERT_POLL_INTERVAL_MS * 10000 / addressing->t_REFI_us_x10;
605         if (is_derated)
606                 interval *= 4;
607         alert |= interval << EMIF_REG_TA_REFINTERVAL_SHIFT;
609         alert |= TEMP_ALERT_CONFIG_DEVCT_1 << EMIF_REG_TA_DEVCNT_SHIFT;
611         alert |= TEMP_ALERT_CONFIG_DEVWDT_32 << EMIF_REG_TA_DEVWDT_SHIFT;
613         alert |= 1 << EMIF_REG_TA_SFEXITEN_SHIFT;
615         alert |= 1 << EMIF_REG_TA_CS0EN_SHIFT;
617         alert |= (cs1_device ? 1 : 0) << EMIF_REG_TA_CS1EN_SHIFT;
619         return alert;
622 static u32 get_read_idle_ctrl_reg(u8 volt_ramp)
624         u32 idle = 0, val = 0;
625         if (volt_ramp)
626                 val = ns_2_cycles(READ_IDLE_INTERVAL_DVFS) / 64 - 1;
627         else
628                 /*Maximum value in normal conditions - suggested by hw team */
629                 val = 0x1FF;
630         idle |= val << EMIF_REG_READ_IDLE_INTERVAL_SHIFT;
632         idle |= EMIF_REG_READ_IDLE_LEN_VAL << EMIF_REG_READ_IDLE_LEN_SHIFT;
634         return idle;
637 static u32 get_ddr_phy_ctrl_1(u32 freq, u8 RL)
639         u32 phy = 0, val = 0;
641         phy |= (RL + 2) << EMIF_REG_READ_LATENCY_SHIFT;
643         if (freq <= 100000000)
644                 val = EMIF_DLL_SLAVE_DLY_CTRL_100_MHZ_AND_LESS;
645         else if (freq <= 200000000)
646                 val = EMIF_DLL_SLAVE_DLY_CTRL_200_MHZ;
647         else
648                 val = EMIF_DLL_SLAVE_DLY_CTRL_400_MHZ;
649         phy |= val << EMIF_REG_DLL_SLAVE_DLY_CTRL_SHIFT;
651         /* Other fields are constant magic values. Hardcode them together */
652         phy |= EMIF_DDR_PHY_CTRL_1_BASE_VAL <<
653                 EMIF_EMIF_DDR_PHY_CTRL_1_BASE_VAL_SHIFT;
655         return phy;
658 static u32 get_emif_mem_size(struct emif_device_details *devices)
660         u32 size_mbytes = 0, temp;
662         if (!devices)
663                 return 0;
665         if (devices->cs0_device_details) {
666                 temp = devices->cs0_device_details->density;
667                 size_mbytes += lpddr2_density_2_size_in_mbytes[temp];
668         }
670         if (devices->cs1_device_details) {
671                 temp = devices->cs1_device_details->density;
672                 size_mbytes += lpddr2_density_2_size_in_mbytes[temp];
673         }
674         /* convert to bytes */
675         return size_mbytes << 20;
678 /* Gets the encoding corresponding to a given DMM section size */
679 u32 get_dmm_section_size_map(u32 section_size)
681         /*
682          * Section size mapping:
683          * 0x0: 16-MiB section
684          * 0x1: 32-MiB section
685          * 0x2: 64-MiB section
686          * 0x3: 128-MiB section
687          * 0x4: 256-MiB section
688          * 0x5: 512-MiB section
689          * 0x6: 1-GiB section
690          * 0x7: 2-GiB section
691          */
692         section_size >>= 24; /* divide by 16 MB */
693         return log_2_n_round_down(section_size);
696 static void emif_calculate_regs(
697                 const struct emif_device_details *emif_dev_details,
698                 u32 freq, struct emif_regs *regs)
700         u32 temp, sys_freq;
701         const struct lpddr2_addressing *addressing;
702         const struct lpddr2_ac_timings *timings;
703         const struct lpddr2_min_tck *min_tck;
704         const struct lpddr2_device_details *cs0_dev_details =
705                                         emif_dev_details->cs0_device_details;
706         const struct lpddr2_device_details *cs1_dev_details =
707                                         emif_dev_details->cs1_device_details;
708         const struct lpddr2_device_timings *cs0_dev_timings =
709                                         emif_dev_details->cs0_device_timings;
711         emif_assert(emif_dev_details);
712         emif_assert(regs);
713         /*
714          * You can not have a device on CS1 without one on CS0
715          * So configuring EMIF without a device on CS0 doesn't
716          * make sense
717          */
718         emif_assert(cs0_dev_details);
719         emif_assert(cs0_dev_details->type != LPDDR2_TYPE_NVM);
720         /*
721          * If there is a device on CS1 it should be same type as CS0
722          * (or NVM. But NVM is not supported in this driver yet)
723          */
724         emif_assert((cs1_dev_details == NULL) ||
725                     (cs1_dev_details->type == LPDDR2_TYPE_NVM) ||
726                     (cs0_dev_details->type == cs1_dev_details->type));
727         emif_assert(freq <= MAX_LPDDR2_FREQ);
729         set_ddr_clk_period(freq);
731         /*
732          * The device on CS0 is used for all timing calculations
733          * There is only one set of registers for timings per EMIF. So, if the
734          * second CS(CS1) has a device, it should have the same timings as the
735          * device on CS0
736          */
737         timings = get_timings_table(cs0_dev_timings->ac_timings, freq);
738         emif_assert(timings);
739         min_tck = cs0_dev_timings->min_tck;
741         temp = addressing_table_index(cs0_dev_details->type,
742                                       cs0_dev_details->density,
743                                       cs0_dev_details->io_width);
745         emif_assert((temp >= 0));
746         addressing = &(addressing_table[temp]);
747         emif_assert(addressing);
749         sys_freq = get_sys_clk_freq();
751         regs->sdram_config_init = get_sdram_config_reg(cs0_dev_details,
752                                                         cs1_dev_details,
753                                                         addressing, RL_BOOT);
755         regs->sdram_config = get_sdram_config_reg(cs0_dev_details,
756                                                 cs1_dev_details,
757                                                 addressing, RL_FINAL);
759         regs->ref_ctrl = get_sdram_ref_ctrl(freq, addressing);
761         regs->sdram_tim1 = get_sdram_tim_1_reg(timings, min_tck, addressing);
763         regs->sdram_tim2 = get_sdram_tim_2_reg(timings, min_tck);
765         regs->sdram_tim3 = get_sdram_tim_3_reg(timings, min_tck, addressing);
767         regs->read_idle_ctrl = get_read_idle_ctrl_reg(LPDDR2_VOLTAGE_STABLE);
769         regs->temp_alert_config =
770             get_temp_alert_config(cs1_dev_details, addressing, 0);
772         regs->zq_config = get_zq_config_reg(cs1_dev_details, addressing,
773                                             LPDDR2_VOLTAGE_STABLE);
775         regs->emif_ddr_phy_ctlr_1_init =
776                         get_ddr_phy_ctrl_1(sys_freq / 2, RL_BOOT);
778         regs->emif_ddr_phy_ctlr_1 =
779                         get_ddr_phy_ctrl_1(freq, RL_FINAL);
781         regs->freq = freq;
783         print_timing_reg(regs->sdram_config_init);
784         print_timing_reg(regs->sdram_config);
785         print_timing_reg(regs->ref_ctrl);
786         print_timing_reg(regs->sdram_tim1);
787         print_timing_reg(regs->sdram_tim2);
788         print_timing_reg(regs->sdram_tim3);
789         print_timing_reg(regs->read_idle_ctrl);
790         print_timing_reg(regs->temp_alert_config);
791         print_timing_reg(regs->zq_config);
792         print_timing_reg(regs->emif_ddr_phy_ctlr_1);
793         print_timing_reg(regs->emif_ddr_phy_ctlr_1_init);
795 #endif /* CONFIG_SYS_EMIF_PRECALCULATED_TIMING_REGS */
797 #ifdef CONFIG_SYS_AUTOMATIC_SDRAM_DETECTION
798 const char *get_lpddr2_type(u8 type_id)
800         switch (type_id) {
801         case LPDDR2_TYPE_S4:
802                 return "LPDDR2-S4";
803         case LPDDR2_TYPE_S2:
804                 return "LPDDR2-S2";
805         default:
806                 return NULL;
807         }
810 const char *get_lpddr2_io_width(u8 width_id)
812         switch (width_id) {
813         case LPDDR2_IO_WIDTH_8:
814                 return "x8";
815         case LPDDR2_IO_WIDTH_16:
816                 return "x16";
817         case LPDDR2_IO_WIDTH_32:
818                 return "x32";
819         default:
820                 return NULL;
821         }
824 const char *get_lpddr2_manufacturer(u32 manufacturer)
826         switch (manufacturer) {
827         case LPDDR2_MANUFACTURER_SAMSUNG:
828                 return "Samsung";
829         case LPDDR2_MANUFACTURER_QIMONDA:
830                 return "Qimonda";
831         case LPDDR2_MANUFACTURER_ELPIDA:
832                 return "Elpida";
833         case LPDDR2_MANUFACTURER_ETRON:
834                 return "Etron";
835         case LPDDR2_MANUFACTURER_NANYA:
836                 return "Nanya";
837         case LPDDR2_MANUFACTURER_HYNIX:
838                 return "Hynix";
839         case LPDDR2_MANUFACTURER_MOSEL:
840                 return "Mosel";
841         case LPDDR2_MANUFACTURER_WINBOND:
842                 return "Winbond";
843         case LPDDR2_MANUFACTURER_ESMT:
844                 return "ESMT";
845         case LPDDR2_MANUFACTURER_SPANSION:
846                 return "Spansion";
847         case LPDDR2_MANUFACTURER_SST:
848                 return "SST";
849         case LPDDR2_MANUFACTURER_ZMOS:
850                 return "ZMOS";
851         case LPDDR2_MANUFACTURER_INTEL:
852                 return "Intel";
853         case LPDDR2_MANUFACTURER_NUMONYX:
854                 return "Numonyx";
855         case LPDDR2_MANUFACTURER_MICRON:
856                 return "Micron";
857         default:
858                 return NULL;
859         }
862 static void display_sdram_details(u32 emif_nr, u32 cs,
863                                   struct lpddr2_device_details *device)
865         const char *mfg_str;
866         const char *type_str;
867         char density_str[10];
868         u32 density;
870         debug("EMIF%d CS%d\t", emif_nr, cs);
872         if (!device) {
873                 debug("None\n");
874                 return;
875         }
877         mfg_str = get_lpddr2_manufacturer(device->manufacturer);
878         type_str = get_lpddr2_type(device->type);
880         density = lpddr2_density_2_size_in_mbytes[device->density];
881         if ((density / 1024 * 1024) == density) {
882                 density /= 1024;
883                 sprintf(density_str, "%d GB", density);
884         } else
885                 sprintf(density_str, "%d MB", density);
886         if (mfg_str && type_str)
887                 debug("%s\t\t%s\t%s\n", mfg_str, type_str, density_str);
890 static u8 is_lpddr2_sdram_present(u32 base, u32 cs,
891                                   struct lpddr2_device_details *lpddr2_device)
893         u32 mr = 0, temp;
895         mr = get_mr(base, cs, LPDDR2_MR0);
896         if (mr > 0xFF) {
897                 /* Mode register value bigger than 8 bit */
898                 return 0;
899         }
901         temp = (mr & LPDDR2_MR0_DI_MASK) >> LPDDR2_MR0_DI_SHIFT;
902         if (temp) {
903                 /* Not SDRAM */
904                 return 0;
905         }
906         temp = (mr & LPDDR2_MR0_DNVI_MASK) >> LPDDR2_MR0_DNVI_SHIFT;
908         if (temp) {
909                 /* DNV supported - But DNV is only supported for NVM */
910                 return 0;
911         }
913         mr = get_mr(base, cs, LPDDR2_MR4);
914         if (mr > 0xFF) {
915                 /* Mode register value bigger than 8 bit */
916                 return 0;
917         }
919         mr = get_mr(base, cs, LPDDR2_MR5);
920         if (mr > 0xFF) {
921                 /* Mode register value bigger than 8 bit */
922                 return 0;
923         }
925         if (!get_lpddr2_manufacturer(mr)) {
926                 /* Manufacturer not identified */
927                 return 0;
928         }
929         lpddr2_device->manufacturer = mr;
931         mr = get_mr(base, cs, LPDDR2_MR6);
932         if (mr >= 0xFF) {
933                 /* Mode register value bigger than 8 bit */
934                 return 0;
935         }
937         mr = get_mr(base, cs, LPDDR2_MR7);
938         if (mr >= 0xFF) {
939                 /* Mode register value bigger than 8 bit */
940                 return 0;
941         }
943         mr = get_mr(base, cs, LPDDR2_MR8);
944         if (mr >= 0xFF) {
945                 /* Mode register value bigger than 8 bit */
946                 return 0;
947         }
949         temp = (mr & MR8_TYPE_MASK) >> MR8_TYPE_SHIFT;
950         if (!get_lpddr2_type(temp)) {
951                 /* Not SDRAM */
952                 return 0;
953         }
954         lpddr2_device->type = temp;
956         temp = (mr & MR8_DENSITY_MASK) >> MR8_DENSITY_SHIFT;
957         if (temp > LPDDR2_DENSITY_32Gb) {
958                 /* Density not supported */
959                 return 0;
960         }
961         lpddr2_device->density = temp;
963         temp = (mr & MR8_IO_WIDTH_MASK) >> MR8_IO_WIDTH_SHIFT;
964         if (!get_lpddr2_io_width(temp)) {
965                 /* IO width unsupported value */
966                 return 0;
967         }
968         lpddr2_device->io_width = temp;
970         /*
971          * If all the above tests pass we should
972          * have a device on this chip-select
973          */
974         return 1;
977 struct lpddr2_device_details *emif_get_device_details(u32 emif_nr, u8 cs,
978                         struct lpddr2_device_details *lpddr2_dev_details)
980         u32 phy;
981         u32 base = (emif_nr == 1) ? EMIF1_BASE : EMIF2_BASE;
983         struct emif_reg_struct *emif = (struct emif_reg_struct *)base;
985         if (!lpddr2_dev_details)
986                 return NULL;
988         /* Do the minimum init for mode register accesses */
989         if (!(running_from_sdram() || warm_reset())) {
990                 phy = get_ddr_phy_ctrl_1(get_sys_clk_freq() / 2, RL_BOOT);
991                 writel(phy, &emif->emif_ddr_phy_ctrl_1);
992         }
994         if (!(is_lpddr2_sdram_present(base, cs, lpddr2_dev_details)))
995                 return NULL;
997         display_sdram_details(emif_num(base), cs, lpddr2_dev_details);
999         return lpddr2_dev_details;
1001 #endif /* CONFIG_SYS_AUTOMATIC_SDRAM_DETECTION */
1003 static void do_sdram_init(u32 base)
1005         const struct emif_regs *regs;
1006         u32 in_sdram, emif_nr;
1008         debug(">>do_sdram_init() %x\n", base);
1010         in_sdram = running_from_sdram();
1011         emif_nr = (base == EMIF1_BASE) ? 1 : 2;
1013 #ifdef CONFIG_SYS_EMIF_PRECALCULATED_TIMING_REGS
1014         emif_get_reg_dump(emif_nr, &regs);
1015         if (!regs) {
1016                 debug("EMIF: reg dump not provided\n");
1017                 return;
1018         }
1019 #else
1020         /*
1021          * The user has not provided the register values. We need to
1022          * calculate it based on the timings and the DDR frequency
1023          */
1024         struct emif_device_details dev_details;
1025         struct emif_regs calculated_regs;
1027         /*
1028          * Get device details:
1029          * - Discovered if CONFIG_SYS_AUTOMATIC_SDRAM_DETECTION is set
1030          * - Obtained from user otherwise
1031          */
1032         struct lpddr2_device_details cs0_dev_details, cs1_dev_details;
1033         emif_reset_phy(base);
1034         dev_details.cs0_device_details = emif_get_device_details(emif_nr, CS0,
1035                                                 &cs0_dev_details);
1036         dev_details.cs1_device_details = emif_get_device_details(emif_nr, CS1,
1037                                                 &cs1_dev_details);
1038         emif_reset_phy(base);
1040         /* Return if no devices on this EMIF */
1041         if (!dev_details.cs0_device_details &&
1042             !dev_details.cs1_device_details) {
1043                 emif_sizes[emif_nr - 1] = 0;
1044                 return;
1045         }
1047         if (!in_sdram)
1048                 emif_sizes[emif_nr - 1] = get_emif_mem_size(&dev_details);
1050         /*
1051          * Get device timings:
1052          * - Default timings specified by JESD209-2 if
1053          *   CONFIG_SYS_DEFAULT_LPDDR2_TIMINGS is set
1054          * - Obtained from user otherwise
1055          */
1056         emif_get_device_timings(emif_nr, &dev_details.cs0_device_timings,
1057                                 &dev_details.cs1_device_timings);
1059         /* Calculate the register values */
1060         emif_calculate_regs(&dev_details, omap_ddr_clk(), &calculated_regs);
1061         regs = &calculated_regs;
1062 #endif /* CONFIG_SYS_EMIF_PRECALCULATED_TIMING_REGS */
1064         /*
1065          * Initializing the LPDDR2 device can not happen from SDRAM.
1066          * Changing the timing registers in EMIF can happen(going from one
1067          * OPP to another)
1068          */
1069         if (!(in_sdram || warm_reset())) {
1070                 if (emif_sdram_type() == EMIF_SDRAM_TYPE_LPDDR2)
1071                         lpddr2_init(base, regs);
1072                 else
1073                         ddr3_init(base, regs);
1074         }
1076         /* Write to the shadow registers */
1077         emif_update_timings(base, regs);
1079         debug("<<do_sdram_init() %x\n", base);
1082 void emif_post_init_config(u32 base)
1084         struct emif_reg_struct *emif = (struct emif_reg_struct *)base;
1085         u32 omap_rev = omap_revision();
1087         /* reset phy on ES2.0 */
1088         if (omap_rev == OMAP4430_ES2_0)
1089                 emif_reset_phy(base);
1091         /* Put EMIF back in smart idle on ES1.0 */
1092         if (omap_rev == OMAP4430_ES1_0)
1093                 writel(0x80000000, &emif->emif_pwr_mgmt_ctrl);
1096 void dmm_init(u32 base)
1098         const struct dmm_lisa_map_regs *lisa_map_regs;
1099         u32 i, section, valid;
1101 #ifdef CONFIG_SYS_EMIF_PRECALCULATED_TIMING_REGS
1102         emif_get_dmm_regs(&lisa_map_regs);
1103 #else
1104         u32 emif1_size, emif2_size, mapped_size, section_map = 0;
1105         u32 section_cnt, sys_addr;
1106         struct dmm_lisa_map_regs lis_map_regs_calculated = {0};
1108         mapped_size = 0;
1109         section_cnt = 3;
1110         sys_addr = CONFIG_SYS_SDRAM_BASE;
1111         emif1_size = emif_sizes[0];
1112         emif2_size = emif_sizes[1];
1113         debug("emif1_size 0x%x emif2_size 0x%x\n", emif1_size, emif2_size);
1115         if (!emif1_size && !emif2_size)
1116                 return;
1118         /* symmetric interleaved section */
1119         if (emif1_size && emif2_size) {
1120                 mapped_size = min(emif1_size, emif2_size);
1121                 section_map = DMM_LISA_MAP_INTERLEAVED_BASE_VAL;
1122                 section_map |= 0 << EMIF_SDRC_ADDR_SHIFT;
1123                 /* only MSB */
1124                 section_map |= (sys_addr >> 24) <<
1125                                 EMIF_SYS_ADDR_SHIFT;
1126                 section_map |= get_dmm_section_size_map(mapped_size * 2)
1127                                 << EMIF_SYS_SIZE_SHIFT;
1128                 lis_map_regs_calculated.dmm_lisa_map_3 = section_map;
1129                 emif1_size -= mapped_size;
1130                 emif2_size -= mapped_size;
1131                 sys_addr += (mapped_size * 2);
1132                 section_cnt--;
1133         }
1135         /*
1136          * Single EMIF section(we can have a maximum of 1 single EMIF
1137          * section- either EMIF1 or EMIF2 or none, but not both)
1138          */
1139         if (emif1_size) {
1140                 section_map = DMM_LISA_MAP_EMIF1_ONLY_BASE_VAL;
1141                 section_map |= get_dmm_section_size_map(emif1_size)
1142                                 << EMIF_SYS_SIZE_SHIFT;
1143                 /* only MSB */
1144                 section_map |= (mapped_size >> 24) <<
1145                                 EMIF_SDRC_ADDR_SHIFT;
1146                 /* only MSB */
1147                 section_map |= (sys_addr >> 24) << EMIF_SYS_ADDR_SHIFT;
1148                 section_cnt--;
1149         }
1150         if (emif2_size) {
1151                 section_map = DMM_LISA_MAP_EMIF2_ONLY_BASE_VAL;
1152                 section_map |= get_dmm_section_size_map(emif2_size) <<
1153                                 EMIF_SYS_SIZE_SHIFT;
1154                 /* only MSB */
1155                 section_map |= mapped_size >> 24 << EMIF_SDRC_ADDR_SHIFT;
1156                 /* only MSB */
1157                 section_map |= sys_addr >> 24 << EMIF_SYS_ADDR_SHIFT;
1158                 section_cnt--;
1159         }
1161         if (section_cnt == 2) {
1162                 /* Only 1 section - either symmetric or single EMIF */
1163                 lis_map_regs_calculated.dmm_lisa_map_3 = section_map;
1164                 lis_map_regs_calculated.dmm_lisa_map_2 = 0;
1165                 lis_map_regs_calculated.dmm_lisa_map_1 = 0;
1166         } else {
1167                 /* 2 sections - 1 symmetric, 1 single EMIF */
1168                 lis_map_regs_calculated.dmm_lisa_map_2 = section_map;
1169                 lis_map_regs_calculated.dmm_lisa_map_1 = 0;
1170         }
1172         /* TRAP for invalid TILER mappings in section 0 */
1173         lis_map_regs_calculated.dmm_lisa_map_0 = DMM_LISA_MAP_0_INVAL_ADDR_TRAP;
1175         lisa_map_regs = &lis_map_regs_calculated;
1176 #endif
1177         struct dmm_lisa_map_regs *hw_lisa_map_regs =
1178             (struct dmm_lisa_map_regs *)base;
1180         writel(0, &hw_lisa_map_regs->dmm_lisa_map_3);
1181         writel(0, &hw_lisa_map_regs->dmm_lisa_map_2);
1182         writel(0, &hw_lisa_map_regs->dmm_lisa_map_1);
1183         writel(0, &hw_lisa_map_regs->dmm_lisa_map_0);
1185         writel(lisa_map_regs->dmm_lisa_map_3,
1186                 &hw_lisa_map_regs->dmm_lisa_map_3);
1187         writel(lisa_map_regs->dmm_lisa_map_2,
1188                 &hw_lisa_map_regs->dmm_lisa_map_2);
1189         writel(lisa_map_regs->dmm_lisa_map_1,
1190                 &hw_lisa_map_regs->dmm_lisa_map_1);
1191         writel(lisa_map_regs->dmm_lisa_map_0,
1192                 &hw_lisa_map_regs->dmm_lisa_map_0);
1194         if (omap_revision() >= OMAP4460_ES1_0) {
1195                 hw_lisa_map_regs =
1196                     (struct dmm_lisa_map_regs *)MA_BASE;
1198                 writel(lisa_map_regs->dmm_lisa_map_3,
1199                         &hw_lisa_map_regs->dmm_lisa_map_3);
1200                 writel(lisa_map_regs->dmm_lisa_map_2,
1201                         &hw_lisa_map_regs->dmm_lisa_map_2);
1202                 writel(lisa_map_regs->dmm_lisa_map_1,
1203                         &hw_lisa_map_regs->dmm_lisa_map_1);
1204                 writel(lisa_map_regs->dmm_lisa_map_0,
1205                         &hw_lisa_map_regs->dmm_lisa_map_0);
1206         }
1208         /*
1209          * EMIF should be configured only when
1210          * memory is mapped on it. Using emif1_enabled
1211          * and emif2_enabled variables for this.
1212          */
1213         emif1_enabled = 0;
1214         emif2_enabled = 0;
1215         for (i = 0; i < 4; i++) {
1216                 section = __raw_readl(DMM_BASE + i*4);
1217                 valid = (section & EMIF_SDRC_MAP_MASK) >>
1218                         (EMIF_SDRC_MAP_SHIFT);
1219                 if (valid == 3) {
1220                         emif1_enabled = 1;
1221                         emif2_enabled = 1;
1222                         break;
1223                 } else if (valid == 1) {
1224                         emif1_enabled = 1;
1225                 } else if (valid == 2) {
1226                         emif2_enabled = 1;
1227                 }
1228         }
1232 /*
1233  * SDRAM initialization:
1234  * SDRAM initialization has two parts:
1235  * 1. Configuring the SDRAM device
1236  * 2. Update the AC timings related parameters in the EMIF module
1237  * (1) should be done only once and should not be done while we are
1238  * running from SDRAM.
1239  * (2) can and should be done more than once if OPP changes.
1240  * Particularly, this may be needed when we boot without SPL and
1241  * and using Configuration Header(CH). ROM code supports only at 50% OPP
1242  * at boot (low power boot). So u-boot has to switch to OPP100 and update
1243  * the frequency. So,
1244  * Doing (1) and (2) makes sense - first time initialization
1245  * Doing (2) and not (1) makes sense - OPP change (when using CH)
1246  * Doing (1) and not (2) doen't make sense
1247  * See do_sdram_init() for the details
1248  */
1249 void sdram_init(void)
1251         u32 in_sdram, size_prog, size_detect;
1252         u32 sdram_type = emif_sdram_type();
1254         debug(">>sdram_init()\n");
1256         if (omap_hw_init_context() == OMAP_INIT_CONTEXT_UBOOT_AFTER_SPL)
1257                 return;
1259         in_sdram = running_from_sdram();
1260         debug("in_sdram = %d\n", in_sdram);
1262         if (!(in_sdram || warm_reset())) {
1263                 if (sdram_type == EMIF_SDRAM_TYPE_LPDDR2)
1264                         bypass_dpll((*prcm)->cm_clkmode_dpll_core);
1265                 else
1266                         writel(CM_DLL_CTRL_NO_OVERRIDE, (*prcm)->cm_dll_ctrl);
1267         }
1269         if (!in_sdram)
1270                 dmm_init(DMM_BASE);
1272         if (emif1_enabled)
1273                 do_sdram_init(EMIF1_BASE);
1275         if (emif2_enabled)
1276                 do_sdram_init(EMIF2_BASE);
1278         if (!(in_sdram || warm_reset())) {
1279                 if (emif1_enabled)
1280                         emif_post_init_config(EMIF1_BASE);
1281                 if (emif2_enabled)
1282                         emif_post_init_config(EMIF2_BASE);
1283         }
1285         /* for the shadow registers to take effect */
1286         if (sdram_type == EMIF_SDRAM_TYPE_LPDDR2)
1287                 freq_update_core();
1289         /* Do some testing after the init */
1290         if (!in_sdram) {
1291                 size_prog = omap_sdram_size();
1292                 size_prog = log_2_n_round_down(size_prog);
1293                 size_prog = (1 << size_prog);
1295                 size_detect = get_ram_size((long *)CONFIG_SYS_SDRAM_BASE,
1296                                                 size_prog);
1297                 /* Compare with the size programmed */
1298                 if (size_detect != size_prog) {
1299                         printf("SDRAM: identified size not same as expected"
1300                                 " size identified: %x expected: %x\n",
1301                                 size_detect,
1302                                 size_prog);
1303                 } else
1304                         debug("get_ram_size() successful");
1305         }
1307         debug("<<sdram_init()\n");