5602b0e1998923b14e95f5baadf275e2c8c191dc
[glsdk/glsdk-u-boot.git] / arch / arm / cpu / armv7 / omap-common / hwinit-common.c
1 /*
2  *
3  * Common functions for OMAP4/5 based boards
4  *
5  * (C) Copyright 2010
6  * Texas Instruments, <www.ti.com>
7  *
8  * Author :
9  *      Aneesh V        <aneesh@ti.com>
10  *      Steve Sakoman   <steve@sakoman.com>
11  *
12  * See file CREDITS for list of people who contributed to this
13  * project.
14  *
15  * This program is free software; you can redistribute it and/or
16  * modify it under the terms of the GNU General Public License as
17  * published by the Free Software Foundation; either version 2 of
18  * the License, or (at your option) any later version.
19  *
20  * This program is distributed in the hope that it will be useful,
21  * but WITHOUT ANY WARRANTY; without even the implied warranty of
22  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
23  * GNU General Public License for more details.
24  *
25  * You should have received a copy of the GNU General Public License
26  * along with this program; if not, write to the Free Software
27  * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
28  * MA 02111-1307 USA
29  */
30 #include <common.h>
31 #include <spl.h>
32 #include <asm/arch/sys_proto.h>
33 #include <asm/sizes.h>
34 #include <asm/emif.h>
35 #include <asm/omap_common.h>
36 #include <linux/compiler.h>
37 #include <asm/cache.h>
38 #include <asm/system.h>
40 #define ARMV7_DCACHE_WRITEBACK  0xe
41 #define ARMV7_DOMAIN_CLIENT     1
42 #define ARMV7_DOMAIN_MASK       (0x3 << 0)
44 DECLARE_GLOBAL_DATA_PTR;
46 void do_set_mux(u32 base, struct pad_conf_entry const *array, int size)
47 {
48         int i;
49         struct pad_conf_entry *pad = (struct pad_conf_entry *) array;
51         for (i = 0; i < size; i++, pad++)
52                 writew(pad->val, base + pad->offset);
53 }
55 static void set_mux_conf_regs(void)
56 {
57         switch (omap_hw_init_context()) {
58         case OMAP_INIT_CONTEXT_SPL:
59                 set_muxconf_regs_essential();
60                 break;
61         case OMAP_INIT_CONTEXT_UBOOT_AFTER_SPL:
62 #ifdef CONFIG_SYS_ENABLE_PADS_ALL
63                 set_muxconf_regs_non_essential();
64 #endif
65                 break;
66         case OMAP_INIT_CONTEXT_UBOOT_FROM_NOR:
67         case OMAP_INIT_CONTEXT_UBOOT_AFTER_CH:
68                 set_muxconf_regs_essential();
69 #ifdef CONFIG_SYS_ENABLE_PADS_ALL
70                 set_muxconf_regs_non_essential();
71 #endif
72                 break;
73         }
74 }
76 u32 cortex_rev(void)
77 {
79         unsigned int rev;
81         /* Read Main ID Register (MIDR) */
82         asm ("mrc p15, 0, %0, c0, c0, 0" : "=r" (rev));
84         return rev;
85 }
87 void omap_rev_string(void)
88 {
89         u32 omap_rev = omap_revision();
90         u32 soc_variant = (omap_rev & 0xF0000000) >> 28;
91         u32 omap_variant = (omap_rev & 0xFFFF0000) >> 16;
92         u32 major_rev = (omap_rev & 0x00000F00) >> 8;
93         u32 minor_rev = (omap_rev & 0x000000F0) >> 4;
95         if (soc_variant)
96                 printf("OMAP");
97         else
98                 printf("DRA");
99         printf("%x ES%x.%x\n", omap_variant, major_rev,
100                minor_rev);
103 #ifdef CONFIG_SPL_BUILD
104 void spl_display_print(void)
106         omap_rev_string();
108 #endif
110 void __weak srcomp_enable(void)
114 static void save_omap_boot_params(void)
116         u32 rom_params = *((u32 *)OMAP_SRAM_SCRATCH_BOOT_PARAMS);
117         u8 boot_device;
118         u32 dev_desc, dev_data;
120         if ((rom_params <  NON_SECURE_SRAM_START) ||
121             (rom_params > NON_SECURE_SRAM_END))
122                 return;
124         /*
125          * rom_params can be type casted to omap_boot_parameters and
126          * used. But it not correct to assume that romcode structure
127          * encoding would be same as u-boot. So use the defined offsets.
128          */
129         gd->arch.omap_boot_params.omap_bootdevice = boot_device =
130                                    *((u8 *)(rom_params + BOOT_DEVICE_OFFSET));
132         gd->arch.omap_boot_params.ch_flags =
133                                 *((u8 *)(rom_params + CH_FLAGS_OFFSET));
135         if ((boot_device >= MMC_BOOT_DEVICES_START) &&
136             (boot_device <= MMC_BOOT_DEVICES_END)) {
137                 if ((omap_hw_init_context() ==
138                                       OMAP_INIT_CONTEXT_UBOOT_AFTER_SPL)) {
139                         gd->arch.omap_boot_params.omap_bootmode =
140                         *((u8 *)(rom_params + BOOT_MODE_OFFSET));
141                 } else {
142                         dev_desc = *((u32 *)(rom_params + DEV_DESC_PTR_OFFSET));
143                         dev_data = *((u32 *)(dev_desc + DEV_DATA_PTR_OFFSET));
144                         gd->arch.omap_boot_params.omap_bootmode =
145                                         *((u32 *)(dev_data + BOOT_MODE_OFFSET));
146                 }
147         }
150 #ifdef CONFIG_ARCH_CPU_INIT
151 /*
152  * SOC specific cpu init
153  */
154 int arch_cpu_init(void)
156         save_omap_boot_params();
157         return 0;
159 #endif /* CONFIG_ARCH_CPU_INIT */
161 /*
162  * Routine: s_init
163  * Description: Does early system init of watchdog, muxing,  andclocks
164  * Watchdog disable is done always. For the rest what gets done
165  * depends on the boot mode in which this function is executed
166  *   1. s_init of SPL running from SRAM
167  *   2. s_init of U-Boot running from FLASH
168  *   3. s_init of U-Boot loaded to SDRAM by SPL
169  *   4. s_init of U-Boot loaded to SDRAM by ROM code using the
170  *      Configuration Header feature
171  * Please have a look at the respective functions to see what gets
172  * done in each of these cases
173  * This function is called with SRAM stack.
174  */
175 void s_init(void)
177         /*
178          * Save the boot parameters passed from romcode.
179          * We cannot delay the saving further than this,
180          * to prevent overwrites.
181          */
182 #ifdef CONFIG_SPL_BUILD
183         save_omap_boot_params();
184 #endif
185         init_omap_revision();
186         hw_data_init();
188 #ifdef CONFIG_SPL_BUILD
189         if (warm_reset() && (omap_revision() <= OMAP5430_ES1_0))
190                 force_emif_self_refresh();
191 #endif
192         watchdog_init();
193         set_mux_conf_regs();
194 #ifdef CONFIG_SPL_BUILD
195         srcomp_enable();
196         setup_clocks_for_console();
198         gd = &gdata;
200         preloader_console_init();
201         do_io_settings();
202 #endif
203         prcm_init();
204 #ifdef CONFIG_SPL_BUILD
205         /* For regular u-boot sdram_init() is called from dram_init() */
206         sdram_init();
207 #endif
210 /*
211  * Routine: wait_for_command_complete
212  * Description: Wait for posting to finish on watchdog
213  */
214 void wait_for_command_complete(struct watchdog *wd_base)
216         int pending = 1;
217         do {
218                 pending = readl(&wd_base->wwps);
219         } while (pending);
222 /*
223  * Routine: watchdog_init
224  * Description: Shut down watch dogs
225  */
226 void watchdog_init(void)
228         struct watchdog *wd2_base = (struct watchdog *)WDT2_BASE;
230         writel(WD_UNLOCK1, &wd2_base->wspr);
231         wait_for_command_complete(wd2_base);
232         writel(WD_UNLOCK2, &wd2_base->wspr);
236 /*
237  * This function finds the SDRAM size available in the system
238  * based on DMM section configurations
239  * This is needed because the size of memory installed may be
240  * different on different versions of the board
241  */
242 u32 omap_sdram_size(void)
244         u32 section, i, valid;
245         u64 sdram_start = 0, sdram_end = 0, addr,
246             size, total_size = 0, trap_size = 0;
248         for (i = 0; i < 4; i++) {
249                 section = __raw_readl(DMM_BASE + i*4);
250                 valid = (section & EMIF_SDRC_ADDRSPC_MASK) >>
251                         (EMIF_SDRC_ADDRSPC_SHIFT);
252                 addr = section & EMIF_SYS_ADDR_MASK;
254                 /* See if the address is valid */
255                 if ((addr >= DRAM_ADDR_SPACE_START) &&
256                     (addr < DRAM_ADDR_SPACE_END)) {
257                         size = ((section & EMIF_SYS_SIZE_MASK) >>
258                                    EMIF_SYS_SIZE_SHIFT);
259                         size = 1 << size;
260                         size *= SZ_16M;
262                         if (valid != DMM_SDRC_ADDR_SPC_INVALID) {
263                                 if (!sdram_start || (addr < sdram_start))
264                                         sdram_start = addr;
265                                 if (!sdram_end || ((addr + size) > sdram_end))
266                                         sdram_end = addr + size;
267                         } else {
268                                 trap_size = size;
269                         }
271                 }
273         }
274         total_size = (sdram_end - sdram_start) - (trap_size);
276         return total_size;
280 /*
281  * Routine: dram_init
282  * Description: sets uboots idea of sdram size
283  */
284 int dram_init(void)
286         sdram_init();
287         gd->ram_size = omap_sdram_size();
288         return 0;
291 /*
292  * Print board information
293  */
294 int checkboard(void)
296         puts(sysinfo.board_string);
297         return 0;
300 /*
301  *  get_device_type(): tell if GP/HS/EMU/TST
302  */
303 u32 get_device_type(void)
305         return (readl((*ctrl)->control_status) &
306                                       (DEVICE_TYPE_MASK)) >> DEVICE_TYPE_SHIFT;
309 /*
310  * Print CPU information
311  */
312 int print_cpuinfo(void)
314         puts("CPU  : ");
315         omap_rev_string();
317         return 0;
319 #ifndef CONFIG_SYS_DCACHE_OFF
320 void enable_caches(void)
322         /* Enable D-cache. I-cache is already enabled in start.S */
323         dcache_enable();
326 void dram_bank_mmu_setup(int bank)
328         bd_t *bd = gd->bd;
329         int     i;
331         u32 start = bd->bi_dram[bank].start >> 20;
332         u32 size = bd->bi_dram[bank].size >> 20;
333         u32 end = start + size;
335         debug("%s: bank: %d\n", __func__, bank);
336         for (i = start; i < end; i++)
337                 set_section_dcache(i, ARMV7_DCACHE_WRITEBACK);
341 void arm_init_domains(void)
343         u32 reg;
345         reg = get_dacr();
346         /*
347         * Set DOMAIN to client access so that all permissions
348         * set in pagetables are validated by the mmu.
349         */
350         reg &= ~ARMV7_DOMAIN_MASK;
351         reg |= ARMV7_DOMAIN_CLIENT;
352         set_dacr(reg);
354 #endif