660032330ef0563ea9af5440f2ff14a8afef1385
[glsdk/glsdk-u-boot.git] / arch / arm / cpu / armv7 / omap-common / hwinit-common.c
1 /*
2  *
3  * Common functions for OMAP4/5 based boards
4  *
5  * (C) Copyright 2010
6  * Texas Instruments, <www.ti.com>
7  *
8  * Author :
9  *      Aneesh V        <aneesh@ti.com>
10  *      Steve Sakoman   <steve@sakoman.com>
11  *
12  * See file CREDITS for list of people who contributed to this
13  * project.
14  *
15  * This program is free software; you can redistribute it and/or
16  * modify it under the terms of the GNU General Public License as
17  * published by the Free Software Foundation; either version 2 of
18  * the License, or (at your option) any later version.
19  *
20  * This program is distributed in the hope that it will be useful,
21  * but WITHOUT ANY WARRANTY; without even the implied warranty of
22  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
23  * GNU General Public License for more details.
24  *
25  * You should have received a copy of the GNU General Public License
26  * along with this program; if not, write to the Free Software
27  * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
28  * MA 02111-1307 USA
29  */
30 #include <common.h>
31 #include <asm/arch/sys_proto.h>
32 #include <asm/sizes.h>
33 #include <asm/emif.h>
34 #include <asm/omap_common.h>
36 DECLARE_GLOBAL_DATA_PTR;
38 void do_set_mux(u32 base, struct pad_conf_entry const *array, int size)
39 {
40         int i;
41         struct pad_conf_entry *pad = (struct pad_conf_entry *) array;
43         for (i = 0; i < size; i++, pad++)
44                 writew(pad->val, base + pad->offset);
45 }
47 static void set_mux_conf_regs(void)
48 {
49         switch (omap_hw_init_context()) {
50         case OMAP_INIT_CONTEXT_SPL:
51                 set_muxconf_regs_essential();
52                 break;
53         case OMAP_INIT_CONTEXT_UBOOT_AFTER_SPL:
54 #ifdef CONFIG_SYS_ENABLE_PADS_ALL
55                 set_muxconf_regs_non_essential();
56 #endif
57                 break;
58         case OMAP_INIT_CONTEXT_UBOOT_FROM_NOR:
59         case OMAP_INIT_CONTEXT_UBOOT_AFTER_CH:
60                 set_muxconf_regs_essential();
61 #ifdef CONFIG_SYS_ENABLE_PADS_ALL
62                 set_muxconf_regs_non_essential();
63 #endif
64                 break;
65         }
66 }
68 u32 cortex_rev(void)
69 {
71         unsigned int rev;
73         /* Read Main ID Register (MIDR) */
74         asm ("mrc p15, 0, %0, c0, c0, 0" : "=r" (rev));
76         return rev;
77 }
79 void omap_rev_string(void)
80 {
81         u32 omap_rev = omap_revision();
82         u32 omap_variant = (omap_rev & 0xFFFF0000) >> 16;
83         u32 major_rev = (omap_rev & 0x00000F00) >> 8;
84         u32 minor_rev = (omap_rev & 0x000000F0) >> 4;
86         printf("OMAP%x ES%x.%x\n", omap_variant, major_rev,
87                 minor_rev);
88 }
90 #ifdef CONFIG_SPL_BUILD
91 static void init_boot_params(void)
92 {
93         boot_params_ptr = (u32 *) &boot_params;
94 }
95 #endif
97 /*
98  * Routine: s_init
99  * Description: Does early system init of watchdog, muxing,  andclocks
100  * Watchdog disable is done always. For the rest what gets done
101  * depends on the boot mode in which this function is executed
102  *   1. s_init of SPL running from SRAM
103  *   2. s_init of U-Boot running from FLASH
104  *   3. s_init of U-Boot loaded to SDRAM by SPL
105  *   4. s_init of U-Boot loaded to SDRAM by ROM code using the
106  *      Configuration Header feature
107  * Please have a look at the respective functions to see what gets
108  * done in each of these cases
109  * This function is called with SRAM stack.
110  */
111 void s_init(void)
113         init_omap_revision();
114         watchdog_init();
115         set_mux_conf_regs();
116 #ifdef CONFIG_SPL_BUILD
117         setup_clocks_for_console();
118         preloader_console_init();
119         do_io_settings();
120 #endif
121         prcm_init();
122 #ifdef CONFIG_SPL_BUILD
123         timer_init();
125         /* For regular u-boot sdram_init() is called from dram_init() */
126         sdram_init();
127         init_boot_params();
128 #endif
131 /*
132  * Routine: wait_for_command_complete
133  * Description: Wait for posting to finish on watchdog
134  */
135 void wait_for_command_complete(struct watchdog *wd_base)
137         int pending = 1;
138         do {
139                 pending = readl(&wd_base->wwps);
140         } while (pending);
143 /*
144  * Routine: watchdog_init
145  * Description: Shut down watch dogs
146  */
147 void watchdog_init(void)
149         struct watchdog *wd2_base = (struct watchdog *)WDT2_BASE;
151         writel(WD_UNLOCK1, &wd2_base->wspr);
152         wait_for_command_complete(wd2_base);
153         writel(WD_UNLOCK2, &wd2_base->wspr);
157 /*
158  * This function finds the SDRAM size available in the system
159  * based on DMM section configurations
160  * This is needed because the size of memory installed may be
161  * different on different versions of the board
162  */
163 u32 omap_sdram_size(void)
165         u32 section, i, valid;
166         u64 sdram_start = 0, sdram_end = 0, addr,
167             size, total_size = 0, trap_size = 0;
169         for (i = 0; i < 4; i++) {
170                 section = __raw_readl(DMM_BASE + i*4);
171                 valid = (section & EMIF_SDRC_ADDRSPC_MASK) >>
172                         (EMIF_SDRC_ADDRSPC_SHIFT);
173                 addr = section & EMIF_SYS_ADDR_MASK;
175                 /* See if the address is valid */
176                 if ((addr >= DRAM_ADDR_SPACE_START) &&
177                     (addr < DRAM_ADDR_SPACE_END)) {
178                         size = ((section & EMIF_SYS_SIZE_MASK) >>
179                                    EMIF_SYS_SIZE_SHIFT);
180                         size = 1 << size;
181                         size *= SZ_16M;
183                         if (valid != DMM_SDRC_ADDR_SPC_INVALID) {
184                                 if (!sdram_start || (addr < sdram_start))
185                                         sdram_start = addr;
186                                 if (!sdram_end || ((addr + size) > sdram_end))
187                                         sdram_end = addr + size;
188                         } else {
189                                 trap_size = size;
190                         }
192                 }
194         }
195         total_size = (sdram_end - sdram_start) - (trap_size);
197         return total_size;
201 /*
202  * Routine: dram_init
203  * Description: sets uboots idea of sdram size
204  */
205 int dram_init(void)
207         sdram_init();
208         gd->ram_size = omap_sdram_size();
209         return 0;
212 /*
213  * Print board information
214  */
215 int checkboard(void)
217         puts(sysinfo.board_string);
218         return 0;
221 /*
222  *  get_device_type(): tell if GP/HS/EMU/TST
223  */
224 u32 get_device_type(void)
226         struct omap_sys_ctrl_regs *ctrl =
227                       (struct omap_sys_ctrl_regs *) SYSCTRL_GENERAL_CORE_BASE;
229         return (readl(&ctrl->control_status) &
230                                       (DEVICE_TYPE_MASK)) >> DEVICE_TYPE_SHIFT;
233 /*
234  * Print CPU information
235  */
236 int print_cpuinfo(void)
238         puts("CPU  : ");
239         omap_rev_string();
241         return 0;
243 #ifndef CONFIG_SYS_DCACHE_OFF
244 void enable_caches(void)
246         /* Enable D-cache. I-cache is already enabled in start.S */
247         dcache_enable();
249 #endif