fff89da571071e8c25a8d2d73643b0a2d53366f0
[glsdk/glsdk-u-boot.git] / arch / arm / cpu / armv7 / omap-common / hwinit-common.c
1 /*
2  *
3  * Common functions for OMAP4/5 based boards
4  *
5  * (C) Copyright 2010
6  * Texas Instruments, <www.ti.com>
7  *
8  * Author :
9  *      Aneesh V        <aneesh@ti.com>
10  *      Steve Sakoman   <steve@sakoman.com>
11  *
12  * See file CREDITS for list of people who contributed to this
13  * project.
14  *
15  * This program is free software; you can redistribute it and/or
16  * modify it under the terms of the GNU General Public License as
17  * published by the Free Software Foundation; either version 2 of
18  * the License, or (at your option) any later version.
19  *
20  * This program is distributed in the hope that it will be useful,
21  * but WITHOUT ANY WARRANTY; without even the implied warranty of
22  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
23  * GNU General Public License for more details.
24  *
25  * You should have received a copy of the GNU General Public License
26  * along with this program; if not, write to the Free Software
27  * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
28  * MA 02111-1307 USA
29  */
30 #include <common.h>
31 #include <spl.h>
32 #include <asm/arch/sys_proto.h>
33 #include <asm/sizes.h>
34 #include <asm/emif.h>
35 #include <asm/omap_common.h>
37 DECLARE_GLOBAL_DATA_PTR;
39 void do_set_mux(u32 base, struct pad_conf_entry const *array, int size)
40 {
41         int i;
42         struct pad_conf_entry *pad = (struct pad_conf_entry *) array;
44         for (i = 0; i < size; i++, pad++)
45                 writew(pad->val, base + pad->offset);
46 }
48 static void set_mux_conf_regs(void)
49 {
50         switch (omap_hw_init_context()) {
51         case OMAP_INIT_CONTEXT_SPL:
52                 set_muxconf_regs_essential();
53                 break;
54         case OMAP_INIT_CONTEXT_UBOOT_AFTER_SPL:
55 #ifdef CONFIG_SYS_ENABLE_PADS_ALL
56                 set_muxconf_regs_non_essential();
57 #endif
58                 break;
59         case OMAP_INIT_CONTEXT_UBOOT_FROM_NOR:
60         case OMAP_INIT_CONTEXT_UBOOT_AFTER_CH:
61                 set_muxconf_regs_essential();
62 #ifdef CONFIG_SYS_ENABLE_PADS_ALL
63                 set_muxconf_regs_non_essential();
64 #endif
65                 break;
66         }
67 }
69 u32 cortex_rev(void)
70 {
72         unsigned int rev;
74         /* Read Main ID Register (MIDR) */
75         asm ("mrc p15, 0, %0, c0, c0, 0" : "=r" (rev));
77         return rev;
78 }
80 void omap_rev_string(void)
81 {
82         u32 omap_rev = omap_revision();
83         u32 omap_variant = (omap_rev & 0xFFFF0000) >> 16;
84         u32 major_rev = (omap_rev & 0x00000F00) >> 8;
85         u32 minor_rev = (omap_rev & 0x000000F0) >> 4;
87         printf("OMAP%x ES%x.%x\n", omap_variant, major_rev,
88                 minor_rev);
89 }
91 #ifdef CONFIG_SPL_BUILD
92 static void init_boot_params(void)
93 {
94         boot_params_ptr = (u32 *) &boot_params;
95 }
97 void spl_display_print(void)
98 {
99         omap_rev_string();
101 #endif
103 /*
104  * Routine: s_init
105  * Description: Does early system init of watchdog, muxing,  andclocks
106  * Watchdog disable is done always. For the rest what gets done
107  * depends on the boot mode in which this function is executed
108  *   1. s_init of SPL running from SRAM
109  *   2. s_init of U-Boot running from FLASH
110  *   3. s_init of U-Boot loaded to SDRAM by SPL
111  *   4. s_init of U-Boot loaded to SDRAM by ROM code using the
112  *      Configuration Header feature
113  * Please have a look at the respective functions to see what gets
114  * done in each of these cases
115  * This function is called with SRAM stack.
116  */
117 void s_init(void)
119         init_omap_revision();
120         hw_data_init();
122 #ifdef CONFIG_SPL_BUILD
123         if (warm_reset() && (omap_revision() <= OMAP5430_ES1_0))
124                 force_emif_self_refresh();
125 #endif
126         watchdog_init();
127         set_mux_conf_regs();
128 #ifdef CONFIG_SPL_BUILD
129         setup_clocks_for_console();
131         gd = &gdata;
133         preloader_console_init();
134         do_io_settings();
135 #endif
136         prcm_init();
137 #ifdef CONFIG_SPL_BUILD
138         timer_init();
140         /* For regular u-boot sdram_init() is called from dram_init() */
141         sdram_init();
142         init_boot_params();
143 #endif
146 /*
147  * Routine: wait_for_command_complete
148  * Description: Wait for posting to finish on watchdog
149  */
150 void wait_for_command_complete(struct watchdog *wd_base)
152         int pending = 1;
153         do {
154                 pending = readl(&wd_base->wwps);
155         } while (pending);
158 /*
159  * Routine: watchdog_init
160  * Description: Shut down watch dogs
161  */
162 void watchdog_init(void)
164         struct watchdog *wd2_base = (struct watchdog *)WDT2_BASE;
166         writel(WD_UNLOCK1, &wd2_base->wspr);
167         wait_for_command_complete(wd2_base);
168         writel(WD_UNLOCK2, &wd2_base->wspr);
172 /*
173  * This function finds the SDRAM size available in the system
174  * based on DMM section configurations
175  * This is needed because the size of memory installed may be
176  * different on different versions of the board
177  */
178 u32 omap_sdram_size(void)
180         u32 section, i, valid;
181         u64 sdram_start = 0, sdram_end = 0, addr,
182             size, total_size = 0, trap_size = 0;
184         for (i = 0; i < 4; i++) {
185                 section = __raw_readl(DMM_BASE + i*4);
186                 valid = (section & EMIF_SDRC_ADDRSPC_MASK) >>
187                         (EMIF_SDRC_ADDRSPC_SHIFT);
188                 addr = section & EMIF_SYS_ADDR_MASK;
190                 /* See if the address is valid */
191                 if ((addr >= DRAM_ADDR_SPACE_START) &&
192                     (addr < DRAM_ADDR_SPACE_END)) {
193                         size = ((section & EMIF_SYS_SIZE_MASK) >>
194                                    EMIF_SYS_SIZE_SHIFT);
195                         size = 1 << size;
196                         size *= SZ_16M;
198                         if (valid != DMM_SDRC_ADDR_SPC_INVALID) {
199                                 if (!sdram_start || (addr < sdram_start))
200                                         sdram_start = addr;
201                                 if (!sdram_end || ((addr + size) > sdram_end))
202                                         sdram_end = addr + size;
203                         } else {
204                                 trap_size = size;
205                         }
207                 }
209         }
210         total_size = (sdram_end - sdram_start) - (trap_size);
212         return total_size;
216 /*
217  * Routine: dram_init
218  * Description: sets uboots idea of sdram size
219  */
220 int dram_init(void)
222         sdram_init();
223         gd->ram_size = omap_sdram_size();
224         return 0;
227 /*
228  * Print board information
229  */
230 int checkboard(void)
232         puts(sysinfo.board_string);
233         return 0;
236 /*
237  *  get_device_type(): tell if GP/HS/EMU/TST
238  */
239 u32 get_device_type(void)
241         struct omap_sys_ctrl_regs *ctrl =
242                       (struct omap_sys_ctrl_regs *) SYSCTRL_GENERAL_CORE_BASE;
244         return (readl(&ctrl->control_status) &
245                                       (DEVICE_TYPE_MASK)) >> DEVICE_TYPE_SHIFT;
248 /*
249  * Print CPU information
250  */
251 int print_cpuinfo(void)
253         puts("CPU  : ");
254         omap_rev_string();
256         return 0;
258 #ifndef CONFIG_SYS_DCACHE_OFF
259 void enable_caches(void)
261         /* Enable D-cache. I-cache is already enabled in start.S */
262         dcache_enable();
264 #endif