]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/glsdk-u-boot.git/blob - arch/arm/cpu/armv7/omap-common/hwinit-common.c
omap-common: SPL: Add CONFIG_SPL_DISPLAY_PRINT / spl_display_print()
[glsdk/glsdk-u-boot.git] / arch / arm / cpu / armv7 / omap-common / hwinit-common.c
1 /*
2  *
3  * Common functions for OMAP4/5 based boards
4  *
5  * (C) Copyright 2010
6  * Texas Instruments, <www.ti.com>
7  *
8  * Author :
9  *      Aneesh V        <aneesh@ti.com>
10  *      Steve Sakoman   <steve@sakoman.com>
11  *
12  * See file CREDITS for list of people who contributed to this
13  * project.
14  *
15  * This program is free software; you can redistribute it and/or
16  * modify it under the terms of the GNU General Public License as
17  * published by the Free Software Foundation; either version 2 of
18  * the License, or (at your option) any later version.
19  *
20  * This program is distributed in the hope that it will be useful,
21  * but WITHOUT ANY WARRANTY; without even the implied warranty of
22  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
23  * GNU General Public License for more details.
24  *
25  * You should have received a copy of the GNU General Public License
26  * along with this program; if not, write to the Free Software
27  * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
28  * MA 02111-1307 USA
29  */
30 #include <common.h>
31 #include <asm/arch/sys_proto.h>
32 #include <asm/sizes.h>
33 #include <asm/emif.h>
34 #include <asm/omap_common.h>
36 DECLARE_GLOBAL_DATA_PTR;
38 void do_set_mux(u32 base, struct pad_conf_entry const *array, int size)
39 {
40         int i;
41         struct pad_conf_entry *pad = (struct pad_conf_entry *) array;
43         for (i = 0; i < size; i++, pad++)
44                 writew(pad->val, base + pad->offset);
45 }
47 static void set_mux_conf_regs(void)
48 {
49         switch (omap_hw_init_context()) {
50         case OMAP_INIT_CONTEXT_SPL:
51                 set_muxconf_regs_essential();
52                 break;
53         case OMAP_INIT_CONTEXT_UBOOT_AFTER_SPL:
54 #ifdef CONFIG_SYS_ENABLE_PADS_ALL
55                 set_muxconf_regs_non_essential();
56 #endif
57                 break;
58         case OMAP_INIT_CONTEXT_UBOOT_FROM_NOR:
59         case OMAP_INIT_CONTEXT_UBOOT_AFTER_CH:
60                 set_muxconf_regs_essential();
61 #ifdef CONFIG_SYS_ENABLE_PADS_ALL
62                 set_muxconf_regs_non_essential();
63 #endif
64                 break;
65         }
66 }
68 u32 cortex_rev(void)
69 {
71         unsigned int rev;
73         /* Read Main ID Register (MIDR) */
74         asm ("mrc p15, 0, %0, c0, c0, 0" : "=r" (rev));
76         return rev;
77 }
79 void omap_rev_string(void)
80 {
81         u32 omap_rev = omap_revision();
82         u32 omap_variant = (omap_rev & 0xFFFF0000) >> 16;
83         u32 major_rev = (omap_rev & 0x00000F00) >> 8;
84         u32 minor_rev = (omap_rev & 0x000000F0) >> 4;
86         printf("OMAP%x ES%x.%x\n", omap_variant, major_rev,
87                 minor_rev);
88 }
90 #ifdef CONFIG_SPL_BUILD
91 static void init_boot_params(void)
92 {
93         boot_params_ptr = (u32 *) &boot_params;
94 }
96 void spl_display_print(void)
97 {
98         omap_rev_string();
99 }
100 #endif
102 /*
103  * Routine: s_init
104  * Description: Does early system init of watchdog, muxing,  andclocks
105  * Watchdog disable is done always. For the rest what gets done
106  * depends on the boot mode in which this function is executed
107  *   1. s_init of SPL running from SRAM
108  *   2. s_init of U-Boot running from FLASH
109  *   3. s_init of U-Boot loaded to SDRAM by SPL
110  *   4. s_init of U-Boot loaded to SDRAM by ROM code using the
111  *      Configuration Header feature
112  * Please have a look at the respective functions to see what gets
113  * done in each of these cases
114  * This function is called with SRAM stack.
115  */
116 void s_init(void)
118         init_omap_revision();
119 #ifdef CONFIG_SPL_BUILD
120         if (warm_reset() && (omap_revision() <= OMAP5430_ES1_0))
121                 force_emif_self_refresh();
122 #endif
123         watchdog_init();
124         set_mux_conf_regs();
125 #ifdef CONFIG_SPL_BUILD
126         setup_clocks_for_console();
127         preloader_console_init();
128         do_io_settings();
129 #endif
130         prcm_init();
131 #ifdef CONFIG_SPL_BUILD
132         timer_init();
134         /* For regular u-boot sdram_init() is called from dram_init() */
135         sdram_init();
136         init_boot_params();
137 #endif
140 /*
141  * Routine: wait_for_command_complete
142  * Description: Wait for posting to finish on watchdog
143  */
144 void wait_for_command_complete(struct watchdog *wd_base)
146         int pending = 1;
147         do {
148                 pending = readl(&wd_base->wwps);
149         } while (pending);
152 /*
153  * Routine: watchdog_init
154  * Description: Shut down watch dogs
155  */
156 void watchdog_init(void)
158         struct watchdog *wd2_base = (struct watchdog *)WDT2_BASE;
160         writel(WD_UNLOCK1, &wd2_base->wspr);
161         wait_for_command_complete(wd2_base);
162         writel(WD_UNLOCK2, &wd2_base->wspr);
166 /*
167  * This function finds the SDRAM size available in the system
168  * based on DMM section configurations
169  * This is needed because the size of memory installed may be
170  * different on different versions of the board
171  */
172 u32 omap_sdram_size(void)
174         u32 section, i, valid;
175         u64 sdram_start = 0, sdram_end = 0, addr,
176             size, total_size = 0, trap_size = 0;
178         for (i = 0; i < 4; i++) {
179                 section = __raw_readl(DMM_BASE + i*4);
180                 valid = (section & EMIF_SDRC_ADDRSPC_MASK) >>
181                         (EMIF_SDRC_ADDRSPC_SHIFT);
182                 addr = section & EMIF_SYS_ADDR_MASK;
184                 /* See if the address is valid */
185                 if ((addr >= DRAM_ADDR_SPACE_START) &&
186                     (addr < DRAM_ADDR_SPACE_END)) {
187                         size = ((section & EMIF_SYS_SIZE_MASK) >>
188                                    EMIF_SYS_SIZE_SHIFT);
189                         size = 1 << size;
190                         size *= SZ_16M;
192                         if (valid != DMM_SDRC_ADDR_SPC_INVALID) {
193                                 if (!sdram_start || (addr < sdram_start))
194                                         sdram_start = addr;
195                                 if (!sdram_end || ((addr + size) > sdram_end))
196                                         sdram_end = addr + size;
197                         } else {
198                                 trap_size = size;
199                         }
201                 }
203         }
204         total_size = (sdram_end - sdram_start) - (trap_size);
206         return total_size;
210 /*
211  * Routine: dram_init
212  * Description: sets uboots idea of sdram size
213  */
214 int dram_init(void)
216         sdram_init();
217         gd->ram_size = omap_sdram_size();
218         return 0;
221 /*
222  * Print board information
223  */
224 int checkboard(void)
226         puts(sysinfo.board_string);
227         return 0;
230 /*
231  *  get_device_type(): tell if GP/HS/EMU/TST
232  */
233 u32 get_device_type(void)
235         struct omap_sys_ctrl_regs *ctrl =
236                       (struct omap_sys_ctrl_regs *) SYSCTRL_GENERAL_CORE_BASE;
238         return (readl(&ctrl->control_status) &
239                                       (DEVICE_TYPE_MASK)) >> DEVICE_TYPE_SHIFT;
242 /*
243  * Print CPU information
244  */
245 int print_cpuinfo(void)
247         puts("CPU  : ");
248         omap_rev_string();
250         return 0;
252 #ifndef CONFIG_SYS_DCACHE_OFF
253 void enable_caches(void)
255         /* Enable D-cache. I-cache is already enabled in start.S */
256         dcache_enable();
258 #endif