]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/glsdk-u-boot.git/blob - arch/arm/cpu/armv7/omap-common/hwinit-common.c
Merge branch 'for-v2013.04'
[glsdk/glsdk-u-boot.git] / arch / arm / cpu / armv7 / omap-common / hwinit-common.c
1 /*
2  *
3  * Common functions for OMAP4/5 based boards
4  *
5  * (C) Copyright 2010
6  * Texas Instruments, <www.ti.com>
7  *
8  * Author :
9  *      Aneesh V        <aneesh@ti.com>
10  *      Steve Sakoman   <steve@sakoman.com>
11  *
12  * See file CREDITS for list of people who contributed to this
13  * project.
14  *
15  * This program is free software; you can redistribute it and/or
16  * modify it under the terms of the GNU General Public License as
17  * published by the Free Software Foundation; either version 2 of
18  * the License, or (at your option) any later version.
19  *
20  * This program is distributed in the hope that it will be useful,
21  * but WITHOUT ANY WARRANTY; without even the implied warranty of
22  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
23  * GNU General Public License for more details.
24  *
25  * You should have received a copy of the GNU General Public License
26  * along with this program; if not, write to the Free Software
27  * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
28  * MA 02111-1307 USA
29  */
30 #include <common.h>
31 #include <spl.h>
32 #include <asm/arch/sys_proto.h>
33 #include <asm/sizes.h>
34 #include <asm/emif.h>
35 #include <asm/omap_common.h>
36 #include <linux/compiler.h>
37 #include <asm/cache.h>
38 #include <asm/system.h>
40 #define ARMV7_DCACHE_WRITEBACK  0xe
41 #define ARMV7_DOMAIN_CLIENT     1
42 #define ARMV7_DOMAIN_MASK       (0x3 << 0)
44 DECLARE_GLOBAL_DATA_PTR;
46 void do_set_mux(u32 base, struct pad_conf_entry const *array, int size)
47 {
48         int i;
49         struct pad_conf_entry *pad = (struct pad_conf_entry *) array;
51         for (i = 0; i < size; i++, pad++)
52                 writew(pad->val, base + pad->offset);
53 }
55 static void set_mux_conf_regs(void)
56 {
57         switch (omap_hw_init_context()) {
58         case OMAP_INIT_CONTEXT_SPL:
59                 set_muxconf_regs_essential();
60                 break;
61         case OMAP_INIT_CONTEXT_UBOOT_AFTER_SPL:
62 #ifdef CONFIG_SYS_ENABLE_PADS_ALL
63                 set_muxconf_regs_non_essential();
64 #endif
65                 break;
66         case OMAP_INIT_CONTEXT_UBOOT_FROM_NOR:
67         case OMAP_INIT_CONTEXT_UBOOT_AFTER_CH:
68                 set_muxconf_regs_essential();
69 #ifdef CONFIG_SYS_ENABLE_PADS_ALL
70                 set_muxconf_regs_non_essential();
71 #endif
72                 break;
73         }
74 }
76 u32 cortex_rev(void)
77 {
79         unsigned int rev;
81         /* Read Main ID Register (MIDR) */
82         asm ("mrc p15, 0, %0, c0, c0, 0" : "=r" (rev));
84         return rev;
85 }
87 void omap_rev_string(void)
88 {
89         u32 omap_rev = omap_revision();
90         u32 soc_variant = (omap_rev & 0xF0000000) >> 28;
91         u32 omap_variant = (omap_rev & 0xFFFF0000) >> 16;
92         u32 major_rev = (omap_rev & 0x00000F00) >> 8;
93         u32 minor_rev = (omap_rev & 0x000000F0) >> 4;
95         if (soc_variant)
96                 printf("OMAP");
97         else
98                 printf("DRA");
99         printf("%x ES%x.%x\n", omap_variant, major_rev,
100                minor_rev);
103 #ifdef CONFIG_SPL_BUILD
104 static void init_boot_params(void)
106         boot_params_ptr = (u32 *) &boot_params;
109 void spl_display_print(void)
111         omap_rev_string();
113 #endif
115 void __weak srcomp_enable(void)
119 /*
120  * Routine: s_init
121  * Description: Does early system init of watchdog, muxing,  andclocks
122  * Watchdog disable is done always. For the rest what gets done
123  * depends on the boot mode in which this function is executed
124  *   1. s_init of SPL running from SRAM
125  *   2. s_init of U-Boot running from FLASH
126  *   3. s_init of U-Boot loaded to SDRAM by SPL
127  *   4. s_init of U-Boot loaded to SDRAM by ROM code using the
128  *      Configuration Header feature
129  * Please have a look at the respective functions to see what gets
130  * done in each of these cases
131  * This function is called with SRAM stack.
132  */
133 void s_init(void)
135         init_omap_revision();
136         hw_data_init();
138 #ifdef CONFIG_SPL_BUILD
139         if (warm_reset() && (omap_revision() <= OMAP5430_ES1_0))
140                 force_emif_self_refresh();
141 #endif
142         watchdog_init();
143         set_mux_conf_regs();
144 #ifdef CONFIG_SPL_BUILD
145         srcomp_enable();
146         setup_clocks_for_console();
148         gd = &gdata;
150         preloader_console_init();
151         do_io_settings();
152 #endif
153         prcm_init();
154 #ifdef CONFIG_SPL_BUILD
155         timer_init();
157         /* For regular u-boot sdram_init() is called from dram_init() */
158         sdram_init();
159         init_boot_params();
160 #endif
163 /*
164  * Routine: wait_for_command_complete
165  * Description: Wait for posting to finish on watchdog
166  */
167 void wait_for_command_complete(struct watchdog *wd_base)
169         int pending = 1;
170         do {
171                 pending = readl(&wd_base->wwps);
172         } while (pending);
175 /*
176  * Routine: watchdog_init
177  * Description: Shut down watch dogs
178  */
179 void watchdog_init(void)
181         struct watchdog *wd2_base = (struct watchdog *)WDT2_BASE;
183         writel(WD_UNLOCK1, &wd2_base->wspr);
184         wait_for_command_complete(wd2_base);
185         writel(WD_UNLOCK2, &wd2_base->wspr);
189 /*
190  * This function finds the SDRAM size available in the system
191  * based on DMM section configurations
192  * This is needed because the size of memory installed may be
193  * different on different versions of the board
194  */
195 u32 omap_sdram_size(void)
197         u32 section, i, valid;
198         u64 sdram_start = 0, sdram_end = 0, addr,
199             size, total_size = 0, trap_size = 0;
201         for (i = 0; i < 4; i++) {
202                 section = __raw_readl(DMM_BASE + i*4);
203                 valid = (section & EMIF_SDRC_ADDRSPC_MASK) >>
204                         (EMIF_SDRC_ADDRSPC_SHIFT);
205                 addr = section & EMIF_SYS_ADDR_MASK;
207                 /* See if the address is valid */
208                 if ((addr >= DRAM_ADDR_SPACE_START) &&
209                     (addr < DRAM_ADDR_SPACE_END)) {
210                         size = ((section & EMIF_SYS_SIZE_MASK) >>
211                                    EMIF_SYS_SIZE_SHIFT);
212                         size = 1 << size;
213                         size *= SZ_16M;
215                         if (valid != DMM_SDRC_ADDR_SPC_INVALID) {
216                                 if (!sdram_start || (addr < sdram_start))
217                                         sdram_start = addr;
218                                 if (!sdram_end || ((addr + size) > sdram_end))
219                                         sdram_end = addr + size;
220                         } else {
221                                 trap_size = size;
222                         }
224                 }
226         }
227         total_size = (sdram_end - sdram_start) - (trap_size);
229         return total_size;
233 /*
234  * Routine: dram_init
235  * Description: sets uboots idea of sdram size
236  */
237 int dram_init(void)
239         sdram_init();
240         gd->ram_size = omap_sdram_size();
241         return 0;
244 /*
245  * Print board information
246  */
247 int checkboard(void)
249         puts(sysinfo.board_string);
250         return 0;
253 /*
254  *  get_device_type(): tell if GP/HS/EMU/TST
255  */
256 u32 get_device_type(void)
258         return (readl((*ctrl)->control_status) &
259                                       (DEVICE_TYPE_MASK)) >> DEVICE_TYPE_SHIFT;
262 /*
263  * Print CPU information
264  */
265 int print_cpuinfo(void)
267         puts("CPU  : ");
268         omap_rev_string();
270         return 0;
272 #ifndef CONFIG_SYS_DCACHE_OFF
273 void enable_caches(void)
275         /* Enable D-cache. I-cache is already enabled in start.S */
276         dcache_enable();
279 void dram_bank_mmu_setup(int bank)
281         bd_t *bd = gd->bd;
282         int     i;
284         u32 start = bd->bi_dram[bank].start >> 20;
285         u32 size = bd->bi_dram[bank].size >> 20;
286         u32 end = start + size;
288         debug("%s: bank: %d\n", __func__, bank);
289         for (i = start; i < end; i++)
290                 set_section_dcache(i, ARMV7_DCACHE_WRITEBACK);
294 void arm_init_domains(void)
296         u32 reg;
298         reg = get_dacr();
299         /*
300         * Set DOMAIN to client access so that all permissions
301         * set in pagetables are validated by the mmu.
302         */
303         reg &= ~ARMV7_DOMAIN_MASK;
304         reg |= ARMV7_DOMAIN_CLIENT;
305         set_dacr(reg);
307 #endif