]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/glsdk-u-boot.git/blob - arch/arm/cpu/armv7/omap3/board.c
Merge remote-tracking branch 'u-boot-ti/master'
[glsdk/glsdk-u-boot.git] / arch / arm / cpu / armv7 / omap3 / board.c
1 /*
2  *
3  * Common board functions for OMAP3 based boards.
4  *
5  * (C) Copyright 2004-2008
6  * Texas Instruments, <www.ti.com>
7  *
8  * Author :
9  *      Sunil Kumar <sunilsaini05@gmail.com>
10  *      Shashi Ranjan <shashiranjanmca05@gmail.com>
11  *
12  * Derived from Beagle Board and 3430 SDP code by
13  *      Richard Woodruff <r-woodruff2@ti.com>
14  *      Syed Mohammed Khasim <khasim@ti.com>
15  *
16  *
17  * See file CREDITS for list of people who contributed to this
18  * project.
19  *
20  * This program is free software; you can redistribute it and/or
21  * modify it under the terms of the GNU General Public License as
22  * published by the Free Software Foundation; either version 2 of
23  * the License, or (at your option) any later version.
24  *
25  * This program is distributed in the hope that it will be useful,
26  * but WITHOUT ANY WARRANTY; without even the implied warranty of
27  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
28  * GNU General Public License for more details.
29  *
30  * You should have received a copy of the GNU General Public License
31  * along with this program; if not, write to the Free Software
32  * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
33  * MA 02111-1307 USA
34  */
35 #include <common.h>
36 #include <spl.h>
37 #include <asm/io.h>
38 #include <asm/arch/sys_proto.h>
39 #include <asm/arch/mem.h>
40 #include <asm/cache.h>
41 #include <asm/armv7.h>
42 #include <asm/arch/gpio.h>
43 #include <asm/omap_common.h>
44 #include <asm/arch/mmc_host_def.h>
45 #include <i2c.h>
46 #include <linux/compiler.h>
48 DECLARE_GLOBAL_DATA_PTR;
50 /* Declarations */
51 extern omap3_sysinfo sysinfo;
52 static void omap3_setup_aux_cr(void);
53 #ifndef CONFIG_SYS_L2CACHE_OFF
54 static void omap3_invalidate_l2_cache_secure(void);
55 #endif
57 static const struct gpio_bank gpio_bank_34xx[6] = {
58         { (void *)OMAP34XX_GPIO1_BASE, METHOD_GPIO_24XX },
59         { (void *)OMAP34XX_GPIO2_BASE, METHOD_GPIO_24XX },
60         { (void *)OMAP34XX_GPIO3_BASE, METHOD_GPIO_24XX },
61         { (void *)OMAP34XX_GPIO4_BASE, METHOD_GPIO_24XX },
62         { (void *)OMAP34XX_GPIO5_BASE, METHOD_GPIO_24XX },
63         { (void *)OMAP34XX_GPIO6_BASE, METHOD_GPIO_24XX },
64 };
66 const struct gpio_bank *const omap_gpio_bank = gpio_bank_34xx;
68 #ifdef CONFIG_SPL_BUILD
69 /*
70 * We use static variables because global data is not ready yet.
71 * Initialized data is available in SPL right from the beginning.
72 * We would not typically need to save these parameters in regular
73 * U-Boot. This is needed only in SPL at the moment.
74 */
75 u32 omap3_boot_device = BOOT_DEVICE_NAND;
77 /* auto boot mode detection is not possible for OMAP3 - hard code */
78 u32 spl_boot_mode(void)
79 {
80         switch (spl_boot_device()) {
81         case BOOT_DEVICE_MMC2:
82                 return MMCSD_MODE_RAW;
83         case BOOT_DEVICE_MMC1:
84                 return MMCSD_MODE_FAT;
85                 break;
86         default:
87                 puts("spl: ERROR:  unknown device - can't select boot mode\n");
88                 hang();
89         }
90 }
92 u32 spl_boot_device(void)
93 {
94         return omap3_boot_device;
95 }
97 int board_mmc_init(bd_t *bis)
98 {
99         switch (spl_boot_device()) {
100         case BOOT_DEVICE_MMC1:
101                 omap_mmc_init(0, 0, 0);
102                 break;
103         case BOOT_DEVICE_MMC2:
104         case BOOT_DEVICE_MMC2_2:
105                 omap_mmc_init(1, 0, 0);
106                 break;
107         }
108         return 0;
111 void spl_board_init(void)
113 #ifdef CONFIG_SPL_NAND_SUPPORT
114         gpmc_init();
115 #endif
116 #ifdef CONFIG_SPL_I2C_SUPPORT
117         i2c_init(CONFIG_SYS_I2C_SPEED, CONFIG_SYS_I2C_SLAVE);
118 #endif
120 #endif /* CONFIG_SPL_BUILD */
123 /******************************************************************************
124  * Routine: secure_unlock
125  * Description: Setup security registers for access
126  *              (GP Device only)
127  *****************************************************************************/
128 void secure_unlock_mem(void)
130         struct pm *pm_rt_ape_base = (struct pm *)PM_RT_APE_BASE_ADDR_ARM;
131         struct pm *pm_gpmc_base = (struct pm *)PM_GPMC_BASE_ADDR_ARM;
132         struct pm *pm_ocm_ram_base = (struct pm *)PM_OCM_RAM_BASE_ADDR_ARM;
133         struct pm *pm_iva2_base = (struct pm *)PM_IVA2_BASE_ADDR_ARM;
134         struct sms *sms_base = (struct sms *)OMAP34XX_SMS_BASE;
136         /* Protection Module Register Target APE (PM_RT) */
137         writel(UNLOCK_1, &pm_rt_ape_base->req_info_permission_1);
138         writel(UNLOCK_1, &pm_rt_ape_base->read_permission_0);
139         writel(UNLOCK_1, &pm_rt_ape_base->wirte_permission_0);
140         writel(UNLOCK_2, &pm_rt_ape_base->addr_match_1);
142         writel(UNLOCK_3, &pm_gpmc_base->req_info_permission_0);
143         writel(UNLOCK_3, &pm_gpmc_base->read_permission_0);
144         writel(UNLOCK_3, &pm_gpmc_base->wirte_permission_0);
146         writel(UNLOCK_3, &pm_ocm_ram_base->req_info_permission_0);
147         writel(UNLOCK_3, &pm_ocm_ram_base->read_permission_0);
148         writel(UNLOCK_3, &pm_ocm_ram_base->wirte_permission_0);
149         writel(UNLOCK_2, &pm_ocm_ram_base->addr_match_2);
151         /* IVA Changes */
152         writel(UNLOCK_3, &pm_iva2_base->req_info_permission_0);
153         writel(UNLOCK_3, &pm_iva2_base->read_permission_0);
154         writel(UNLOCK_3, &pm_iva2_base->wirte_permission_0);
156         /* SDRC region 0 public */
157         writel(UNLOCK_1, &sms_base->rg_att0);
160 /******************************************************************************
161  * Routine: secureworld_exit()
162  * Description: If chip is EMU and boot type is external
163  *              configure secure registers and exit secure world
164  *              general use.
165  *****************************************************************************/
166 void secureworld_exit()
168         unsigned long i;
170         /* configure non-secure access control register */
171         __asm__ __volatile__("mrc p15, 0, %0, c1, c1, 2":"=r"(i));
172         /* enabling co-processor CP10 and CP11 accesses in NS world */
173         __asm__ __volatile__("orr %0, %0, #0xC00":"=r"(i));
174         /*
175          * allow allocation of locked TLBs and L2 lines in NS world
176          * allow use of PLE registers in NS world also
177          */
178         __asm__ __volatile__("orr %0, %0, #0x70000":"=r"(i));
179         __asm__ __volatile__("mcr p15, 0, %0, c1, c1, 2":"=r"(i));
181         /* Enable ASA in ACR register */
182         __asm__ __volatile__("mrc p15, 0, %0, c1, c0, 1":"=r"(i));
183         __asm__ __volatile__("orr %0, %0, #0x10":"=r"(i));
184         __asm__ __volatile__("mcr p15, 0, %0, c1, c0, 1":"=r"(i));
186         /* Exiting secure world */
187         __asm__ __volatile__("mrc p15, 0, %0, c1, c1, 0":"=r"(i));
188         __asm__ __volatile__("orr %0, %0, #0x31":"=r"(i));
189         __asm__ __volatile__("mcr p15, 0, %0, c1, c1, 0":"=r"(i));
192 /******************************************************************************
193  * Routine: try_unlock_sram()
194  * Description: If chip is GP/EMU(special) type, unlock the SRAM for
195  *              general use.
196  *****************************************************************************/
197 void try_unlock_memory()
199         int mode;
200         int in_sdram = is_running_in_sdram();
202         /*
203          * if GP device unlock device SRAM for general use
204          * secure code breaks for Secure/Emulation device - HS/E/T
205          */
206         mode = get_device_type();
207         if (mode == GP_DEVICE)
208                 secure_unlock_mem();
210         /*
211          * If device is EMU and boot is XIP external booting
212          * Unlock firewalls and disable L2 and put chip
213          * out of secure world
214          *
215          * Assuming memories are unlocked by the demon who put us in SDRAM
216          */
217         if ((mode <= EMU_DEVICE) && (get_boot_type() == 0x1F)
218             && (!in_sdram)) {
219                 secure_unlock_mem();
220                 secureworld_exit();
221         }
223         return;
226 /******************************************************************************
227  * Routine: s_init
228  * Description: Does early system init of muxing and clocks.
229  *              - Called path is with SRAM stack.
230  *****************************************************************************/
231 void s_init(void)
233         int in_sdram = is_running_in_sdram();
235         watchdog_init();
237         try_unlock_memory();
239         /* Errata workarounds */
240         omap3_setup_aux_cr();
242 #ifndef CONFIG_SYS_L2CACHE_OFF
243         /* Invalidate L2-cache from secure mode */
244         omap3_invalidate_l2_cache_secure();
245 #endif
247         set_muxconf_regs();
248         sdelay(100);
250         prcm_init();
252         per_clocks_enable();
254 #ifdef CONFIG_USB_EHCI_OMAP
255         ehci_clocks_enable();
256 #endif
258 #ifdef CONFIG_SPL_BUILD
259         gd = &gdata;
261         preloader_console_init();
263         timer_init();
264 #endif
266         if (!in_sdram)
267                 mem_init();
270 /*
271  * Routine: misc_init_r
272  * Description: A basic misc_init_r that just displays the die ID
273  */
274 int __weak misc_init_r(void)
276         dieid_num_r();
278         return 0;
281 /******************************************************************************
282  * Routine: wait_for_command_complete
283  * Description: Wait for posting to finish on watchdog
284  *****************************************************************************/
285 void wait_for_command_complete(struct watchdog *wd_base)
287         int pending = 1;
288         do {
289                 pending = readl(&wd_base->wwps);
290         } while (pending);
293 /******************************************************************************
294  * Routine: watchdog_init
295  * Description: Shut down watch dogs
296  *****************************************************************************/
297 void watchdog_init(void)
299         struct watchdog *wd2_base = (struct watchdog *)WD2_BASE;
300         struct prcm *prcm_base = (struct prcm *)PRCM_BASE;
302         /*
303          * There are 3 watch dogs WD1=Secure, WD2=MPU, WD3=IVA. WD1 is
304          * either taken care of by ROM (HS/EMU) or not accessible (GP).
305          * We need to take care of WD2-MPU or take a PRCM reset. WD3
306          * should not be running and does not generate a PRCM reset.
307          */
309         sr32(&prcm_base->fclken_wkup, 5, 1, 1);
310         sr32(&prcm_base->iclken_wkup, 5, 1, 1);
311         wait_on_value(ST_WDT2, 0x20, &prcm_base->idlest_wkup, 5);
313         writel(WD_UNLOCK1, &wd2_base->wspr);
314         wait_for_command_complete(wd2_base);
315         writel(WD_UNLOCK2, &wd2_base->wspr);
318 /******************************************************************************
319  * Dummy function to handle errors for EABI incompatibility
320  *****************************************************************************/
321 void abort(void)
325 #if defined(CONFIG_NAND_OMAP_GPMC) & !defined(CONFIG_SPL_BUILD)
326 /******************************************************************************
327  * OMAP3 specific command to switch between NAND HW and SW ecc
328  *****************************************************************************/
329 static int do_switch_ecc(cmd_tbl_t * cmdtp, int flag, int argc, char * const argv[])
331         if (argc != 2)
332                 goto usage;
333         if (strncmp(argv[1], "hw", 2) == 0)
334                 omap_nand_switch_ecc(1);
335         else if (strncmp(argv[1], "sw", 2) == 0)
336                 omap_nand_switch_ecc(0);
337         else
338                 goto usage;
340         return 0;
342 usage:
343         printf ("Usage: nandecc %s\n", cmdtp->usage);
344         return 1;
347 U_BOOT_CMD(
348         nandecc, 2, 1,  do_switch_ecc,
349         "switch OMAP3 NAND ECC calculation algorithm",
350         "[hw/sw] - Switch between NAND hardware (hw) or software (sw) ecc algorithm"
351 );
353 #endif /* CONFIG_NAND_OMAP_GPMC & !CONFIG_SPL_BUILD */
355 #ifdef CONFIG_DISPLAY_BOARDINFO
356 /**
357  * Print board information
358  */
359 int checkboard (void)
361         char *mem_s ;
363         if (is_mem_sdr())
364                 mem_s = "mSDR";
365         else
366                 mem_s = "LPDDR";
368         printf("%s + %s/%s\n", sysinfo.board_string, mem_s,
369                         sysinfo.nand_string);
371         return 0;
373 #endif  /* CONFIG_DISPLAY_BOARDINFO */
375 static void omap3_emu_romcode_call(u32 service_id, u32 *parameters)
377         u32 i, num_params = *parameters;
378         u32 *sram_scratch_space = (u32 *)OMAP3_PUBLIC_SRAM_SCRATCH_AREA;
380         /*
381          * copy the parameters to an un-cached area to avoid coherency
382          * issues
383          */
384         for (i = 0; i < num_params; i++) {
385                 __raw_writel(*parameters, sram_scratch_space);
386                 parameters++;
387                 sram_scratch_space++;
388         }
390         /* Now make the PPA call */
391         do_omap3_emu_romcode_call(service_id, OMAP3_PUBLIC_SRAM_SCRATCH_AREA);
394 static void omap3_update_aux_cr_secure(u32 set_bits, u32 clear_bits)
396         u32 acr;
398         /* Read ACR */
399         asm volatile ("mrc p15, 0, %0, c1, c0, 1" : "=r" (acr));
400         acr &= ~clear_bits;
401         acr |= set_bits;
403         if (get_device_type() == GP_DEVICE) {
404                 omap3_gp_romcode_call(OMAP3_GP_ROMCODE_API_WRITE_ACR,
405                                        acr);
406         } else {
407                 struct emu_hal_params emu_romcode_params;
408                 emu_romcode_params.num_params = 1;
409                 emu_romcode_params.param1 = acr;
410                 omap3_emu_romcode_call(OMAP3_EMU_HAL_API_WRITE_ACR,
411                                        (u32 *)&emu_romcode_params);
412         }
415 static void omap3_setup_aux_cr(void)
417         /* Workaround for Cortex-A8 errata: #454179 #430973
418          *      Set "IBE" bit
419          *      Set "Disable Branch Size Mispredicts" bit
420          * Workaround for erratum #621766
421          *      Enable L1NEON bit
422          * ACR |= (IBE | DBSM | L1NEON) => ACR |= 0xE0
423          */
424         omap3_update_aux_cr_secure(0xE0, 0);
427 #ifndef CONFIG_SYS_L2CACHE_OFF
428 static void omap3_update_aux_cr(u32 set_bits, u32 clear_bits)
430         u32 acr;
432         /* Read ACR */
433         asm volatile ("mrc p15, 0, %0, c1, c0, 1" : "=r" (acr));
434         acr &= ~clear_bits;
435         acr |= set_bits;
437         /* Write ACR - affects non-secure banked bits */
438         asm volatile ("mcr p15, 0, %0, c1, c0, 1" : : "r" (acr));
441 /* Invalidate the entire L2 cache from secure mode */
442 static void omap3_invalidate_l2_cache_secure(void)
444         if (get_device_type() == GP_DEVICE) {
445                 omap3_gp_romcode_call(OMAP3_GP_ROMCODE_API_L2_INVAL,
446                                       0);
447         } else {
448                 struct emu_hal_params emu_romcode_params;
449                 emu_romcode_params.num_params = 1;
450                 emu_romcode_params.param1 = 0;
451                 omap3_emu_romcode_call(OMAP3_EMU_HAL_API_L2_INVAL,
452                                        (u32 *)&emu_romcode_params);
453         }
456 void v7_outer_cache_enable(void)
458         /* Set L2EN */
459         omap3_update_aux_cr_secure(0x2, 0);
461         /*
462          * On some revisions L2EN bit is banked on some revisions it's not
463          * No harm in setting both banked bits(in fact this is required
464          * by an erratum)
465          */
466         omap3_update_aux_cr(0x2, 0);
469 void omap3_outer_cache_disable(void)
471         /* Clear L2EN */
472         omap3_update_aux_cr_secure(0, 0x2);
474         /*
475          * On some revisions L2EN bit is banked on some revisions it's not
476          * No harm in clearing both banked bits(in fact this is required
477          * by an erratum)
478          */
479         omap3_update_aux_cr(0, 0x2);
481 #endif
483 #ifndef CONFIG_SYS_DCACHE_OFF
484 void enable_caches(void)
486         /* Enable D-cache. I-cache is already enabled in start.S */
487         dcache_enable();
489 #endif