]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/glsdk-u-boot.git/blob - arch/arm/cpu/armv7/omap3/sdrc.c
tools: imximage: Load a size that is multiple of 512
[glsdk/glsdk-u-boot.git] / arch / arm / cpu / armv7 / omap3 / sdrc.c
1 /*
2  * Functions related to OMAP3 SDRC.
3  *
4  * This file has been created after exctracting and consolidating
5  * the SDRC related content from mem.c and board.c, also created
6  * generic init function (mem_init).
7  *
8  * Copyright (C) 2004-2010
9  * Texas Instruments Incorporated - http://www.ti.com/
10  *
11  * Copyright (C) 2011
12  * Corscience GmbH & Co. KG - Simon Schwarz <schwarz@corscience.de>
13  *
14  * Author :
15  *     Vaibhav Hiremath <hvaibhav@ti.com>
16  *
17  * Original implementation by (mem.c, board.c) :
18  *      Sunil Kumar <sunilsaini05@gmail.com>
19  *      Shashi Ranjan <shashiranjanmca05@gmail.com>
20  *      Manikandan Pillai <mani.pillai@ti.com>
21  *
22  * This program is free software; you can redistribute it and/or
23  * modify it under the terms of the GNU General Public License as
24  * published by the Free Software Foundation; either version 2 of
25  * the License, or (at your option) any later version.
26  *
27  * This program is distributed in the hope that it will be useful,
28  * but WITHOUT ANY WARRANTY; without even the implied warranty of
29  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
30  * GNU General Public License for more details.
31  *
32  * You should have received a copy of the GNU General Public License
33  * along with this program; if not, write to the Free Software
34  * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
35  * MA 02111-1307 USA
36  */
38 #include <common.h>
39 #include <asm/io.h>
40 #include <asm/arch/mem.h>
41 #include <asm/arch/sys_proto.h>
43 DECLARE_GLOBAL_DATA_PTR;
44 extern omap3_sysinfo sysinfo;
46 static struct sdrc *sdrc_base = (struct sdrc *)OMAP34XX_SDRC_BASE;
48 /*
49  * is_mem_sdr -
50  *  - Return 1 if mem type in use is SDR
51  */
52 u32 is_mem_sdr(void)
53 {
54         if (readl(&sdrc_base->cs[CS0].mr) == SDRC_MR_0_SDR)
55                 return 1;
56         return 0;
57 }
59 /*
60  * make_cs1_contiguous -
61  * - When we have CS1 populated we want to have it mapped after cs0 to allow
62  *   command line mem=xyz use all memory with out discontinuous support
63  *   compiled in.  We could do it in the ATAG, but there really is two banks...
64  */
65 void make_cs1_contiguous(void)
66 {
67         u32 size, a_add_low, a_add_high;
69         size = get_sdr_cs_size(CS0);
70         size >>= 25;    /* divide by 32 MiB to find size to offset CS1 */
71         a_add_high = (size & 3) << 8;   /* set up low field */
72         a_add_low = (size & 0x3C) >> 2; /* set up high field */
73         writel((a_add_high | a_add_low), &sdrc_base->cs_cfg);
75 }
78 /*
79  * get_sdr_cs_size -
80  *  - Get size of chip select 0/1
81  */
82 u32 get_sdr_cs_size(u32 cs)
83 {
84         u32 size;
86         /* get ram size field */
87         size = readl(&sdrc_base->cs[cs].mcfg) >> 8;
88         size &= 0x3FF;          /* remove unwanted bits */
89         size <<= 21;            /* multiply by 2 MiB to find size in MB */
90         return size;
91 }
93 /*
94  * get_sdr_cs_offset -
95  *  - Get offset of cs from cs0 start
96  */
97 u32 get_sdr_cs_offset(u32 cs)
98 {
99         u32 offset;
101         if (!cs)
102                 return 0;
104         offset = readl(&sdrc_base->cs_cfg);
105         offset = (offset & 15) << 27 | (offset & 0x300) << 17;
107         return offset;
110 /*
111  * write_sdrc_timings -
112  *  - Takes CS and associated timings and initalize SDRAM
113  *  - Test CS to make sure it's OK for use
114  */
115 static void write_sdrc_timings(u32 cs, struct sdrc_actim *sdrc_actim_base,
116                 u32 mcfg, u32 ctrla, u32 ctrlb, u32 rfr_ctrl, u32 mr)
118         /* Setup timings we got from the board. */
119         writel(mcfg, &sdrc_base->cs[cs].mcfg);
120         writel(ctrla, &sdrc_actim_base->ctrla);
121         writel(ctrlb, &sdrc_actim_base->ctrlb);
122         writel(rfr_ctrl, &sdrc_base->cs[cs].rfr_ctrl);
123         writel(CMD_NOP, &sdrc_base->cs[cs].manual);
124         writel(CMD_PRECHARGE, &sdrc_base->cs[cs].manual);
125         writel(CMD_AUTOREFRESH, &sdrc_base->cs[cs].manual);
126         writel(CMD_AUTOREFRESH, &sdrc_base->cs[cs].manual);
127         writel(mr, &sdrc_base->cs[cs].mr);
129         /*
130          * Test ram in this bank
131          * Disable if bad or not present
132          */
133         if (!mem_ok(cs))
134                 writel(0, &sdrc_base->cs[cs].mcfg);
137 /*
138  * do_sdrc_init -
139  *  - Code called once in C-Stack only context for CS0 and with early being
140  *    true and a possible 2nd time depending on memory configuration from
141  *    stack+global context.
142  */
143 void do_sdrc_init(u32 cs, u32 early)
145         struct sdrc_actim *sdrc_actim_base0, *sdrc_actim_base1;
146         u32 mcfg, ctrla, ctrlb, rfr_ctrl, mr;
148         sdrc_actim_base0 = (struct sdrc_actim *)SDRC_ACTIM_CTRL0_BASE;
149         sdrc_actim_base1 = (struct sdrc_actim *)SDRC_ACTIM_CTRL1_BASE;
151         /*
152          * When called in the early context this may be SPL and we will
153          * need to set all of the timings.  This ends up being board
154          * specific so we call a helper function to take care of this
155          * for us.  Otherwise, to be safe, we need to copy the settings
156          * from the first bank to the second.  We will setup CS0,
157          * then set cs_cfg to the appropriate value then try and
158          * setup CS1.
159          */
160 #ifdef CONFIG_SPL_BUILD
161         get_board_mem_timings(&mcfg, &ctrla, &ctrlb, &rfr_ctrl, &mr);
162 #endif
163         if (early) {
164                 /* reset sdrc controller */
165                 writel(SOFTRESET, &sdrc_base->sysconfig);
166                 wait_on_value(RESETDONE, RESETDONE, &sdrc_base->status,
167                                 12000000);
168                 writel(0, &sdrc_base->sysconfig);
170                 /* setup sdrc to ball mux */
171                 writel(SDRC_SHARING, &sdrc_base->sharing);
173                 /* Disable Power Down of CKE because of 1 CKE on combo part */
174                 writel(WAKEUPPROC | SRFRONRESET | PAGEPOLICY_HIGH,
175                                 &sdrc_base->power);
177                 writel(ENADLL | DLLPHASE_90, &sdrc_base->dlla_ctrl);
178                 sdelay(0x20000);
179 #ifdef CONFIG_SPL_BUILD
180                 write_sdrc_timings(CS0, sdrc_actim_base0, mcfg, ctrla, ctrlb,
181                                 rfr_ctrl, mr);
182                 make_cs1_contiguous();
183                 write_sdrc_timings(CS1, sdrc_actim_base1, mcfg, ctrla, ctrlb,
184                                 rfr_ctrl, mr);
185 #endif
187         }
189         /*
190          * If we aren't using SPL we have been loaded by some
191          * other means which may not have correctly initialized
192          * both CS0 and CS1 (such as some older versions of x-loader)
193          * so we may be asked now to setup CS1.
194          */
195         if (cs == CS1) {
196                 mcfg = readl(&sdrc_base->cs[CS0].mcfg),
197                 rfr_ctrl = readl(&sdrc_base->cs[CS0].rfr_ctrl);
198                 ctrla = readl(&sdrc_actim_base0->ctrla),
199                 ctrlb = readl(&sdrc_actim_base0->ctrlb);
200                 mr = readl(&sdrc_base->cs[CS0].mr);
201                 write_sdrc_timings(cs, sdrc_actim_base1, mcfg, ctrla, ctrlb,
202                                 rfr_ctrl, mr);
204         }
207 /*
208  * dram_init -
209  *  - Sets uboots idea of sdram size
210  */
211 int dram_init(void)
213         unsigned int size0 = 0, size1 = 0;
215         size0 = get_sdr_cs_size(CS0);
216         /*
217          * We always need to have cs_cfg point at where the second
218          * bank would be, if present.  Failure to do so can lead to
219          * strange situations where memory isn't detected and
220          * configured correctly.  CS0 will already have been setup
221          * at this point.
222          */
223         make_cs1_contiguous();
224         do_sdrc_init(CS1, NOT_EARLY);
225         size1 = get_sdr_cs_size(CS1);
227         gd->ram_size = size0 + size1;
229         return 0;
232 void dram_init_banksize (void)
234         unsigned int size0 = 0, size1 = 0;
236         size0 = get_sdr_cs_size(CS0);
237         size1 = get_sdr_cs_size(CS1);
239         gd->bd->bi_dram[0].start = PHYS_SDRAM_1;
240         gd->bd->bi_dram[0].size = size0;
241         gd->bd->bi_dram[1].start = PHYS_SDRAM_1 + get_sdr_cs_offset(CS1);
242         gd->bd->bi_dram[1].size = size1;
245 /*
246  * mem_init -
247  *  - Init the sdrc chip,
248  *  - Selects CS0 and CS1,
249  */
250 void mem_init(void)
252         /* only init up first bank here */
253         do_sdrc_init(CS0, EARLY_INIT);