]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/glsdk-u-boot.git/blob - arch/arm/cpu/armv7/omap4/clocks.c
x86: Enable CONFIG_OF_CONTROL on coreboot
[glsdk/glsdk-u-boot.git] / arch / arm / cpu / armv7 / omap4 / clocks.c
1 /*
2  *
3  * Clock initialization for OMAP4
4  *
5  * (C) Copyright 2010
6  * Texas Instruments, <www.ti.com>
7  *
8  * Aneesh V <aneesh@ti.com>
9  *
10  * Based on previous work by:
11  *      Santosh Shilimkar <santosh.shilimkar@ti.com>
12  *      Rajendra Nayak <rnayak@ti.com>
13  *
14  * See file CREDITS for list of people who contributed to this
15  * project.
16  *
17  * This program is free software; you can redistribute it and/or
18  * modify it under the terms of the GNU General Public License as
19  * published by the Free Software Foundation; either version 2 of
20  * the License, or (at your option) any later version.
21  *
22  * This program is distributed in the hope that it will be useful,
23  * but WITHOUT ANY WARRANTY; without even the implied warranty of
24  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
25  * GNU General Public License for more details.
26  *
27  * You should have received a copy of the GNU General Public License
28  * along with this program; if not, write to the Free Software
29  * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
30  * MA 02111-1307 USA
31  */
32 #include <common.h>
33 #include <asm/omap_common.h>
34 #include <asm/gpio.h>
35 #include <asm/arch/clocks.h>
36 #include <asm/arch/sys_proto.h>
37 #include <asm/utils.h>
38 #include <asm/omap_gpio.h>
40 #ifndef CONFIG_SPL_BUILD
41 /*
42  * printing to console doesn't work unless
43  * this code is executed from SPL
44  */
45 #define printf(fmt, args...)
46 #define puts(s)
47 #endif /* !CONFIG_SPL_BUILD */
49 struct omap4_prcm_regs *const prcm = (struct omap4_prcm_regs *)0x4A004100;
51 const u32 sys_clk_array[8] = {
52         12000000,              /* 12 MHz */
53         13000000,              /* 13 MHz */
54         16800000,              /* 16.8 MHz */
55         19200000,              /* 19.2 MHz */
56         26000000,              /* 26 MHz */
57         27000000,              /* 27 MHz */
58         38400000,              /* 38.4 MHz */
59 };
61 /*
62  * The M & N values in the following tables are created using the
63  * following tool:
64  * tools/omap/clocks_get_m_n.c
65  * Please use this tool for creating the table for any new frequency.
66  */
68 /* dpll locked at 1400 MHz MPU clk at 700 MHz(OPP100) - DCC OFF */
69 static const struct dpll_params mpu_dpll_params_1400mhz[NUM_SYS_CLKS] = {
70         {175, 2, 1, -1, -1, -1, -1, -1},        /* 12 MHz   */
71         {700, 12, 1, -1, -1, -1, -1, -1},       /* 13 MHz   */
72         {125, 2, 1, -1, -1, -1, -1, -1},        /* 16.8 MHz */
73         {401, 10, 1, -1, -1, -1, -1, -1},       /* 19.2 MHz */
74         {350, 12, 1, -1, -1, -1, -1, -1},       /* 26 MHz   */
75         {700, 26, 1, -1, -1, -1, -1, -1},       /* 27 MHz   */
76         {638, 34, 1, -1, -1, -1, -1, -1}        /* 38.4 MHz */
77 };
79 /* dpll locked at 1584 MHz - MPU clk at 792 MHz(OPP Turbo 4430) */
80 static const struct dpll_params mpu_dpll_params_1600mhz[NUM_SYS_CLKS] = {
81         {200, 2, 1, -1, -1, -1, -1, -1},        /* 12 MHz   */
82         {800, 12, 1, -1, -1, -1, -1, -1},       /* 13 MHz   */
83         {619, 12, 1, -1, -1, -1, -1, -1},       /* 16.8 MHz */
84         {125, 2, 1, -1, -1, -1, -1, -1},        /* 19.2 MHz */
85         {400, 12, 1, -1, -1, -1, -1, -1},       /* 26 MHz   */
86         {800, 26, 1, -1, -1, -1, -1, -1},       /* 27 MHz   */
87         {125, 5, 1, -1, -1, -1, -1, -1}         /* 38.4 MHz */
88 };
90 /* dpll locked at 1200 MHz - MPU clk at 600 MHz */
91 static const struct dpll_params mpu_dpll_params_1200mhz[NUM_SYS_CLKS] = {
92         {50, 0, 1, -1, -1, -1, -1, -1},         /* 12 MHz   */
93         {600, 12, 1, -1, -1, -1, -1, -1},       /* 13 MHz   */
94         {250, 6, 1, -1, -1, -1, -1, -1},        /* 16.8 MHz */
95         {125, 3, 1, -1, -1, -1, -1, -1},        /* 19.2 MHz */
96         {300, 12, 1, -1, -1, -1, -1, -1},       /* 26 MHz   */
97         {200, 8, 1, -1, -1, -1, -1, -1},        /* 27 MHz   */
98         {125, 7, 1, -1, -1, -1, -1, -1}         /* 38.4 MHz */
99 };
101 static const struct dpll_params core_dpll_params_1600mhz[NUM_SYS_CLKS] = {
102         {200, 2, 1, 5, 8, 4, 6, 5},     /* 12 MHz   */
103         {800, 12, 1, 5, 8, 4, 6, 5},    /* 13 MHz   */
104         {619, 12, 1, 5, 8, 4, 6, 5},    /* 16.8 MHz */
105         {125, 2, 1, 5, 8, 4, 6, 5},     /* 19.2 MHz */
106         {400, 12, 1, 5, 8, 4, 6, 5},    /* 26 MHz   */
107         {800, 26, 1, 5, 8, 4, 6, 5},    /* 27 MHz   */
108         {125, 5, 1, 5, 8, 4, 6, 5}      /* 38.4 MHz */
109 };
111 static const struct dpll_params core_dpll_params_es1_1524mhz[NUM_SYS_CLKS] = {
112         {127, 1, 1, 5, 8, 4, 6, 5},     /* 12 MHz   */
113         {762, 12, 1, 5, 8, 4, 6, 5},    /* 13 MHz   */
114         {635, 13, 1, 5, 8, 4, 6, 5},    /* 16.8 MHz */
115         {635, 15, 1, 5, 8, 4, 6, 5},    /* 19.2 MHz */
116         {381, 12, 1, 5, 8, 4, 6, 5},    /* 26 MHz   */
117         {254, 8, 1, 5, 8, 4, 6, 5},     /* 27 MHz   */
118         {496, 24, 1, 5, 8, 4, 6, 5}     /* 38.4 MHz */
119 };
121 static const struct dpll_params
122                 core_dpll_params_es2_1600mhz_ddr200mhz[NUM_SYS_CLKS] = {
123         {200, 2, 2, 5, 8, 4, 6, 5},     /* 12 MHz   */
124         {800, 12, 2, 5, 8, 4, 6, 5},    /* 13 MHz   */
125         {619, 12, 2, 5, 8, 4, 6, 5},    /* 16.8 MHz */
126         {125, 2, 2, 5, 8, 4, 6, 5},     /* 19.2 MHz */
127         {400, 12, 2, 5, 8, 4, 6, 5},    /* 26 MHz   */
128         {800, 26, 2, 5, 8, 4, 6, 5},    /* 27 MHz   */
129         {125, 5, 2, 5, 8, 4, 6, 5}      /* 38.4 MHz */
130 };
132 static const struct dpll_params per_dpll_params_1536mhz[NUM_SYS_CLKS] = {
133         {64, 0, 8, 6, 12, 9, 4, 5},     /* 12 MHz   */
134         {768, 12, 8, 6, 12, 9, 4, 5},   /* 13 MHz   */
135         {320, 6, 8, 6, 12, 9, 4, 5},    /* 16.8 MHz */
136         {40, 0, 8, 6, 12, 9, 4, 5},     /* 19.2 MHz */
137         {384, 12, 8, 6, 12, 9, 4, 5},   /* 26 MHz   */
138         {256, 8, 8, 6, 12, 9, 4, 5},    /* 27 MHz   */
139         {20, 0, 8, 6, 12, 9, 4, 5}      /* 38.4 MHz */
140 };
142 static const struct dpll_params iva_dpll_params_1862mhz[NUM_SYS_CLKS] = {
143         {931, 11, -1, -1, 4, 7, -1, -1},        /* 12 MHz   */
144         {931, 12, -1, -1, 4, 7, -1, -1},        /* 13 MHz   */
145         {665, 11, -1, -1, 4, 7, -1, -1},        /* 16.8 MHz */
146         {727, 14, -1, -1, 4, 7, -1, -1},        /* 19.2 MHz */
147         {931, 25, -1, -1, 4, 7, -1, -1},        /* 26 MHz   */
148         {931, 26, -1, -1, 4, 7, -1, -1},        /* 27 MHz   */
149         {291, 11, -1, -1, 4, 7, -1, -1}         /* 38.4 MHz */
150 };
152 /* ABE M & N values with sys_clk as source */
153 static const struct dpll_params
154                 abe_dpll_params_sysclk_196608khz[NUM_SYS_CLKS] = {
155         {49, 5, 1, 1, -1, -1, -1, -1},  /* 12 MHz   */
156         {68, 8, 1, 1, -1, -1, -1, -1},  /* 13 MHz   */
157         {35, 5, 1, 1, -1, -1, -1, -1},  /* 16.8 MHz */
158         {46, 8, 1, 1, -1, -1, -1, -1},  /* 19.2 MHz */
159         {34, 8, 1, 1, -1, -1, -1, -1},  /* 26 MHz   */
160         {29, 7, 1, 1, -1, -1, -1, -1},  /* 27 MHz   */
161         {64, 24, 1, 1, -1, -1, -1, -1}  /* 38.4 MHz */
162 };
164 /* ABE M & N values with 32K clock as source */
165 static const struct dpll_params abe_dpll_params_32k_196608khz = {
166         750, 0, 1, 1, -1, -1, -1, -1
167 };
169 static const struct dpll_params usb_dpll_params_1920mhz[NUM_SYS_CLKS] = {
170         {80, 0, 2, -1, -1, -1, -1, -1},         /* 12 MHz   */
171         {960, 12, 2, -1, -1, -1, -1, -1},       /* 13 MHz   */
172         {400, 6, 2, -1, -1, -1, -1, -1},        /* 16.8 MHz */
173         {50, 0, 2, -1, -1, -1, -1, -1},         /* 19.2 MHz */
174         {480, 12, 2, -1, -1, -1, -1, -1},       /* 26 MHz   */
175         {320, 8, 2, -1, -1, -1, -1, -1},        /* 27 MHz   */
176         {25, 0, 2, -1, -1, -1, -1, -1}          /* 38.4 MHz */
177 };
179 void setup_post_dividers(u32 *const base, const struct dpll_params *params)
181         struct dpll_regs *const dpll_regs = (struct dpll_regs *)base;
183         /* Setup post-dividers */
184         if (params->m2 >= 0)
185                 writel(params->m2, &dpll_regs->cm_div_m2_dpll);
186         if (params->m3 >= 0)
187                 writel(params->m3, &dpll_regs->cm_div_m3_dpll);
188         if (params->m4 >= 0)
189                 writel(params->m4, &dpll_regs->cm_div_m4_dpll);
190         if (params->m5 >= 0)
191                 writel(params->m5, &dpll_regs->cm_div_m5_dpll);
192         if (params->m6 >= 0)
193                 writel(params->m6, &dpll_regs->cm_div_m6_dpll);
194         if (params->m7 >= 0)
195                 writel(params->m7, &dpll_regs->cm_div_m7_dpll);
198 /*
199  * Lock MPU dpll
200  *
201  * Resulting MPU frequencies:
202  * 4430 ES1.0   : 600 MHz
203  * 4430 ES2.x   : 792 MHz (OPP Turbo)
204  * 4460         : 920 MHz (OPP Turbo) - DCC disabled
205  */
206 const struct dpll_params *get_mpu_dpll_params(void)
208         u32 omap_rev, sysclk_ind;
210         omap_rev = omap_revision();
211         sysclk_ind = get_sys_clk_index();
213         if (omap_rev == OMAP4430_ES1_0)
214                 return &mpu_dpll_params_1200mhz[sysclk_ind];
215         else if (omap_rev < OMAP4460_ES1_0)
216                 return &mpu_dpll_params_1600mhz[sysclk_ind];
217         else
218                 return &mpu_dpll_params_1400mhz[sysclk_ind];
221 const struct dpll_params *get_core_dpll_params(void)
223         u32 sysclk_ind = get_sys_clk_index();
225         switch (omap_revision()) {
226         case OMAP4430_ES1_0:
227                 return &core_dpll_params_es1_1524mhz[sysclk_ind];
228         case OMAP4430_ES2_0:
229         case OMAP4430_SILICON_ID_INVALID:
230                  /* safest */
231                 return &core_dpll_params_es2_1600mhz_ddr200mhz[sysclk_ind];
232         default:
233                 return &core_dpll_params_1600mhz[sysclk_ind];
234         }
238 const struct dpll_params *get_per_dpll_params(void)
240         u32 sysclk_ind = get_sys_clk_index();
241         return &per_dpll_params_1536mhz[sysclk_ind];
244 const struct dpll_params *get_iva_dpll_params(void)
246         u32 sysclk_ind = get_sys_clk_index();
247         return &iva_dpll_params_1862mhz[sysclk_ind];
250 const struct dpll_params *get_usb_dpll_params(void)
252         u32 sysclk_ind = get_sys_clk_index();
253         return &usb_dpll_params_1920mhz[sysclk_ind];
256 const struct dpll_params *get_abe_dpll_params(void)
258 #ifdef CONFIG_SYS_OMAP_ABE_SYSCK
259         u32 sysclk_ind = get_sys_clk_index();
260         return &abe_dpll_params_sysclk_196608khz[sysclk_ind];
261 #else
262         return &abe_dpll_params_32k_196608khz;
263 #endif
266 /*
267  * Setup the voltages for vdd_mpu, vdd_core, and vdd_iva
268  * We set the maximum voltages allowed here because Smart-Reflex is not
269  * enabled in bootloader. Voltage initialization in the kernel will set
270  * these to the nominal values after enabling Smart-Reflex
271  */
272 void scale_vcores(void)
274         u32 volt, omap_rev;
276         omap_vc_init(PRM_VC_I2C_CHANNEL_FREQ_KHZ);
278         omap_rev = omap_revision();
280         /*
281          * Scale Voltage rails:
282          * 1. VDD_CORE
283          * 3. VDD_MPU
284          * 3. VDD_IVA
285          */
286         if (omap_rev < OMAP4460_ES1_0) {
287                 /*
288                  * OMAP4430:
289                  * VDD_CORE = TWL6030 VCORE3
290                  * VDD_MPU = TWL6030 VCORE1
291                  * VDD_IVA = TWL6030 VCORE2
292                  */
293                 volt = 1200;
294                 do_scale_vcore(SMPS_REG_ADDR_VCORE3, volt);
296                 /*
297                  * note on VDD_MPU:
298                  * Setting a high voltage for Nitro mode as smart reflex is not
299                  * enabled. We use the maximum possible value in the AVS range
300                  * because the next higher voltage in the discrete range
301                  * (code >= 0b111010) is way too high.
302                  */
303                 volt = 1325;
304                 do_scale_vcore(SMPS_REG_ADDR_VCORE1, volt);
305                 volt = 1200;
306                 do_scale_vcore(SMPS_REG_ADDR_VCORE2, volt);
308         } else {
309                 /*
310                  * OMAP4460:
311                  * VDD_CORE = TWL6030 VCORE1
312                  * VDD_MPU = TPS62361
313                  * VDD_IVA = TWL6030 VCORE2
314                  */
315                 volt = 1200;
316                 do_scale_vcore(SMPS_REG_ADDR_VCORE1, volt);
317                 /* TPS62361 */
318                 volt = 1203;
319                 do_scale_tps62361(TPS62361_VSEL0_GPIO,
320                                   TPS62361_REG_ADDR_SET1, volt);
321                 /* VCORE 2 - supplies vdd_iva */
322                 volt = 1200;
323                 do_scale_vcore(SMPS_REG_ADDR_VCORE2, volt);
324         }
327 u32 get_offset_code(u32 offset)
329         u32 offset_code, step = 12660; /* 12.66 mV represented in uV */
331         if (omap_revision() == OMAP4430_ES1_0)
332                 offset -= PHOENIX_SMPS_BASE_VOLT_STD_MODE_UV;
333         else
334                 offset -= PHOENIX_SMPS_BASE_VOLT_STD_MODE_WITH_OFFSET_UV;
336         offset_code = (offset + step - 1) / step;
338         /* The code starts at 1 not 0 */
339         return ++offset_code;
342 /*
343  * Enable essential clock domains, modules and
344  * do some additional special settings needed
345  */
346 void enable_basic_clocks(void)
348         u32 *const clk_domains_essential[] = {
349                 &prcm->cm_l4per_clkstctrl,
350                 &prcm->cm_l3init_clkstctrl,
351                 &prcm->cm_memif_clkstctrl,
352                 &prcm->cm_l4cfg_clkstctrl,
353                 0
354         };
356         u32 *const clk_modules_hw_auto_essential[] = {
357                 &prcm->cm_l3_2_gpmc_clkctrl,
358                 &prcm->cm_memif_emif_1_clkctrl,
359                 &prcm->cm_memif_emif_2_clkctrl,
360                 &prcm->cm_l4cfg_l4_cfg_clkctrl,
361                 &prcm->cm_wkup_gpio1_clkctrl,
362                 &prcm->cm_l4per_gpio2_clkctrl,
363                 &prcm->cm_l4per_gpio3_clkctrl,
364                 &prcm->cm_l4per_gpio4_clkctrl,
365                 &prcm->cm_l4per_gpio5_clkctrl,
366                 &prcm->cm_l4per_gpio6_clkctrl,
367                 0
368         };
370         u32 *const clk_modules_explicit_en_essential[] = {
371                 &prcm->cm_wkup_gptimer1_clkctrl,
372                 &prcm->cm_l3init_hsmmc1_clkctrl,
373                 &prcm->cm_l3init_hsmmc2_clkctrl,
374                 &prcm->cm_l4per_gptimer2_clkctrl,
375                 &prcm->cm_wkup_wdtimer2_clkctrl,
376                 &prcm->cm_l4per_uart3_clkctrl,
377                 0
378         };
380         /* Enable optional additional functional clock for GPIO4 */
381         setbits_le32(&prcm->cm_l4per_gpio4_clkctrl,
382                         GPIO4_CLKCTRL_OPTFCLKEN_MASK);
384         /* Enable 96 MHz clock for MMC1 & MMC2 */
385         setbits_le32(&prcm->cm_l3init_hsmmc1_clkctrl,
386                         HSMMC_CLKCTRL_CLKSEL_MASK);
387         setbits_le32(&prcm->cm_l3init_hsmmc2_clkctrl,
388                         HSMMC_CLKCTRL_CLKSEL_MASK);
390         /* Select 32KHz clock as the source of GPTIMER1 */
391         setbits_le32(&prcm->cm_wkup_gptimer1_clkctrl,
392                         GPTIMER1_CLKCTRL_CLKSEL_MASK);
394         /* Enable optional 48M functional clock for USB  PHY */
395         setbits_le32(&prcm->cm_l3init_usbphy_clkctrl,
396                         USBPHY_CLKCTRL_OPTFCLKEN_PHY_48M_MASK);
398         do_enable_clocks(clk_domains_essential,
399                          clk_modules_hw_auto_essential,
400                          clk_modules_explicit_en_essential,
401                          1);
404 void enable_basic_uboot_clocks(void)
406         u32 *const clk_domains_essential[] = {
407                 0
408         };
410         u32 *const clk_modules_hw_auto_essential[] = {
411                 &prcm->cm_l3init_hsusbotg_clkctrl,
412                 &prcm->cm_l3init_usbphy_clkctrl,
413                 &prcm->cm_l3init_usbphy_clkctrl,
414                 &prcm->cm_clksel_usb_60mhz,
415                 &prcm->cm_l3init_hsusbtll_clkctrl,
416                 0
417         };
419         u32 *const clk_modules_explicit_en_essential[] = {
420                 &prcm->cm_l4per_mcspi1_clkctrl,
421                 &prcm->cm_l4per_i2c1_clkctrl,
422                 &prcm->cm_l4per_i2c2_clkctrl,
423                 &prcm->cm_l4per_i2c3_clkctrl,
424                 &prcm->cm_l4per_i2c4_clkctrl,
425                 &prcm->cm_l3init_hsusbhost_clkctrl,
426                 0
427         };
429         do_enable_clocks(clk_domains_essential,
430                          clk_modules_hw_auto_essential,
431                          clk_modules_explicit_en_essential,
432                          1);
435 /*
436  * Enable non-essential clock domains, modules and
437  * do some additional special settings needed
438  */
439 void enable_non_essential_clocks(void)
441         u32 *const clk_domains_non_essential[] = {
442                 &prcm->cm_mpu_m3_clkstctrl,
443                 &prcm->cm_ivahd_clkstctrl,
444                 &prcm->cm_dsp_clkstctrl,
445                 &prcm->cm_dss_clkstctrl,
446                 &prcm->cm_sgx_clkstctrl,
447                 &prcm->cm1_abe_clkstctrl,
448                 &prcm->cm_c2c_clkstctrl,
449                 &prcm->cm_cam_clkstctrl,
450                 &prcm->cm_dss_clkstctrl,
451                 &prcm->cm_sdma_clkstctrl,
452                 0
453         };
455         u32 *const clk_modules_hw_auto_non_essential[] = {
456                 &prcm->cm_l3instr_l3_3_clkctrl,
457                 &prcm->cm_l3instr_l3_instr_clkctrl,
458                 &prcm->cm_l3instr_intrconn_wp1_clkctrl,
459                 &prcm->cm_l3init_hsi_clkctrl,
460                 0
461         };
463         u32 *const clk_modules_explicit_en_non_essential[] = {
464                 &prcm->cm1_abe_aess_clkctrl,
465                 &prcm->cm1_abe_pdm_clkctrl,
466                 &prcm->cm1_abe_dmic_clkctrl,
467                 &prcm->cm1_abe_mcasp_clkctrl,
468                 &prcm->cm1_abe_mcbsp1_clkctrl,
469                 &prcm->cm1_abe_mcbsp2_clkctrl,
470                 &prcm->cm1_abe_mcbsp3_clkctrl,
471                 &prcm->cm1_abe_slimbus_clkctrl,
472                 &prcm->cm1_abe_timer5_clkctrl,
473                 &prcm->cm1_abe_timer6_clkctrl,
474                 &prcm->cm1_abe_timer7_clkctrl,
475                 &prcm->cm1_abe_timer8_clkctrl,
476                 &prcm->cm1_abe_wdt3_clkctrl,
477                 &prcm->cm_l4per_gptimer9_clkctrl,
478                 &prcm->cm_l4per_gptimer10_clkctrl,
479                 &prcm->cm_l4per_gptimer11_clkctrl,
480                 &prcm->cm_l4per_gptimer3_clkctrl,
481                 &prcm->cm_l4per_gptimer4_clkctrl,
482                 &prcm->cm_l4per_hdq1w_clkctrl,
483                 &prcm->cm_l4per_mcbsp4_clkctrl,
484                 &prcm->cm_l4per_mcspi2_clkctrl,
485                 &prcm->cm_l4per_mcspi3_clkctrl,
486                 &prcm->cm_l4per_mcspi4_clkctrl,
487                 &prcm->cm_l4per_mmcsd3_clkctrl,
488                 &prcm->cm_l4per_mmcsd4_clkctrl,
489                 &prcm->cm_l4per_mmcsd5_clkctrl,
490                 &prcm->cm_l4per_uart1_clkctrl,
491                 &prcm->cm_l4per_uart2_clkctrl,
492                 &prcm->cm_l4per_uart4_clkctrl,
493                 &prcm->cm_wkup_keyboard_clkctrl,
494                 &prcm->cm_wkup_wdtimer2_clkctrl,
495                 &prcm->cm_cam_iss_clkctrl,
496                 &prcm->cm_cam_fdif_clkctrl,
497                 &prcm->cm_dss_dss_clkctrl,
498                 &prcm->cm_sgx_sgx_clkctrl,
499                 0
500         };
502         /* Enable optional functional clock for ISS */
503         setbits_le32(&prcm->cm_cam_iss_clkctrl, ISS_CLKCTRL_OPTFCLKEN_MASK);
505         /* Enable all optional functional clocks of DSS */
506         setbits_le32(&prcm->cm_dss_dss_clkctrl, DSS_CLKCTRL_OPTFCLKEN_MASK);
508         do_enable_clocks(clk_domains_non_essential,
509                          clk_modules_hw_auto_non_essential,
510                          clk_modules_explicit_en_non_essential,
511                          0);
513         /* Put camera module in no sleep mode */
514         clrsetbits_le32(&prcm->cm_cam_clkstctrl, MODULE_CLKCTRL_MODULEMODE_MASK,
515                         CD_CLKCTRL_CLKTRCTRL_NO_SLEEP <<
516                         MODULE_CLKCTRL_MODULEMODE_SHIFT);