]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/glsdk-u-boot.git/blob - arch/arm/cpu/armv7/omap4/clocks.c
omap4: clock init support for omap4460
[glsdk/glsdk-u-boot.git] / arch / arm / cpu / armv7 / omap4 / clocks.c
1 /*
2  *
3  * Clock initialization for OMAP4
4  *
5  * (C) Copyright 2010
6  * Texas Instruments, <www.ti.com>
7  *
8  * Aneesh V <aneesh@ti.com>
9  *
10  * Based on previous work by:
11  *      Santosh Shilimkar <santosh.shilimkar@ti.com>
12  *      Rajendra Nayak <rnayak@ti.com>
13  *
14  * See file CREDITS for list of people who contributed to this
15  * project.
16  *
17  * This program is free software; you can redistribute it and/or
18  * modify it under the terms of the GNU General Public License as
19  * published by the Free Software Foundation; either version 2 of
20  * the License, or (at your option) any later version.
21  *
22  * This program is distributed in the hope that it will be useful,
23  * but WITHOUT ANY WARRANTY; without even the implied warranty of
24  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
25  * GNU General Public License for more details.
26  *
27  * You should have received a copy of the GNU General Public License
28  * along with this program; if not, write to the Free Software
29  * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
30  * MA 02111-1307 USA
31  */
32 #include <common.h>
33 #include <asm/omap_common.h>
34 #include <asm/arch/clocks.h>
35 #include <asm/arch/sys_proto.h>
36 #include <asm/utils.h>
37 #include <asm/omap_gpio.h>
39 #ifndef CONFIG_SPL_BUILD
40 /*
41  * printing to console doesn't work unless
42  * this code is executed from SPL
43  */
44 #define printf(fmt, args...)
45 #define puts(s)
46 #endif
48 #define abs(x) (((x) < 0) ? ((x)*-1) : (x))
50 struct omap4_prcm_regs *const prcm = (struct omap4_prcm_regs *)0x4A004100;
52 static const u32 sys_clk_array[8] = {
53         12000000,              /* 12 MHz */
54         13000000,              /* 13 MHz */
55         16800000,              /* 16.8 MHz */
56         19200000,              /* 19.2 MHz */
57         26000000,              /* 26 MHz */
58         27000000,              /* 27 MHz */
59         38400000,              /* 38.4 MHz */
60 };
62 /*
63  * The M & N values in the following tables are created using the
64  * following tool:
65  * tools/omap/clocks_get_m_n.c
66  * Please use this tool for creating the table for any new frequency.
67  */
69 /* dpll locked at 1840 MHz MPU clk at 920 MHz(OPP Turbo 4460) - DCC OFF */
70 static const struct dpll_params mpu_dpll_params_1840mhz[NUM_SYS_CLKS] = {
71         {230, 2, 1, -1, -1, -1, -1, -1},        /* 12 MHz   */
72         {920, 12, 1, -1, -1, -1, -1, -1},       /* 13 MHz   */
73         {219, 3, 1, -1, -1, -1, -1, -1},        /* 16.8 MHz */
74         {575, 11, 1, -1, -1, -1, -1, -1},       /* 19.2 MHz */
75         {460, 12, 1, -1, -1, -1, -1, -1},       /* 26 MHz   */
76         {920, 26, 1, -1, -1, -1, -1, -1},       /* 27 MHz   */
77         {575, 23, 1, -1, -1, -1, -1, -1}        /* 38.4 MHz */
78 };
80 /* dpll locked at 1584 MHz - MPU clk at 792 MHz(OPP Turbo 4430) */
81 static const struct dpll_params mpu_dpll_params_1584mhz[NUM_SYS_CLKS] = {
82         {66, 0, 1, -1, -1, -1, -1, -1},         /* 12 MHz   */
83         {792, 12, 1, -1, -1, -1, -1, -1},       /* 13 MHz   */
84         {330, 6, 1, -1, -1, -1, -1, -1},        /* 16.8 MHz */
85         {165, 3, 1, -1, -1, -1, -1, -1},        /* 19.2 MHz */
86         {396, 12, 1, -1, -1, -1, -1, -1},       /* 26 MHz   */
87         {88, 2, 1, -1, -1, -1, -1, -1},         /* 27 MHz   */
88         {165, 7, 1, -1, -1, -1, -1, -1}         /* 38.4 MHz */
89 };
91 /* dpll locked at 1200 MHz - MPU clk at 600 MHz */
92 static const struct dpll_params mpu_dpll_params_1200mhz[NUM_SYS_CLKS] = {
93         {50, 0, 1, -1, -1, -1, -1, -1},         /* 12 MHz   */
94         {600, 12, 1, -1, -1, -1, -1, -1},       /* 13 MHz   */
95         {250, 6, 1, -1, -1, -1, -1, -1},        /* 16.8 MHz */
96         {125, 3, 1, -1, -1, -1, -1, -1},        /* 19.2 MHz */
97         {300, 12, 1, -1, -1, -1, -1, -1},       /* 26 MHz   */
98         {200, 8, 1, -1, -1, -1, -1, -1},        /* 27 MHz   */
99         {125, 7, 1, -1, -1, -1, -1, -1}         /* 38.4 MHz */
100 };
102 static const struct dpll_params core_dpll_params_1600mhz[NUM_SYS_CLKS] = {
103         {200, 2, 1, 5, 8, 4, 6, 5},     /* 12 MHz   */
104         {800, 12, 1, 5, 8, 4, 6, 5},    /* 13 MHz   */
105         {619, 12, 1, 5, 8, 4, 6, 5},    /* 16.8 MHz */
106         {125, 2, 1, 5, 8, 4, 6, 5},     /* 19.2 MHz */
107         {400, 12, 1, 5, 8, 4, 6, 5},    /* 26 MHz   */
108         {800, 26, 1, 5, 8, 4, 6, 5},    /* 27 MHz   */
109         {125, 5, 1, 5, 8, 4, 6, 5}      /* 38.4 MHz */
110 };
112 static const struct dpll_params core_dpll_params_es1_1524mhz[NUM_SYS_CLKS] = {
113         {127, 1, 1, 5, 8, 4, 6, 5},     /* 12 MHz   */
114         {762, 12, 1, 5, 8, 4, 6, 5},    /* 13 MHz   */
115         {635, 13, 1, 5, 8, 4, 6, 5},    /* 16.8 MHz */
116         {635, 15, 1, 5, 8, 4, 6, 5},    /* 19.2 MHz */
117         {381, 12, 1, 5, 8, 4, 6, 5},    /* 26 MHz   */
118         {254, 8, 1, 5, 8, 4, 6, 5},     /* 27 MHz   */
119         {496, 24, 1, 5, 8, 4, 6, 5}     /* 38.4 MHz */
120 };
122 static const struct dpll_params
123                 core_dpll_params_es2_1600mhz_ddr200mhz[NUM_SYS_CLKS] = {
124         {200, 2, 2, 5, 8, 4, 6, 5},     /* 12 MHz   */
125         {800, 12, 2, 5, 8, 4, 6, 5},    /* 13 MHz   */
126         {619, 12, 2, 5, 8, 4, 6, 5},    /* 16.8 MHz */
127         {125, 2, 2, 5, 8, 4, 6, 5},     /* 19.2 MHz */
128         {400, 12, 2, 5, 8, 4, 6, 5},    /* 26 MHz   */
129         {800, 26, 2, 5, 8, 4, 6, 5},    /* 27 MHz   */
130         {125, 5, 2, 5, 8, 4, 6, 5}      /* 38.4 MHz */
131 };
133 static const struct dpll_params per_dpll_params_1536mhz[NUM_SYS_CLKS] = {
134         {64, 0, 8, 6, 12, 9, 4, 5},     /* 12 MHz   */
135         {768, 12, 8, 6, 12, 9, 4, 5},   /* 13 MHz   */
136         {320, 6, 8, 6, 12, 9, 4, 5},    /* 16.8 MHz */
137         {40, 0, 8, 6, 12, 9, 4, 5},     /* 19.2 MHz */
138         {384, 12, 8, 6, 12, 9, 4, 5},   /* 26 MHz   */
139         {256, 8, 8, 6, 12, 9, 4, 5},    /* 27 MHz   */
140         {20, 0, 8, 6, 12, 9, 4, 5}      /* 38.4 MHz */
141 };
143 static const struct dpll_params iva_dpll_params_1862mhz[NUM_SYS_CLKS] = {
144         {931, 11, -1, -1, 4, 7, -1, -1},        /* 12 MHz   */
145         {931, 12, -1, -1, 4, 7, -1, -1},        /* 13 MHz   */
146         {665, 11, -1, -1, 4, 7, -1, -1},        /* 16.8 MHz */
147         {727, 14, -1, -1, 4, 7, -1, -1},        /* 19.2 MHz */
148         {931, 25, -1, -1, 4, 7, -1, -1},        /* 26 MHz   */
149         {931, 26, -1, -1, 4, 7, -1, -1},        /* 27 MHz   */
150         {412, 16, -1, -1, 4, 7, -1, -1}         /* 38.4 MHz */
151 };
153 /* ABE M & N values with sys_clk as source */
154 static const struct dpll_params
155                 abe_dpll_params_sysclk_196608khz[NUM_SYS_CLKS] = {
156         {49, 5, 1, 1, -1, -1, -1, -1},  /* 12 MHz   */
157         {68, 8, 1, 1, -1, -1, -1, -1},  /* 13 MHz   */
158         {35, 5, 1, 1, -1, -1, -1, -1},  /* 16.8 MHz */
159         {46, 8, 1, 1, -1, -1, -1, -1},  /* 19.2 MHz */
160         {34, 8, 1, 1, -1, -1, -1, -1},  /* 26 MHz   */
161         {29, 7, 1, 1, -1, -1, -1, -1},  /* 27 MHz   */
162         {64, 24, 1, 1, -1, -1, -1, -1}  /* 38.4 MHz */
163 };
165 /* ABE M & N values with 32K clock as source */
166 static const struct dpll_params abe_dpll_params_32k_196608khz = {
167         750, 0, 1, 1, -1, -1, -1, -1
168 };
171 static const struct dpll_params usb_dpll_params_1920mhz[NUM_SYS_CLKS] = {
172         {80, 0, 2, -1, -1, -1, -1, -1},         /* 12 MHz   */
173         {960, 12, 2, -1, -1, -1, -1, -1},       /* 13 MHz   */
174         {400, 6, 2, -1, -1, -1, -1, -1},        /* 16.8 MHz */
175         {50, 0, 2, -1, -1, -1, -1, -1},         /* 19.2 MHz */
176         {480, 12, 2, -1, -1, -1, -1, -1},       /* 26 MHz   */
177         {320, 8, 2, -1, -1, -1, -1, -1},        /* 27 MHz   */
178         {25, 0, 2, -1, -1, -1, -1, -1}          /* 38.4 MHz */
179 };
181 static inline u32 __get_sys_clk_index(void)
183         u32 ind;
184         /*
185          * For ES1 the ROM code calibration of sys clock is not reliable
186          * due to hw issue. So, use hard-coded value. If this value is not
187          * correct for any board over-ride this function in board file
188          * From ES2.0 onwards you will get this information from
189          * CM_SYS_CLKSEL
190          */
191         if (omap_revision() == OMAP4430_ES1_0)
192                 ind = OMAP_SYS_CLK_IND_38_4_MHZ;
193         else {
194                 /* SYS_CLKSEL - 1 to match the dpll param array indices */
195                 ind = (readl(&prcm->cm_sys_clksel) &
196                         CM_SYS_CLKSEL_SYS_CLKSEL_MASK) - 1;
197         }
198         return ind;
201 u32 get_sys_clk_index(void)
202         __attribute__ ((weak, alias("__get_sys_clk_index")));
204 u32 get_sys_clk_freq(void)
206         u8 index = get_sys_clk_index();
207         return sys_clk_array[index];
210 static inline void do_bypass_dpll(u32 *const base)
212         struct dpll_regs *dpll_regs = (struct dpll_regs *)base;
214         clrsetbits_le32(&dpll_regs->cm_clkmode_dpll,
215                         CM_CLKMODE_DPLL_DPLL_EN_MASK,
216                         DPLL_EN_FAST_RELOCK_BYPASS <<
217                         CM_CLKMODE_DPLL_EN_SHIFT);
220 static inline void wait_for_bypass(u32 *const base)
222         struct dpll_regs *const dpll_regs = (struct dpll_regs *)base;
224         if (!wait_on_value(ST_DPLL_CLK_MASK, 0, &dpll_regs->cm_idlest_dpll,
225                                 LDELAY)) {
226                 printf("Bypassing DPLL failed %p\n", base);
227         }
230 static inline void do_lock_dpll(u32 *const base)
232         struct dpll_regs *const dpll_regs = (struct dpll_regs *)base;
234         clrsetbits_le32(&dpll_regs->cm_clkmode_dpll,
235                       CM_CLKMODE_DPLL_DPLL_EN_MASK,
236                       DPLL_EN_LOCK << CM_CLKMODE_DPLL_EN_SHIFT);
239 static inline void wait_for_lock(u32 *const base)
241         struct dpll_regs *const dpll_regs = (struct dpll_regs *)base;
243         if (!wait_on_value(ST_DPLL_CLK_MASK, ST_DPLL_CLK_MASK,
244                 &dpll_regs->cm_idlest_dpll, LDELAY)) {
245                 printf("DPLL locking failed for %p\n", base);
246                 hang();
247         }
250 static void do_setup_dpll(u32 *const base, const struct dpll_params *params,
251                                 u8 lock)
253         u32 temp;
254         struct dpll_regs *const dpll_regs = (struct dpll_regs *)base;
256         bypass_dpll(base);
258         /* Set M & N */
259         temp = readl(&dpll_regs->cm_clksel_dpll);
261         temp &= ~CM_CLKSEL_DPLL_M_MASK;
262         temp |= (params->m << CM_CLKSEL_DPLL_M_SHIFT) & CM_CLKSEL_DPLL_M_MASK;
264         temp &= ~CM_CLKSEL_DPLL_N_MASK;
265         temp |= (params->n << CM_CLKSEL_DPLL_N_SHIFT) & CM_CLKSEL_DPLL_N_MASK;
267         writel(temp, &dpll_regs->cm_clksel_dpll);
269         /* Lock */
270         if (lock)
271                 do_lock_dpll(base);
273         /* Setup post-dividers */
274         if (params->m2 >= 0)
275                 writel(params->m2, &dpll_regs->cm_div_m2_dpll);
276         if (params->m3 >= 0)
277                 writel(params->m3, &dpll_regs->cm_div_m3_dpll);
278         if (params->m4 >= 0)
279                 writel(params->m4, &dpll_regs->cm_div_m4_dpll);
280         if (params->m5 >= 0)
281                 writel(params->m5, &dpll_regs->cm_div_m5_dpll);
282         if (params->m6 >= 0)
283                 writel(params->m6, &dpll_regs->cm_div_m6_dpll);
284         if (params->m7 >= 0)
285                 writel(params->m7, &dpll_regs->cm_div_m7_dpll);
287         /* Wait till the DPLL locks */
288         if (lock)
289                 wait_for_lock(base);
292 const struct dpll_params *get_core_dpll_params(void)
294         u32 sysclk_ind = get_sys_clk_index();
296         switch (omap_revision()) {
297         case OMAP4430_ES1_0:
298                 return &core_dpll_params_es1_1524mhz[sysclk_ind];
299         case OMAP4430_ES2_0:
300         case OMAP4430_SILICON_ID_INVALID:
301                  /* safest */
302                 return &core_dpll_params_es2_1600mhz_ddr200mhz[sysclk_ind];
303         default:
304                 return &core_dpll_params_1600mhz[sysclk_ind];
305         }
308 u32 omap4_ddr_clk(void)
310         u32 ddr_clk, sys_clk_khz;
311         const struct dpll_params *core_dpll_params;
313         sys_clk_khz = get_sys_clk_freq() / 1000;
315         core_dpll_params = get_core_dpll_params();
317         debug("sys_clk %d\n ", sys_clk_khz * 1000);
319         /* Find Core DPLL locked frequency first */
320         ddr_clk = sys_clk_khz * 2 * core_dpll_params->m /
321                         (core_dpll_params->n + 1);
322         /*
323          * DDR frequency is PHY_ROOT_CLK/2
324          * PHY_ROOT_CLK = Fdpll/2/M2
325          */
326         ddr_clk = ddr_clk / 4 / core_dpll_params->m2;
328         ddr_clk *= 1000;        /* convert to Hz */
329         debug("ddr_clk %d\n ", ddr_clk);
331         return ddr_clk;
334 /*
335  * Lock MPU dpll
336  *
337  * Resulting MPU frequencies:
338  * 4430 ES1.0   : 600 MHz
339  * 4430 ES2.x   : 792 MHz (OPP Turbo)
340  * 4460         : 920 MHz (OPP Turbo) - DCC disabled
341  */
342 void configure_mpu_dpll(void)
344         const struct dpll_params *params;
345         struct dpll_regs *mpu_dpll_regs;
346         u32 omap4_rev, sysclk_ind;
348         omap4_rev = omap_revision();
349         sysclk_ind = get_sys_clk_index();
351         if (omap4_rev == OMAP4430_ES1_0)
352                 params = &mpu_dpll_params_1200mhz[sysclk_ind];
353         else if (omap4_rev < OMAP4460_ES1_0)
354                 params = &mpu_dpll_params_1584mhz[sysclk_ind];
355         else
356                 params = &mpu_dpll_params_1840mhz[sysclk_ind];
358         /* DCC and clock divider settings for 4460 */
359         if (omap4_rev >= OMAP4460_ES1_0) {
360                 mpu_dpll_regs =
361                         (struct dpll_regs *)&prcm->cm_clkmode_dpll_mpu;
362                 bypass_dpll(&prcm->cm_clkmode_dpll_mpu);
363                 clrbits_le32(&prcm->cm_mpu_mpu_clkctrl,
364                         MPU_CLKCTRL_CLKSEL_EMIF_DIV_MODE_MASK);
365                 setbits_le32(&prcm->cm_mpu_mpu_clkctrl,
366                         MPU_CLKCTRL_CLKSEL_ABE_DIV_MODE_MASK);
367                 clrbits_le32(&mpu_dpll_regs->cm_clksel_dpll,
368                         CM_CLKSEL_DCC_EN_MASK);
369         }
371         do_setup_dpll(&prcm->cm_clkmode_dpll_mpu, params, DPLL_LOCK);
372         debug("MPU DPLL locked\n");
375 static void setup_dplls(void)
377         u32 sysclk_ind, temp;
378         const struct dpll_params *params;
379         debug("setup_dplls\n");
381         sysclk_ind = get_sys_clk_index();
383         /* CORE dpll */
384         params = get_core_dpll_params();        /* default - safest */
385         /*
386          * Do not lock the core DPLL now. Just set it up.
387          * Core DPLL will be locked after setting up EMIF
388          * using the FREQ_UPDATE method(freq_update_core())
389          */
390         do_setup_dpll(&prcm->cm_clkmode_dpll_core, params, DPLL_NO_LOCK);
391         /* Set the ratios for CORE_CLK, L3_CLK, L4_CLK */
392         temp = (CLKSEL_CORE_X2_DIV_1 << CLKSEL_CORE_SHIFT) |
393             (CLKSEL_L3_CORE_DIV_2 << CLKSEL_L3_SHIFT) |
394             (CLKSEL_L4_L3_DIV_2 << CLKSEL_L4_SHIFT);
395         writel(temp, &prcm->cm_clksel_core);
396         debug("Core DPLL configured\n");
398         /* lock PER dpll */
399         do_setup_dpll(&prcm->cm_clkmode_dpll_per,
400                         &per_dpll_params_1536mhz[sysclk_ind], DPLL_LOCK);
401         debug("PER DPLL locked\n");
403         /* MPU dpll */
404         configure_mpu_dpll();
407 static void setup_non_essential_dplls(void)
409         u32 sys_clk_khz, abe_ref_clk;
410         u32 sysclk_ind, sd_div, num, den;
411         const struct dpll_params *params;
413         sysclk_ind = get_sys_clk_index();
414         sys_clk_khz = get_sys_clk_freq() / 1000;
416         /* IVA */
417         clrsetbits_le32(&prcm->cm_bypclk_dpll_iva,
418                 CM_BYPCLK_DPLL_IVA_CLKSEL_MASK, DPLL_IVA_CLKSEL_CORE_X2_DIV_2);
420         do_setup_dpll(&prcm->cm_clkmode_dpll_iva,
421                         &iva_dpll_params_1862mhz[sysclk_ind], DPLL_LOCK);
423         /*
424          * USB:
425          * USB dpll is J-type. Need to set DPLL_SD_DIV for jitter correction
426          * DPLL_SD_DIV = CEILING ([DPLL_MULT/(DPLL_DIV+1)]* CLKINP / 250)
427          *      - where CLKINP is sys_clk in MHz
428          * Use CLKINP in KHz and adjust the denominator accordingly so
429          * that we have enough accuracy and at the same time no overflow
430          */
431         params = &usb_dpll_params_1920mhz[sysclk_ind];
432         num = params->m * sys_clk_khz;
433         den = (params->n + 1) * 250 * 1000;
434         num += den - 1;
435         sd_div = num / den;
436         clrsetbits_le32(&prcm->cm_clksel_dpll_usb,
437                         CM_CLKSEL_DPLL_DPLL_SD_DIV_MASK,
438                         sd_div << CM_CLKSEL_DPLL_DPLL_SD_DIV_SHIFT);
440         /* Now setup the dpll with the regular function */
441         do_setup_dpll(&prcm->cm_clkmode_dpll_usb, params, DPLL_LOCK);
443 #ifdef CONFIG_SYS_OMAP4_ABE_SYSCK
444         params = &abe_dpll_params_sysclk_196608khz[sysclk_ind];
445         abe_ref_clk = CM_ABE_PLL_REF_CLKSEL_CLKSEL_SYSCLK;
446 #else
447         params = &abe_dpll_params_32k_196608khz;
448         abe_ref_clk = CM_ABE_PLL_REF_CLKSEL_CLKSEL_32KCLK;
449         /*
450          * We need to enable some additional options to achieve
451          * 196.608MHz from 32768 Hz
452          */
453         setbits_le32(&prcm->cm_clkmode_dpll_abe,
454                         CM_CLKMODE_DPLL_DRIFTGUARD_EN_MASK|
455                         CM_CLKMODE_DPLL_RELOCK_RAMP_EN_MASK|
456                         CM_CLKMODE_DPLL_LPMODE_EN_MASK|
457                         CM_CLKMODE_DPLL_REGM4XEN_MASK);
458         /* Spend 4 REFCLK cycles at each stage */
459         clrsetbits_le32(&prcm->cm_clkmode_dpll_abe,
460                         CM_CLKMODE_DPLL_RAMP_RATE_MASK,
461                         1 << CM_CLKMODE_DPLL_RAMP_RATE_SHIFT);
462 #endif
464         /* Select the right reference clk */
465         clrsetbits_le32(&prcm->cm_abe_pll_ref_clksel,
466                         CM_ABE_PLL_REF_CLKSEL_CLKSEL_MASK,
467                         abe_ref_clk << CM_ABE_PLL_REF_CLKSEL_CLKSEL_SHIFT);
468         /* Lock the dpll */
469         do_setup_dpll(&prcm->cm_clkmode_dpll_abe, params, DPLL_LOCK);
472 static void do_scale_tps62361(u32 reg, u32 volt_mv)
474         u32 temp, step;
476         step = volt_mv - TPS62361_BASE_VOLT_MV;
477         step /= 10;
479         /*
480          * Select SET1 in TPS62361:
481          * VSEL1 is grounded on board. So the following selects
482          * VSEL1 = 0 and VSEL0 = 1
483          */
484         omap_set_gpio_direction(TPS62361_VSEL0_GPIO, 0);
485         omap_set_gpio_dataout(TPS62361_VSEL0_GPIO, 1);
487         temp = TPS62361_I2C_SLAVE_ADDR |
488             (reg << PRM_VC_VAL_BYPASS_REGADDR_SHIFT) |
489             (step << PRM_VC_VAL_BYPASS_DATA_SHIFT) |
490             PRM_VC_VAL_BYPASS_VALID_BIT;
491         debug("do_scale_tps62361: volt - %d step - 0x%x\n", volt_mv, step);
493         writel(temp, &prcm->prm_vc_val_bypass);
494         if (!wait_on_value(PRM_VC_VAL_BYPASS_VALID_BIT, 0,
495                                 &prcm->prm_vc_val_bypass, LDELAY)) {
496                 puts("Scaling voltage failed for vdd_mpu from TPS\n");
497         }
500 static void do_scale_vcore(u32 vcore_reg, u32 volt_mv)
502         u32 temp, offset_code;
503         u32 step = 12660; /* 12.66 mV represented in uV */
504         u32 offset = volt_mv;
506         /* convert to uV for better accuracy in the calculations */
507         offset *= 1000;
509         if (omap_revision() == OMAP4430_ES1_0)
510                 offset -= PHOENIX_SMPS_BASE_VOLT_STD_MODE_UV;
511         else
512                 offset -= PHOENIX_SMPS_BASE_VOLT_STD_MODE_WITH_OFFSET_UV;
514         offset_code = (offset + step - 1) / step;
515         /* The code starts at 1 not 0 */
516         offset_code++;
518         debug("do_scale_vcore: volt - %d offset_code - 0x%x\n", volt_mv,
519                 offset_code);
521         temp = SMPS_I2C_SLAVE_ADDR |
522             (vcore_reg << PRM_VC_VAL_BYPASS_REGADDR_SHIFT) |
523             (offset_code << PRM_VC_VAL_BYPASS_DATA_SHIFT) |
524             PRM_VC_VAL_BYPASS_VALID_BIT;
525         writel(temp, &prcm->prm_vc_val_bypass);
526         if (!wait_on_value(PRM_VC_VAL_BYPASS_VALID_BIT, 0,
527                                 &prcm->prm_vc_val_bypass, LDELAY)) {
528                 printf("Scaling voltage failed for 0x%x\n", vcore_reg);
529         }
532 /*
533  * Setup the voltages for vdd_mpu, vdd_core, and vdd_iva
534  * We set the maximum voltages allowed here because Smart-Reflex is not
535  * enabled in bootloader. Voltage initialization in the kernel will set
536  * these to the nominal values after enabling Smart-Reflex
537  */
538 static void scale_vcores(void)
540         u32 volt, sys_clk_khz, cycles_hi, cycles_low, temp, omap4_rev;
542         sys_clk_khz = get_sys_clk_freq() / 1000;
544         /*
545          * Setup the dedicated I2C controller for Voltage Control
546          * I2C clk - high period 40% low period 60%
547          */
548         cycles_hi = sys_clk_khz * 4 / PRM_VC_I2C_CHANNEL_FREQ_KHZ / 10;
549         cycles_low = sys_clk_khz * 6 / PRM_VC_I2C_CHANNEL_FREQ_KHZ / 10;
550         /* values to be set in register - less by 5 & 7 respectively */
551         cycles_hi -= 5;
552         cycles_low -= 7;
553         temp = (cycles_hi << PRM_VC_CFG_I2C_CLK_SCLH_SHIFT) |
554                (cycles_low << PRM_VC_CFG_I2C_CLK_SCLL_SHIFT);
555         writel(temp, &prcm->prm_vc_cfg_i2c_clk);
557         /* Disable high speed mode and all advanced features */
558         writel(0x0, &prcm->prm_vc_cfg_i2c_mode);
560         omap4_rev = omap_revision();
561         /* TPS - supplies vdd_mpu on 4460 */
562         if (omap4_rev >= OMAP4460_ES1_0) {
563                 volt = 1430;
564                 do_scale_tps62361(TPS62361_REG_ADDR_SET1, volt);
565         }
567         /*
568          * VCORE 1
569          *
570          * 4430 : supplies vdd_mpu
571          * Setting a high voltage for Nitro mode as smart reflex is not enabled.
572          * We use the maximum possible value in the AVS range because the next
573          * higher voltage in the discrete range (code >= 0b111010) is way too
574          * high
575          *
576          * 4460 : supplies vdd_core
577          */
578         if (omap4_rev < OMAP4460_ES1_0) {
579                 volt = 1417;
580                 do_scale_vcore(SMPS_REG_ADDR_VCORE1, volt);
581         } else {
582                 volt = 1200;
583                 do_scale_vcore(SMPS_REG_ADDR_VCORE1, volt);
584         }
586         /* VCORE 2 - supplies vdd_iva */
587         volt = 1200;
588         do_scale_vcore(SMPS_REG_ADDR_VCORE2, volt);
590         /*
591          * VCORE 3
592          * 4430 : supplies vdd_core
593          * 4460 : not connected
594          */
595         if (omap4_rev < OMAP4460_ES1_0) {
596                 volt = 1200;
597                 do_scale_vcore(SMPS_REG_ADDR_VCORE3, volt);
598         }
601 static inline void enable_clock_domain(u32 *const clkctrl_reg, u32 enable_mode)
603         clrsetbits_le32(clkctrl_reg, CD_CLKCTRL_CLKTRCTRL_MASK,
604                         enable_mode << CD_CLKCTRL_CLKTRCTRL_SHIFT);
605         debug("Enable clock domain - 0x%08x\n", clkctrl_reg);
608 static inline void wait_for_clk_enable(u32 *clkctrl_addr)
610         u32 clkctrl, idlest = MODULE_CLKCTRL_IDLEST_DISABLED;
611         u32 bound = LDELAY;
613         while ((idlest == MODULE_CLKCTRL_IDLEST_DISABLED) ||
614                 (idlest == MODULE_CLKCTRL_IDLEST_TRANSITIONING)) {
616                 clkctrl = readl(clkctrl_addr);
617                 idlest = (clkctrl & MODULE_CLKCTRL_IDLEST_MASK) >>
618                          MODULE_CLKCTRL_IDLEST_SHIFT;
619                 if (--bound == 0) {
620                         printf("Clock enable failed for 0x%p idlest 0x%x\n",
621                                 clkctrl_addr, clkctrl);
622                         return;
623                 }
624         }
627 static inline void enable_clock_module(u32 *const clkctrl_addr, u32 enable_mode,
628                                 u32 wait_for_enable)
630         clrsetbits_le32(clkctrl_addr, MODULE_CLKCTRL_MODULEMODE_MASK,
631                         enable_mode << MODULE_CLKCTRL_MODULEMODE_SHIFT);
632         debug("Enable clock module - 0x%08x\n", clkctrl_addr);
633         if (wait_for_enable)
634                 wait_for_clk_enable(clkctrl_addr);
637 /*
638  * Enable essential clock domains, modules and
639  * do some additional special settings needed
640  */
641 static void enable_basic_clocks(void)
643         u32 i, max = 100, wait_for_enable = 1;
644         u32 *const clk_domains_essential[] = {
645                 &prcm->cm_l4per_clkstctrl,
646                 &prcm->cm_l3init_clkstctrl,
647                 &prcm->cm_memif_clkstctrl,
648                 &prcm->cm_l4cfg_clkstctrl,
649                 0
650         };
652         u32 *const clk_modules_hw_auto_essential[] = {
653                 &prcm->cm_wkup_gpio1_clkctrl,
654                 &prcm->cm_l4per_gpio2_clkctrl,
655                 &prcm->cm_l4per_gpio3_clkctrl,
656                 &prcm->cm_l4per_gpio4_clkctrl,
657                 &prcm->cm_l4per_gpio5_clkctrl,
658                 &prcm->cm_l4per_gpio6_clkctrl,
659                 &prcm->cm_memif_emif_1_clkctrl,
660                 &prcm->cm_memif_emif_2_clkctrl,
661                 &prcm->cm_l3init_hsusbotg_clkctrl,
662                 &prcm->cm_l3init_usbphy_clkctrl,
663                 &prcm->cm_l4cfg_l4_cfg_clkctrl,
664                 0
665         };
667         u32 *const clk_modules_explicit_en_essential[] = {
668                 &prcm->cm_l4per_gptimer2_clkctrl,
669                 &prcm->cm_l3init_hsmmc1_clkctrl,
670                 &prcm->cm_l3init_hsmmc2_clkctrl,
671                 &prcm->cm_l4per_mcspi1_clkctrl,
672                 &prcm->cm_wkup_gptimer1_clkctrl,
673                 &prcm->cm_l4per_i2c1_clkctrl,
674                 &prcm->cm_l4per_i2c2_clkctrl,
675                 &prcm->cm_l4per_i2c3_clkctrl,
676                 &prcm->cm_l4per_i2c4_clkctrl,
677                 &prcm->cm_wkup_wdtimer2_clkctrl,
678                 &prcm->cm_l4per_uart3_clkctrl,
679                 0
680         };
682         /* Enable optional additional functional clock for GPIO4 */
683         setbits_le32(&prcm->cm_l4per_gpio4_clkctrl,
684                         GPIO4_CLKCTRL_OPTFCLKEN_MASK);
686         /* Enable 96 MHz clock for MMC1 & MMC2 */
687         setbits_le32(&prcm->cm_l3init_hsmmc1_clkctrl,
688                         HSMMC_CLKCTRL_CLKSEL_MASK);
689         setbits_le32(&prcm->cm_l3init_hsmmc2_clkctrl,
690                         HSMMC_CLKCTRL_CLKSEL_MASK);
692         /* Select 32KHz clock as the source of GPTIMER1 */
693         setbits_le32(&prcm->cm_wkup_gptimer1_clkctrl,
694                         GPTIMER1_CLKCTRL_CLKSEL_MASK);
696         /* Enable optional 48M functional clock for USB  PHY */
697         setbits_le32(&prcm->cm_l3init_usbphy_clkctrl,
698                         USBPHY_CLKCTRL_OPTFCLKEN_PHY_48M_MASK);
700         /* Put the clock domains in SW_WKUP mode */
701         for (i = 0; (i < max) && clk_domains_essential[i]; i++) {
702                 enable_clock_domain(clk_domains_essential[i],
703                                     CD_CLKCTRL_CLKTRCTRL_SW_WKUP);
704         }
706         /* Clock modules that need to be put in HW_AUTO */
707         for (i = 0; (i < max) && clk_modules_hw_auto_essential[i]; i++) {
708                 enable_clock_module(clk_modules_hw_auto_essential[i],
709                                     MODULE_CLKCTRL_MODULEMODE_HW_AUTO,
710                                     wait_for_enable);
711         };
713         /* Clock modules that need to be put in SW_EXPLICIT_EN mode */
714         for (i = 0; (i < max) && clk_modules_explicit_en_essential[i]; i++) {
715                 enable_clock_module(clk_modules_explicit_en_essential[i],
716                                     MODULE_CLKCTRL_MODULEMODE_SW_EXPLICIT_EN,
717                                     wait_for_enable);
718         };
720         /* Put the clock domains in HW_AUTO mode now */
721         for (i = 0; (i < max) && clk_domains_essential[i]; i++) {
722                 enable_clock_domain(clk_domains_essential[i],
723                                     CD_CLKCTRL_CLKTRCTRL_HW_AUTO);
724         }
727 /*
728  * Enable non-essential clock domains, modules and
729  * do some additional special settings needed
730  */
731 static void enable_non_essential_clocks(void)
733         u32 i, max = 100, wait_for_enable = 0;
734         u32 *const clk_domains_non_essential[] = {
735                 &prcm->cm_mpu_m3_clkstctrl,
736                 &prcm->cm_ivahd_clkstctrl,
737                 &prcm->cm_dsp_clkstctrl,
738                 &prcm->cm_dss_clkstctrl,
739                 &prcm->cm_sgx_clkstctrl,
740                 &prcm->cm1_abe_clkstctrl,
741                 &prcm->cm_c2c_clkstctrl,
742                 &prcm->cm_cam_clkstctrl,
743                 &prcm->cm_dss_clkstctrl,
744                 &prcm->cm_sdma_clkstctrl,
745                 0
746         };
748         u32 *const clk_modules_hw_auto_non_essential[] = {
749                 &prcm->cm_mpu_m3_mpu_m3_clkctrl,
750                 &prcm->cm_ivahd_ivahd_clkctrl,
751                 &prcm->cm_ivahd_sl2_clkctrl,
752                 &prcm->cm_dsp_dsp_clkctrl,
753                 &prcm->cm_l3_2_gpmc_clkctrl,
754                 &prcm->cm_l3instr_l3_3_clkctrl,
755                 &prcm->cm_l3instr_l3_instr_clkctrl,
756                 &prcm->cm_l3instr_intrconn_wp1_clkctrl,
757                 &prcm->cm_l3init_hsi_clkctrl,
758                 &prcm->cm_l3init_hsusbtll_clkctrl,
759                 0
760         };
762         u32 *const clk_modules_explicit_en_non_essential[] = {
763                 &prcm->cm1_abe_aess_clkctrl,
764                 &prcm->cm1_abe_pdm_clkctrl,
765                 &prcm->cm1_abe_dmic_clkctrl,
766                 &prcm->cm1_abe_mcasp_clkctrl,
767                 &prcm->cm1_abe_mcbsp1_clkctrl,
768                 &prcm->cm1_abe_mcbsp2_clkctrl,
769                 &prcm->cm1_abe_mcbsp3_clkctrl,
770                 &prcm->cm1_abe_slimbus_clkctrl,
771                 &prcm->cm1_abe_timer5_clkctrl,
772                 &prcm->cm1_abe_timer6_clkctrl,
773                 &prcm->cm1_abe_timer7_clkctrl,
774                 &prcm->cm1_abe_timer8_clkctrl,
775                 &prcm->cm1_abe_wdt3_clkctrl,
776                 &prcm->cm_l4per_gptimer9_clkctrl,
777                 &prcm->cm_l4per_gptimer10_clkctrl,
778                 &prcm->cm_l4per_gptimer11_clkctrl,
779                 &prcm->cm_l4per_gptimer3_clkctrl,
780                 &prcm->cm_l4per_gptimer4_clkctrl,
781                 &prcm->cm_l4per_hdq1w_clkctrl,
782                 &prcm->cm_l4per_mcbsp4_clkctrl,
783                 &prcm->cm_l4per_mcspi2_clkctrl,
784                 &prcm->cm_l4per_mcspi3_clkctrl,
785                 &prcm->cm_l4per_mcspi4_clkctrl,
786                 &prcm->cm_l4per_mmcsd3_clkctrl,
787                 &prcm->cm_l4per_mmcsd4_clkctrl,
788                 &prcm->cm_l4per_mmcsd5_clkctrl,
789                 &prcm->cm_l4per_uart1_clkctrl,
790                 &prcm->cm_l4per_uart2_clkctrl,
791                 &prcm->cm_l4per_uart4_clkctrl,
792                 &prcm->cm_wkup_keyboard_clkctrl,
793                 &prcm->cm_wkup_wdtimer2_clkctrl,
794                 &prcm->cm_cam_iss_clkctrl,
795                 &prcm->cm_cam_fdif_clkctrl,
796                 &prcm->cm_dss_dss_clkctrl,
797                 &prcm->cm_sgx_sgx_clkctrl,
798                 &prcm->cm_l3init_hsusbhost_clkctrl,
799                 &prcm->cm_l3init_fsusb_clkctrl,
800                 0
801         };
803         /* Enable optional functional clock for ISS */
804         setbits_le32(&prcm->cm_cam_iss_clkctrl, ISS_CLKCTRL_OPTFCLKEN_MASK);
806         /* Enable all optional functional clocks of DSS */
807         setbits_le32(&prcm->cm_dss_dss_clkctrl, DSS_CLKCTRL_OPTFCLKEN_MASK);
810         /* Put the clock domains in SW_WKUP mode */
811         for (i = 0; (i < max) && clk_domains_non_essential[i]; i++) {
812                 enable_clock_domain(clk_domains_non_essential[i],
813                                     CD_CLKCTRL_CLKTRCTRL_SW_WKUP);
814         }
816         /* Clock modules that need to be put in HW_AUTO */
817         for (i = 0; (i < max) && clk_modules_hw_auto_non_essential[i]; i++) {
818                 enable_clock_module(clk_modules_hw_auto_non_essential[i],
819                                     MODULE_CLKCTRL_MODULEMODE_HW_AUTO,
820                                     wait_for_enable);
821         };
823         /* Clock modules that need to be put in SW_EXPLICIT_EN mode */
824         for (i = 0; (i < max) && clk_modules_explicit_en_non_essential[i];
825              i++) {
826                 enable_clock_module(clk_modules_explicit_en_non_essential[i],
827                                     MODULE_CLKCTRL_MODULEMODE_SW_EXPLICIT_EN,
828                                     wait_for_enable);
829         };
831         /* Put the clock domains in HW_AUTO mode now */
832         for (i = 0; (i < max) && clk_domains_non_essential[i]; i++) {
833                 enable_clock_domain(clk_domains_non_essential[i],
834                                     CD_CLKCTRL_CLKTRCTRL_HW_AUTO);
835         }
837         /* Put camera module in no sleep mode */
838         clrsetbits_le32(&prcm->cm_cam_clkstctrl, MODULE_CLKCTRL_MODULEMODE_MASK,
839                         CD_CLKCTRL_CLKTRCTRL_NO_SLEEP <<
840                         MODULE_CLKCTRL_MODULEMODE_SHIFT);
844 void freq_update_core(void)
846         u32 freq_config1 = 0;
847         const struct dpll_params *core_dpll_params;
849         core_dpll_params = get_core_dpll_params();
850         /* Put EMIF clock domain in sw wakeup mode */
851         enable_clock_domain(&prcm->cm_memif_clkstctrl,
852                                 CD_CLKCTRL_CLKTRCTRL_SW_WKUP);
853         wait_for_clk_enable(&prcm->cm_memif_emif_1_clkctrl);
854         wait_for_clk_enable(&prcm->cm_memif_emif_2_clkctrl);
856         freq_config1 = SHADOW_FREQ_CONFIG1_FREQ_UPDATE_MASK |
857             SHADOW_FREQ_CONFIG1_DLL_RESET_MASK;
859         freq_config1 |= (DPLL_EN_LOCK << SHADOW_FREQ_CONFIG1_DPLL_EN_SHIFT) &
860                                 SHADOW_FREQ_CONFIG1_DPLL_EN_MASK;
862         freq_config1 |= (core_dpll_params->m2 <<
863                         SHADOW_FREQ_CONFIG1_M2_DIV_SHIFT) &
864                         SHADOW_FREQ_CONFIG1_M2_DIV_MASK;
866         writel(freq_config1, &prcm->cm_shadow_freq_config1);
867         if (!wait_on_value(SHADOW_FREQ_CONFIG1_FREQ_UPDATE_MASK, 0,
868                                 &prcm->cm_shadow_freq_config1, LDELAY)) {
869                 puts("FREQ UPDATE procedure failed!!");
870                 hang();
871         }
873         /* Put EMIF clock domain back in hw auto mode */
874         enable_clock_domain(&prcm->cm_memif_clkstctrl,
875                                 CD_CLKCTRL_CLKTRCTRL_HW_AUTO);
876         wait_for_clk_enable(&prcm->cm_memif_emif_1_clkctrl);
877         wait_for_clk_enable(&prcm->cm_memif_emif_2_clkctrl);
880 void bypass_dpll(u32 *const base)
882         do_bypass_dpll(base);
883         wait_for_bypass(base);
886 void lock_dpll(u32 *const base)
888         do_lock_dpll(base);
889         wait_for_lock(base);
892 void setup_clocks_for_console(void)
894         /* Do not add any spl_debug prints in this function */
895         clrsetbits_le32(&prcm->cm_l4per_clkstctrl, CD_CLKCTRL_CLKTRCTRL_MASK,
896                         CD_CLKCTRL_CLKTRCTRL_SW_WKUP <<
897                         CD_CLKCTRL_CLKTRCTRL_SHIFT);
899         /* Enable all UARTs - console will be on one of them */
900         clrsetbits_le32(&prcm->cm_l4per_uart1_clkctrl,
901                         MODULE_CLKCTRL_MODULEMODE_MASK,
902                         MODULE_CLKCTRL_MODULEMODE_SW_EXPLICIT_EN <<
903                         MODULE_CLKCTRL_MODULEMODE_SHIFT);
905         clrsetbits_le32(&prcm->cm_l4per_uart2_clkctrl,
906                         MODULE_CLKCTRL_MODULEMODE_MASK,
907                         MODULE_CLKCTRL_MODULEMODE_SW_EXPLICIT_EN <<
908                         MODULE_CLKCTRL_MODULEMODE_SHIFT);
910         clrsetbits_le32(&prcm->cm_l4per_uart3_clkctrl,
911                         MODULE_CLKCTRL_MODULEMODE_MASK,
912                         MODULE_CLKCTRL_MODULEMODE_SW_EXPLICIT_EN <<
913                         MODULE_CLKCTRL_MODULEMODE_SHIFT);
915         clrsetbits_le32(&prcm->cm_l4per_uart3_clkctrl,
916                         MODULE_CLKCTRL_MODULEMODE_MASK,
917                         MODULE_CLKCTRL_MODULEMODE_SW_EXPLICIT_EN <<
918                         MODULE_CLKCTRL_MODULEMODE_SHIFT);
920         clrsetbits_le32(&prcm->cm_l4per_clkstctrl, CD_CLKCTRL_CLKTRCTRL_MASK,
921                         CD_CLKCTRL_CLKTRCTRL_HW_AUTO <<
922                         CD_CLKCTRL_CLKTRCTRL_SHIFT);
925 void prcm_init(void)
927         switch (omap4_hw_init_context()) {
928         case OMAP_INIT_CONTEXT_SPL:
929         case OMAP_INIT_CONTEXT_UBOOT_FROM_NOR:
930         case OMAP_INIT_CONTEXT_UBOOT_AFTER_CH:
931                 enable_basic_clocks();
932                 scale_vcores();
933                 setup_dplls();
934                 setup_non_essential_dplls();
935                 enable_non_essential_clocks();
936                 break;
937         default:
938                 break;
939         }