1 /*
2 * Copyright (c) 2011 The Chromium OS Authors.
3 * See file CREDITS for list of people who contributed to this
4 * project.
5 *
6 * This program is free software; you can redistribute it and/or
7 * modify it under the terms of the GNU General Public License as
8 * published by the Free Software Foundation; either version 2 of
9 * the License, or (at your option) any later version.
10 *
11 * This program is distributed in the hope that it will be useful,
12 * but WITHOUT ANY WARRANTY; without even the implied warranty of
13 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
14 * GNU General Public License for more details.
15 *
16 * You should have received a copy of the GNU General Public License
17 * along with this program; if not, write to the Free Software
18 * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
19 * MA 02111-1307 USA
20 */
22 /* Tegra20 high-level function multiplexing */
23 #include <common.h>
24 #include <asm/arch/clock.h>
25 #include <asm/arch/funcmux.h>
26 #include <asm/arch/pinmux.h>
28 /*
29 * The PINMUX macro is used to set up pinmux tables.
30 */
31 #define PINMUX(grp, mux, pupd, tri) \
32 {PINGRP_##grp, PMUX_FUNC_##mux, PMUX_PULL_##pupd, PMUX_TRI_##tri}
34 static const struct pingroup_config disp1_default[] = {
35 PINMUX(LDI, DISPA, NORMAL, NORMAL),
36 PINMUX(LHP0, DISPA, NORMAL, NORMAL),
37 PINMUX(LHP1, DISPA, NORMAL, NORMAL),
38 PINMUX(LHP2, DISPA, NORMAL, NORMAL),
39 PINMUX(LHS, DISPA, NORMAL, NORMAL),
40 PINMUX(LM0, RSVD4, NORMAL, NORMAL),
41 PINMUX(LPP, DISPA, NORMAL, NORMAL),
42 PINMUX(LPW0, DISPA, NORMAL, NORMAL),
43 PINMUX(LPW2, DISPA, NORMAL, NORMAL),
44 PINMUX(LSC0, DISPA, NORMAL, NORMAL),
45 PINMUX(LSPI, DISPA, NORMAL, NORMAL),
46 PINMUX(LVP1, DISPA, NORMAL, NORMAL),
47 PINMUX(LVS, DISPA, NORMAL, NORMAL),
48 PINMUX(SLXD, SPDIF, NORMAL, NORMAL),
49 };
52 int funcmux_select(enum periph_id id, int config)
53 {
54 int bad_config = config != FUNCMUX_DEFAULT;
56 switch (id) {
57 case PERIPH_ID_UART1:
58 switch (config) {
59 case FUNCMUX_UART1_IRRX_IRTX:
60 pinmux_set_func(PINGRP_IRRX, PMUX_FUNC_UARTA);
61 pinmux_set_func(PINGRP_IRTX, PMUX_FUNC_UARTA);
62 pinmux_tristate_disable(PINGRP_IRRX);
63 pinmux_tristate_disable(PINGRP_IRTX);
64 break;
65 case FUNCMUX_UART1_UAA_UAB:
66 pinmux_set_func(PINGRP_UAA, PMUX_FUNC_UARTA);
67 pinmux_set_func(PINGRP_UAB, PMUX_FUNC_UARTA);
68 pinmux_tristate_disable(PINGRP_UAA);
69 pinmux_tristate_disable(PINGRP_UAB);
70 bad_config = 0;
71 break;
72 case FUNCMUX_UART1_GPU:
73 pinmux_set_func(PINGRP_GPU, PMUX_FUNC_UARTA);
74 pinmux_tristate_disable(PINGRP_GPU);
75 bad_config = 0;
76 break;
77 case FUNCMUX_UART1_SDIO1:
78 pinmux_set_func(PINGRP_SDIO1, PMUX_FUNC_UARTA);
79 pinmux_tristate_disable(PINGRP_SDIO1);
80 bad_config = 0;
81 break;
82 }
83 if (!bad_config) {
84 /*
85 * Tegra appears to boot with function UARTA pre-
86 * selected on mux group SDB. If two mux groups are
87 * both set to the same function, it's unclear which
88 * group's pins drive the RX signals into the HW.
89 * For UARTA, SDB certainly overrides group IRTX in
90 * practice. To solve this, configure some alternative
91 * function on SDB to avoid the conflict. Also, tri-
92 * state the group to avoid driving any signal onto it
93 * until we know what's connected.
94 */
95 pinmux_tristate_enable(PINGRP_SDB);
96 pinmux_set_func(PINGRP_SDB, PMUX_FUNC_SDIO3);
97 }
98 break;
100 case PERIPH_ID_UART2:
101 if (config == FUNCMUX_UART2_IRDA) {
102 pinmux_set_func(PINGRP_UAD, PMUX_FUNC_IRDA);
103 pinmux_tristate_disable(PINGRP_UAD);
104 }
105 break;
107 case PERIPH_ID_UART4:
108 if (config == FUNCMUX_UART4_GMC) {
109 pinmux_set_func(PINGRP_GMC, PMUX_FUNC_UARTD);
110 pinmux_tristate_disable(PINGRP_GMC);
111 }
112 break;
114 case PERIPH_ID_DVC_I2C:
115 /* there is only one selection, pinmux_config is ignored */
116 if (config == FUNCMUX_DVC_I2CP) {
117 pinmux_set_func(PINGRP_I2CP, PMUX_FUNC_I2C);
118 pinmux_tristate_disable(PINGRP_I2CP);
119 }
120 break;
122 case PERIPH_ID_I2C1:
123 /* support pinmux_config of 0 for now, */
124 if (config == FUNCMUX_I2C1_RM) {
125 pinmux_set_func(PINGRP_RM, PMUX_FUNC_I2C);
126 pinmux_tristate_disable(PINGRP_RM);
127 }
128 break;
129 case PERIPH_ID_I2C2: /* I2C2 */
130 switch (config) {
131 case FUNCMUX_I2C2_DDC: /* DDC pin group, select I2C2 */
132 pinmux_set_func(PINGRP_DDC, PMUX_FUNC_I2C2);
133 /* PTA to HDMI */
134 pinmux_set_func(PINGRP_PTA, PMUX_FUNC_HDMI);
135 pinmux_tristate_disable(PINGRP_DDC);
136 break;
137 case FUNCMUX_I2C2_PTA: /* PTA pin group, select I2C2 */
138 pinmux_set_func(PINGRP_PTA, PMUX_FUNC_I2C2);
139 /* set DDC_SEL to RSVDx (RSVD2 works for now) */
140 pinmux_set_func(PINGRP_DDC, PMUX_FUNC_RSVD2);
141 pinmux_tristate_disable(PINGRP_PTA);
142 bad_config = 0;
143 break;
144 }
145 break;
146 case PERIPH_ID_I2C3: /* I2C3 */
147 /* support pinmux_config of 0 for now */
148 if (config == FUNCMUX_I2C3_DTF) {
149 pinmux_set_func(PINGRP_DTF, PMUX_FUNC_I2C3);
150 pinmux_tristate_disable(PINGRP_DTF);
151 }
152 break;
154 case PERIPH_ID_SDMMC1:
155 if (config == FUNCMUX_SDMMC1_SDIO1_4BIT) {
156 pinmux_set_func(PINGRP_SDIO1, PMUX_FUNC_SDIO1);
157 pinmux_tristate_disable(PINGRP_SDIO1);
158 }
159 break;
161 case PERIPH_ID_SDMMC2:
162 if (config == FUNCMUX_SDMMC2_DTA_DTD_8BIT) {
163 pinmux_set_func(PINGRP_DTA, PMUX_FUNC_SDIO2);
164 pinmux_set_func(PINGRP_DTD, PMUX_FUNC_SDIO2);
166 pinmux_tristate_disable(PINGRP_DTA);
167 pinmux_tristate_disable(PINGRP_DTD);
168 }
169 break;
171 case PERIPH_ID_SDMMC3:
172 switch (config) {
173 case FUNCMUX_SDMMC3_SDB_SLXA_8BIT:
174 pinmux_set_func(PINGRP_SLXA, PMUX_FUNC_SDIO3);
175 pinmux_set_func(PINGRP_SLXC, PMUX_FUNC_SDIO3);
176 pinmux_set_func(PINGRP_SLXD, PMUX_FUNC_SDIO3);
177 pinmux_set_func(PINGRP_SLXK, PMUX_FUNC_SDIO3);
179 pinmux_tristate_disable(PINGRP_SLXA);
180 pinmux_tristate_disable(PINGRP_SLXC);
181 pinmux_tristate_disable(PINGRP_SLXD);
182 pinmux_tristate_disable(PINGRP_SLXK);
183 /* fall through */
185 case FUNCMUX_SDMMC3_SDB_4BIT:
186 pinmux_set_func(PINGRP_SDB, PMUX_FUNC_SDIO3);
187 pinmux_set_func(PINGRP_SDC, PMUX_FUNC_SDIO3);
188 pinmux_set_func(PINGRP_SDD, PMUX_FUNC_SDIO3);
190 pinmux_tristate_disable(PINGRP_SDB);
191 pinmux_tristate_disable(PINGRP_SDC);
192 pinmux_tristate_disable(PINGRP_SDD);
193 bad_config = 0;
194 break;
195 }
196 break;
198 case PERIPH_ID_SDMMC4:
199 switch (config) {
200 case FUNCMUX_SDMMC4_ATC_ATD_8BIT:
201 pinmux_set_func(PINGRP_ATC, PMUX_FUNC_SDIO4);
202 pinmux_set_func(PINGRP_ATD, PMUX_FUNC_SDIO4);
204 pinmux_tristate_disable(PINGRP_ATC);
205 pinmux_tristate_disable(PINGRP_ATD);
206 break;
208 case FUNCMUX_SDMMC4_ATB_GMA_GME_8_BIT:
209 pinmux_set_func(PINGRP_GME, PMUX_FUNC_SDIO4);
210 pinmux_tristate_disable(PINGRP_GME);
211 /* fall through */
213 case FUNCMUX_SDMMC4_ATB_GMA_4_BIT:
214 pinmux_set_func(PINGRP_ATB, PMUX_FUNC_SDIO4);
215 pinmux_set_func(PINGRP_GMA, PMUX_FUNC_SDIO4);
217 pinmux_tristate_disable(PINGRP_ATB);
218 pinmux_tristate_disable(PINGRP_GMA);
219 bad_config = 0;
220 break;
221 }
222 break;
224 case PERIPH_ID_KBC:
225 if (config == FUNCMUX_DEFAULT) {
226 enum pmux_pingrp grp[] = {PINGRP_KBCA, PINGRP_KBCB,
227 PINGRP_KBCC, PINGRP_KBCD, PINGRP_KBCE,
228 PINGRP_KBCF};
229 int i;
231 for (i = 0; i < ARRAY_SIZE(grp); i++) {
232 pinmux_tristate_disable(grp[i]);
233 pinmux_set_func(grp[i], PMUX_FUNC_KBC);
234 pinmux_set_pullupdown(grp[i], PMUX_PULL_UP);
235 }
236 }
237 break;
239 case PERIPH_ID_USB2:
240 if (config == FUNCMUX_USB2_ULPI) {
241 pinmux_set_func(PINGRP_UAA, PMUX_FUNC_ULPI);
242 pinmux_set_func(PINGRP_UAB, PMUX_FUNC_ULPI);
243 pinmux_set_func(PINGRP_UDA, PMUX_FUNC_ULPI);
245 pinmux_tristate_disable(PINGRP_UAA);
246 pinmux_tristate_disable(PINGRP_UAB);
247 pinmux_tristate_disable(PINGRP_UDA);
248 }
249 break;
251 case PERIPH_ID_SPI1:
252 if (config == FUNCMUX_SPI1_GMC_GMD) {
253 pinmux_set_func(PINGRP_GMC, PMUX_FUNC_SFLASH);
254 pinmux_set_func(PINGRP_GMD, PMUX_FUNC_SFLASH);
256 pinmux_tristate_disable(PINGRP_GMC);
257 pinmux_tristate_disable(PINGRP_GMD);
258 }
259 break;
261 case PERIPH_ID_NDFLASH:
262 switch (config) {
263 case FUNCMUX_NDFLASH_ATC:
264 pinmux_set_func(PINGRP_ATC, PMUX_FUNC_NAND);
265 pinmux_tristate_disable(PINGRP_ATC);
266 break;
267 case FUNCMUX_NDFLASH_KBC_8_BIT:
268 pinmux_set_func(PINGRP_KBCA, PMUX_FUNC_NAND);
269 pinmux_set_func(PINGRP_KBCC, PMUX_FUNC_NAND);
270 pinmux_set_func(PINGRP_KBCD, PMUX_FUNC_NAND);
271 pinmux_set_func(PINGRP_KBCE, PMUX_FUNC_NAND);
272 pinmux_set_func(PINGRP_KBCF, PMUX_FUNC_NAND);
274 pinmux_tristate_disable(PINGRP_KBCA);
275 pinmux_tristate_disable(PINGRP_KBCC);
276 pinmux_tristate_disable(PINGRP_KBCD);
277 pinmux_tristate_disable(PINGRP_KBCE);
278 pinmux_tristate_disable(PINGRP_KBCF);
280 bad_config = 0;
281 break;
282 }
283 break;
284 case PERIPH_ID_DISP1:
285 if (config == FUNCMUX_DEFAULT) {
286 int i;
288 for (i = PINGRP_LD0; i <= PINGRP_LD17; i++) {
289 pinmux_set_func(i, PMUX_FUNC_DISPA);
290 pinmux_tristate_disable(i);
291 pinmux_set_pullupdown(i, PMUX_PULL_NORMAL);
292 }
293 pinmux_config_table(disp1_default,
294 ARRAY_SIZE(disp1_default));
295 }
296 break;
298 default:
299 debug("%s: invalid periph_id %d", __func__, id);
300 return -1;
301 }
303 if (bad_config) {
304 debug("%s: invalid config %d for periph_id %d", __func__,
305 config, id);
306 return -1;
307 }
309 return 0;
310 }