1 /*
2 * (C) Copyright 2012 SAMSUNG Electronics
3 * Padmavathi Venna <padma.v@samsung.com>
4 *
5 * This program is free software; you can redistribute it and/or modify
6 * it under the terms of the GNU General Public License as published by
7 * the Free Software Foundation; either version 2 of the License, or
8 * (at your option) any later version.
9 *
10 * This program is distributed in the hope that it will be useful,
11 * but WITHOUT ANY WARRANTY; without even the implied warranty of
12 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
13 * GNU General Public License for more details.
14 *
15 * You should have received a copy of the GNU General Public License
16 * along with this program; if not, write to the Free Software
17 * Foundation, Inc., 59 Temple Place, Suite 330, Boston, MA 02111-1307 USA
18 */
20 #ifndef __ASM_ARCH_EXYNOS_COMMON_SPI_H_
21 #define __ASM_ARCH_EXYNOS_COMMON_SPI_H_
23 #ifndef __ASSEMBLY__
25 /* SPI peripheral register map; padded to 64KB */
26 struct exynos_spi {
27 unsigned int ch_cfg; /* 0x00 */
28 unsigned char reserved0[4];
29 unsigned int mode_cfg; /* 0x08 */
30 unsigned int cs_reg; /* 0x0c */
31 unsigned char reserved1[4];
32 unsigned int spi_sts; /* 0x14 */
33 unsigned int tx_data; /* 0x18 */
34 unsigned int rx_data; /* 0x1c */
35 unsigned int pkt_cnt; /* 0x20 */
36 unsigned char reserved2[4];
37 unsigned char reserved3[4];
38 unsigned int fb_clk; /* 0x2c */
39 unsigned char padding[0xffd0];
40 };
42 #define EXYNOS_SPI_MAX_FREQ 50000000
44 #define SPI_TIMEOUT_MS 10
46 /* SPI_CHCFG */
47 #define SPI_CH_HS_EN (1 << 6)
48 #define SPI_CH_RST (1 << 5)
49 #define SPI_SLAVE_MODE (1 << 4)
50 #define SPI_CH_CPOL_L (1 << 3)
51 #define SPI_CH_CPHA_B (1 << 2)
52 #define SPI_RX_CH_ON (1 << 1)
53 #define SPI_TX_CH_ON (1 << 0)
55 /* SPI_MODECFG */
56 #define SPI_MODE_CH_WIDTH_WORD (0x2 << 29)
57 #define SPI_MODE_BUS_WIDTH_WORD (0x2 << 17)
59 /* SPI_CSREG */
60 #define SPI_SLAVE_SIG_INACT (1 << 0)
62 /* SPI_STS */
63 #define SPI_ST_TX_DONE (1 << 25)
64 #define SPI_FIFO_LVL_MASK 0x1ff
65 #define SPI_TX_LVL_OFFSET 6
66 #define SPI_RX_LVL_OFFSET 15
68 /* Feedback Delay */
69 #define SPI_CLK_BYPASS (0 << 0)
70 #define SPI_FB_DELAY_90 (1 << 0)
71 #define SPI_FB_DELAY_180 (2 << 0)
72 #define SPI_FB_DELAY_270 (3 << 0)
74 /* Packet Count */
75 #define SPI_PACKET_CNT_EN (1 << 16)
77 #endif /* __ASSEMBLY__ */
78 #endif