]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/glsdk-u-boot.git/blob - arch/arm/include/asm/arch-omap4/sys_proto.h
omap: add basic SPL support
[glsdk/glsdk-u-boot.git] / arch / arm / include / asm / arch-omap4 / sys_proto.h
1 /*
2  * (C) Copyright 2010
3  * Texas Instruments, <www.ti.com>
4  *
5  * This program is free software; you can redistribute it and/or
6  * modify it under the terms of the GNU General Public License as
7  * published by the Free Software Foundation; either version 2 of
8  * the License, or (at your option) any later version.
9  *
10  * This program is distributed in the hope that it will be useful,
11  * but WITHOUT ANY WARRANTY; without even the implied warranty of
12  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
13  * GNU General Public License for more details.
14  *
15  * You should have received a copy of the GNU General Public License
16  * along with this program; if not, write to the Free Software
17  * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
18  * MA 02111-1307 USA
19  */
21 #ifndef _SYS_PROTO_H_
22 #define _SYS_PROTO_H_
24 #include <asm/arch/omap4.h>
25 #include <asm/arch/clocks.h>
26 #include <asm/io.h>
27 #include <asm/omap_common.h>
28 #include <asm/arch/mux_omap4.h>
30 struct omap_sysinfo {
31         char *board_string;
32 };
33 extern const struct omap_sysinfo sysinfo;
35 extern struct omap4_prcm_regs *const prcm;
37 void gpmc_init(void);
38 void watchdog_init(void);
39 u32 get_device_type(void);
40 void do_set_mux(u32 base, struct pad_conf_entry const *array, int size);
41 void set_muxconf_regs_non_essential(void);
42 void sr32(void *, u32, u32, u32);
43 u32 wait_on_value(u32, u32, void *, u32);
44 void sdelay(unsigned long);
45 void set_pl310_ctrl_reg(u32 val);
46 void omap_rev_string(char *omap4_rev_string);
47 void setup_clocks_for_console(void);
48 void prcm_init(void);
49 void bypass_dpll(u32 *const base);
50 void freq_update_core(void);
51 u32 get_sys_clk_freq(void);
52 u32 omap4_ddr_clk(void);
53 void cancel_out(u32 *num, u32 *den, u32 den_limit);
54 void sdram_init(void);
55 u32 omap4_sdram_size(void);
57 static inline u32 running_from_sdram(void)
58 {
59         u32 pc;
60         asm volatile ("mov %0, pc" : "=r" (pc));
61         return ((pc >= OMAP44XX_DRAM_ADDR_SPACE_START) &&
62             (pc < OMAP44XX_DRAM_ADDR_SPACE_END));
63 }
65 static inline u8 uboot_loaded_by_spl(void)
66 {
67         /*
68          * Configuration Header is not supported yet, so u-boot init running
69          * from SDRAM implies that it was loaded by SPL. When this situation
70          * changes one of these approaches could be taken:
71          * i.  Pass a magic from SPL to U-Boot and U-Boot save it at a known
72          *     location.
73          * ii. Check the OPP. CH can support only 50% OPP while SPL initializes
74          *     the DPLLs at 100% OPP.
75          */
76         return running_from_sdram();
77 }
78 /*
79  * The basic hardware init of OMAP(s_init()) can happen in 4
80  * different contexts:
81  *  1. SPL running from SRAM
82  *  2. U-Boot running from FLASH
83  *  3. Non-XIP U-Boot loaded to SDRAM by SPL
84  *  4. Non-XIP U-Boot loaded to SDRAM by ROM code using the
85  *     Configuration Header feature
86  *
87  * This function finds this context.
88  * Defining as inline may help in compiling out unused functions in SPL
89  */
90 static inline u32 omap4_hw_init_context(void)
91 {
92 #ifdef CONFIG_SPL_BUILD
93         return OMAP_INIT_CONTEXT_SPL;
94 #else
95         if (uboot_loaded_by_spl())
96                 return OMAP_INIT_CONTEXT_UBOOT_AFTER_SPL;
97         else if (running_from_sdram())
98                 return OMAP_INIT_CONTEXT_UBOOT_AFTER_CH;
99         else
100                 return OMAP_INIT_CONTEXT_UBOOT_FROM_NOR;
101 #endif
104 static inline u32 omap_revision(void)
106         extern u32 *const omap4_revision;
107         return *omap4_revision;
110 #endif