36cfc6f74e2f97fa51115f8176094f132d0804cb
[glsdk/glsdk-u-boot.git] / arch / arm / include / asm / arch-omap5 / sys_proto.h
1 /*
2  * (C) Copyright 2010
3  * Texas Instruments, <www.ti.com>
4  *
5  * This program is free software; you can redistribute it and/or
6  * modify it under the terms of the GNU General Public License as
7  * published by the Free Software Foundation; either version 2 of
8  * the License, or (at your option) any later version.
9  *
10  * This program is distributed in the hope that it will be useful,
11  * but WITHOUT ANY WARRANTY; without even the implied warranty of
12  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
13  * GNU General Public License for more details.
14  *
15  * You should have received a copy of the GNU General Public License
16  * along with this program; if not, write to the Free Software
17  * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
18  * MA 02111-1307 USA
19  */
21 #ifndef _SYS_PROTO_H_
22 #define _SYS_PROTO_H_
24 #include <asm/arch/omap.h>
25 #include <asm/io.h>
26 #include <asm/arch/clocks.h>
27 #include <asm/omap_common.h>
28 #include <asm/arch/clocks.h>
30 DECLARE_GLOBAL_DATA_PTR;
32 struct pad_conf_entry {
33         u32 offset;
34         u32 val;
35 };
37 struct omap_sysinfo {
38         char *board_string;
39 };
40 extern const struct omap_sysinfo sysinfo;
42 void gpmc_init(void);
43 void watchdog_init(void);
44 u32 get_device_type(void);
45 void do_set_mux(u32 base, struct pad_conf_entry const *array, int size);
46 void set_muxconf_regs_essential(void);
47 void set_muxconf_regs_non_essential(void);
48 void sr32(void *, u32, u32, u32);
49 u32 wait_on_value(u32, u32, void *, u32);
50 void sdelay(unsigned long);
51 void setup_clocks_for_console(void);
52 void prcm_init(void);
53 void bypass_dpll(u32 const base);
54 void freq_update_core(void);
55 u32 get_sys_clk_freq(void);
56 u32 omap5_ddr_clk(void);
57 void cancel_out(u32 *num, u32 *den, u32 den_limit);
58 void sdram_init(void);
59 u32 omap_sdram_size(void);
60 u32 cortex_rev(void);
61 void init_omap_revision(void);
62 void do_io_settings(void);
63 void sri2c_init(void);
64 void gpi2c_init(void);
65 int omap_vc_bypass_send_value(u8 sa, u8 reg_addr, u8 reg_data);
66 u32 warm_reset(void);
67 void force_emif_self_refresh(void);
68 void get_ioregs(const struct ctrl_ioregs **regs);
69 void srcomp_enable(void);
70 void setup_warmreset_time(void);
72 static inline u32 running_from_sdram(void)
73 {
74         u32 pc;
75         asm volatile ("mov %0, pc" : "=r" (pc));
76         return ((pc >= OMAP54XX_DRAM_ADDR_SPACE_START) &&
77             (pc < OMAP54XX_DRAM_ADDR_SPACE_END));
78 }
80 static inline u8 uboot_loaded_by_spl(void)
81 {
82         /*
83          * u-boot can be running from sdram either because of configuration
84          * Header or by SPL. If because of CH, then the romcode sets the
85          * CHSETTINGS executed bit to true in the boot parameter structure that
86          * it passes to the bootloader.This parameter is stored in the ch_flags
87          * variable by both SPL and u-boot.Check out for CHSETTINGS, which is a
88          * mandatory section if CH is present.
89          */
90         if ((gd->arch.omap_boot_params.ch_flags) & (CH_FLAGS_CHSETTINGS))
91                 return 0;
92         else
93                 return running_from_sdram();
94 }
95 /*
96  * The basic hardware init of OMAP(s_init()) can happen in 4
97  * different contexts:
98  *  1. SPL running from SRAM
99  *  2. U-Boot running from FLASH
100  *  3. Non-XIP U-Boot loaded to SDRAM by SPL
101  *  4. Non-XIP U-Boot loaded to SDRAM by ROM code using the
102  *     Configuration Header feature
103  *
104  * This function finds this context.
105  * Defining as inline may help in compiling out unused functions in SPL
106  */
107 static inline u32 omap_hw_init_context(void)
109 #ifdef CONFIG_SPL_BUILD
110         return OMAP_INIT_CONTEXT_SPL;
111 #else
112         if (uboot_loaded_by_spl())
113                 return OMAP_INIT_CONTEXT_UBOOT_AFTER_SPL;
114         else if (running_from_sdram())
115                 return OMAP_INIT_CONTEXT_UBOOT_AFTER_CH;
116         else
117                 return OMAP_INIT_CONTEXT_UBOOT_FROM_NOR;
118 #endif
121 static inline u32 div_round_up(u32 num, u32 den)
123         return (num + den - 1)/den;
126 static inline u32 usec_to_32k(u32 usec)
128         return div_round_up(32768 * usec, 1000000);
130 #endif