OMAP4+: Force DDR in self-refresh after warm reset
[glsdk/glsdk-u-boot.git] / arch / arm / include / asm / arch-omap5 / sys_proto.h
1 /*
2  * (C) Copyright 2010
3  * Texas Instruments, <www.ti.com>
4  *
5  * This program is free software; you can redistribute it and/or
6  * modify it under the terms of the GNU General Public License as
7  * published by the Free Software Foundation; either version 2 of
8  * the License, or (at your option) any later version.
9  *
10  * This program is distributed in the hope that it will be useful,
11  * but WITHOUT ANY WARRANTY; without even the implied warranty of
12  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
13  * GNU General Public License for more details.
14  *
15  * You should have received a copy of the GNU General Public License
16  * along with this program; if not, write to the Free Software
17  * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
18  * MA 02111-1307 USA
19  */
21 #ifndef _SYS_PROTO_H_
22 #define _SYS_PROTO_H_
24 #include <asm/arch/omap.h>
25 #include <asm/io.h>
26 #include <asm/arch/clocks.h>
27 #include <asm/omap_common.h>
28 #include <asm/arch/mux_omap5.h>
29 #include <asm/arch/clocks.h>
31 struct omap_sysinfo {
32         char *board_string;
33 };
34 extern const struct omap_sysinfo sysinfo;
36 void gpmc_init(void);
37 void watchdog_init(void);
38 u32 get_device_type(void);
39 void do_set_mux(u32 base, struct pad_conf_entry const *array, int size);
40 void set_muxconf_regs_essential(void);
41 void set_muxconf_regs_non_essential(void);
42 void sr32(void *, u32, u32, u32);
43 u32 wait_on_value(u32, u32, void *, u32);
44 void sdelay(unsigned long);
45 void omap_rev_string(void);
46 void setup_clocks_for_console(void);
47 void prcm_init(void);
48 void bypass_dpll(u32 *const base);
49 void freq_update_core(void);
50 u32 get_sys_clk_freq(void);
51 u32 omap5_ddr_clk(void);
52 void cancel_out(u32 *num, u32 *den, u32 den_limit);
53 void sdram_init(void);
54 u32 omap_sdram_size(void);
55 u32 cortex_rev(void);
56 void init_omap_revision(void);
57 void do_io_settings(void);
58 void omap_vc_init(u16 speed_khz);
59 int omap_vc_bypass_send_value(u8 sa, u8 reg_addr, u8 reg_data);
60 u32 warm_reset(void);
61 void force_emif_self_refresh(void);
63 /*
64  * This is used to verify if the configuration header
65  * was executed by Romcode prior to control of transfer
66  * to the bootloader. SPL is responsible for saving and
67  * passing this to the u-boot.
68  */
69 extern struct omap_boot_parameters boot_params;
71 static inline u32 running_from_sdram(void)
72 {
73         u32 pc;
74         asm volatile ("mov %0, pc" : "=r" (pc));
75         return ((pc >= OMAP54XX_DRAM_ADDR_SPACE_START) &&
76             (pc < OMAP54XX_DRAM_ADDR_SPACE_END));
77 }
79 static inline u8 uboot_loaded_by_spl(void)
80 {
81         /*
82          * u-boot can be running from sdram either because of configuration
83          * Header or by SPL. If because of CH, then the romcode sets the
84          * CHSETTINGS executed bit to true in the boot parameter structure that
85          * it passes to the bootloader.This parameter is stored in the ch_flags
86          * variable by both SPL and u-boot.Check out for CHSETTINGS, which is a
87          * mandatory section if CH is present.
88          */
89         if ((boot_params.ch_flags) & (CH_FLAGS_CHSETTINGS))
90                 return 0;
91         else
92                 return running_from_sdram();
93 }
94 /*
95  * The basic hardware init of OMAP(s_init()) can happen in 4
96  * different contexts:
97  *  1. SPL running from SRAM
98  *  2. U-Boot running from FLASH
99  *  3. Non-XIP U-Boot loaded to SDRAM by SPL
100  *  4. Non-XIP U-Boot loaded to SDRAM by ROM code using the
101  *     Configuration Header feature
102  *
103  * This function finds this context.
104  * Defining as inline may help in compiling out unused functions in SPL
105  */
106 static inline u32 omap_hw_init_context(void)
108 #ifdef CONFIG_SPL_BUILD
109         return OMAP_INIT_CONTEXT_SPL;
110 #else
111         if (uboot_loaded_by_spl())
112                 return OMAP_INIT_CONTEXT_UBOOT_AFTER_SPL;
113         else if (running_from_sdram())
114                 return OMAP_INIT_CONTEXT_UBOOT_AFTER_CH;
115         else
116                 return OMAP_INIT_CONTEXT_UBOOT_FROM_NOR;
117 #endif
120 #endif