arm: dra7xx: Add board files for DRA7XX socs
[glsdk/glsdk-u-boot.git] / arch / arm / include / asm / arch-omap5 / sys_proto.h
1 /*
2  * (C) Copyright 2010
3  * Texas Instruments, <www.ti.com>
4  *
5  * This program is free software; you can redistribute it and/or
6  * modify it under the terms of the GNU General Public License as
7  * published by the Free Software Foundation; either version 2 of
8  * the License, or (at your option) any later version.
9  *
10  * This program is distributed in the hope that it will be useful,
11  * but WITHOUT ANY WARRANTY; without even the implied warranty of
12  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
13  * GNU General Public License for more details.
14  *
15  * You should have received a copy of the GNU General Public License
16  * along with this program; if not, write to the Free Software
17  * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
18  * MA 02111-1307 USA
19  */
21 #ifndef _SYS_PROTO_H_
22 #define _SYS_PROTO_H_
24 #include <asm/arch/omap.h>
25 #include <asm/io.h>
26 #include <asm/arch/clocks.h>
27 #include <asm/omap_common.h>
28 #include <asm/arch/clocks.h>
30 struct pad_conf_entry {
31         u32 offset;
32         u32 val;
33 };
35 struct omap_sysinfo {
36         char *board_string;
37 };
38 extern const struct omap_sysinfo sysinfo;
40 void gpmc_init(void);
41 void watchdog_init(void);
42 u32 get_device_type(void);
43 void do_set_mux(u32 base, struct pad_conf_entry const *array, int size);
44 void set_muxconf_regs_essential(void);
45 void set_muxconf_regs_non_essential(void);
46 void sr32(void *, u32, u32, u32);
47 u32 wait_on_value(u32, u32, void *, u32);
48 void sdelay(unsigned long);
49 void setup_clocks_for_console(void);
50 void prcm_init(void);
51 void bypass_dpll(u32 const base);
52 void freq_update_core(void);
53 u32 get_sys_clk_freq(void);
54 u32 omap5_ddr_clk(void);
55 void cancel_out(u32 *num, u32 *den, u32 den_limit);
56 void sdram_init(void);
57 u32 omap_sdram_size(void);
58 u32 cortex_rev(void);
59 void init_omap_revision(void);
60 void do_io_settings(void);
61 void omap_vc_init(u16 speed_khz);
62 int omap_vc_bypass_send_value(u8 sa, u8 reg_addr, u8 reg_data);
63 u32 warm_reset(void);
64 void force_emif_self_refresh(void);
65 void get_ioregs(const struct ctrl_ioregs **regs);
66 void srcomp_enable(void);
68 /*
69  * This is used to verify if the configuration header
70  * was executed by Romcode prior to control of transfer
71  * to the bootloader. SPL is responsible for saving and
72  * passing this to the u-boot.
73  */
74 extern struct omap_boot_parameters boot_params;
76 static inline u32 running_from_sdram(void)
77 {
78         u32 pc;
79         asm volatile ("mov %0, pc" : "=r" (pc));
80         return ((pc >= OMAP54XX_DRAM_ADDR_SPACE_START) &&
81             (pc < OMAP54XX_DRAM_ADDR_SPACE_END));
82 }
84 static inline u8 uboot_loaded_by_spl(void)
85 {
86         /*
87          * u-boot can be running from sdram either because of configuration
88          * Header or by SPL. If because of CH, then the romcode sets the
89          * CHSETTINGS executed bit to true in the boot parameter structure that
90          * it passes to the bootloader.This parameter is stored in the ch_flags
91          * variable by both SPL and u-boot.Check out for CHSETTINGS, which is a
92          * mandatory section if CH is present.
93          */
94         if ((boot_params.ch_flags) & (CH_FLAGS_CHSETTINGS))
95                 return 0;
96         else
97                 return running_from_sdram();
98 }
99 /*
100  * The basic hardware init of OMAP(s_init()) can happen in 4
101  * different contexts:
102  *  1. SPL running from SRAM
103  *  2. U-Boot running from FLASH
104  *  3. Non-XIP U-Boot loaded to SDRAM by SPL
105  *  4. Non-XIP U-Boot loaded to SDRAM by ROM code using the
106  *     Configuration Header feature
107  *
108  * This function finds this context.
109  * Defining as inline may help in compiling out unused functions in SPL
110  */
111 static inline u32 omap_hw_init_context(void)
113 #ifdef CONFIG_SPL_BUILD
114         return OMAP_INIT_CONTEXT_SPL;
115 #else
116         if (uboot_loaded_by_spl())
117                 return OMAP_INIT_CONTEXT_UBOOT_AFTER_SPL;
118         else if (running_from_sdram())
119                 return OMAP_INIT_CONTEXT_UBOOT_AFTER_CH;
120         else
121                 return OMAP_INIT_CONTEXT_UBOOT_FROM_NOR;
122 #endif
125 #endif