1 /*
2 * (C) Copyright 2002-2010
3 * Wolfgang Denk, DENX Software Engineering, wd@denx.de.
4 *
5 * See file CREDITS for list of people who contributed to this
6 * project.
7 *
8 * This program is free software; you can redistribute it and/or
9 * modify it under the terms of the GNU General Public License as
10 * published by the Free Software Foundation; either version 2 of
11 * the License, or (at your option) any later version.
12 *
13 * This program is distributed in the hope that it will be useful,
14 * but WITHOUT ANY WARRANTY; without even the implied warranty of
15 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
16 * GNU General Public License for more details.
17 *
18 * You should have received a copy of the GNU General Public License
19 * along with this program; if not, write to the Free Software
20 * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
21 * MA 02111-1307 USA
22 */
24 #ifndef __ASM_GBL_DATA_H
25 #define __ASM_GBL_DATA_H
26 /*
27 * The following data structure is placed in some memory which is
28 * available very early after boot (like DPRAM on MPC8xx/MPC82xx, or
29 * some locked parts of the data cache) to allow for a minimum set of
30 * global variables during system initialization (until we have set
31 * up the memory controller so that we can use RAM).
32 */
34 typedef struct global_data {
35 bd_t *bd;
36 unsigned long flags;
37 unsigned int baudrate;
38 unsigned long have_console; /* serial_init() was called */
39 #ifdef CONFIG_PRE_CONSOLE_BUFFER
40 unsigned long precon_buf_idx; /* Pre-Console buffer index */
41 #endif
42 unsigned long env_addr; /* Address of Environment struct */
43 unsigned long env_valid; /* Checksum of Environment valid? */
44 unsigned long fb_base; /* base address of frame buffer */
45 #ifdef CONFIG_FSL_ESDHC
46 unsigned long sdhc_clk;
47 #endif
48 #ifdef CONFIG_AT91FAMILY
49 /* "static data" needed by at91's clock.c */
50 unsigned long cpu_clk_rate_hz;
51 unsigned long main_clk_rate_hz;
52 unsigned long mck_rate_hz;
53 unsigned long plla_rate_hz;
54 unsigned long pllb_rate_hz;
55 unsigned long at91_pllb_usb_init;
56 #endif
57 #ifdef CONFIG_ARM
58 /* "static data" needed by most of timer.c on ARM platforms */
59 unsigned long timer_rate_hz;
60 unsigned long tbl;
61 unsigned long tbu;
62 unsigned long long timer_reset_value;
63 unsigned long lastinc;
64 #endif
65 #ifdef CONFIG_IXP425
66 unsigned long timestamp;
67 #endif
68 unsigned long relocaddr; /* Start address of U-Boot in RAM */
69 phys_size_t ram_size; /* RAM size */
70 unsigned long mon_len; /* monitor len */
71 unsigned long irq_sp; /* irq stack pointer */
72 unsigned long start_addr_sp; /* start_addr_stackpointer */
73 unsigned long reloc_off;
74 #if !(defined(CONFIG_SYS_ICACHE_OFF) && defined(CONFIG_SYS_DCACHE_OFF))
75 unsigned long tlb_addr;
76 unsigned long tlb_size;
77 #endif
78 const void *fdt_blob; /* Our device tree, NULL if none */
79 void **jt; /* jump table */
80 char env_buf[32]; /* buffer for getenv() before reloc. */
81 #if defined(CONFIG_POST) || defined(CONFIG_LOGBUFFER)
82 unsigned long post_log_word; /* Record POST activities */
83 unsigned long post_log_res; /* success of POST test */
84 unsigned long post_init_f_time; /* When post_init_f started */
85 #endif
86 } gd_t;
88 #include <asm-generic/global_data_flags.h>
90 #define DECLARE_GLOBAL_DATA_PTR register volatile gd_t *gd asm ("r8")
92 #endif /* __ASM_GBL_DATA_H */