1 /*
2 * (C) Copyright 2010
3 * Texas Instruments, <www.ti.com>
4 *
5 * Aneesh V <aneesh@ti.com>
6 *
7 * See file CREDITS for list of people who contributed to this
8 * project.
9 *
10 * This program is free software; you can redistribute it and/or
11 * modify it under the terms of the GNU General Public License as
12 * published by the Free Software Foundation; either version 2 of
13 * the License, or (at your option) any later version.
14 *
15 * This program is distributed in the hope that it will be useful,
16 * but WITHOUT ANY WARRANTY; without even the implied warranty of
17 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
18 * GNU General Public License for more details.
19 *
20 * You should have received a copy of the GNU General Public License
21 * along with this program; if not, write to the Free Software
22 * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
23 * MA 02111-1307 USA
24 */
25 #ifndef _OMAP_COMMON_H_
26 #define _OMAP_COMMON_H_
28 /* Max value for DPLL multiplier M */
29 #define OMAP_DPLL_MAX_N 127
31 /* HW Init Context */
32 #define OMAP_INIT_CONTEXT_SPL 0
33 #define OMAP_INIT_CONTEXT_UBOOT_FROM_NOR 1
34 #define OMAP_INIT_CONTEXT_UBOOT_AFTER_SPL 2
35 #define OMAP_INIT_CONTEXT_UBOOT_AFTER_CH 3
37 static inline u32 omap_revision(void)
38 {
39 extern u32 *const omap_si_rev;
40 return *omap_si_rev;
41 }
43 /*
44 * silicon revisions.
45 * Moving this to common, so that most of code can be moved to common,
46 * directories.
47 */
49 /* omap4 */
50 #define OMAP4430_SILICON_ID_INVALID 0xFFFFFFFF
51 #define OMAP4430_ES1_0 0x44300100
52 #define OMAP4430_ES2_0 0x44300200
53 #define OMAP4430_ES2_1 0x44300210
54 #define OMAP4430_ES2_2 0x44300220
55 #define OMAP4430_ES2_3 0x44300230
56 #define OMAP4460_ES1_0 0x44600100
57 #define OMAP4460_ES1_1 0x44600110
59 /* omap5 */
60 #define OMAP5430_SILICON_ID_INVALID 0
61 #define OMAP5430_ES1_0 0x54300100
62 #define OMAP5432_ES1_0 0x54320100
63 #endif /* _OMAP_COMMON_H_ */