]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/glsdk-u-boot.git/blob - arch/arm/include/asm/u-boot.h
OMAP4+: Force DDR in self-refresh after warm reset
[glsdk/glsdk-u-boot.git] / arch / arm / include / asm / u-boot.h
1 /*
2  * (C) Copyright 2002
3  * Sysgo Real-Time Solutions, GmbH <www.elinos.com>
4  * Marius Groeger <mgroeger@sysgo.de>
5  *
6  * (C) Copyright 2002
7  * Sysgo Real-Time Solutions, GmbH <www.elinos.com>
8  * Alex Zuepke <azu@sysgo.de>
9  *
10  * See file CREDITS for list of people who contributed to this
11  * project.
12  *
13  * This program is free software; you can redistribute it and/or
14  * modify it under the terms of the GNU General Public License as
15  * published by the Free Software Foundation; either version 2 of
16  * the License, or (at your option) any later version.
17  *
18  * This program is distributed in the hope that it will be useful,
19  * but WITHOUT ANY WARRANTY; without even the implied warranty of
20  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
21  * GNU General Public License for more details.
22  *
23  * You should have received a copy of the GNU General Public License
24  * along with this program; if not, write to the Free Software
25  * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
26  * MA 02111-1307 USA
27  *
28  ********************************************************************
29  * NOTE: This header file defines an interface to U-Boot. Including
30  * this (unmodified) header file in another file is considered normal
31  * use of U-Boot, and does *not* fall under the heading of "derived
32  * work".
33  ********************************************************************
34  */
36 #ifndef _U_BOOT_H_
37 #define _U_BOOT_H_      1
39 typedef struct bd_info {
40     int                 bi_baudrate;    /* serial console baudrate */
41     ulong               bi_arch_number; /* unique id for this board */
42     ulong               bi_boot_params; /* where this board expects params */
43         unsigned long   bi_arm_freq; /* arm frequency */
44         unsigned long   bi_dsp_freq; /* dsp core frequency */
45         unsigned long   bi_ddr_freq; /* ddr frequency */
46     struct                              /* RAM configuration */
47     {
48         ulong start;
49         ulong size;
50     }                   bi_dram[CONFIG_NR_DRAM_BANKS];
51 } bd_t;
53 /* For image.h:image_check_target_arch() */
54 #define IH_ARCH_DEFAULT IH_ARCH_ARM
56 #endif  /* _U_BOOT_H_ */