1 /*
2 * (C) Copyright 2002-2006
3 * Wolfgang Denk, DENX Software Engineering, wd@denx.de.
4 *
5 * (C) Copyright 2002
6 * Sysgo Real-Time Solutions, GmbH <www.elinos.com>
7 * Marius Groeger <mgroeger@sysgo.de>
8 *
9 * See file CREDITS for list of people who contributed to this
10 * project.
11 *
12 * This program is free software; you can redistribute it and/or
13 * modify it under the terms of the GNU General Public License as
14 * published by the Free Software Foundation; either version 2 of
15 * the License, or (at your option) any later version.
16 *
17 * This program is distributed in the hope that it will be useful,
18 * but WITHOUT ANY WARRANTY; without even the implied warranty of
19 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
20 * GNU General Public License for more details.
21 *
22 * You should have received a copy of the GNU General Public License
23 * along with this program; if not, write to the Free Software
24 * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
25 * MA 02111-1307 USA
26 */
28 /*
29 * To match the U-Boot user interface on ARM platforms to the U-Boot
30 * standard (as on PPC platforms), some messages with debug character
31 * are removed from the default U-Boot build.
32 *
33 * Define DEBUG here if you want additional info as shown below
34 * printed upon startup:
35 *
36 * U-Boot code: 00F00000 -> 00F3C774 BSS: -> 00FC3274
37 * IRQ Stack: 00ebff7c
38 * FIQ Stack: 00ebef7c
39 */
41 #include <common.h>
42 #include <command.h>
43 #include <environment.h>
44 #include <malloc.h>
45 #include <stdio_dev.h>
46 #include <version.h>
47 #include <net.h>
48 #include <serial.h>
49 #include <nand.h>
50 #include <onenand_uboot.h>
51 #include <mmc.h>
52 #include <libfdt.h>
53 #include <fdtdec.h>
54 #include <post.h>
55 #include <logbuff.h>
57 #ifdef CONFIG_BITBANGMII
58 #include <miiphy.h>
59 #endif
61 DECLARE_GLOBAL_DATA_PTR;
63 ulong monitor_flash_len;
65 #ifdef CONFIG_HAS_DATAFLASH
66 extern int AT91F_DataflashInit(void);
67 extern void dataflash_print_info(void);
68 #endif
70 #if defined(CONFIG_HARD_I2C) || \
71 defined(CONFIG_SOFT_I2C)
72 #include <i2c.h>
73 #endif
75 /************************************************************************
76 * Coloured LED functionality
77 ************************************************************************
78 * May be supplied by boards if desired
79 */
80 inline void __coloured_LED_init(void) {}
81 void coloured_LED_init(void)
82 __attribute__((weak, alias("__coloured_LED_init")));
83 inline void __red_led_on(void) {}
84 void red_led_on(void) __attribute__((weak, alias("__red_led_on")));
85 inline void __red_led_off(void) {}
86 void red_led_off(void) __attribute__((weak, alias("__red_led_off")));
87 inline void __green_led_on(void) {}
88 void green_led_on(void) __attribute__((weak, alias("__green_led_on")));
89 inline void __green_led_off(void) {}
90 void green_led_off(void) __attribute__((weak, alias("__green_led_off")));
91 inline void __yellow_led_on(void) {}
92 void yellow_led_on(void) __attribute__((weak, alias("__yellow_led_on")));
93 inline void __yellow_led_off(void) {}
94 void yellow_led_off(void) __attribute__((weak, alias("__yellow_led_off")));
95 inline void __blue_led_on(void) {}
96 void blue_led_on(void) __attribute__((weak, alias("__blue_led_on")));
97 inline void __blue_led_off(void) {}
98 void blue_led_off(void) __attribute__((weak, alias("__blue_led_off")));
100 /*
101 ************************************************************************
102 * Init Utilities *
103 ************************************************************************
104 * Some of this code should be moved into the core functions,
105 * or dropped completely,
106 * but let's get it working (again) first...
107 */
109 #if defined(CONFIG_ARM_DCC) && !defined(CONFIG_BAUDRATE)
110 #define CONFIG_BAUDRATE 115200
111 #endif
113 static int init_baudrate(void)
114 {
115 gd->baudrate = getenv_ulong("baudrate", 10, CONFIG_BAUDRATE);
116 return 0;
117 }
119 static int display_banner(void)
120 {
121 printf("\n\n%s\n\n", version_string);
122 debug("U-Boot code: %08lX -> %08lX BSS: -> %08lX\n",
123 _TEXT_BASE,
124 _bss_start_ofs + _TEXT_BASE, _bss_end_ofs + _TEXT_BASE);
125 #ifdef CONFIG_MODEM_SUPPORT
126 debug("Modem Support enabled\n");
127 #endif
128 #ifdef CONFIG_USE_IRQ
129 debug("IRQ Stack: %08lx\n", IRQ_STACK_START);
130 debug("FIQ Stack: %08lx\n", FIQ_STACK_START);
131 #endif
133 return (0);
134 }
136 /*
137 * WARNING: this code looks "cleaner" than the PowerPC version, but
138 * has the disadvantage that you either get nothing, or everything.
139 * On PowerPC, you might see "DRAM: " before the system hangs - which
140 * gives a simple yet clear indication which part of the
141 * initialization if failing.
142 */
143 static int display_dram_config(void)
144 {
145 int i;
147 #ifdef DEBUG
148 puts("RAM Configuration:\n");
150 for (i = 0; i < CONFIG_NR_DRAM_BANKS; i++) {
151 printf("Bank #%d: %08lx ", i, gd->bd->bi_dram[i].start);
152 print_size(gd->bd->bi_dram[i].size, "\n");
153 }
154 #else
155 ulong size = 0;
157 for (i = 0; i < CONFIG_NR_DRAM_BANKS; i++)
158 size += gd->bd->bi_dram[i].size;
160 puts("DRAM: ");
161 print_size(size, "\n");
162 #endif
164 return (0);
165 }
167 #if defined(CONFIG_HARD_I2C) || defined(CONFIG_SOFT_I2C)
168 static int init_func_i2c(void)
169 {
170 puts("I2C: ");
171 i2c_init(CONFIG_SYS_I2C_SPEED, CONFIG_SYS_I2C_SLAVE);
172 puts("ready\n");
173 return (0);
174 }
175 #endif
177 #if defined(CONFIG_CMD_PCI) || defined (CONFIG_PCI)
178 #include <pci.h>
179 static int arm_pci_init(void)
180 {
181 pci_init();
182 return 0;
183 }
184 #endif /* CONFIG_CMD_PCI || CONFIG_PCI */
186 /*
187 * Breathe some life into the board...
188 *
189 * Initialize a serial port as console, and carry out some hardware
190 * tests.
191 *
192 * The first part of initialization is running from Flash memory;
193 * its main purpose is to initialize the RAM so that we
194 * can relocate the monitor code to RAM.
195 */
197 /*
198 * All attempts to come up with a "common" initialization sequence
199 * that works for all boards and architectures failed: some of the
200 * requirements are just _too_ different. To get rid of the resulting
201 * mess of board dependent #ifdef'ed code we now make the whole
202 * initialization sequence configurable to the user.
203 *
204 * The requirements for any new initalization function is simple: it
205 * receives a pointer to the "global data" structure as it's only
206 * argument, and returns an integer return code, where 0 means
207 * "continue" and != 0 means "fatal error, hang the system".
208 */
209 typedef int (init_fnc_t) (void);
211 int print_cpuinfo(void);
213 void __dram_init_banksize(void)
214 {
215 gd->bd->bi_dram[0].start = CONFIG_SYS_SDRAM_BASE;
216 gd->bd->bi_dram[0].size = gd->ram_size;
217 }
218 void dram_init_banksize(void)
219 __attribute__((weak, alias("__dram_init_banksize")));
221 int __arch_cpu_init(void)
222 {
223 return 0;
224 }
225 int arch_cpu_init(void)
226 __attribute__((weak, alias("__arch_cpu_init")));
228 int __power_init_board(void)
229 {
230 return 0;
231 }
232 int power_init_board(void)
233 __attribute__((weak, alias("__power_init_board")));
235 /* Record the board_init_f() bootstage (after arch_cpu_init()) */
236 static int mark_bootstage(void)
237 {
238 bootstage_mark_name(BOOTSTAGE_ID_START_UBOOT_F, "board_init_f");
240 return 0;
241 }
243 init_fnc_t *init_sequence[] = {
244 arch_cpu_init, /* basic arch cpu dependent setup */
245 mark_bootstage,
246 #ifdef CONFIG_OF_CONTROL
247 fdtdec_check_fdt,
248 #endif
249 #if defined(CONFIG_BOARD_EARLY_INIT_F)
250 board_early_init_f,
251 #endif
252 timer_init, /* initialize timer */
253 #ifdef CONFIG_BOARD_POSTCLK_INIT
254 board_postclk_init,
255 #endif
256 #ifdef CONFIG_FSL_ESDHC
257 get_clocks,
258 #endif
259 env_init, /* initialize environment */
260 init_baudrate, /* initialze baudrate settings */
261 serial_init, /* serial communications setup */
262 console_init_f, /* stage 1 init of console */
263 display_banner, /* say that we are here */
264 #if defined(CONFIG_DISPLAY_CPUINFO)
265 print_cpuinfo, /* display cpu info (and speed) */
266 #endif
267 #if defined(CONFIG_DISPLAY_BOARDINFO)
268 checkboard, /* display board info */
269 #endif
270 #if defined(CONFIG_HARD_I2C) || defined(CONFIG_SOFT_I2C)
271 init_func_i2c,
272 #endif
273 dram_init, /* configure available RAM banks */
274 NULL,
275 };
277 void board_init_f(ulong bootflag)
278 {
279 bd_t *bd;
280 init_fnc_t **init_fnc_ptr;
281 gd_t *id;
282 ulong addr, addr_sp;
283 #ifdef CONFIG_PRAM
284 ulong reg;
285 #endif
286 void *new_fdt = NULL;
287 size_t fdt_size = 0;
289 memset((void *)gd, 0, sizeof(gd_t));
291 gd->mon_len = _bss_end_ofs;
292 #ifdef CONFIG_OF_EMBED
293 /* Get a pointer to the FDT */
294 gd->fdt_blob = _binary_dt_dtb_start;
295 #elif defined CONFIG_OF_SEPARATE
296 /* FDT is at end of image */
297 gd->fdt_blob = (void *)(_end_ofs + _TEXT_BASE);
298 #endif
299 /* Allow the early environment to override the fdt address */
300 gd->fdt_blob = (void *)getenv_ulong("fdtcontroladdr", 16,
301 (uintptr_t)gd->fdt_blob);
303 for (init_fnc_ptr = init_sequence; *init_fnc_ptr; ++init_fnc_ptr) {
304 if ((*init_fnc_ptr)() != 0) {
305 hang ();
306 }
307 }
309 #ifdef CONFIG_OF_CONTROL
310 /* For now, put this check after the console is ready */
311 if (fdtdec_prepare_fdt()) {
312 panic("** CONFIG_OF_CONTROL defined but no FDT - please see "
313 "doc/README.fdt-control");
314 }
315 #endif
317 debug("monitor len: %08lX\n", gd->mon_len);
318 /*
319 * Ram is setup, size stored in gd !!
320 */
321 debug("ramsize: %08lX\n", gd->ram_size);
322 #if defined(CONFIG_SYS_MEM_TOP_HIDE)
323 /*
324 * Subtract specified amount of memory to hide so that it won't
325 * get "touched" at all by U-Boot. By fixing up gd->ram_size
326 * the Linux kernel should now get passed the now "corrected"
327 * memory size and won't touch it either. This should work
328 * for arch/ppc and arch/powerpc. Only Linux board ports in
329 * arch/powerpc with bootwrapper support, that recalculate the
330 * memory size from the SDRAM controller setup will have to
331 * get fixed.
332 */
333 gd->ram_size -= CONFIG_SYS_MEM_TOP_HIDE;
334 #endif
336 addr = CONFIG_SYS_SDRAM_BASE + gd->ram_size;
338 #ifdef CONFIG_LOGBUFFER
339 #ifndef CONFIG_ALT_LB_ADDR
340 /* reserve kernel log buffer */
341 addr -= (LOGBUFF_RESERVE);
342 debug("Reserving %dk for kernel logbuffer at %08lx\n", LOGBUFF_LEN,
343 addr);
344 #endif
345 #endif
347 #ifdef CONFIG_PRAM
348 /*
349 * reserve protected RAM
350 */
351 reg = getenv_ulong("pram", 10, CONFIG_PRAM);
352 addr -= (reg << 10); /* size is in kB */
353 debug("Reserving %ldk for protected RAM at %08lx\n", reg, addr);
354 #endif /* CONFIG_PRAM */
356 #if !(defined(CONFIG_SYS_ICACHE_OFF) && defined(CONFIG_SYS_DCACHE_OFF))
357 /* reserve TLB table */
358 gd->tlb_size = 4096 * 4;
359 addr -= gd->tlb_size;
361 /* round down to next 64 kB limit */
362 addr &= ~(0x10000 - 1);
364 gd->tlb_addr = addr;
365 debug("TLB table from %08lx to %08lx\n", addr, addr + gd->tlb_size);
366 #endif
368 /* round down to next 4 kB limit */
369 addr &= ~(4096 - 1);
370 debug("Top of RAM usable for U-Boot at: %08lx\n", addr);
372 #ifdef CONFIG_LCD
373 #ifdef CONFIG_FB_ADDR
374 gd->fb_base = CONFIG_FB_ADDR;
375 #else
376 /* reserve memory for LCD display (always full pages) */
377 addr = lcd_setmem(addr);
378 gd->fb_base = addr;
379 #endif /* CONFIG_FB_ADDR */
380 #endif /* CONFIG_LCD */
382 /*
383 * reserve memory for U-Boot code, data & bss
384 * round down to next 4 kB limit
385 */
386 addr -= gd->mon_len;
387 addr &= ~(4096 - 1);
389 debug("Reserving %ldk for U-Boot at: %08lx\n", gd->mon_len >> 10, addr);
391 #ifndef CONFIG_SPL_BUILD
392 /*
393 * reserve memory for malloc() arena
394 */
395 addr_sp = addr - TOTAL_MALLOC_LEN;
396 debug("Reserving %dk for malloc() at: %08lx\n",
397 TOTAL_MALLOC_LEN >> 10, addr_sp);
398 /*
399 * (permanently) allocate a Board Info struct
400 * and a permanent copy of the "global" data
401 */
402 addr_sp -= sizeof (bd_t);
403 bd = (bd_t *) addr_sp;
404 gd->bd = bd;
405 debug("Reserving %zu Bytes for Board Info at: %08lx\n",
406 sizeof (bd_t), addr_sp);
408 #ifdef CONFIG_MACH_TYPE
409 gd->bd->bi_arch_number = CONFIG_MACH_TYPE; /* board id for Linux */
410 #endif
412 addr_sp -= sizeof (gd_t);
413 id = (gd_t *) addr_sp;
414 debug("Reserving %zu Bytes for Global Data at: %08lx\n",
415 sizeof (gd_t), addr_sp);
417 #if defined(CONFIG_OF_SEPARATE) && defined(CONFIG_OF_CONTROL)
418 /*
419 * If the device tree is sitting immediate above our image then we
420 * must relocate it. If it is embedded in the data section, then it
421 * will be relocated with other data.
422 */
423 if (gd->fdt_blob) {
424 fdt_size = ALIGN(fdt_totalsize(gd->fdt_blob) + 0x1000, 32);
426 addr_sp -= fdt_size;
427 new_fdt = (void *)addr_sp;
428 debug("Reserving %zu Bytes for FDT at: %08lx\n",
429 fdt_size, addr_sp);
430 }
431 #endif
433 /* setup stackpointer for exeptions */
434 gd->irq_sp = addr_sp;
435 #ifdef CONFIG_USE_IRQ
436 addr_sp -= (CONFIG_STACKSIZE_IRQ+CONFIG_STACKSIZE_FIQ);
437 debug("Reserving %zu Bytes for IRQ stack at: %08lx\n",
438 CONFIG_STACKSIZE_IRQ+CONFIG_STACKSIZE_FIQ, addr_sp);
439 #endif
440 /* leave 3 words for abort-stack */
441 addr_sp -= 12;
443 /* 8-byte alignment for ABI compliance */
444 addr_sp &= ~0x07;
445 #else
446 addr_sp += 128; /* leave 32 words for abort-stack */
447 gd->irq_sp = addr_sp;
448 #endif
450 debug("New Stack Pointer is: %08lx\n", addr_sp);
452 #ifdef CONFIG_POST
453 post_bootmode_init();
454 post_run(NULL, POST_ROM | post_bootmode_get(0));
455 #endif
457 gd->bd->bi_baudrate = gd->baudrate;
458 /* Ram ist board specific, so move it to board code ... */
459 dram_init_banksize();
460 display_dram_config(); /* and display it */
462 gd->relocaddr = addr;
463 gd->start_addr_sp = addr_sp;
464 gd->reloc_off = addr - _TEXT_BASE;
465 debug("relocation Offset is: %08lx\n", gd->reloc_off);
466 if (new_fdt) {
467 memcpy(new_fdt, gd->fdt_blob, fdt_size);
468 gd->fdt_blob = new_fdt;
469 }
470 memcpy(id, (void *)gd, sizeof(gd_t));
471 }
473 #if !defined(CONFIG_SYS_NO_FLASH)
474 static char *failed = "*** failed ***\n";
475 #endif
477 /*
478 * Tell if it's OK to load the environment early in boot.
479 *
480 * If CONFIG_OF_CONFIG is defined, we'll check with the FDT to see
481 * if this is OK (defaulting to saying it's not OK).
482 *
483 * NOTE: Loading the environment early can be a bad idea if security is
484 * important, since no verification is done on the environment.
485 *
486 * @return 0 if environment should not be loaded, !=0 if it is ok to load
487 */
488 static int should_load_env(void)
489 {
490 #ifdef CONFIG_OF_CONTROL
491 return fdtdec_get_config_int(gd->fdt_blob, "load-environment", 0);
492 #elif defined CONFIG_DELAY_ENVIRONMENT
493 return 0;
494 #else
495 return 1;
496 #endif
497 }
499 #if defined(CONFIG_DISPLAY_BOARDINFO_LATE) && defined(CONFIG_OF_CONTROL)
500 static void display_fdt_model(const void *blob)
501 {
502 const char *model;
504 model = (char *)fdt_getprop(blob, 0, "model", NULL);
505 printf("Model: %s\n", model ? model : "<unknown>");
506 }
507 #endif
509 /************************************************************************
510 *
511 * This is the next part if the initialization sequence: we are now
512 * running from RAM and have a "normal" C environment, i. e. global
513 * data can be written, BSS has been cleared, the stack size in not
514 * that critical any more, etc.
515 *
516 ************************************************************************
517 */
519 void board_init_r(gd_t *id, ulong dest_addr)
520 {
521 ulong malloc_start;
522 #if !defined(CONFIG_SYS_NO_FLASH)
523 ulong flash_size;
524 #endif
526 gd->flags |= GD_FLG_RELOC; /* tell others: relocation done */
527 bootstage_mark_name(BOOTSTAGE_ID_START_UBOOT_R, "board_init_r");
529 monitor_flash_len = _end_ofs;
531 /* Enable caches */
532 enable_caches();
534 debug("monitor flash len: %08lX\n", monitor_flash_len);
535 board_init(); /* Setup chipselects */
536 /*
537 * TODO: printing of the clock inforamtion of the board is now
538 * implemented as part of bdinfo command. Currently only support for
539 * davinci SOC's is added. Remove this check once all the board
540 * implement this.
541 */
542 #ifdef CONFIG_CLOCKS
543 set_cpu_clk_info(); /* Setup clock information */
544 #endif
545 serial_initialize();
547 debug("Now running in RAM - U-Boot at: %08lx\n", dest_addr);
549 #ifdef CONFIG_LOGBUFFER
550 logbuff_init_ptrs();
551 #endif
552 #ifdef CONFIG_POST
553 post_output_backlog();
554 #endif
556 /* The Malloc area is immediately below the monitor copy in DRAM */
557 malloc_start = dest_addr - TOTAL_MALLOC_LEN;
558 mem_malloc_init (malloc_start, TOTAL_MALLOC_LEN);
560 #ifdef CONFIG_ARCH_EARLY_INIT_R
561 arch_early_init_r();
562 #endif
563 power_init_board();
565 #if !defined(CONFIG_SYS_NO_FLASH)
566 puts("Flash: ");
568 flash_size = flash_init();
569 if (flash_size > 0) {
570 # ifdef CONFIG_SYS_FLASH_CHECKSUM
571 print_size(flash_size, "");
572 /*
573 * Compute and print flash CRC if flashchecksum is set to 'y'
574 *
575 * NOTE: Maybe we should add some WATCHDOG_RESET()? XXX
576 */
577 if (getenv_yesno("flashchecksum") == 1) {
578 printf(" CRC: %08X", crc32(0,
579 (const unsigned char *) CONFIG_SYS_FLASH_BASE,
580 flash_size));
581 }
582 putc('\n');
583 # else /* !CONFIG_SYS_FLASH_CHECKSUM */
584 print_size(flash_size, "\n");
585 # endif /* CONFIG_SYS_FLASH_CHECKSUM */
586 } else {
587 puts(failed);
588 hang();
589 }
590 #endif
592 #if defined(CONFIG_CMD_NAND)
593 puts("NAND: ");
594 nand_init(); /* go init the NAND */
595 #endif
597 #if defined(CONFIG_CMD_ONENAND)
598 onenand_init();
599 #endif
601 #ifdef CONFIG_GENERIC_MMC
602 puts("MMC: ");
603 mmc_initialize(gd->bd);
604 #endif
606 #ifdef CONFIG_HAS_DATAFLASH
607 AT91F_DataflashInit();
608 dataflash_print_info();
609 #endif
611 /* initialize environment */
612 if (should_load_env())
613 env_relocate();
614 else
615 set_default_env(NULL);
617 #if defined(CONFIG_CMD_PCI) || defined(CONFIG_PCI)
618 arm_pci_init();
619 #endif
621 stdio_init(); /* get the devices list going. */
623 jumptable_init();
625 #if defined(CONFIG_API)
626 /* Initialize API */
627 api_init();
628 #endif
630 console_init_r(); /* fully init console as a device */
632 #ifdef CONFIG_DISPLAY_BOARDINFO_LATE
633 # ifdef CONFIG_OF_CONTROL
634 /* Put this here so it appears on the LCD, now it is ready */
635 display_fdt_model(gd->fdt_blob);
636 # else
637 checkboard();
638 # endif
639 #endif
641 #if defined(CONFIG_ARCH_MISC_INIT)
642 /* miscellaneous arch dependent initialisations */
643 arch_misc_init();
644 #endif
645 #if defined(CONFIG_MISC_INIT_R)
646 /* miscellaneous platform dependent initialisations */
647 misc_init_r();
648 #endif
650 /* set up exceptions */
651 interrupt_init();
652 /* enable exceptions */
653 enable_interrupts();
655 /* Initialize from environment */
656 load_addr = getenv_ulong("loadaddr", 16, load_addr);
658 #ifdef CONFIG_BOARD_LATE_INIT
659 board_late_init();
660 #endif
662 #ifdef CONFIG_BITBANGMII
663 bb_miiphy_init();
664 #endif
665 #if defined(CONFIG_CMD_NET)
666 puts("Net: ");
667 eth_initialize(gd->bd);
668 #if defined(CONFIG_RESET_PHY_R)
669 debug("Reset Ethernet PHY\n");
670 reset_phy();
671 #endif
672 #endif
674 #ifdef CONFIG_POST
675 post_run(NULL, POST_RAM | post_bootmode_get(0));
676 #endif
678 #if defined(CONFIG_PRAM) || defined(CONFIG_LOGBUFFER)
679 /*
680 * Export available size of memory for Linux,
681 * taking into account the protected RAM at top of memory
682 */
683 {
684 ulong pram = 0;
685 uchar memsz[32];
687 #ifdef CONFIG_PRAM
688 pram = getenv_ulong("pram", 10, CONFIG_PRAM);
689 #endif
690 #ifdef CONFIG_LOGBUFFER
691 #ifndef CONFIG_ALT_LB_ADDR
692 /* Also take the logbuffer into account (pram is in kB) */
693 pram += (LOGBUFF_LEN + LOGBUFF_OVERHEAD) / 1024;
694 #endif
695 #endif
696 sprintf((char *)memsz, "%ldk", (gd->ram_size / 1024) - pram);
697 setenv("mem", (char *)memsz);
698 }
699 #endif
701 /* main_loop() can return to retry autoboot, if so just run it again. */
702 for (;;) {
703 main_loop();
704 }
706 /* NOTREACHED - no way out of command loop except booting */
707 }
709 void hang(void)
710 {
711 puts("### ERROR ### Please RESET the board ###\n");
712 for (;;);
713 }