]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/glsdk-u-boot.git/blob - arch/avr32/lib/board.c
am33xx/ddr_defs.h: rename DDR2/DDR3 defines to their actual part numbers
[glsdk/glsdk-u-boot.git] / arch / avr32 / lib / board.c
1 /*
2  * Copyright (C) 2004-2006 Atmel Corporation
3  *
4  * See file CREDITS for list of people who contributed to this
5  * project.
6  *
7  * This program is free software; you can redistribute it and/or
8  * modify it under the terms of the GNU General Public License as
9  * published by the Free Software Foundation; either version 2 of
10  * the License, or (at your option) any later version.
11  *
12  * This program is distributed in the hope that it will be useful,
13  * but WITHOUT ANY WARRANTY; without even the implied warranty of
14  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
15  * GNU General Public License for more details.
16  *
17  * You should have received a copy of the GNU General Public License
18  * along with this program; if not, write to the Free Software
19  * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
20  * MA 02111-1307 USA
21  */
22 #include <common.h>
23 #include <command.h>
24 #include <malloc.h>
25 #include <stdio_dev.h>
26 #include <version.h>
27 #include <net.h>
28 #include <atmel_mci.h>
30 #ifdef CONFIG_BITBANGMII
31 #include <miiphy.h>
32 #endif
34 #include <asm/sections.h>
35 #include <asm/arch/mmu.h>
36 #include <asm/arch/hardware.h>
38 #ifndef CONFIG_IDENT_STRING
39 #define CONFIG_IDENT_STRING ""
40 #endif
42 #ifdef CONFIG_GENERIC_ATMEL_MCI
43 #include <mmc.h>
44 #endif
45 DECLARE_GLOBAL_DATA_PTR;
47 unsigned long monitor_flash_len;
49 /* Weak aliases for optional board functions */
50 static int __do_nothing(void)
51 {
52         return 0;
53 }
54 int board_postclk_init(void) __attribute__((weak, alias("__do_nothing")));
55 int board_early_init_r(void) __attribute__((weak, alias("__do_nothing")));
57 /* provide cpu_mmc_init, to overwrite provide board_mmc_init */
58 int cpu_mmc_init(bd_t *bd)
59 {
60         /* This calls the atmel_mci_init in gen_atmel_mci.c */
61         return atmel_mci_init((void *)ATMEL_BASE_MMCI);
62 }
64 #ifdef CONFIG_SYS_DMA_ALLOC_LEN
65 #include <asm/arch/cacheflush.h>
66 #include <asm/io.h>
68 static unsigned long dma_alloc_start;
69 static unsigned long dma_alloc_end;
70 static unsigned long dma_alloc_brk;
72 static void dma_alloc_init(void)
73 {
74         unsigned long monitor_addr;
76         monitor_addr = CONFIG_SYS_MONITOR_BASE + gd->reloc_off;
77         dma_alloc_end = monitor_addr - CONFIG_SYS_MALLOC_LEN;
78         dma_alloc_start = dma_alloc_end - CONFIG_SYS_DMA_ALLOC_LEN;
79         dma_alloc_brk = dma_alloc_start;
81         printf("DMA: Using memory from 0x%08lx to 0x%08lx\n",
82                dma_alloc_start, dma_alloc_end);
84         dcache_invalidate_range(cached(dma_alloc_start),
85                                 dma_alloc_end - dma_alloc_start);
86 }
88 void *dma_alloc_coherent(size_t len, unsigned long *handle)
89 {
90         unsigned long paddr = dma_alloc_brk;
92         if (dma_alloc_brk + len > dma_alloc_end)
93                 return NULL;
95         dma_alloc_brk = ((paddr + len + CONFIG_SYS_DCACHE_LINESZ - 1)
96                          & ~(CONFIG_SYS_DCACHE_LINESZ - 1));
98         *handle = paddr;
99         return uncached(paddr);
101 #else
102 static inline void dma_alloc_init(void)
106 #endif
108 static int init_baudrate(void)
110         gd->baudrate = getenv_ulong("baudrate", 10, CONFIG_BAUDRATE);
111         return 0;
114 static int display_banner (void)
116         printf ("\n\n%s\n\n", version_string);
117         printf ("U-Boot code: %08lx -> %08lx  data: %08lx -> %08lx\n",
118                 (unsigned long)_text, (unsigned long)_etext,
119                 (unsigned long)_data, (unsigned long)__bss_end__);
120         return 0;
123 void hang(void)
125         for (;;) ;
128 static int display_dram_config (void)
130         int i;
132         puts ("DRAM Configuration:\n");
134         for (i = 0; i < CONFIG_NR_DRAM_BANKS; i++) {
135                 printf ("Bank #%d: %08lx ", i, gd->bd->bi_dram[i].start);
136                 print_size (gd->bd->bi_dram[i].size, "\n");
137         }
139         return 0;
142 static void display_flash_config (void)
144         puts ("Flash: ");
145         print_size(gd->bd->bi_flashsize, " ");
146         printf("at address 0x%08lx\n", gd->bd->bi_flashstart);
149 void board_init_f(ulong board_type)
151         gd_t gd_data;
152         gd_t *new_gd;
153         bd_t *bd;
154         unsigned long *new_sp;
155         unsigned long monitor_len;
156         unsigned long monitor_addr;
157         unsigned long addr;
158         long sdram_size;
160         /* Initialize the global data pointer */
161         memset(&gd_data, 0, sizeof(gd_data));
162         gd = &gd_data;
164         /* Perform initialization sequence */
165         board_early_init_f();
166         cpu_init();
167         board_postclk_init();
168         env_init();
169         init_baudrate();
170         serial_init();
171         console_init_f();
172         display_banner();
173         sdram_size = initdram(board_type);
175         /* If we have no SDRAM, we can't go on */
176         if (sdram_size <= 0)
177                 panic("No working SDRAM available\n");
179         /*
180          * Now that we have DRAM mapped and working, we can
181          * relocate the code and continue running from DRAM.
182          *
183          * Reserve memory at end of RAM for (top down in that order):
184          *  - u-boot image
185          *  - heap for malloc()
186          *  - board info struct
187          *  - global data struct
188          *  - stack
189          */
190         addr = CONFIG_SYS_SDRAM_BASE + sdram_size;
191         monitor_len = __bss_end__ - _text;
193         /*
194          * Reserve memory for u-boot code, data and bss.
195          * Round down to next 4 kB limit.
196          */
197         addr -= monitor_len;
198         addr &= ~(4096UL - 1);
199         monitor_addr = addr;
201         /* Reserve memory for malloc() */
202         addr -= CONFIG_SYS_MALLOC_LEN;
204 #ifdef CONFIG_SYS_DMA_ALLOC_LEN
205         /* Reserve DMA memory (must be cache aligned) */
206         addr &= ~(CONFIG_SYS_DCACHE_LINESZ - 1);
207         addr -= CONFIG_SYS_DMA_ALLOC_LEN;
208 #endif
210 #ifdef CONFIG_LCD
211 #ifdef CONFIG_FB_ADDR
212         printf("LCD: Frame buffer allocated at preset 0x%08x\n",
213                CONFIG_FB_ADDR);
214         gd->fb_base = (void *)CONFIG_FB_ADDR;
215 #else
216         addr = lcd_setmem(addr);
217         printf("LCD: Frame buffer allocated at 0x%08lx\n", addr);
218         gd->fb_base = (void *)addr;
219 #endif /* CONFIG_FB_ADDR */
220 #endif /* CONFIG_LCD */
222         /* Allocate a Board Info struct on a word boundary */
223         addr -= sizeof(bd_t);
224         addr &= ~3UL;
225         gd->bd = bd = (bd_t *)addr;
227         /* Allocate a new global data copy on a 8-byte boundary. */
228         addr -= sizeof(gd_t);
229         addr &= ~7UL;
230         new_gd = (gd_t *)addr;
232         /* And finally, a new, bigger stack. */
233         new_sp = (unsigned long *)addr;
234         gd->stack_end = addr;
235         *(--new_sp) = 0;
236         *(--new_sp) = 0;
238         /*
239          * Initialize the board information struct with the
240          * information we have.
241          */
242         bd->bi_dram[0].start = CONFIG_SYS_SDRAM_BASE;
243         bd->bi_dram[0].size = sdram_size;
244         bd->bi_baudrate = gd->baudrate;
246         memcpy(new_gd, gd, sizeof(gd_t));
248         relocate_code((unsigned long)new_sp, new_gd, monitor_addr);
251 void board_init_r(gd_t *new_gd, ulong dest_addr)
253 #ifndef CONFIG_ENV_IS_NOWHERE
254         extern char * env_name_spec;
255 #endif
256         bd_t *bd;
258         gd = new_gd;
259         bd = gd->bd;
261         gd->flags |= GD_FLG_RELOC;
262         gd->reloc_off = dest_addr - CONFIG_SYS_MONITOR_BASE;
264         /* Enable the MMU so that we can keep u-boot simple */
265         mmu_init_r(dest_addr);
267         board_early_init_r();
269         monitor_flash_len = _edata - _text;
271 #if defined(CONFIG_NEEDS_MANUAL_RELOC)
272         /*
273          * We have to relocate the command table manually
274          */
275         fixup_cmdtable(&__u_boot_cmd_start,
276                 (ulong)(&__u_boot_cmd_end - &__u_boot_cmd_start));
277 #endif /* defined(CONFIG_NEEDS_MANUAL_RELOC) */
279         /* there are some other pointer constants we must deal with */
280 #ifndef CONFIG_ENV_IS_NOWHERE
281         env_name_spec += gd->reloc_off;
282 #endif
284         timer_init();
286         /* The malloc area is right below the monitor image in RAM */
287         mem_malloc_init(CONFIG_SYS_MONITOR_BASE + gd->reloc_off -
288                         CONFIG_SYS_MALLOC_LEN, CONFIG_SYS_MALLOC_LEN);
289         malloc_bin_reloc();
290         dma_alloc_init();
292         enable_interrupts();
294         bd->bi_flashstart = 0;
295         bd->bi_flashsize = 0;
296         bd->bi_flashoffset = 0;
298 #ifndef CONFIG_SYS_NO_FLASH
299         bd->bi_flashstart = CONFIG_SYS_FLASH_BASE;
300         bd->bi_flashsize = flash_init();
301         bd->bi_flashoffset = (unsigned long)_edata - (unsigned long)_text;
303         if (bd->bi_flashsize)
304                 display_flash_config();
305 #endif
307         if (bd->bi_dram[0].size)
308                 display_dram_config();
310         gd->bd->bi_boot_params = malloc(CONFIG_SYS_BOOTPARAMS_LEN);
311         if (!gd->bd->bi_boot_params)
312                 puts("WARNING: Cannot allocate space for boot parameters\n");
314         /* initialize environment */
315         env_relocate();
317         stdio_init();
318         jumptable_init();
319         console_init_r();
321         /* Initialize from environment */
322         load_addr = getenv_ulong("loadaddr", 16, load_addr);
324 #ifdef CONFIG_BITBANGMII
325         bb_miiphy_init();
326 #endif
327 #if defined(CONFIG_CMD_NET)
328         puts("Net:   ");
329         eth_initialize(gd->bd);
330 #endif
332 #ifdef CONFIG_GENERIC_ATMEL_MCI
333         mmc_initialize(gd->bd);
334 #endif
335         for (;;) {
336                 main_loop();
337         }